Blood Glucose Meters

Description

Blood glucose meters are handheld instruments that detect glucose levels in blood samples. The devices are used primarily by diabetics.

There are continuous and discrete (single-test) meters on the market today. In addition, continuous meters are available by prescription. These use a subcutaneous electrochemical sensor to measure at a programmed interval.

Single-test meters use electrochemical or optical reflectometry to measure the glucose level in units of mg/dL or mmol/L. The majority of blood glucose meters are electrochemical. Electrochemical test strips have electrodes to which a precise bias voltage is applied. The applied voltage causes an electrochemical reaction on the test strip with the resulting current being proportional to the glucose in the blood. The current is then converted to a glucose scale for display.

Each packet of test strips contains a calibration code that must be entered into the meter for calibration purposes prior to use, although some newer test strip designs have eliminated the calibration step.

Please click the "Design Considerations," "Circuits," and "Block Diagrams" tabs above for information that will help you build your design.


A blood glucose meter is a handheld instrument that consists of an electrochemical sensor and a battery-powered embedded system with a display that reads the sensor, processes the sensor reading, displays it, and optionally stores it.

These meters require very precise analog processing in order to determine the glucose level of the sample. Both optical-reflectometry and electrochemical meters need to resolve currents in the single-digit nano-amp range. The devices are generally accurate within a narrow temperature range, so accurate temperature measurement is also required.

Many new designs store readings and can communicate the readings to a PC or smartphone for record keeping.

Electrochemical Test-Strip Configurations


Most test strips are proprietary and vary by meter manufacturer. The variations include the reagent formulation, the number of electrodes, the number of channels, and biasing method of the reagent. The simplest configuration is a self-biased test strip (Figure 1) that has two electrodes with current measured at the working electrode and the common electrode grounded.

Figure 1. Electrochemical test strip in a self-biased configuration
Figure 1. Electrochemical test strip in a self-biased configuration

There can be multiple channels on a single test strip; the additional channels are used for a reference measurement, initial blood detection, or to ensure that the blood has saturated the reaction site. An alternate configuration actively drives both electrodes and measures at the common electrode. Another more advanced design is a counter configuration (Figure 2).

Figure 2. Electrochemical test strip in a counter configuration
Figure 2. Electrochemical test strip in a counter configuration

Here there are three electrodes with current measured at the working electrode, and a force-sense circuit drives the common and reference electrodes. There is an important advantage to this configuration: the bias voltage at the reaction site on the test strip is set and maintained more accurately throughout the measurement. The disadvantage of this design is its additional complexity and the larger headroom required to allow the force-sense amplifier to swing negative to maintain the bias voltage during current flow.

Back to Top |

Sensor Analog Signal Chain


Both optical-reflectometry and electrochemical meters need to resolve currents in the single-digit nano-amp range. To meet the error budget for a meter, components must have extremely low leakage and drift over supply voltage, temperature, and time once the meter has been calibrated during manufacture. An operational amplifier's key specifications are ultra-low input bias current (< 1nA), high linearity, and stability when connected to a capacitive electrochemical test strip. The operational amplifier is typically configured as a TIA for both types of meters. A voltage reference's key specifications include a temperature coefficient less than 50ppm/°C, low drift over time, and good line and load regulation. A 10- or 12-bit DAC is used to set the bias voltage for an electrochemical test strip and to set the LED current for an optical-reflectometry test strip. Sometimes a comparator is employed with electrochemical test strips to detect when blood has been applied to the test strip. This saves power while waiting for blood to be applied to the test strip, and ensures that the reaction site is fully saturated with blood. The ADC requirements vary depending on the type of meter, but most require ≥ 14-bit resolution and low noise for repeatable results. Sometimes 12-bit resolution is used when there is a programmable gain stage before the ADC to extend the dynamic range.

Part Selection

Maxim offers precision single-chip data acquisition systems (DAS) that integrate all the functionality discussed in the previous sections. Our recommended DAS ICs are designed to meet the specifications and performance required in blood glucose meters. These DAS ICs are also suitable for similar applications such as coagulation and cholesterol meters. Click the DAS block in the block diagrams to view recommended products.

Back to Top |

Temperature Measurement


Ideally, the temperature of the blood on the test strip should be measured, but usually the ambient temperature near the test strip is measured. Temperature measurement accuracy varies by test-strip type and chemistry, but is typically in the ±1°C to ±2°C range. This measurement can be accomplished with stand-alone temperature-sensor ICs, or with a remote thermistor or PN junction together with an ADC. Using a thermistor in a half-bridge configuration driven by the same reference as the ADC provides more accurate results because this design eliminates any voltage-reference errors. Remote or internal PN junctions can be measured with highly precise integrated analog front-ends (AFEs).

Part Selection

Maxim's single-chip DAS ICs offer integrated temperature sensors that provide the required level of accuracy for this application.

Back to Top |

User Interface: Display, Audio


Most blood glucose meters use a simple liquid-crystal display (LCD) with approximately 100 segments that can be driven with an LCD driver integrated in the microcontroller. Color displays require additional and higher voltages than both the segment LCDs. Backlighting can be added by using one or two white LEDs.

Audible indicators range from simple buzzers to more advanced talking meters for the vision impaired. A simple buzzer can be driven by one or two microcontroller port pins with pulse-width modulation (PWM) capability. More advanced voice indicators and even voice recording for test result notes can be achieved by adding an audio codec along with speaker and microphone amplifiers.

Part Selection

Maxim offers step-up switching regulators that might be required to power the LCD display and high-brightness LED drivers for display backlighting applications. Click the block diagram to view recommended products.

Back to Top |

Electrostatic Discharge


All meters must pass IEC 61000-4-2 electrostatic discharge (ESD) requirements. Using electronics with built-in ESD protection or adding ESD line protectors to exposed traces can help meet this requirement.

Back to Top |

Power and Battery Management


Meters with simple displays can run directly off of a single lithium coin cell or two alkaline AAA primary batteries. To maximize battery life, this meter requires electronics capable of running from 3.6V down to 2.2V for the lithium coin cell or 1.8V for the alkaline AAAs. If the electronics require a higher or regulated supply voltage a step-up switching regulator can be used. Powering down the switching regulator during sleep mode and running directly off the batteries extends battery life, as long as the sleep circuitry can run from the lower battery voltages. Adding a backlit or a more advanced display will require higher and sometimes additional voltages. A more advanced power management scheme may be required at this point. Rechargeable batteries such as single-cell lithium ion (Li+) can be used by adding a battery charger and fuel-gauge circuitry. Charging with USB is a convenient option for the user, if USB is available in the meter.

Part Selection

Maxim offers several power regulation and battery management circuits for this application. The exact products for a design will depend on the size and type of battery that is selected.

Please see the block diagram and click on the power supply and battery symbols to view recommended Maxim ICs for this application.

Back to Top |


Creating Assistive Devices with Maxim Biosensors

 

"You have a solution (Health Sensor Platform 2.0) that is really quite excellent. I was able to leverage everything. All the sensors are Maxim sensors."
 -Marty Stone, Founder and President, Atec Inc.


Featured products: MAX30001, Health Sensor Platform 2.0, MAX86141, MAX30205, MAX32630, MAX20303, MAX32664

Read Their Story ›

Unlocking Human Performance with MAX32652

 

With 3MB flash, 1MB SRAM, and multiple memory-expansion interfaces, the MAX32652 provides the onboard memory and processing power at low power consumption WHOOP needed.

Featured products: MAX32652, MAX14745, MAX17223

Read Their Story ›

Advancing Digital TV Technologies

 

"Our DVB-C modulators based on the MAX5862 and MAX5868 integrate 32 channels on a single board and up to 96 channels in a single chassis."
 -Mr. Gang Ma, General Manager, R&D, Gospell Digital Technology


Featured products: MAX5862, MAX5868

Read Their Story ›

Mouth-Based Biometrics Monitoring

 

"The Maxim chips performed beautifully when we used them. It really has become a standard with many companies."
 -Mike Saigh, CEO, Equine SmartBits


Featured products: MAX30102, MAX32664, MAX30205, MAX8808X, MAX40200, MAX8902, MAX6775

Read Their Story ›

Simplifying Creation of IoT and Robotic Devices

 

"In the case of the MAX3051, low data error rate and a competitive price were factors in our choice."
 -Hanjun Kim, Hardware Technical Lead, LUXROBO


Featured products: MAX3051, MAX38902C, MAX8969, MAX40200

Read Their Story ›

Creating High-End ATE Products

 

NCATEST was able to reduce its design cycle while creating an ATE solution that is smaller, lower power, and better performing than its predecessor.

Featured products: MAX6350, MAX6325, MAX811, MAX3232, MAX541, MAX4820, MAX11160, MAX14783, MAX6696

Read Their Story ›

High-Efficiency Boost Converter Extends Wearable Medical Patch Battery Life

 

High-Efficiency Boost Converter Extends Wearable Medical Patch Battery Life
The Internet of Things, combined with low power wireless data transmission protocols, is enabling the continuous and real-time monitoring of patient life signs by means of wearable devices. We reviewe the challenges of powering a wearable medical patch with a small disposable 160mAh zinc-air battery. A typical boost converter that regulates the battery voltage falls short of the five-day operating requirement for wearables. On the other hand, a high-efficiency, low-quiescent boost converter can meet and exceed the requirement of five-day operation.

Featured parts: MAX17220, MAX17221, MAX17222, MAX17223, MAX17224, MAX17225
Read more ›

Introduction to the DS28C50 DeepCover® Secure SHA-3 Authenticator with ChipDNATM PUF Protection

This video provides an introduction to Maxim's DeepCover® Secure SHA-3 Authenticator with ChipDNA™ PUF Protection - the DS28C50.

Data Center

Maxim’s analog PAM4 chipset delivers DSP-like performance for hyperscale data center applications, without DSP costs, power, or latency.

Equine SmartBits horse bridle bit

Biometric sensors integrated into a horse bridle bit from Equine SmartBits measure horse biometrics.

Automotive Surround-View Camera System

An ASIL-grade camera protector IC like the MAX20087 can support reliable operation of automotive surround-view camera systems

Self-Driving Car Sensors

Autonomous vehicles require many sets of “eyes,” courtesy of cameras, radar, and LiDAR sensors.

MAX22191 digital Input IC block diagram

Wearable sports technologies provide runners and other fitness buffs with valuable insights about performance and overall well-being

Wearable sports technologies provide runners and other fitness buffs with valuable insights about performance and overall well-being.

Healthcare Wearables

Healthcare wearables like smartwatches that continuously monitor vital signs are enabling users to proactively manage their health and wellbeing.

MAX11410

Diagram of MAX11410 multichannel 24-bit ADC delivers accurate sensing

Low-Power Microcontroller for Wearables

To infuse its fitness tracker with high levels of processing power at low power consumption, WHOOP turned to Maxim’s DARWIN low-power microcontrollers.

Circuit Board

EE-Sim speeds the design of switching power converters.

Digital Frontier wafer tester

Reduce power usage using NAND flash wafer tester with Maxim’s MAX9972 low-power ATE driver/comparator.

Mikroe RTC 7 Click

Mikroe’s Real Time Clock 7 Click provides an affordable way to evaluate the MAX31341B nanoPower Real Time Clock

A standard AC induction motor

Industrial Automation

Future of IC Automation in Factory Setting

Wireless Weather Station

Protect IoT applications, including remote sensors in wireless designs, using secure microcontrollers and physically unclonable function technology

Introduction to the MAX17670 MAX17671 MAX17672 Integrated 4V-60V, 150mA, High-Efficiency, Synchronous Step-Down DC-DC Converter with 50mA Linear Regulator

This video provides an introduction to the MAX17670/71/72, a dual-output regulator integrating a 4V to 60V, 150mA high-voltage, high-efficiency synchronous step-down converter with internal MOSFETs and a high-PSRR, low-noise, 2.35V to 5V, 50mA linear regulator.

Power management architecture for car camera system

A car camera power protector IC can be part of a fusion ECU for the camera system.

Introduction to the MAXM17536 MAXM17537 4.5V to 60V, 4A Himalaya Step-Down Power Modules

This video provides an introduction to Maxim’s 4.5V to 60V, 4A High Efficiency, DC-DC Step-Down Power Module with Integrated Inductor – the MAXM17536/7

electronica 2018 – 360 View

See the full view of Maxim solutions at electronica 2018.

Learn more ›

Service Robot at CES 2020

Service robots were all the rage at CES 2020

Arnold Schwarzenegger Robot at CES 2020

A robotic bust of Arnold Schwarzenegger at CES 2020 moves its face in a life-like manner.

Robot System Block Diagram

A variety of power management ICs, including protectors, LDOs, and buck converters, is needed in robotic systems.

Back to Black with Backlight Local Dimming

 

Back to Black with Backlight Local Dimming
In this design solution, we show how a 12.3-inch automotive LCD display backlight panel housing a full-array of 256 LEDs implements local dimming for true black using only four chips. The LED driver ICs and the voltage source that powers the LED strings are connected with a feedback loop that assures proper voltage headroom to the four LED drivers’ output, minimizing overall system power dissipation.

Featured part: MAX21610
Read more ›

Efficient Earbud Charging is All About Keeping a Cool Head

 

Efficient Earbud Charging is All About Keeping a Cool Head
True wireless earbuds commonly use three (or more) pins to interface with their charging case, for data and power transfer. Extra pins need more space while also causing a reliability concern. Additionally, a fixed voltage is commonly used during earbud battery charging, an approach that can cause unwanted heating. In this design solution, we examine the shortcomings of these approaches in more detail before presenting a composite approach that uses two ICs to address these concerns.

Featured parts: MAX20340, MAX20343
Read more ›

Introduction to the MAX86171 Best-in-Class Optical Pulse Oximeter and Heart-Rate Sensor AFE for Wearable Health

This video provides an introduction to Maxim's Best-in-Class Optical Pulse Oximeter and Heart-Rate Sensor AFE for Wearable Health - the MAX86171

Xilinx Zynq Ultrascale+ FPGA Power Solution

 

Complete Power Solutions for Zynq Ultrascale+ Reference Designs

Learn more ›

Xilinx Versal VC1902 AI Core

 

High Performance, Small Solution Size, and High Scalability for the Latest Generation of Xilinx FPGAs and SoCs.

Learn more ›

Xilinx Spartan-7 FPGA Power Solution

 

Cost- and Efficiency-Optimized Power Solutions for Spartan-7 Reference Designs

Learn more ›

Xilinx Artix-7 FPGA Power Solution

 

Cost- and Efficiency-Optimized Power Solutions for Artix-7 Reference Designs

Learn more ›

Xilinx VCU108 FPGA Power Solution

 

Complete Power Solution for the Virtex Ultrascale VCU108 Reference Design

Learn more ›

Xilinx KCU105 FPGA Power Solution

 

Complete Power Solution for the Kintex Ultrascale KCU105 Reference Design

Learn more ›

Xilinx VCU110 FPGA Power Solution

 

Complete Power Solution for the Virtex Ultrascale VCU110 Reference Design

Learn more ›

Bluetooth Low Energy: The Physical Layer—Part 1 of 7

In the first video of this series on Bluetooth® Low Energy, we investigate the radio (or physical) layer, including operating frequency, modulation, and channel management techniques. In Part 2, “Bluetooth Low Energy: How to Define a BLE Application,” we’ll explore using a sample BLE application.

Learn more: MAX32666 ›

Bluetooth Low Energy: How to Define a BLE Application—Part 2 of 7

In the second video in this series, we explore a typical Bluetooth® Low Energy application - a heart rate monitor - to examine how BLE devices use profiles to organize and share information. In Part 3, “Bluetooth Low Energy: Understanding GAP Roles,” learn how to use Generic Access Profiles in BLE applications.

Learn more: MAX32666 ›

Bluetooth Low Energy: Understanding GAP Roles—Part 3 of 7

The third video in this series describes how the Generic Access Profile assigns a set of roles used by Bluetooth® Low Energy (BLE) devices to form a Piconet. We define those roles, explain how peripherals and centrals establish a connection, and introduce the concept of the host and controller pieces of the Bluetooth stack. In Part 4, “Bluetooth Low Energy: Unpacking the Physical Layer Packets,” learn how packets are used for data communication.

Learn more: MAX32666 ›

Bluetooth Low Energy: Unpacking the Physical Layer Packets—Part 4 of 7

In Part 4 of this series, we show how Bluetooth® Low Energy (BLE) uses packets for data communication. We describe the BLE packet structure, before examining an advertising packet in more detail. In Part 5, “Bluetooth Low Energy: Dissecting the Controller Layer,” we’ll examine the host and controller layers.

Learn more: MAX32666 ›

Bluetooth Low Energy: Dissecting the Controller Layer—Part 5 of 7

The Bluetooth® Low Energy stack consists of two parts: the host, which is home to the higher layer protocols and profiles, and the controller, where the radio and associated PDU control logic is located. In the fifth part of this series, we dissect the controller into its constituent components and show how the individual blocks work together to ensure a reliable transfer of information. In Part 6, “Bluetooth Low Energy: All About BLE Security,” we’ll learn how BLE keeps information private.

Learn more: MAX32666 ›

Bluetooth Low Energy: All About BLE Security—Part 6 of 7

Bluetooth® Low Energy (BLE) is often used to transport sensitive information, such as health-related data. The sixth video in this series shows how BLE keeps this information private by using security protocols to protect the data transport link. In Part 7, “Bluetooth Low Energy: Developing an Application,” we’ll explain the concept of an API.

Learn more: MAX32666 ›

Introduction to the MAX22520 One-Time Programmable (OTP) Industrial Sensor Output Driver

This video provides an introduction to Maxim's One-Time Programmable (OTP) Industrial Sensor Output Driver - the MAX22520.

Introduction to the MAX2223 Ultra-Wideband, Direct-Conversion, L-Band Satellite Tuner

This video provides an introduction to Maxim’s Ultra-Wideband, Direct-Conversion, L-Band Satellite Tuner – the MAX2223.

Introduction to the MAX16141 MAX16141A 3.5V to 36V Ideal Diode Controller with Voltage and Current Circuit Breaker

This video provides an introduction to Maxim's 3.5V to 36V Ideal Diode Controller with Voltage and Current Circuit Breaker - the MAX16141 MAX16141A.

698MHz to 3800MHz RF Power Amplifier Linearizer

SC1905

True RFin/RFout solution supports 100MHz BW for modular power amp designs, including 3G, 4G, and 5G cellular infrastructure.

Learn More ›

300MHz–960MHz (G)FSK Transmitter with I2C Interface

MAX41464

Includes Bits-to-RF single-wire MCU for low-cost implementation, up to +16dBm output power to increase short-range transmissions.

Learn More ›

Low-Power DOCSIS 3.1 Programmable-Gain Amplifier

MAX3523

Passes stringent DOCSIS 3.1 specifications. Low 3.5W power dissipation surpasses cable modem/gateway requirements.

Learn More ›

Frequency Synthesizer Shield

MAXREFDES161

Frequency synthesizer generates 23.5MHz to 6GHz microwave radio signals. Level translators connect to +3.3V and +5V microcontrollers.

Learn more ›

Evaluation Kit for Multiband Universal GNSS Receivers

MAX2771EVKIT

Provides multi-constellation/multi-band support with superior RF performance for the highest position accuracy.

Learn More ›

Evaluation Kit for Universal GNSS Receivers

MAX2769CEVKIT

Fully programmable, supports GPS, GLONASS, and Galileo systems in a single chip.

Learn More ›

Frequency Synthesizer Shield

MAXREFDES161

Frequency synthesizer generates 23.5MHz to 6GHz microwave radio signals. Level translators connect to +3.3V and +5V microcontrollers.

Learn more ›

Evaluation Kit for Multiband Universal GNSS Receivers

MAX2771EVKIT

Provides multi-constellation/multi-band support with superior RF performance for the highest position accuracy.

Learn More ›

Evaluation Kit for Universal GNSS Receivers

MAX2769CEVKIT

Fully programmable, supports GPS, GLONASS, and Galileo systems in a single chip.

Learn More ›

LiDAR system

Diagram of LiDAR system with the TIA and COMP optical receiver system.

MAX40660 and MAX40661 transimpedance amplifiers block diagram

Diagram of MAX40660/MAX40661 transimpedance amplifiers (TIA1 and TIA2) for automotive LiDAR.

MAX40025 and MAX40026 high-speed comparators

MAX40025 and MAX40026 stabilize the TIA optical signal in LiDAR applications.

Ultra-High CMTI Isolated Gate Driver

MAX22701E

Features single-ended input with Miller clamp output.

Learn more ›

How to Design a Negative Voltage Reference Using MAX828

Katie explains the purpose of a stable voltage reference and describes three common methods used to create one. Next, she shows how the MAX828 can be used to quickly and easily create a small, efficient negative voltage reference for applications which use a bipolar supply.

Learn more: MAX828 ›

Bluetooth Low Energy: Developing an Application—Part 7 of 7

Nobody writes programs for Bluetooth® Low Energy (BLE) from scratch. In the final video of this series, a sample fitness tracking application is used to explain the concept of an API (Applications Programming Interface).

Learn more: MAX32666EVKIT ›

Fan motor efficiency and power factor for 38–50W shaded-pole motor and PMSM motors

Fan motor efficiency and power factor for 38–50W shaded-pole motor and PMSM motors. Image courtesy of Oak Ridge National Laboratory.

Fan motor efficiency and power factor for 38–50W ECM and PMSM motors

Fan motor efficiency and power factor for 38–50W ECM and PMSM motors.

11.5A, 900V silicon carbide power MOSFET from Wolfspeed

An 11.5A, 900V silicon carbide power MOSFET from Wolfspeed. Image courtesy of Wolfspeed, a Cree company.

A standard AC induction motor

Compact Development Board for Secure IoT Applications

MAX32520-KIT

Cortex®-M4 secure microcontroller provides secure boot and protection against physical tampering for IoT applications.

Learn more ›

Introduction to the MAX20075D MAX20076D MAX20076E MAX25276D 36V, 600mA/1.2A Mini Buck Converter with 3.5µA IQ

This video provides an introduction to Maxim's 36V, 600mA/1.2A Mini Buck Converter with 3.5µA IQ - the MAX20075D MAX25275 MAX20076D MAX25276D

Introduction to the MAXM17712 MAXM17720 and MAXM17724 Integrated 4V-60V, 150mA, Himalaya uSLIC Step-Down Power Module with 50mA Linear Regulator

This video provides an introduction to Maxim's Integrated 4V-60V, 150mA, Himalaya uSLIC Step-Down Power Module with 50mA Linear Regulator - the MAXM17712 MAXM17720 and MAXM17724

EE-Sim DC-DC Tool Overview

See a demonstration of the most commonly used functionality in EE-Sim. Includes opening a new DC-DC design, changing design requirements, creating a schematic, running simulations, comparing designs, and generating a report.

Learn more: EE-Sim Design and Simulation Tool ›

EE-Sim Design Requirements

How to set the Design Requirement specifications and create a schematic.

Learn more: EE-Sim Design and Simulation Tool ›

EE-Sim Working with Components

Review the manufacturer, part number, and key properties for each recommended component in your schematic. Select a different component, or define your own component. How ceramic capacitor performance is derated, and why that is important.

Learn more: EE-Sim Design and Simulation Tool ›

EE-Sim Simulation

Use the Simulation Setup Window to run up to six simulation types. If desired, customize a variety of simulation settings. Places to access the resulting waveforms.

Learn more: EE-Sim Design and Simulation Tool ›

EE-Sim Design Tradeoffs

Prioritize the design size, efficiency, or BOM cost based on your design needs. Learn how this selection is implemented in your schematic.

Learn more: EE-Sim Design and Simulation Tool ›

NFC/RFID Tags and Readers

Fundamentals of NFC/RFID Communications

What’s the difference between NFC and RFID? Learn about the technology behind near field communication (NFC) and radio frequency identification (RFID) and the unique application characteristics of each. See how NFC and RFID ICs use modulation and demodulation processes, and through electromagnetic waves, move from the transmitter or tag to the receiver or reader.

Learn more › NFC/RFID Tags and Readers

Enabling High-Performance Automotive Infotainment

 

"MAX9286 is highly integrated and can support up to four camera links. This compact integration takes up less space on the mainboard and also reduces the bill of materials cost for customers.”
-JC Hsu, Corporate Vice President, MediaTek


Featured products: MAX9286, MAX96705, MAX15007C, MAX8902B

Read Their Story ›

Introduction to the MAX14828 Low-Power, Ultra-Small IO-Link Device Transceiver

This video provides an introduction to the MAX14828, a Single 250mA IO-Link Transceiver + DI.

Redefining Motion Capture

 

"Maxim ICs are making our products work in a more stable and reliable manner.”
-Dr. Tristan RuoLi Dai, CTO, Noitom


Featured products: MAX17224, MAX14841E, MAX809S, MAX14527, MAX8887, DS3231M, MAX8881

Read Their Story ›

Making Clothes Smarter

 

“Maxim support enabled us to use these parts effectively, and we created a design that is more or less without compromise.”
 -Dylan Jackson, Lead Embedded Engineer, Spire


Featured products: MAX30110 and MAX17223

Read Their Story ›

Dual-Channel, Synchronous Buck High-Brightness LED Controller with SPI Interface

MAX20096

Ultra-fast transient response with near-fixed frequency minimizes EMI for matrix lighting, wide dimming ratio allows high contrast.

Learn more ›

2A Synchronous Buck LED Driver with Integrated MOSFETs

MAX20050

High-performance, compact, and efficient buck LED driver simplifies automotive and general lighting designs.

Learn more ›

Automotive High-Voltage, High-Brightness LED Controller

MAX20090

Single-channel HB LED driver for front-light applications such as high-beam, low-beam, and daytime running lights.

Learn more ›

12-Switch Matrix Manager for Automotive Lighting

MAX20092

Single/dual/quad-string configurations, programmable 12-bit PWM dimming, enables matrix/pixel lighting up to 1.5A

Learn more ›

Synchronous Buck, High-Brightness LED Controller

MAX20078

Industry's First Automotive Buck Controller with Ultra-Fast Response and Pseudo Fixed-Frequency Regulation

Learn more ›

60V, 1A, Automotive Synchronous Step-Down DC-DC Converter

MAX20058

60V Synchronous Buck Converter with Internal FETs Enables High Efficiency and Low Temperature Rise

Learn more ›

36V, 2.5MHz Automotive Boost/SEPIC Controllers

MAX16990

2.5MHz Automotive PWM Controller Enables Space-Efficient Preboost Supplies for Cold/Warm Crank Applications

Learn more ›

High-Voltage, 3-Channel Linear High-Brightness LED Driver with Open LED Detection

MAX16823

Highly Integrated, High-Voltage LED Driver Ideal for Automotive Applications

Learn more ›

Introduction to the MAX17662 3.5V to 36V, 2A, High-Efficiency, Synchronous Step-Down DC-DC Converter

This video provides an introduction to Maxim's 3.5V to 36V, 2A, High-Efficiency, Synchronous Step-Down DC-DC Converter - the MAX17662.

MAX77654 block diagram

MAX77654 SIMO PMIC diagram of location-tracking chips IoT devices like e-bikes and e-scooters

E-scooter

Location Tracking Chips Design Enabling e-Scooter Navigation

Understanding Power Losses in Buck Converters

Anthony examines the large power losses associated with the rectification diode of a traditional buck converter. He then shows how a synchronous buck converter, like the MAX17506 or MAX17503, can significantly improve efficiency, thermal performance, and reliability by replacing the diode with an integrated MOSFET.

Learn More > Himalaya Buck Converters

Transimpedance Amplifier with 100mA Input Current Clamp for Automotive LiDAR

MAX40660

Small 3x3 TDFN with wide 490MHz bandwidth captures road condition detail and low 2.1pA/√Hz noise density reduces signal distortion and misinterpretation.

Learn more ›

How to Use DC-Biasing Configurations to Extend the Operating Voltage Range of a Flyback Converter

Teja considers the advantages and disadvantages of three commonly used DC biasing configurations that allow a flyback converter to operate above its absolute maximum voltage rating. He explains why transformer auxiliary winding is the best option, before using the MAXREFDES1193 to calculate the efficiency of this configuration.

Learn more: MAXREFDES1193 ›

Simplify System Power Designs and Achieve Bigger, Sharper Automotive Displays

Maxim's automotive-grade power ICs enable a wide range of display capabilities, helping you implement solutions to support higher luminance, higher current, and increased channel, making it easier to design bigger, sharper automotive displays. Our automotive display ICs also meet ASIL-B and high power requirements for greater reliability.

Learn more: Automotive Display Power ›

Michael Kratsios, U.S. Chief Technology Officer

U.S. Chief Technology Officer Michael Kratsios discusses AI leadership at CES

Elaine Chao, U.S. Secretary of Transportation

Elaine Chao announced AV 4.0, the U.S. initiative on autonomous vehicles, at CES 2020.

5G Technology

5G technology promises to bring the IoT to more people.

Driverless Taxi

Hyundai and Uber are teaming up to bring a driverless taxi to the market.

How to Fix a Corrupted EEPROM on an SC1905EVKIT or SC1894EVKIT

Samantha shows how to identify if your SC1905EVKIT or SC1894EVKIT has a corrupted EEPROM by measuring the supply current or by running the GUI. She then shows some simple fixes to restore your EV kit if this is the case.

Learn more: SC1905 ›

Beacon Current Profile

Typical Beacon Block Diagram

Bluetooth Beacons in the Smart Factory

Tutorial: All About Frequency Synthesis

Learn how variable frequency synthesis is achieved with the phase-locked loop (PLL). This video covers PLL theory and design including the phase detector, loop filter, voltage-controlled oscillator (VCO), integer dividers/multipliers, and the benefits of fractional division. Resources for finding integrated frequency synthesizer ICs are provided.

Learn More › PLLS and VCOs

USB to 1-Wire adapter

DS9481R-3C7

With the OneWireViewer PC utility, easily exercise and evaluate 1-Wire devices.

Learn more ›

Evaluation kit for the DS9090EVKIT

DS9090EVKIT

With the OneWireViewer PC utility, exercise and evaluate a broad range of 1-Wire devices.

Learn more ›

MAX17301/11 functional diagram

Pack-side fuel-gauge implementation

Host-side fuel-gauge implementation

1-Wire Technology Overview - Part 2

In “1-Wire Technology Overview - Part 1," you learned about the 1-Wire® protocol. In part 2, learn how the 1-Wire communication protocol can be used in authentication, memory, and temperature sensing applications.

Learn more: 1-Wire ›

1-Wire Technology Overview - Part 1

Learn how the 1-Wire® communication protocol works, its advantages over other types of serial communication, common implementation configurations, and popular 1-Wire applications. In the next video, “1-Wire Technology Overview - Part 2,” you’ll learn how the 1-Wire protocol is used in applications.

Learn more: 1-Wire ›

Introduction to the MAX77504 14Vin 3A High Efficiency Buck Converter

This video provides an introduction to Maxim's 14Vin 3A High-Efficiency Buck Converter - the MAX77504.

Introduction to the MAX77501 110VPK-PK High Efficiency Piezo Haptic Actuator Boost Driver

This video provides an introduction to Maxim’s first high voltage high efficiency piezo haptic driver – the MAX77501.

Introduction to the MAX20412 Automotive Low-Voltage 2-Channel Step-Down Controller

This video provides an introduction to the MAX20412, a dual-output, high-efficiency synchronous step-down controller IC that operates with a 3.0V to 5.5V input voltage range and provides a 0.25V to 1.275V output voltage range.

Introduction to the MAX14813 Ultra-Compact Octal 3L/Quad 5L Pulser with T/R Switches and Beamforming Capability

This video provides an introduction to Maxim's Ultra-Compact Octal 3L/Quad 5L Pulser with T/R Switches and Beamforming Capability - the MAX14813.

Evaluation Platform for Wrist-Based Heart-Rate and SpO2 Monitoring

MAXREFDES103#: Health Sensor Band

Demonstrates the high sensitivity and algorithm processing functions of health-sensing applications.

Learn more ›

3.5V to 36V Ideal Diode Controllers with Voltage and Current Circuit Breaker

MAX16141/MAX16141A

Mitigates high-voltage transient spikes, fast (0.3µs typ) shutdown response prevents reverse currents, and 5μA (typ) shutdown current reduces battery drain.

Learn more ›

280ps High-Speed Comparator, Ultra-Low Dispersion with LVDS Outputs

MAX40026

10ps overdrive delay at 20mV to 100mV output drive (dispersion) for 0.018cm time-of-flight measurement error in 2mm x 2mm TDFN.

Learn more ›

Introduction to the MAX25249 MAX25249B Quad Output Mini PMIC for Automotive Camera Applications

This video provides an introduction to Maxim’s Flexible Mini Dual 2.2MHz, 500mA Buck Converter with LDOs for Automotive Camera Supplies – the MAX25249 and MAX25249B

Introduction to the MAX98360A MAX98360B MAX98360C MAX98360D Tiny, Cost-Effective, Plug and Play Digital Class-D Amplifier

This video provides an introduction to Maxim's Tiny, Cost-Effective, Plug and Play Digital Class-D Amplifier - the MAX98360A MAX98360B MAX98360C MAX98360D

Meeting Food Quality Criteria

 

"For our purpose, the iButton is the perfect choice because it’s so small, robust, and can be reused many times.”
 -Dr. Thijs Defraeye, Laboratory for Biomimetic Membranes and Textiles, Empa


Featured product: DS1922L

Read Their Story ›

Introduction to the MAX20340 Bidirectional DC Powerline Communication Management IC

This video provides an introduction to Maxim's Bidirectional DC Powerline Communication Management IC - the MAX20340.

How to Measure Current with the MAX4173 Current-Sense Amplifier and a Microcontroller

In this video, Sean uses the MAX4173 Evaluation Kit together with an Arduino® Uno to measure current. He also discusses the principle behind measuring current and why a current-sense amplifier is a very useful addition to this technique.

Learn more › MAX4173

Ultra-Low Power Octal, Digital Input Translator/Serializer

MAX31910

Translates, conditions, and serializes digital output of industrial sensors and switches.

Learn more ›

Octal, High-Speed, Industrial, High-Side Switch

MAX14900E

Fast 24V driver, low propagation delay, and 100kHz load-switching speed for high-speed PLCs.

Learn more ›

Introduction to the MAX20057 MAX20457 MAX20458 36V Boost Controller with Two Synchronous Buck Converters (3.5A/2A) for Automotive Applications

This video provides an introduction to Maxim's Synchronous Buck Converters for Automotive Applications.

Introduction to the MAX40056F/T/U Bidirectional Current Sense Amplifier with PWM-Rejection

This video provides an introduction to the MAX40056, a bi-directional current-sense amplifier with an input common-mode range that extends from -0.1Vto +65V together with protection against negative inductive kickback voltages to -5V.

Introduction to the MAX17673 Integrated 4.5V to 60V Synchronous 1.5A High Voltage Buck and Dual 2.7V to 5.5V, 1A Buck Regulators

This video provides an introduction to the MAX17673, an integrated 4.5V to 60V Synchronous 1.5A High Voltage Buck and Dual 2.7V to 5.5V, 1A Buck Regulators.

How to Set Up a SerDes Reverse Control Channel When PCLK is Not Available - Using the MAX96705/MAX96706 GMSL SerDes

Learn how to establish the I2C reverse control channel when PCLK is not available using the MAX96705 Gigabit Multimedia Serial Link (GMSL) serializer and MAX96706 GMSL deserializer.

Also see: How do I program the remote side of a SerDes link when PCLK is not present?

Learn more: MAX96705 16-Bit GMSL Serializer ›

Learn more: MAX96706 14-Bit GMSL Deserializer ›

Automotive displays

Bigger, sharper automotive displays benefit from highly integrated power management ICs.

MAXREFDES103#

The MAXREFDES103# is a full wrist-worn wearable reference design for heart-rate, heart-rate variability, and SpO2 measurements.

Introduction to the MAX17634A, MAX17634B and MAX17634C 4.5V to 36V, 4.25A, High-Efficiency, Synchronous Step-Down DC-DC Converter

This video provides an introduction to Maxim's 4.5V to 36V, 4.25A, High-Efficiency, Synchronous Step-Down DC-DC Converter - the MAX17634A, MAX17634B and MAX17634C.

Kingston A2000 SSD

The Kingston A2000 SSD delivers fast, reliable performance for laptops.

LynQ people compass

The LynQ device creates a private network to help users find one another.

Sublue WhiteShark Mix underwater scooter

Sublue’s WhiteShark Mix underwater scooter propels users underwater, in pools or in the ocean.

Sublue WhiteShark Mix underwater scooter

Explore the ocean with Sublue’s WhiteShark Mix underwater scooter.

Ricoh Imaging Theta SC2 360° camera

The Theta SC2 360° camera creates still or video images that you can rotate around.

Miracle-Gro Twelve

The Miracle-Gro Twelve Indoor Growing System is a smart hydroponic garden for growing herbs and vegetables inside.

Blood-Pressure Monitoring Smartwatch

Smartwatches and other wearables deliver accurate, continuous monitoring of blood pressure for better preventive health measures and disease management.

Introduction to the MAX22700E/D, MAX22701E/D and MAX22702E/D Ultra-High CMTI Isolated Gate Drivers

This video provides an introduction to Maxim's Ultra-High CMTI Isolated Gate Drivers - the MAX22700E/D, MAX22701E/D and MAX22702E/D.

Introduction to the MAX17576 4.5V to 60V, 4A, High-Efficiency, Synchronous Step-Down DC-DC Converter with Internal Compensation

This video provides an introduction to Maxim's 4.5V to 60V, 4A, High-Efficiency, Synchronous Step-Down DC-DC Converter with Internal Compensation - the MAX17576.

Evaluation Kit for Octal Digital Output with SafeDemag

MAX14912EVKIT

Octal HS or push-pull, SafeDemag surge protection with integrated diagnostics and LED matrix.

Learn more ›

Evaluation Kit for Single-Channel Configurable DIO IC

MAX14914EVKIT

The only fully software-configurable DIO push-pull, fast, and surge protection product with SafeDemag.

Learn more ›

Evaluation Kit for Octal Digital Input for Type 1, 3, and 2 Inputs

MAX22190EVKIT

Fully IEC61131-2-compliant octal digital input with wire-break detection, integrated diagnostics, and LED matrix.

Learn more ›

Wireless and wired battery management systems

Compared to its wired counterpart, a wireless battery management system reduces weight and manufacturing complexity.

Wireless battery management system diagram

Maxim’s CES wireless BMS demo compares a wired and wireless BMS solution based on an ISM-band radio.

Wireless Battery Management System

In Maxim’s wireless BMS demo, the wireless architecture features an RF gateway client that acts as a central controller and BMS secondary nodes that communicate data wirelessly back to the gateway.

High CMTI Isolated Gate Driver

The MAX22700D/MAX22702D isolated gate drivers with high CMTI and low propagation delay skew increase efficiency.

Half-bridge push-pull circuit

In a half-bridge push-pull circuit, both switches should not be on at the same time, as this would lead to a short circuit condition.

Isolated Power Converter Circuit

Circuit with galvanically isolated low-voltage microcontroller.

How to Use the MAX745 as a Maximum Power Point Tracker Solar Charger

Sean explains a maximum power point tracker (MPPT) solar charger and how it is used to optimize the efficiency of a solar panel. He then demonstrates how the MAX745 switch-mode lithium-ion battery charger can be used as an MPPT solar charger.

Learn more: MAX745 ›

How to Optimize the Efficiency Performance of a Flyback Converter Using the MAX17606

Furqan explains why a discontinuous conduction mode (DCM) flyback converter, using a secondary-side rectification diode, is unsuitable for low-voltage high-current applications. He then proposes a high-efficiency solution where a MOSFET, controlled by the MAX17606 synchronous MOSFET driver, replaces the secondary-side diode.

Learn more: MAX17606 ›

Object identification application

New ICs are needed to bring intelligence to the edge for applications such as machine learning.

Evaluation Kit for the MAXM17624 3.3V Output-Voltage Application

MAXM17624EVKIT

The MAXM17624 3.3V output evaluation kit (EV kit) provides a proven design to evaluate the MAXM17624 high frequency, high-efficiency, synchronous step-down DC-DC power module.

Learn more ›

Automotive DeepCover Secure Authenticators Stop Counterfeit Parts

Counterfeit after-market automotive parts can ruin the ADAS driving experience. Our DeepCover® secure authenticators, such as the DS28C40, make it impossible for third-party manufacturers to clone critical components for after-market auto repairs.

Learn more: DS28C40 ›

Salesforce Tower at dusk

The Salesforce Tower in San Francisco exemplifies use of modern building automation technologies.

Salesforce Office

Heating, plumbing and other electrical systems inside the Salesforce Tower are controlled via building automation technologies.

Salesforce Tower

Automation technologies inside the Salesforce Tower are making the building more environmentally friendly and, for occupants, comfortable and convenient.

Introduction to the MAX25600 Synchronous High Voltage 4 Switch Buck Boost LED Controller

This video provides an introduction to the MAX25600, a synchronous 4-switch buck-boost LED driver controller.

Blood Pressure Monitoring from Smartphone

An integrated bio-algorithm sensor hub like the MAX32664 accelerates the development cycle for health-monitoring wearables.

Introduction to the MAX17613A MAX17613B MAX17613C 4.5V to 60V, 3A Current Limiter with OV, UV, and Reverse Protection

This video provides an introduction to the MAX17613A MAX17613B MAX17613C, a 4.5V to 60V, 3A Current Limiter with OV, UV, and reverse protection.

Introduction to the MAX77863 Complete System PMIC, Featuring 13 Regulators, 8 GPIOs, RTCD, and Flexible Power Sequencing for Multicore Applications

This video provides an introduction to Maxim's Complete System PMIC, Featuring 13 Regulators, 8 GPIOs, RTCD, and Flexible Power Sequencing for Multicore Applications - the MAX77863.

Evaluation kit for the DS2484

DS2484EVKIT

DS2484 Converts I2C slave to 1-Wire master. Independent and flexible I2C and 1-Wire operating voltage, user programmable 1-Wire timing.

Learn more ›

1-Wire socket boards

DS9120

Designed for use with the DS2484EVKIT and 1-Wire PC adapters such as DS9490R.

Learn more ›

1-Wire device programmer

DS9488-GP8

Simultaneously programs up to eight 1-Wire devices.

Learn more ›

Introduction to the MAX20336 Ultra-Small, Low-RON, Beyond-the-Rails DPST Analog Switches

This video provides an introduction to the MAX20336, an ultra-small, low-on-resistance, double-pole/single-throw analog switches which features Beyond-the-Rails™ capability that allows signals from -5.5V to +5.5V to pass without distortion, even when the power supply is below the signal range.

GSEE-Tech analog input module

GSEE-Tech used the MAX11270 to meet the performance and size requirements of its new analog input module.

Existing Bus/Taxi Surveillance Application

Since the MAX38888 has 2% regulation accuracy and is a bidirectional system, a buck converter and linear charging aren’t required in this bus/taxi surveillance system when rearchitected with the MAX38888 reversible buck/boost regulator.

Bus/Taxi Surveillance Application with MAX38888

Since the MAX38888 has 2% regulation accuracy and is a bidirectional system, a buck converter and linear charging aren’t required in this bus/taxi surveillance system when rearchitected with the MAX38888 reversible buck/boost regulator.

Portable barcode scanner

Supercapacitors are ideal for backup power in applications such as portable barcode scanners.

Introduction to the MAX16972 and MAX16972A 3A Automotive Hi-Speed USB Protectors with Apple iPhone/iPad and USB 2.0 Charge Detection

This video provides an introduction to Maxim's 3A Automotive Hi-Speed USB Protectors with Apple iPhone/iPad and USB 2.0 Charge Detection - the MAX16972 and MAX16972A.

MAXREFDES1177 reference design with ECAD files

Reference designs with ECAD files, like MAXREFDES1177, can help accelerate your circuit design process.

Ultra-High CMTI Isolated Gate Drivers Evaluation Kit

MAX22701EVKIT

Includes two identical ICs for measurement of part-to-part propagation delay matching.

Learn more ›

Introduction to the MAX14916 Compact Industrial Octal 1A/Quad 2A High-Side Switch with Diagnostics

This video provides an introduction to Maxim's Compact Industrial Octal 1A/Quad 2A High-Side Switch with Diagnostics - the MAX14916.

Introduction to the MAX20056B Integrated, 6-Channel High-Brightness LED Driver with Very Wide PWM Dimming Ratio and Phase Shifting for Automotive Displays

This video provides an introduction to Maxim's Integrated, 6-Channel High-Brightness LED Driver with Very Wide PWM Dimming Ratio and Phase Shifting for Automotive Displays - the MAX20056B.

14-Channel High-Voltage Data-Acquisition System

MAX17853

Achieves ASIL-D compliance using a single chip for mid-to-large cell count configurations.

12-Channel, High-Voltage Data-Acquisition Systems

MAX17823H

Manages high-voltage battery modules and features a 12-bit SAR ADC that measures 12 cell voltages and two temperatures.

Learn more ›

Getting Started with Hall-Effect Sensors Using the MAX9921

Jesvin explains the hall effect and how hall-effect sensors can be useful in applications that require contactless sensors such as an automatic door opener. He then demonstrates the MAX9921, which is the industry’s first two-wire hall-effect sensor.

Learn More: MAX9921 ›

GTI NuSeis seismic recording technology

GTI uses Maxim analog ICs in its precise, power-efficient seismic recording technology.

Introduction to the MAX22515 IO-Link Transceiver with Integrated Protection

This video provides an introduction to Maxim's IO-Link Transceiver with Integrated Protection - the MAX22515.

Accelerate Your Design with the MAX5715BOB DAC Breakout Board

David and Kyle present the latest development tool, the ultra-small MAX5715BOB digital-to-analog converter (DAC) breakout board. You’ll learn how to set up the Arduino®- and Mbed®-compatible platform and discover how to customize the Mbed firmware to your own design, saving valuable time on your next project.

Learn More: MAX5715BOB ›

Electronic Toys

With smart audio amplifiers, products featuring micro speakers, such as electronic days, can deliver better sound quality.

Healthcare Wearables

Healthcare wearables could become more integral to overall patient care as doctors come to trust the devices and the data.

Pumpkin Pi Halloween Jack-o-Lantern

Connected jack-o’-lantern comes to life thanks to IoT platform.

The MAX30208 10-pin thin LGA package

Smart Speaker

Getting great audio quality from micro speakers calls for a smart amplifier with Dynamic Speaker Management technology.

Stressed Integrated Circuit Engineer

Guitar

The Ziviz Jamstik electric guitar allows guitarists to produce and record music seamlessly with MIDI.

Electric Vehicle

Electric vehicle battery packs rely on advanced battery management systems for greater safety.

Smartphones

nanoPower comparators can play a key role in temperature monitoring for portable devices like smartphones.

Electrical Engineer

A MyMaxim account provides quick online access to rich technical resources.

Factory Robotics

Industrial communications ICs with isolation support industrial automation equipment.

TWS earbud and cradle with USB charging

Block diagram of a TWS earbud and cradle with USB charging.

TWS earbud

TWS earbud and cradle with USB and wireless charging.

Smartphone

Smartphone for Seniors Gets Smarter with Health Monitoring

MAXNANOPWRBD# evaluation kit

MAXNANOPWRBD# provides a fully assembled and tested kit for evaluating an array of ultra-low-power ICs.

LED headlights

MAX25610A/B LED drivers enable highly efficient and compact LED lighting applications.

Radio Bridge

Radio Bridge develops long-range, low-cost wireless sensor solutions for a variety of end markets.

Radio Bridge

Radio Bridge develops long-range, low-cost wireless sensor solutions for a variety of end markets.

Building automation technology

Power management ICs help support effective building automation technologies.

Smartwatch clock

Small, low-power RTCs are ideal for compact, portable designs.

Industrial Control System

RS-485 is an ideal communications standard for noisy industrial environments.

ProtoCentral MAX30003 breakout board

Breakout boards like ProtoCentral’s MAX30003 product help you quickly evaluate and test-drive the MAX30003 biopotential AFE.

Industrial IoT application

Small, efficient, and rugged ICs are critical components in an IIoT application.

Maxim Summer Interns Showcase Their Technical Talents

Maxim’s summer 2019 interns showcase their talents in areas including electrical engineering, finance, marketing, and legal.

Laptop clock

An accurate, low-power RTC keeps clocking applications running reliably.

How Secure Authenticators Prevent Counterfeiting of Medical Disposables

Medical disposables such as pulse oximeters can be easily protected with secure authenticators.

Clock

In addition to clocking functionality, RTCs can help save power and reduce size for compact designs.

Smartwatch for healthcare

Smartwatches and other wearables can help reduce healthcare costs.

How Dynamic Voltage Scaling Saves Power in Wearables

Wearables that provide continuous, real-time monitoring of vitals such as heart rate are designed to operate reliably under varying conditions and use cases. Dynamic voltage scaling can complement other techniques to minimize power and extend battery life.

Smart Lock

Embedded electronic authentication can help ensure that smart locks do their job.

Battery-powered portable devices

Power converters for portables must be small and efficient.

Camera batteries

Keep portable device batteries safe during operation with battery monitors, protectors, and fuel gauge ICs.

Power management IC diagram

A power management IC provides an efficient way to power wearables.

Startup team brainstorm session

Startups working to get their products off the ground can take advantage of Maxim’s free design pack for fast prototyping.

Sensors Expo: See Wearable Healthcare Technologies in Action

Jogger with Fitness Tracker

Fitness trackers are among the many health and fitness wearables for which designers need reliable, power-efficient, and tiny sensors and ICs.

Silicon wafer probe testing

Silicon wafer probe testing

To reduce semiconductor testing costs, increase throughput with dual-channel pin electronics like the MAX9979.

How to Derive More System Efficiency from Battery-Powered Designs

Video game controller

Buck controllers can support the efficiency and battery life requirements of portable electronics.

Vehicle emissions

Vehicle emissions

Supervisory and watchdog-timer ICs play a role in helping vehicles meet strict emissions standards.

Understand How Physically Unclonable Function Technology Can Benefit Your Design

Understand How Physically Unclonable Function Technology Can Benefit Your Design

Learn why physically unclonable function (PUF) technology should be part of your embedded design security strategy.

MAXREFDES1160 - Full-duplex, 500kbps and 2.75kVRMS Isolated RS-485 Module Using the MAX14853

Learn to design an isolated RS-485 communication module with MAXREFDES1160.

Industry 4.0 manufacturing

Industry 4.0 manufacturing

Small, efficient DC-DC power modules power the sensors that bring intelligence to smart factories.

Smart Building

Smart buildings need smart power management technologies that meet efficiency, size, safety, and reliability requirements.]

Center Information Display

Vehicle displays like the CID must meet ASIL B requirements for functional safety.

Video game console

FPGA designs, such as this video game console, benefit from multiphase buck regulators in the power supply.

How Ceramic Voltage References Enhance Long-Term Drift Performance

In industrial equipment, such as this automated machine, accurate voltage references are essential for high performance.

Maxim Is Going to the Dogs in 2020

As Maxim reaches out to new markets, it has found its newest long-tail opportunity in high-end canine accessories.

Introduction to the MAX5861 DOCSIS 3.1 High-Density SCQAM and OFDM Downstream Cable Modulator

This video provides an introduction to Maxim’s DOCSIS 3.1 High-Density SCQAM and OFDM Downstream Cable Modulator – the MAX5861.

Cost-Effective, Efficient Solar 

 

“The JinkoMX modules (with Maxim cell-string optimizers) provide technology that helps mitigate shading issues at a price point below other alternatives.”
 -Caleb Arthur, CEO, Missouri Sun Solar


Featured products: Cell-string optimizers

Read Their Story ›

Fundamentals of Error Correction Codes

Learn why and how computing devices detect and correct errors. Discover error correction options using the MAX32665 low-power Arm®-Cortex®-M4 microcontroller.

Learn More: MAX32665 ›

Introduction to the MAX14815 Octal 5 Levels Pulser with T/R Switch and Embedded Beamforming

This video provides an introduction to Maxim's Octal 5 Levels Pulser with T/R Switch and Embedded Beamforming - the MAX14815.

Introduction to the MAX30134 4-Channel Ultra-low Power Electrochemical Sensor AFE

This video provides an introduction to Maxim's 4-Channel Ultra-low Power Electrochemical Sensor AFE - the MAX30134.

Introduction to the MAX17630 and MAX17631 4.5V to 36V, 1A and 1.5A, High-Efficiency, Synchronous Step-Down DC-DC Converters

This video provides an introduction to Maxim's high-efficiency, high-voltage, synchronous step-down DC-DC converter with integrated MOSFETs - the MAX17630 and MAX17631.

Introduction to the MAX6078A Low-Power, Low-Drift and Low-Noise Voltage Reference

This video provides an introduction to Maxim’s Low-Power, Low-Drift and Low-Noise Voltage Reference the MAX6078A and MAX6078B

Introduction to the MAX20011 Automotive Single 8A/12A Step-Down Converter with High Efficiency

This video provides an introduction to Maxim's Automotive Single 8A/12A Step-Down Converter with High Efficiency - the MAX20011.

Smartwatch for Health Monitoring

Smartwatches and other wearables provide continuous health monitoring.

Evaluation Kit for 2.9V to 5.5V, 1A uSLIC Power Module for 1.5V Output

MAXM17623EVKIT

Integrated power solution provides 1.5V from an input range of 2.9V to 5.5V with up to 1A of current.

Learn more ›

Get the Highest Level of Safety with an ASIL-D Battery Monitor IC

Achieving safety compliance in automotive applications can require adding redundant components to the system. The MAX17853 is the only ASIL-D-compliant IC for mid-to-large cell count configurations, enabling engineers to create a system that meets the highest level of safety for voltage, temperature, and communication.

Learn more: MAX17853 ›

Boosting Sight for the Visually Impaired

 

“It’s all the little things that Maxim helped us with which add up to make a significant difference.”
 -Patrick Antaki, Co-Founder and President, Evergaze


Featured products: Maxim lens driver, MAX44009, MAX8834, MAX77818, Maxim overvoltage protector ICs

Read Their Story ›

Solar Power in Shady Places

 

“Maxim’s junction box integrated cell-string optimizer has given us maximum design and layout flexibility to put panels on multiple roof planes without compromising performance.”
 -Anand Janaswamy, SVP, Product Development and Utilization at OneRoof Energy


Featured products: Cell-string optimizers

Read Their Story ›

Maxim Power Solutions for Xilinx FPGAs

Here’s evidence that Maxim and Xilinx have been working closely together, to help you power up Xilinx FPGAs without a lot of time, budget, or power supply expertise. Minimize power dissipation and board space, and get to market sooner.

Learn more:  Xilinx Power Partnership ›

Halloween Candy Dispensing Robot

Robot built with Adafruit components dispenses Halloween candy.

Halloween Dropping Spider on Doorbell

Arduino, an ultrasonic sensor, and a servo bring a “dropping spider” prank to life for Halloween.

Laser Tag Game Dispensers

IoT Laser Tag, built with Adafruit components, can be a fun Halloween game.

Haunted Home Automation

Create a haunted home using automation technologies including connected LED light bulbs, Raspberry Pi, and an Amazon Alexa.

Introduction to the MAX32520 ChipDNA™ Secure Arm Cortex M4 Microcontroller with SP800-90A/B TRNG

This video provides an introduction to Maxim's ChipDNA™ Secure Arm Cortex M4 Microcontroller with SP800-90A/B TRNG - the MAX32520.

Introduction to the MAX40660 MAX40661 Transimpedance Amplifier With Low Power Mode for LiDAR Applications

This video provides an introduction to Maxim's Transimpedance Amplifier With Low Power Mode for LiDAR Applications - the MAX40660 MAX40661.

Introduction to the MAX20090 MAX20090B Automotive High-Voltage High-Brightness LED Controller

This video provides an introduction to Maxim’s Simple Automotive High-Voltage HB LED Controller – the MAX0090.

Introduction to the MAX38907 MAX38908 MAX38909 2A/4A High Performance LDO Linear Regulator

This video provides an introduction to Maxim's 2A/4A High Performance LDO Linear Regulator - the MAX38908 product family.

Power Seminar: 24V+ Power Solutions--Power Design Doesn’t Get Any Cooler, Smaller, or Simpler

Introduction and agenda for the Power System Design Seminar series.

Watch first module ›

Developing 77/79GHz CMOS mmWave Radar Sensor ICs

 

"Maxim’s automotive PMIC “perfectly meets our requirements. Not many competitive solutions reach this kind of functional safety level”
 -Jiafeng Wang, Sales Manager, Calterah


Featured product: MAX15027, MAX20014

Read Their Story ›

4-Channel Ultra-Low-Power Electrochemical Sensor AFE

MAX30134

Provides electrochemical impedance spectroscopy measurement capability for 2- and 3-terminal sensors.

Learn more ›

Evaluation System for Electrochemical Sensor AFE

MAX30134EVSYS

Provides a single platform to evaluate DC current and EIS measurement capabilities.

Learn more ›

Understanding DAC Specifications

Understanding DAC Specifications

The digital-to-analog converter (DAC) converts digital words of 0s and 1s to analog voltage signals. This DAC tutorial walks you through the basics of digital-to-analog converter performance, from static to active specifications.

Learn More › Data Converters

MAX30205 Evaluation System

MAX30205EVKIT

System to evaluate the MAX30205 human body temperature sensor. Includes a USB-to-I2C controller and GUI.

Learn more ›

Introduction to the MAXM86161 Single-Supply Integrated Optical Module for HR and SpO2 Measurement

This video provides an introduction to Maxim’s Single-Supply Integrated Optical Module for heart rate and SpO2 Measurement – the MAXM86161.

Introduction to the MAX32570 Low Power ARM Cortex-M4 Microcontroller for Secure Applications

This video provides an introduction to Maxim's Low Power ARM Cortex-M4 Microcontroller for Secure Applications - the MAX32570.

Introduction to the MAX22503E 100 Mbps Full Duplex 3V/5V RS-485/RS422 Transceiver with High EFT Immunity

This video provides an introduction to Maxim's 100 Mbps Full Duplex 3V/5V RS-485/RS422 Transceiver with High EFT Immunity - the MAX22503E.

Introduction to the MAX15158Z High Voltage Multiphase Boost Controller

Introduction to the MAX25612 Automotive Synchronous High-Voltage LED Controller

This video provides an introduction to Maxim's Automotive Synchronous High-Voltage LED Controller - the MAX25612.

Creating an Even Smarter Smartphone

 

Developed by Fujitsu Connected Technologies Limited, the Raku-Raku Smartphone is designed from the ground up to be easy to use, particularly for those who are new to touchscreen operations.

Featured product: MAX30101

Read Their Story ›

Introduction to the MAX25611A MAX25611B MAX25611C MAX25611D Automotive High-Voltage HB LED Controller

This video provides an introduction to Maxim’s Simple Automotive High-Voltage HB LED Controller – the MAX25611.

Introduction to the MAX16160 High Accuracy Quad, Any-Input Voltage Monitor and Reset

This video provides an introduction to Maxim's High Accuracy Quad, Any-Input Voltage Monitor and Reset - the MAX16160.

Introduction to the MAX30208 Low-Power, High-Accuracy Digital Temp Sensor

This video provides an introduction to Maxim’s low-power, high-accuracy digital temp sensor – the MAX30208.

Power Protection Fundamentals

In an imperfect world, unpredictable things can happen such as power surges resulting in failing components. System protection strategies help solve these fault problems and preserve system integrity. Learn some tricks of the trade to solve power protection problems before they even occur.

Learn More: Protection and Control ›

Amplifier Offset and Gain Error in a Signal Chain

Common amplifier factors such as offset and gain can introduce errors into the signal chain. Acquire a better understanding of what is behind amplifier offset and gain errors for more effective signal chain design strategies.

Learn More: Analog Products ›

Introduction to the MAX77654 Ultra-Low Power PMIC Featuring Single-Inductor, 3-Output Buck-Boost, 2-LDOs, Power Path Charger for Small Li+, and Ship Mode

This video provides an introduction to Maxim’s MAX77654, one of the world’s best solutions for low-power consumer applications.

Introduction to the MAX20333 Adjustable Current Limit Switch with Low Power Mode

This video provides an introduction to Maxim’s new Adjustable Current Limit Switch with Low Power Mode – MAX20333.

Introduction to the MAX49017 Micropower Dual Automotive Comparator with Built-In Reference in Small 2x2 TDFN

This video provides an introduction to Maxim’s Nanopower Dual Automotive Comparator with Built-In Reference in Small 2x2 TDFN – the MAX49017.

Overview of Voltage References and Supervisors

In this video, understand the important aspects of voltage references and the key criteria in selecting the right one for your design. Also learn about voltage supervisors, the different types of supervisory products available and their key features.

Learn more: Voltage References ›

Introduction to the MAX86140 and MAX86141 Optical Pulse Oximeter and Heart-Rate Sensor

This video provides an introduction to the MAX86140 and MAX86141, a Best-in-Class Optical Pulse Oximeter and Heart-Rate Sensor for Wearable Health.

Introduction to the MAX40016 4-Decade Current Sense Amplifier with Integrated Rsense Element

This video provides an introduction to the MAX40016, a very wide range current sense amplifier (CSA) with internal sense element that senses from less than 300μA to greater than 3A current range.  

High-Performance, Ultra-Low-Power Stereo Audio Codec with FlexSound® Technology DSP

MAX98090

Fully integrated audio codec includes analog/digital microphone input, stereo Class D speaker amplifier, and DirectDrive headphone amplifier for portable applications.

Learn more ›

Mono 3.2W Smallest Class D Amplifier

MAX98304

0.95mA IQ at 3.7V (1.2mA at 5V), offers five selectable gain settings set by a single gain-select input (GAIN) in 1mm x 1mm package.

Learn more ›

Boosted Class-DG Amplifier with Integrated Dynamic Speaker Management and Industry-Leading Efficiency