mgineer Blog
Top

Power Play: Get Design Tips on Power Applications and Circuits
Understand the Multiphase Buck Voltage Regulator Advantage

May 26, 2020

Reno Rossetti  By: Reno Rossetti
 Power Blogger, Maxim Integrated 


Step-down (buck) voltage regulators have long been the preferred DC-DC conversion electronic workhorse thanks to their inherently high efficiency. Only in buck mode the current is directed to the output during the entire cycle. The higher delivery of current to the output, per cycle, makes the buck converter the most efficient architecture. As one of many examples, modern microprocessors, from those used in powerful server blades to smartphones, operate with very low input voltages, making the buck converter the necessary power source. As these applications grow in sophistication, the power source has to beef up its power delivery while stepping up its efficiency to reduce heat losses. Accordingly, the buck converter has evolved from non-synchronous to synchronous switching and from a single-phase device that delivers a few hundred milliamperes of current to a multiphase device that can successfully deliver tens to hundreds of amperes of current. Figure 1 shows a modern four-phase interleaved buck converter powering a CPU core chip for smartphones and tablets.

Diagram of a Multiphase, Interleaved PCBFigure 1. Diagram of a Multiphase, Interleaved PCB

Two-Phase Interleaved Buck Converter Architecture

For simplicity, we will focus our discussion on a two-phase interleaved, synchronous buck converter architecture (Figure 2).

Diagram of Two-Phase Interleaved Buck ConverterFigure 2. Diagram of Two-Phase Interleaved Buck Converter

The two interleaved phases assure ripple current and, hence, ripple voltage reduction. Low total ripple current is obtained at a relatively low per-phase frequency of operation. As an example, Figure 3 shows that two ripple currents 180° out-of-phase at 33% duty cycle result in a total ripple current with half the amplitude of a single phase at twice the frequency. Lower output current ripple and voltage ripple at higher frequency means fewer capacitors are needed on the output, resulting in a smaller BOM.

Diagram of Two-Phase Interleaved Buck ConverterFigure 3. Illustration of Two-Phase Current Ripple Reduction vs. Time

The two-phase architecture also requires fewer input capacitors. The total input current is the sum of the two out-of-phase currents (IIN1 and IIN2 in Figure 4). Here, spreading the total input current over time reduces the input current's total RMS value, compared to a single-phase operation, allowing for a smaller input current ripple filter.

Illustration of Two-Phase Output Ripple Currents and Input Currents vs. TimeFigure 4. Illustration of Two-Phase Output Ripple Currents and Input Currents vs. Time

Additionally, as shown in Figure 5, two-phase (2Φ, shown in red) is more efficient than single-phase (1Φ, shown in blue) when the two schemes run at the same output ripple frequency. Single-phase, by running at two times the switching frequency (fSW) of two-phase, can also achieve high frequency and low current ripple but at higher switching losses. The two schemes have an equal number of transitions within one period, but the two-phase converter draws half the current of the single-phase converter (over twice the duration), thus reducing the switching losses.

Illustration of Two-Phase Current vs. Single-Phase Current vs. TimeFigure 5. Illustration of Two-Phase Current vs. Single-Phase Current vs. Time

Another great benefit of a two-phase converter is the fast transient response and reduced voltage overshoot/undershoot during load steps. With half the current per phase, reduced current ripple amplitude, and double the ripple frequency, the phase switching frequency can now be pushed higher to further reduce the component size and increase the closed-loop bandwidth of the converter without running into thermal limitations.

Finally, as the total load current increases, the size of the passive components increases. For high loads, the inductor for a single-phase buck can be bulky and inefficient. Multiphase operation reduces the current in each phase, which ensures optimal sizing for passives.

As an example, MAX77812  is a 20A configurable, single-to-quad-phase, single-to-quad-output high-current, buck (step-down) converter. A rich portfolio of multiphase interleaved buck converters is available to system designers.

Why a Coupled Inductor Is Ideal for High-Current Applications

In very high-current applications, where it is important to squeeze out the last percentage point of efficiency, there is another card to play: the coupled inductor, in which the inductors are wound around a common magnetic core. In a two-phase coupled inductor (Figure 6), the winding orientation is such that the magnetic flux cancels out, resulting ideally in a transformer with zero leakage inductance LK and infinite magnetizing inductance. In practice, we end up with a very low inductance per winding (Lk) compared to the uncoupled case.

Diagram of Two-Phase Coupled inductor Model and OperationFigure 6. Diagram of Two-Phase Coupled inductor Model and Operation

Let us write the network equations with SW1 and SW4 on. The ideal 1:1 transformer forces equal winding voltages VW and equal voltage drops VLK across the inductances. For the top branch we have:

VIN = VW + VLK + VOUT

And for the bottom branch:

VW = VOUT + VLK

From which:

VIN = 2VOUT + 2VLK

Where:

VOUT + VLK = VY

Hence:

VY = VIN/2

And:

VLK = VIN/2 -VOUT

Namely, the voltage VLK across each inductance is less than half of the input voltage! This is less than half the value for the case of the uncoupled inductor. At equal inductances, the coupled inductor will develop less than half the ripple current versus two uncoupled inductors, resulting in smaller BOM and higher efficiency. Alternately, operating with lower inductance improves BOM and transient response.

Summary

The buck voltage regulator is the low voltage DC-DC conversion workhorse, providing core power to applications from servers to smartphones. It has evolved from non-synchronous to synchronous, from single-phase to multiphase and, more recently, from uncoupled to coupled inductors, keeping up the pace of its sophisticated load and enabling its continued evolution.

Learn More

About the Author

Nazzareno (Reno) Rossetti is an Analog and Power Management expert at Maxim Integrated. He is a published author with several patents in this field. Reno holds a doctorate in Electrical Engineering from Politecnico di Torino, Italy.