mgineer Blog

5 Ways Solar Power Usage Will Change By 2037

December 05, 2017

December 5, 2017

Ben Smith By: Kyle Pennell
Guest Blogger, PowerScout


As every stockbroker knows, it’s hard to know what the future holds. But following current trends in energy use, energy policy, and the solar industry into the future, there are at least five ways in which the use and creation of solar power will change by about 2037.

1. Solar power will become more affordable. In 1975, solar panels produced energy at a rate of over $100 per watt. Today, the price is less than $1 per watt. That means solar energy is already as cheap as coal in Germany, Spain, Italy, Australia, and the U.S., and is on track to become cheaper than natural gas within the decade.

As solar power installations multiply and solar technology becomes more efficient, costs will continue to decline. According to the International Renewable Energy Agency, the price could decline by an additional 59% by 2025 compared against 2016 prices. Further declines will be difficult to achieve, but by 2040, the price could plummet by two-thirds of its current cost.

Solar panels

The cost of energy produced via solar panels continues to drop.

2. Solar power will become more common. As solar power becomes the economically logical choice for energy production, both residential and utility-scale solar installations will multiply.

Even where fossil fuels remain economically competitive, governments struggling to mitigate climate change and curb pollution will continue demanding higher levels of solar and other forms of renewable energy. The Philippines, for instance, has set a renewable energy production target of 35% by 2040. And Germany, which has one of the highest renewable targets in the world, plans on meeting over 65% of its electricity needs through renewables by 2040. Globally, analysts estimate that almost one-third of the world’s electricity will come from solar by 2040, including 10% from small-scale (residential) solar systems and 22% from utility-scale solar installations. That's 14X greater than the amount of solar power being produced today.

The U.S. has no national renewable energy production quotas (though the federal government has set a target of 30% renewable energy by 2025 for government buildings, about 19% of which will come from solar). These quotas (known formally as renewable energy portfolio standards) are instead determined by individual states. To date, only 29 states and the District of Columbia have developed renewable targets of any kind. States that have targets vary widely in their levels of ambition and their timelines for implementation. Arizona, for instance, aims to produce at least 15% of its energy from renewables by 2025. Hawaii, on the other hand, is on track to produce 30% of its energy from renewables by 2020, 40% by 2030, and 70% by 2040.

Despite the uneven pattern of development, the trend across the U.S. is clear: solar energy will be used far more in 20 years than it is today. Analysts predict that the U.S. will meet about 40% of its total electricity needs through renewable energy by 2040. The exact makeup of each state’s renewable energy portfolio will vary depending on its geography. The sunny South and Southwest will probably rely primarily on solar power, while inland states might rely more on a mix of solar and wind energy. States with plentiful rivers and coastlines will use a proportionally greater volume of hydroelectric power.

3. Solar technology will improve. Over the next two decades, over $7.5 trillion is expected to be invested in renewable technologies, including $2.8 trillion of investment in solar energy. This will result not only in new solar panels, but in research and development that produces panels that are lighter and stronger than those we have today.

Panel efficiency will also improve. Today, the best commercially available solar panels operate with about 20% efficiency. But the next generation of solar technology could be more than 46% efficient.

Other advances will allow solar to become integrated into more devices and surfaces. Scientists at MIT are working on flexible, transparent solar cells made of organic materials and graphene electrodes. The technology is still experimental, but it could hold the key to turning any surface into a source of solar power. In two decades, our phones, laptops, and other devices could be charged simply by exposing them to light, and skyscrapers covered in transparent solar cells could provide energy for entire city blocks.

Solar panels could also start showing up in other unexpected places. Solar roads are a new technology that turn roads into sites of solar energy production. The solar panels are as hard as asphalt but transparent enough to allow light to enter the solar cell within. Some estimates suggest that if every parking lot and road in the U.S. was covered in solar panels, we’d produce over 3X the energy we use today. Solar roads are also safer than traditional roads since they contain a heating element that prevents the buildup of snow and ice in winter. The big problem with solar roads today is that they’re astronomically expensive. Late last year, France installed a single lane of solar road panels along a 1-kilometer stretch in Normandy at a cost of $5.2 million. The average cost of paving an equivalent area is about $620,000 to $1 million. Even factoring in the cost of the energy produced by the solar road, the math doesn’t add up: traditional solar panels can produce an equivalent amount of energy at one-thirteenth the cost. But if trends in other areas of solar technology are any indication, advances in solar road technology and reductions in road panel costs will only accelerate. Two decades from now, we could be walking, biking, or driving on solar panels.

Panel-integrated microinverters will also become more common. Today, 96% of all solar inverters are either central or string inverters. But microinverters are safer and more efficient, and allow for individual panel monitoring. And by integrating microinverters directly into the panel's design—thus eliminating the need for clunky string inverters, conduits, and other system components—installation will become even cheaper and easier.

4. China will lead the solar industry. China is investing more than any other country—$32 billion—in renewable energy, and a large portion of that investment is in solar. Because of more advanced supply chain development and economies of scale, China’s solar panel manufacturers have an estimated 20% cost advantage over their U.S. competitors. Already, the world’s two biggest solar equipment makers are Chinese, and six Chinese companies are among the top 10. Only two American companies, by contrast, made the top 10 list.

5. The developing world will be peppered with solar microgrids. Microgrids are localized, small-scale power networks that are disconnected from a large power plant. A micro-grid on the scale of a small village, for instance, might have a ring of solar panels around it, or cluster them in a central location. Isolated communities in South America, Africa, and Southeast Asia stand to benefit substantially, since it will likely be cheaper and easier to build a microgrid in 2040 than to connect to a distant centralized power plant.