APPLICATION NOTE 93

Design Guidelines for Microcontrollers Incorporating NV RAM

By:  Kevin Self

Abstract: This application note will help the user of the Dallas Semiconductor secure microcontroller and high-speed microcontroller improve reliability when implementing nonvolatile SRAM. This note is applicable to the Secure and High-Speed Secure Microcontroller families as well as the DS87C530 high-speed microcontroller. Out-of-tolerance voltage spikes, protecting I/O pins and negative power supply transients are discussed in this application note.

Overview

Microcontrollers which incorporate battery-backed, nonvolatile SRAM (NV RAM) have found wide acceptance in the embedded marketplace. Unlike Flash memory or EEPROM technology, nonvolatile SRAM has no write limitations, which makes it ideal for real-time data logging applications. In products such as the Dallas Semiconductor Secure Microcontroller family, NV RAM can be used to provide insystem reprogrammable program memory.

This application note discusses design guidelines for microcontroller products which incorporate NV RAM. A number of design suggestions are presented to improve the reliability of microcontrollers which incorporate NV RAM. It should be stressed that battery-backed memory is as reliable as nonvolatile memory as long as standard CMOS design guidelines are used. This application note is applicable to the Secure and High-Speed Secure Microcontroller family of products as well as the DS87C530 High-Speed Microcontroller.

Out-of-Tolerance Voltage Spikes

The real world is a harsh place; electrostatic discharge (ESD), electrical noise, etc. can enter into a system. Many of these phenomena can induce negative voltages on one or more device pins. CMOS design guidelines require that no pin be taken above VCC or below VSS. Violation of this guideline can result in a hard failure (damage to the silicon inside the device) or a soft failure (unintentional modification of memory contents).

Negative voltage spikes are a particular problem for CMOS devices. When a negative voltage spike is experienced, one or more parasitic diodes inside the device can become forward-biased. This will cause the device to consume a large amount of current, and can cause the device to latch-up. In general, the only way to reverse CMOS latch-up is to remove power from the device. If the supply to the device is not limited, the excessive current draw can cause irreparable damage to the device.

Less severe, but just as troublesome, is the effect this can have on nonvolatile memory. When a parasitic diode forms, a high-current path will form. This will drain current away from the device, and may cause the voltage to sag internally. If the internal voltage drops below the minimum needed to maintain the memory, soft errors may be experienced.

In a practical application, it is often difficult or impossible to remove all voltages above VCC or below VSS. Realistically, overshoots or undershoots of 0.3V can be tolerated by most devices. The following cases discuss common causes of such conditions and ways to minimize their effect on systems.

Protecting I/O Pins

The most common way that a device experiences negative voltage spikes is through its general-purpose I/O pins. These are usually the only contact that the microcontroller has with the "outside world." Devices such as electrical motors and keypads can generate large amounts of electrical noise. The shock that one experiences when touching a doorknob, for example, can be as much as 30kV. If this voltage is transmitted from a keypad into a microcontroller system, it can seriously damage electronic components.

Figure 1 demonstrates a diode protection scheme that can be used to protect the I/O pins of a microcontroller. The scheme relies on the use of a Schottky diode and current limiting resistor to reduce the effect of current spikes on the device. When the voltage approaching the device pin exceeds VCC or VSS by more than 0.1V - 0.2V, the Schottky diodes will become forward biased, conducting the excess voltage away from the device pins. The current limiting resistors will also help dampen the effect of the voltage spike on the microcontroller.

Figure 1. External I/O protection scheme.
Figure 1. External I/O protection scheme.

The protection diodes shown in Figure 1 must be chosen carefully. Most Schottky diodes, such as the popular 1N5817, are suitable at room temperature. At high temperatures, however, their reverse bias leakage will begin to load the I/O line, making it difficult for the device to drive a logic 1. For example, a DS87C520 can drive a logic 1 with a maximum current of 50µA. At room temperature, the reverse leakage of a typical 1N5817 is 30µA. At 70°C, however, the reverse leakage is greater than 100µA. The microcontroller will be unable to source enough current to maintain a CMOS logic high of 2.4V.

Any Schottky diode used should have a leakage well below the maximum drive current of the sourcing device. Diodes with low reverse leakage currents are available from many vendors.

Negative Power Supply Transients

Another source of voltage spikes is the power supply. Many simple voltage regulators, such as a 7805 5V regulator, are notorious for generating voltage spikes as they power up. Care must be exercised when designing the power supply so that it does not generate excessive noise when powering up or when switching loads in and out of the system.

The problem of power supply transients can be lessened by using a reverse-biased Schottky diode across VCC and GND, similar to that used for protecting I/O pins. Figure 2 shows one such scheme.

Figure 2. Voltage regulator protection scheme.
Figure 2. Voltage regulator protection scheme.



Related Parts
DS2250 Soft Microcontroller Module  
DS2251T 128k Soft Microcontroller Module  
DS2252T Secure Microcontroller Module  
DS5000 Soft Microcontroller Module  
DS5000FP Soft Microprocessor Chip  
DS5000T Soft Microcontroller Module  
DS5001FP 128k Soft Microprocessor Chip Samples  
DS5002FP Secure Microprocessor Chip Samples  
DS5230 IP Security Microcontroller  
DS5250 High-Speed Secure Microcontroller  
DS87C530 EPROM Microcontrollers with Real-Time Clock Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (34kB)  

© May 01, 2001, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 93: May 01, 2001
APPLICATION NOTE 93, AN93, AN 93, APP93, Appnote93, Appnote 93