APPLICATION NOTE 712

DS80C400 Ethernet Drivers


Abstract: The DS80C400 high-speed microcontroller has a built-in Ethernet media-access controller (MAC) with an industry-standard media independent interface (MII). This application note presents design considerations and fully tested example assembly code for an Ethernet interrupt handler, and code for sending and receiving Ethernet packets. Using these routines, you can develop custom applications such as TCP/IP routers.

Introduction

The DS80C400 high-speed microcontroller has a built-in Ethernet media-access controller (MAC) with an industry-standard media independent interface (MII). Please refer to the High-Speed Microcontroller User's Guide: DS80C400 Supplement and the DS80C400 data sheet for details.
This application note presents design considerations and fully tested example assembly code for an Ethernet interrupt handler, and code for sending and receiving Ethernet packets. Using these routines, you can develop custom application such as TCP/IP routers. Full source code and the header files defining the symbolic constants can be found on the Dallas Semiconductor ftp site at http://files.maximintegrated.com/microcontroller/mxtni/ds80c400/ethdriver/.
Figure 1. DS80C400 Ethernet Buffer.
Figure 1. DS80C400 Ethernet Buffer.

The DS80C400 MAC Hardware

Ethernet Buffer Memory

The DS80C400 communicates with the network via a set of special function registers (SFRs) and 8kB of dual port buffer memory. The buffer memory is divided into the receive and send memory and can be addressed in blocks of 256 bytes ("pages"). The receive pages are organized in a circular fashion, managed by the DS80C400 hardware. The send buffer is managed by the user's application.
The location for the Ethernet buffer is usually address 0FFE000h (default configuration established by ROM loader), assigned to the constant ETH_RECEIVE_BUFFER.

Ethernet Control Status Registers

The primitives ReadCSR and WriteCSR are used to read and write the DS80C400 Ethernet control status registers (CSRs). Note that the example code does not save the processor registers across function calls. When using this code, ensure that you don't destroy the processor state (this is especially important when using interrupt driven data transfer).

Read CSR

ReadCSR reads a control status register.
;****************************************************************************
;*
;* Function Name: ETH_ReadCSR
;*
;* Description: Read from specified register.
;*
;* Input(s): a -> register address
;*
;* Outputs(s): r3:r2:r1:r0 -> 32 bit register byte value
;*
;****************************************************************************
ETH_ReadCSR:
	push 	eie
	clr 	eie.5
	mov 	csra, a 				; Load CSRA SFR with the LSB of the
							; 16-bit address of the targeted CSR
	anl 	bcuc, #0f0h 				; Clear BCUC command bits
	orl 	bcuc, #BCU_READ_CSR 			; Write read CSR command to BCUC SFR
	push 	acc
eth_readcsr_busy: 					; Wait until Busy bit in BCUC SFR is reset
	mov 	a, bcuc 				; Move to acc since BCUC is not bit cap.
	jb 		acc.7, eth_readcsr_busy
	pop 	acc

	mov		r3, csrd 			; Read CSRD SFR for MSB of 32 bit data
	mov 	r2, csrd
	mov 	r1, csrd
	mov 	r0, csrd 				; LSB
	pop 	eie
	ret
Listing 1. ReadCSR Reads a Control Status Register
Note that this code saves, disables, and restores the Ethernet activity interrupt enable (eie.5) to make sure that a write to the CSR is not interrupted by an Ethernet activity interrupt. The definition for the bcuc, csrd and csra SFRs can be found in the include file ds80c400.inc. Constant values such as BCUC_READ_CSR are defined in eth400.inc.

Write CSR

The WriteCSR function writes a 32 bit value to a control status register.
;****************************************************************************
;*
;* Function Name: ETH_WriteCSR
;*
;* Description: Write to specified register.
;*
;* Input(s): a -> register address
;* r3:r2:r1:r0 -> 32 bit value
;*
;* Outputs(s): N/A
;*
;****************************************************************************
ETH_WriteCSR:
	push	eie
	clr 	eie.5
	mov 	csrd, r3 			; Write CSRD SFR for MSB of 32 bit data
	mov 	csrd, r2
	mov 	csrd, r1
	mov 	csrd, r0 			; LSB

	mov 	csra, a 			; Load CSRA SFR with the LSB of the
						; 16-bit address of the targeted CSR
	anl 	bcuc, #0f0h 			; Clear bcuc command bits 0-3
	orl 	bcuc, #BCU_WRITE_CSR 		; Write write CSR command to bcuc SFR

	push 	acc
eth_writecsr_busy: 				; Wait until Busy bit in BCUC SFR is reset
	mov 	a, bcuc
	jb 		acc.7, eth_writecsr_busy
	pop 	acc
	pop 	eie
ret
Listing 2. WriteCSR Writes a Control Status Register

Initialization

MAC Address

In order to use the DS80C400 on the network, a globally unique MAC address needs to be programmed into the device. The MAC address can either be acquired from the DS2502-E48 MAC address 1-Wire® part (Dallas Semiconductor has registered a range of ready-to-go MAC addresses in order to simplify building embedded devices) or from another IEEE® registered source.
Very important: Under NO circumstances select a random MAC address or the address of another existing device. MAC addresses are globally unique and network stability depends on well behaved devices!
;****************************************************************************
;*
;* Function Name: ETH_LoadEthernetAddress
;*
;* Description: Load the 48 bit ethernet address into the controller.
;*
;* Input(s): dptr0 -> pointer to the Ethernet address (big-endian)
; for example 00 60 01 02 03 04
;*
;* Outputs(s): N/A
;*
;****************************************************************************
ETH_LoadEthernetAddress:
	movx 	a, @dptr
	mov 	r0, a
	inc 	dptr
	movx 	a, @dptr
	mov 	r1, a
	inc 	dptr
	movx 	a, @dptr
	mov 	r2, a
	inc 	dptr
	movx 	a, @dptr
	mov 	r3, a
	inc 	dptr
	
	mov 	a, #CSR_MAC_LO
	acall 	ETH_WriteCSR

	movx 	a, @dptr
	mov 	r0, a
	inc 	dptr
	movx 	a, @dptr
	mov 	r1, a
	clr 	a
	mov 	r2, a
	mov 	r3, a

	mov 	a, #CSR_MAC_HI
	acall 	ETH_WriteCSR
	ret
Listing 3. LoadEthernetAddress Loads the MAC Address into the DS80C400
Note that two CSR writes are required to fully load the 6-byte Ethernet MAC address. Since this code is only called during initialization, it is not protected against Ethernet activity interrupts.
Initializing the Ethernet MAC further requires configuration of the partition between receive buffer (incoming packets) and send buffer (outgoing packets). Figure 1 shows this partition between page n-1 and page n.
To simplify code and avoid dropping inbound packets, most applications will benefit from partitioning the buffer memory in a fashion that reserves most of the pages for inbound packets and only allocates enough pages for one outbound packet. The reason for this is that Ethernet is a shared medium and—even in switched networks—only a fraction of incoming packets are of interest to an application. Therefore, we define the constants ETH_TRANSMIT_PAGE to 17h and ETH_SEND_BUFFER to ETH_RECEIVE_BUFFER + 17h x 256.
Constant Value
ETH_TRANSMIT_PAGE 17h
ETH_SEND_BUFFER 0FFF700h
The following code first disables the transmitter and then initializes the DS80C400 buffer memory to select the 23:9 receive:send partition. The code then sets the half/full duplex status (this status can be acquired from the MII, see below) and enables the transmitter.

Enabling the Transceiver

;****************************************************************************
;*
;* Function Name: ETH_EnableTransceiver
;*
;* Description: Enable receiver and transmitter for Ethernet controller.
;*
;* Input(s): N/A
;*
;* Outputs(s): N/A
;*
;****************************************************************************
ETH_EnableTransceiver:
	push 	eie
	clr 	eie.5
	; First, disable transmitter and receiver (full duplex bit is
	; not settable if they are on)
	clr 	a
	mov 	r3, a
	mov 	r2, a
	mov 	r1, a
	mov 	r0, a
	mov 	a, #CSR_MAC_CTRL
	acall	 ETH_WriteCSR
	
	; Set Ethernet buffer sizes
	TIMEDACCESS
	mov 	ebs, #ETH_TRANSMIT_PAGE 	; Also clears the flush filter failed bit
	mov 	r3, #00h 			; Select non-byte swap mode
	mov 	dptr, #ETH_DUPLEX_STATUS
	movx	 a, @dptr
	swap	 a 				; Move bit to position 4 (20:F)
	jnz 	eth_et_fullduplex
	orl 	a, #80h 			; Disable receive own (23:DRO)
eth_et_fullduplex:
	orl 	a, #08h 			; Pass all multicast (19:PM) – OPTIONAL
	mov 	r2, a 				; Set duplex mode according to PHY detection
	mov 	r1, #10h 			; Perfect filtering of multicast,
						; late collision control, no auto pad strip
	mov 	r0, #0ch 			; Block-off limit 10, no deferral check,
						; enable transmitter and receiver
	mov 	a, #CSR_MAC_CTRL
	acall	 ETH_WriteCSR
	pop 	eie
	ret
Listing 4. EnableTransceiver Partitions the Buffer Memory and Enables the Transceiver
Note that this code assumes the duplex status information is stored at location ETH_DUPLEX_STATUS in MOVX memory.

Flushing the Buffer

Next, the Ethernet buffer is flushed to ensure clean startup.
;****************************************************************************
;*
;* Function Name: ETH_Flush
;*
;* Description: Release all resources.
;*
;* Input(s): N/A
;*
;* Outputs(s): N/A
;*
;****************************************************************************
ETH_Flush:
	anl 	bcuc, #0f0h 		; Clear bcuc command bits
	orl 	bcuc, #BCU_INV_CURR 	; Write release command to bcuc SFR
	ret
Listing 5. Flush Flushes the Receive Buffer

Sending and Receiving

Sending a Packet

To send a packet, the user's application must first place the packet data in the Ethernet send buffer. If a previous packet was placed at the same address, the application must wait for the transmit to be complete before modifying the buffer memory.
Note that the first four bytes of the send buffer are reserved for the send status word. The first byte that will be transmitted is at location ETH_SEND_BUFFER+4.
;****************************************************************************
;*
;* Function Name: ETH_Transmit
;*
;* Description: Transmit the raw Ethernet packet currently in the
;* Ethernet send buffer
;*
;* Input(s): r5:r4 = total packet length in bytes
;*
;* Outputs(s): N/A
;*
;****************************************************************************
ETH_Transmit:
	; Ethernet frame is in transmit buffer (Starting at
	; page offset = 4). Byte count is in r5:r4

	; Load MSB of byte count to bcud SFR
	mov 	bcud, r5
	; Load LSB of byte count to bcud SFR
	mov 	bcud, r4

	; Load starting page address to bcud SFR
	mov 	bcud, #ETH_TRANSMIT_PAGE

	; XXX Set transmit in progress flag in your software here
	; XXX so you can avoid interrupting a transmit in progress.
	; XXX e.g.: setb ds400_xmit

	; Write transmit request to bcuc SFR
	anl 	bcuc, #0f0h 			; Clear bcuc command bits
	orl 	bcuc, #BCU_XMIT 		; Write transmit command to bcuc SFR
	ret
Listing 6. Transmit Sends a Packet Onto the Network

Receiving a Packet

When a packet is received (usually indicated by an interrupt, see below), the user code needs to unload the packet from the Ethernet buffer memory and then release the buffer memory, unlike the send buffer, which is managed by the user, the receive buffer is managed by the DS80C400.

Unloading the Packet Data

Note that a received packet can span several pages in the receive buffer and it can wrap from the last page in the receive buffer to the first page in the receive buffer. Ensure that your packet copy routine properly handles this case.
;****************************************************************************
;*
;* Function Name: ETH_Receive
;*
;* Description: Start unloading the last packet from the
;* Ethernet controller.
;*
;* Input(s): N/A
;*
;* Outputs(s): N/A
;*
;****************************************************************************
ETH_Receive:
	; Get location of buffer and set dptr0 accordingly
	mov 	a, bcud
	anl 	a, #1fh 					; we are not interested in the page count
								; so now a contains the starting page number
								; (1 page is 256 bytes)

	mov 	dptr, #ETH_RECEIVE_BUFFER 			; receive buffer starting address
	mov 	b, a 						; "multiply" page by 256 to get byte count
	clr 	a
	acall 	Add_Dptr0_16 					; and add it to receive buffer starting address
	; dptr0 now points to the receive status word of the packet

	movx 	a, @dptr
	inc 	dptr
	mov 	r2, a 						; save LSB of frame length

	movx 	a, @dptr
	inc 	dptr
	mov 	r3, a 						; save this

; check runt frame, watchdog time-out
	anl 	a, #(80h or 40h)
	jnz 	eth_ueh_release

	mov 	a, r3 						; restore and get frame length
	anl 	a, #3fh
	mov 	r3, a 						; save HSB of frame length

	movx 	a, @dptr
	inc 	dptr

	; check CRC error, MII error, collision seen, frame too long
	anl 	a, #(20h or 08h or 02h or 01h)
	jnz 	eth_ueh_release

	movx 	a, @dptr 					; MSB of status word
	; check for length error, control frame, unsupported ctrl frame
	; missed frame
	mov 	b, a
	anl 	a, #(80h or 20h or 04h or 02h or 01h)
	jnz 	eth_ueh_release 				; bad bad bad frame!

	mov 	a, b
	anl 	a, #40h 					; check for filter match
	jz 	eth_ueh_release

	; XXX Copy the packet into your buffer here.
	; XXX r3:r2 contain the length of the packet,
	; XXX dptr0 points to the beginning of the data.
	; XXX Note that the buffer can wrap!
eth_ueh_release:
	ret
Listing 7. Receive Receives a Packet from the Network

Releasing the Buffer

After processing an incoming packet, the user code needs to release the buffer memory in the Ethernet receive buffer.
;****************************************************************************
;*
;* Function Name: ETH_Release
;*
;* Description: Release resources.
;*
;* Input(s): N/A
;*
;* Outputs(s): N/A
;*
;****************************************************************************
ETH_Release:
	anl 	bcuc, #0f0h 			; Clear bcuc command bits
	orl 	bcuc, #BCU_INV_CURR 		; Write release command to bcuc SFR
	ret
Listing 8. Release Releases a Packet from the Receive Buffer

Interrupt Driven Operation

Instead of polling the bit flags in the bcuc SFR, an application should use the Ethernet activity interrupt for better performance. There is one interrupt handler for both receive and transmit complete interrupts. The Ethernet activity interrupt calls location 000073h. Since there are only 8 bytes per interrupt, we suggest installing a long jump to the actual function:
org 73h
ljmp ETH_ProcessInterrupt

Processing Interrupts

The following code handles both receive and transmit complete interrupts.
;****************************************************************************
;*
;* Function Name: ETH_ProcessInterrupt
;*
;* Description: ISR for Ethernet interrupt
;*
;* Input(s): N/A
;*
;* Outputs(s): N/A
;*
;* Destroyed: Nothing.
;****************************************************************************
ETH_ProcessInterrupt:
	push 	acc
	mov 	a, bcuc
	anl 	a, #rif 				; Received data?
	jz 	eth_pi_no_receive
	; XXX Call your receive packet handler here.
	; XXX Ensure it saves and restores all registers!
	; XXX E.g.: acall ETH_ProcessPacket
eth_pi_no_receive:
	mov 	a, bcuc
	anl 	a, #tif
	jz 	eth_pi_exit 				; Transmitted data?
	; XXX If you keep track of a send in progress, here's the place
	; XXX to clear the flag.
	; XXX E.g.: clr ds400_xmit
	anl 	bcuc, #(not(tif) and 0f0h) 		; and NOOP command
	; XXX If you keep transmit queue, send next packet from queue
	; XXX E.g.: acall ETH_SendNextFromQueue
eth_pi_exit:
	pop 	acc
	reti
Listing 9. ProcessInterrupt Handles Ethernet Activity Interrupts

Enabling Interrupts

Finally, after enabling the Ethernet interrupt, the DS80C400 is ready to receive and send packets.
;****************************************************************************
;*
;* Function Name: ETH_EnableInterrupts
;*
;* Description: Enable Ethernet transmit/receive interrupts.
;*
;*
;* Input(s):
;*
;* Outputs(s):
;*
;* Destroyed:
;****************************************************************************
ETH_EnableInterrupts:
	; XXX If you keep track of transmits in progress, clear
	; XXX the flag here.
	; XXX E.g.: clr ds400_xmit
	anl 	bcuc, #(not(rif or tif) and 0f0h) 	; Clear interrupt flags
	setb 	eie.5 					; Enable Ethernet activity interrupt
	clr 	eaip 					; Set network interrupt priority low
	ret
Listing 10. EnableInterrupts Enables the Ethernet Activity Interrupt

Media Independent Interface (MII)

The Media Independent Interface (MII) defines I/O lines that allow the DS80C400 to communicate with the physical layer interface (PHY). Even though many PHYs have a vendor-specific command set, there are common commands that most PHYs share, defined in the IEEE Std. 802.3. Communications with a PHY can be used to query a PHY for its auto negotiation and duplex state, and to isolate and "un-isolate" PHYs (in the case of multiple PHYs) and reconfigure a PHY.
The MII on the DS80C400 is accessed through CSR registers. The following routines read and write an MII register in a given PHY.

Read MII Register

;****************************************************************************
;*
;* Function Name: ETH_ReadMII
;*
;* Description: Read MII register
;*
;* Input(s): a -> register number, b -> PHY number
;*
;* Outputs(s): r1:r0 -> contents of MII register
;*
;* Notes: MII address Register (14h):
;* 31-16 -- reserved
;* 15-11 -- PHY address
;* 10-6 -- MII register
;* 5-2 -- reserved
;* 1 -- MII write
;* 0 -- MII busy
;*
;****************************************************************************
ETH_ReadMII:
	push 	eie
	clr 	eie.5
	mov 	r7, a 			; Save register number
	; Wait until MII is not busy
eth_rmii_busy:
	mov 	a, #CSR_MII_ADDR
	acall 	ETH_ReadCSR

	mov 	a, r0
	jb 		acc.0, eth_rmii_busy

	clr 	a
	mov 	r3, a 			; Reserved - always clear
	mov 	r2, a

	mov 	a, r7 			; Restore register number
	rr 		a
	rr 		a 		; And shift to pos 10:8
	mov 	r7, a 			; Save result of shift
	anl 	a, #07h 		; Select bits 0:2
	mov 	r1, a
	mov 	a, b 			; Load PHY address
	anl 	a, #1fh
	rl 		a
	rl 		a
	rl 		a 		; shift to 7:3
	orl 	a, r1
	mov 	r1, a

	mov 	a, r7 			; Restore result of shift
	anl 	a, #0c0h 		; Select bits 7:6
	mov 	r0, a
	
	mov 	a, #CSR_MII_ADDR
	acall 	ETH_WriteCSR
	; Wait until MII is not busy
eth_rmii_busy2:
	mov 	a, #CSR_MII_ADDR
	acall 	ETH_ReadCSR

	mov 	a, r0
	jb 		acc.0, eth_rmii_busy2

	; Read MII data register
	mov 	a, #CSR_MII_DATA
	acall 	ETH_ReadCSR
	pop 	eie
	ret
Listing 11. ReadMII Reads an MII Register from a Given PHY

Write MII Register

;****************************************************************************
;*
;* Function Name: ETH_WriteMII
;*
;* Description: Write MII register
;*
;* Input(s): a -> register number, b -> PHY number, r1:r0 -> data
;*
;* Outputs(s): N/A
;*
;****************************************************************************
ETH_WriteMII:
	push 	eie
	clr 	eie.5

	push 	0 		; Save r1 and r0
	push 	1

	mov 	r7, a 		; Save register number
	; Wait until MII is not busy
eth_wmii_busy:
	mov 	a, #CSR_MII_ADDR
	acall 	ETH_ReadCSR

	mov 	a, r0
	jb 		acc.0, eth_wmii_busy

	pop 	1
	pop 	0
	
	clr 	a
	mov 	r3, a 		; Reserved - always clear
	mov 	r2, a

	; Write MII data register
	mov 	a, #CSR_MII_DATA
	acall 	ETH_WriteCSR

	mov 	a, r7 		; Restore register number
	rr 		a
	rr 		a 	; And shift to pos 0:2
	mov 	r7, a 		; Save result of shift
	anl 	a, #07h 	; Select bits 0:2
	mov 	r1, a
	mov 	a, b 		; Load PHY address
	anl 	a, #1fh
	rl 		a
	rl 		a
	rl 		a 	; shift to 7:3
	orl 	a, r1
	mov 	r1, a

	mov 	a, r7 		; Restore result of shift
	anl 	a, #0c0h 	; Select bits 7:6
	orl 	a, #2 		; Select write bit :1:
	mov 	r0, a

	mov 	a, #CSR_MII_ADDR
	acall 	ETH_WriteCSR
	pop 	eie
	ret
Listing 12. WriteMII Writes an MII Register to a Given PHY

MII Example

The following code reads the MII status register of a PHY:
	mov 	b, #0
	mov 	a, #MII_STATUS
	acall 	ETH_ReadMII


Related Parts
DS80C400 Network Microcontroller  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (85.4kB)  

© Jun 06, 2003, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 712: Jun 06, 2003
APPLICATION NOTE 712, AN712, AN 712, APP712, Appnote712, Appnote 712