APPLICATION NOTE 605

Data Pointer Decrement Feature Simplifies Copy Operation for Overlapping Memory Buffers


Abstract: Memory management can be simplified by using the data pointer decrement feature found in the Maxim high-speed microcontroller family. This application note explores the use of MOVX operations in the DS80C400, DS5250, DS89C430 and other products in this family of microcontrollers. Sample code highlights the DPTR when doing memory transfer operations.

Overview

One of the essential operations of any microcontroller is the ability to store and retrieve data to/from memory. The MOVX operation provides one facility for doing this on the 8051 architecture. Applications often require the microcontroller to copy and move blocks of data memory around within its MOVX address space. This memory transfer operation is quite simple when the source and destination address ranges do not overlap, i.e., an iterative read/write loop. When the ranges overlap, however, the process requires some intelligence to avoid overwriting (corrupting) the original data before it is transferred. This application note will offer two possible solutions for transferring data between source and destination buffers, which overlap, and explain how Dallas' data pointer decrement feature simplifies the solution.

Overlapping Memory Problem

Most generic memory copy routines do not determine whether the source and destination copy ranges overlap. Without making this assessment prior to the execution of the copy routine, bytes copied to an intended destination range that overlaps the original source range can overwrite and corrupt the original data. A simple illustration of how this might occur is given in Figure 1. As can be seen, the destination address range begins at address = 0104h, which also happens to be an address within the original source byte-array range. As alluded to earlier, the standard memcpy() routine in this situation would not generate the desired destination data array. When data integrity must be maintained for such a transfer, the memmove() operation is generally used to ensure that bytes in the source array are not overwritten when copying to a destination.

Figure 1. Problem: overlapping memory copy.
Figure 1. Problem: overlapping memory copy.

Possible Solutions

With some observation, one can see that the overwrites that occur to the source array (prior to the copy) can be avoided in a couple of ways: 1) determine the overlap and transfer first those bytes in the source buffer that overlap the desired destination buffer or 2) determine the overlap and transfer bytes from the source buffer to the destination buffer in reverse order. These two solutions are shown in Figures 2 and 3. Note that an overlap in the opposite direction (copying source array to destination lower in memory) poses no problem for the standard copy loop that transfers data in ascending address order.

Given the two visuals below (Figures 2 and 3), one should also be able to see that Solution #1 suffers additional overhead in order to calculate, store, and pass different source, destination, and length variables for multiple copy operations, whereas the second solution must do this only once.

Figure 2. Overlapping memory copy solution #1.
Figure 2. Overlapping memory copy solution #1.

Figure 3. Overlapping memory copy solution #2.
Figure 3. Overlapping memory copy solution #2.

Dallas Hardware Simplifies Solution #2

Many Dallas microcontroller products (list provided in Appendix A) implement an Increment/Decrement (IDx) bit for each available data pointer to designate whether the 'INC DPTR' instruction will increment or decrement the active data pointer. Using the data pointer decrement feature, Solution #2 is particularly easy to implement on Dallas products, allowing a linear transfer and minimizing execution time.

In order to take advantage of the data pointer decrement feature, the application code first must determine if and how the source and destination ranges overlap, a task that would be executed even if the data pointer decrement feature weren't available. When a potentially problematic source/destination buffer overlap is detected, the data pointers are placed at the end of the respective source/destination copy ranges and the IDx bits are configured to enable the data pointer decrement mode. Example code for solution #2 is provided below. Note that the DPTR toggling ('INC DPS') and increment/decrement ('INC DPTR') functions have been included in the code for the purpose of understanding only and can be removed if the respective auto-toggle and/or auto-increment/decrement bits have been set.

Example Application Code for Solution #2

;-------------------------------------------------------------
; Example memmove code which tests for overlapping src/dest
; address ranges before the copy operation. Code assumes that
; length>0, the copy is being done within a single 64kB xdata
; bank, and DPTR0 used otherwise (i.e. only DPTR0 saved).
;
; input: R6:R7 (pointer to destination)
; R4:R5 (pointer to source)
; R2:R3 (length)
; uses: R1 (src-dest pointer delta temp store)
; R0:R1 (length-1 later)
;-------------------------------------------------------------
memmove:
push dps ;save DPTR0
push dpl
push dph
;-------< DETECT PROBLEMATIC SRC/DEST BUFFER OVERLAP>---------
clr c ;
mov a, r5 ; check delta between
subb a, r7 ; src/dest pointers
mov r1, a ;
mov a, r4 ;
subb a, r6 ;
jnc domemcpy ; dest pointer <
; src pointer addr?
xch a, r1 ; NO
add a, r3 ; check delta vs.
xch a, r1 ; length
addc a, r2
jnc domemcpy ; length < delta?
xrl a, r1 ; NO
jz domemcpy ; length = delta?
;-----< DATA POINTER DECREMENT MODE / ADJUST POINTERS >-------
overlap: ; NO.
mov dps, #0C0h ; ID1,ID0=11b (dec)
mov a, r3 ;
add a, #0ffh ; add (-1) to length
mov r1, a ; prior to adding to
mov a, r2 ; original src/dest
jc lenless1 ; start pointers
dec a
lenless1:
mov r0, a ; R0:R1 = (length-1)
mov a, r5 ; src pointer
add a, r1 ; starts at the end
mov r5, a ; =src+length-1
mov a, r4
addc a, r0
mov r4, a
mov a, r7 ; dest pointer
add a, r1 ; starts at the end
mov r7, a ; =dest+length-1
mov a, r6
addc a, r0
mov r6, a
;------------------< NORMAL COPY LOOP >------------------
domemcpy:
mov a, r3
jz nomod ; inc msb if lsb<>00h
inc r2 ; for proper loop cntrl
nomod:
mov dph, r4 ; load source
mov dpl, r5
mov dph1, r6 ; load dest
mov dpl1, r7
copyloop:
movx a, @dptr ; read
inc dptr ; inc/dec src pointer
inc dps ; select dest
movx @dptr, a ; write
inc dptr ; inc/dec dest pointer
inc dps ; select src
djnz r3, copyloop
djnz r2, copyloop
pop dps
pop dph
pop dpl
ret
APPENDIX A: DATA POINTER FEATURES
HIGH-SPEED µC DATA POINTERS INCREMENT/DECREMENT SELECTION BITS AUTO-TOGGLE FEATURE AUTO-INCREMENT/DECREMENT FEATURE
DS80C310 2 No No No
DS80C320/323 2 No No No
DS8XC520/530 2 No No No
DS80C390 2 Yes Yes No
DS89C430/450 2 Yes Yes Yes



Related Parts
DS5250 High-Speed Secure Microcontroller  
DS80C390 Dual CAN High-Speed Microprocessor Samples  
DS80C400 Network Microcontroller  
DS89C430 Ultra-High-Speed Flash Microcontrollers Samples  
DS89C450 Ultra-High-Speed Flash Microcontrollers Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (54kB)  

© Apr 03, 2002, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 605: Apr 03, 2002
APPLICATION NOTE 605, AN605, AN 605, APP605, Appnote605, Appnote 605