APPLICATION NOTE 5608

Layout Guidelines with Example Layout for the MAX20021/MAX20022

By:  Jon Wallace

Abstract: This application note explains how to layout the MAX20021/MAX20022 automotive quad power-management ICs (PMICs) to maximize performance and minimize emissions. Example images of a four-layer layout are provided.

Introduction

Good PCB layout is essential, especially when using a high-frequency switching regulator such as the MAX20021 or the MAX20022. An optimized layout provides a clean output supply and saves time debugging emissions issues in the electromagnetic interference (EMI) chamber. This application note outlines some critical areas of the circuit where optimizing the layout provides the most benefit.

General Layout Guidelines

  • Minimize the trace loop area for the input capacitor (C5–C8), inductor (L1–L4), and output capacitor (C1–C4) for each output.
  • Place the VA output capacitor (C9) as close as possible to pin 26 (VA) and pin 24 (GND) without any vias between the pins and the capacitor. This is the analog supply for the IC; any inductance on this connection increases noise on the analog supply, which can, in turn, increase jitter on the LX[1:4] outputs.
  • A shorter trace is better than a wider trace.

Optimizing the AC-DC Current Path

To minimize emissions, the layout of the passive components of the MAX20021/MAX20022 is critical. The paths where there are current-step changes are considered the AC current paths. These AC current paths can be seen by eliminating the paths where current flows on both the ON and OFF parts of the switching cycle. The paths that have current flowing through them during the ON and OFF cycles are considered the DC current paths.

AC Current Path

The MAX20021 synchronous DC-DC converter has three passive components (C1, C5, L1) for each output directly in the switching current path. These three components have the most impact on emissions and device performance. Figures 1 and 2 show the switching current path during the ON and OFF cycles for OUT1; Figure 3 shows the difference between these two current paths where the highest di/dt occurs. Optimizing the layout of component C5 is the highest priority, followed by optimizing for L1 and C1.
Figure 1. OUT1 current flow with PMOS ON.
Figure 1. OUT1 current flow with PMOS ON.
Figure 2. OUT1 current flow with DMOS ON.
Figure 2. OUT1 current flow with DMOS ON.
Figure 3. OUT1 AC current flow showing difference.
Figure 3. OUT1 AC current flow showing difference.

Spread Spectrum

When a good layout is not enough to pass customer-required emissions tests, the MAX20021/MAX20022 can be ordered with spread-spectrum clock enabled. The spread-spectrum-enabled device can reduce the FM-band noise by as much as 12dB over the standard version. See the data sheet for information on how to order the spread-spectrum-enabled versions.

Example: Four-Layer PCB Layout

Figures 4 through 7 show an example of a four-layer layout using the guidelines above.
Figure 4. Example of a four-layer PCB layout—top layer.
Figure 4. Example of a four-layer PCB layout—top layer.
Figure 5. Example of a four-layer PCB layout—PGND layer.
Figure 5. Example of a four-layer PCB layout—PGND layer.
Figure 6. Example of a four-layer PCB layout—VSUP layer.
Figure 6. Example of a four-layer PCB layout—VSUP layer.
Figure 7. Example of a four-layer PCB layout—bottom layer.
Figure 7. Example of a four-layer PCB layout—bottom layer.

Conclusion

Proper layout of the critical passive components for the switching regulators of the MAX20021/MAX20022 (Figure 8) helps to minimize noise and emissions at the source. This saves valuable time and effort during the qualification phase of the project.
Table 1. Component List
Designation Qty Description
C1–C4 4 10µF, 10V ±10% X7R 1206 ceramic capacitor
C5–C8 4 2.2µF, 10V ±10% X7R 0603 ceramic capacitor
C9 1 470nF, 10V ±10% X7R 0402 ceramic capacitor
R1–R4 1 20kΩ ±1% 0402 resistors
L1–L4 4 MTD2520–CN1R5M 1.5µH inductor
U1 1 MAX20021/MAX20022 quad, low-voltage DC-DC converters
Figure 8. Schematic diagram used for PCB layout.
Figure 8. Schematic diagram used for PCB layout.


Related Parts
MAX20021 Automotive Quad, Low-Voltage Step-Down DC-DC Converters Samples  
MAX20022 Automotive Quad, Low-Voltage Step-Down DC-DC Converters Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (158kB)  

© Apr 12, 2013, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 5608: Apr 12, 2013
APPLICATION NOTE 5608, AN5608, AN 5608, APP5608, Appnote5608, Appnote 5608