APPLICATION NOTE 5490

Level Shifting to Control Power MOSFETs


Abstract: Some power architectures require the power supply sequencer (or system manager) to control downstream power MOSFETs to allow power to flow into branch circuits. This application note explains how system power sequencing and level shifting can be accomplished using a low-voltage system manager.

Some power architectures require that the power-supply sequencer (or system manager) control downstream power MOSFETs to allow power to flow into branch circuits. If the incoming power-supply voltage is at least 5V higher than the power-supply output voltage, a power MOSFET can be placed on the output of the power supply with the addition of some level-shifting circuitry. In this case, a low-voltage system manager like the MAX34440/MAX34441 series can be used to enable and disable the power MOSFET.
Figure 1. Level-shifting circuitry.
Figure 1. Level-shifting circuitry.
In the application shown, the system manager is configured with active-low, open-drain outputs. Even if the system manager is not powered up when power is applied to the power supply, the power MOSFET will not be enabled (since the 2N7002 will be enabled). This in turn disables the power MOSFET.
Most power supplies contain an undervoltage lockout (UVLO), which prevents them from providing power until the input voltage is above a minimum level. The minimum UVLO level needs to be high enough to ensure that the 2N7002 is enabled before the power supply starts delivering power.
When the system manager needs to enable the power MOSFET, the open-drain output is pulled low. This disables the 2N7002, allowing the power MOSFET to turn on. The resistor and capacitor tied to the gate of the power MOSFET can be adjusted to slow the turn-on time of the power MOSFET.
As soon as the system manager releases the open-drain output and allows it to go high impedance, the resistor-divider tied from the power-supply input will immediately enable the 2N7002. This immediately shuts off the power MOSFET.


Related Parts
MAX34440 PMBus 6-Channel Power-Supply Manager Samples  
MAX34441 PMBus 5-Channel Power-Supply Manager and Intelligent Fan Controller Samples  
MAX34460 PMBus 12-Channel Voltage Monitor and Sequencer Samples  
MAX34461 PMBus 16-Channel Voltage Monitor and Sequencer  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (55kB)  

© Oct 25, 2012, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 5490: Oct 25, 2012
APPLICATION NOTE 5490, AN5490, AN 5490, APP5490, Appnote5490, Appnote 5490