TUTORIAL 4221

How to Optimize Avalanche Photodiode (APD) Bias Range Using a DS1841 Logarithmic Resistor


Abstract: This article describes how three external resistors on the DS1841 logarithmic resistor are used to adjust the output range of an APD bias circuit. A spreadsheet is supplied that makes the adjustment process easy.

APD Bias Circuit

The DS1841 temperature-controlled, NV, I²C, logarithmic resistor contains one 7-bit logarithmic variable resistor. Used in conjunction with a step-up DC-DC converter, the DS1841 adjusts the bias voltage applied to an avalanche photodiode (APD). Three external resistors (RSER, RTOP, and RPAR) are used to adjust the output range (Figure 1).

Figure 1. APD bias circuit using the DS1841 and a step-up DC-DC, here the MAX5026 or MAX1523.
Figure 1. APD bias circuit using the DS1841 and a step-up DC-DC, here the MAX5026 or MAX1523.

Adjusting the APD Bias Range

A spreadsheet, DS1841 APD Bias Range Adjustment (xls), makes it easy to adjust the APD bias range. The spreadsheet has four input variables: RTOP, RSER, RPAR, and VFB. After inputting these resistor values, the spreadsheet then calculates four outputs: VAPD (max), VAPD (min), STEP (max), STEP (avg). It also generates two graphs: APD Bias vs. DAC Code, Volts Per Step vs. DAC Code. The interface in Figure 2 shows the four variables and the graphics generated from the values input there. Table 1 defines the terms used in the spreadsheet.

Figure 2. The spreadsheet interface with the four variables for data input, which appear at the top left.
Figure 2. The spreadsheet interface with the four variables for data input, which appear at the top left.

Table 1. Variable Definitions for APD Bias Range Adjustment with the DS1841
VFB The voltage present at the feedback node of the DC-DC converter.
VAPD (max) The maximum voltage to which the APD bias can be set under worst-case conditions.
VAPD (min) The minimum voltage to which the APD bias can be set under worst-case conditions.
STEP (max) The maximum calculated voltage step that can occur between two adjacent DAC codes.
STEP (avg) The average voltage step size that occurs across the full range.
VSTEP +20% The voltage step size when the variable resistor is at the maximum of the process range (+20%).
VSTEP -20% The voltage step size when the variable resistor is at the minimum of the process range (-20%).
VAPD +20% The APD bias voltage when the variable resistor is at the maximum of the process range (+20%).
VAPD -20% The APD bias voltage when the variable resistor is at the minimum of the process range (-20%).


Related Parts
DS1841 Temperature-Controlled, NV, I²C, Logarithmic Resistor Samples  
MAX1523 Simple SOT23 Boost Controllers Samples  
MAX5026 500kHz, 36V Output, SOT23, PWM Step-Up DC-DC Converters Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (50kB)  

© Jun 10, 2008, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 4221: Jun 10, 2008
TUTORIAL 4221, AN4221, AN 4221, APP4221, Appnote4221, Appnote 4221