APPLICATION NOTE 4020

Working with MAX9217/MAX9218/MAX9247/MAX9248/MAX9250 Evaluation Boards


Abstract: This application note describes how to prepare and use the evaluation boards for the MAX9217/MAX9247 serializers and the MAX9218/MAX9248/MAX9250 deserializers.

General Description

The MAX9217/MAX9218/MAX9247/MAX9248/MAX9250 evaluation boards (EV kits) are available for customer evaluation. These EV kits consist of two sections: The right half contains one of the single-channel serializer components (MAX9217 or MAX9247) and the left half contains one of the single-channel deserializer components (MAX9218, MAX9248, or MAX9250).

The EV kits require three clock signals, which can be supplied by the same source. The serializer works with two clock signals: PCLK and DE_IN, where DE_IN is normally divided by a factor of 16 or 32 of the PCLK. The deserializer section needs a REFCLK, which can come from the same source, or it can be provided by an independent local oscillator that is within 2% accuracy of the PCLK.

Steps to Prepare the EV kits

  1. Configure the EV kits (Figures 1 and 2) by setting the jumpers according to the configuration tables below (Tables 1–4).
  2. Apply power to the EV kit. A single 3.3V DC power supply is sufficient to support each section of the EV board; however, if component characterization is desired, it is recommended to supply separate sources for each of the component's power-supply pins (Table 2).
  3. Connect the PCLK, DE_IN, and REFCLK clock signals to the EV kit, as explained in Step 2 (also see examples below). An Agilent™ 8133A pulse generator is a good choice for providing all three clock signals from one source.
  4. Apply the input data to the input pins of the serializer (located at the right-half section of the EV kit) and check the deserializer output pins using a logic analyzer and a multimeter. A liquid-crystal display (LCD) can be used if the input to the serializer is a video signal, such as UNIGRAF's VTG-4116 video test patterns.
  5. Special attention should be given to jumper JP13 on the serializer board. By connecting this jumper to DVCC, the ground pins of JP17–JP21 (10 x 2 headers) are connected to 3.3V, and a fixed data pattern can be applied to the data inputs of the MAX9217/MAX9247 serializers. When external data patterns are applied, this jumper should be connected to ground.

Pseudorandom-Bit-Sequence (PRBS) Data Generation by the MAX9217/MAX9247

The MAX9217/MAX9247 can generate PRBS data for eye-diagram measurements by using the following configuration:
  1. Connect the active-low PWRDWN pin to ground.
  2. Connect both MOD0 and MOD1 pins (for the MAX9247, these pins are called I.C. and PRE) to a negative 2.5V DC voltage. The serializer eye diagram can be observed by connecting a differential probe to pins 2 and 3 of JP14/JP24 (4-pin, single-row headers) on the serializer board. The deserializer eye diagram is available on pins 2 and 3 of JP5/JP6 (4-pin, single-row headers) of the deserializer board.
Figure 1. Circuit schematic for the MAX9217 EV kit.
More detailed image
(PDF, 121kB)
Figure 1. Circuit schematic for the MAX9217 EV kit.

Figure 2. Circuit schematic for the MAX9218 EV kit.
More detailed image
(PDF, 128kB)
Figure 2. Circuit schematic for the MAX9218 EV kit.

Quick Functionality Check

The MAX9217/MAX9247/MAX9218/MAX9248/MAX9250 EV kits have headers for connection to a logic analyzer, a graphics generator, or a display. A pattern generator (which can be a part of the logic-analyzer system) such as the HP16500C system generates parallel test words that are applied to the serializer input. The test words are serialized and sent over the LVDS link to the deserializer. The logic analyzer then reads the deserialized test words and checks for errors against the reference or test words that were sent across the serializer and deserializer. The EV kit can also be connected to a graphics generator and LCD for a visual test of the serial link.

The basic function of the serial link can be checked without a logic analyzer, a graphics generator, or a display. For a quick check of the setup, the serializer input-logic levels can be set with jumpers, and the corresponding bits/voltages can be read with a voltmeter at the deserializer output. To configure the EV kit for a quick functionality check, refer to the MAX9217/MAX9218 EV kit schematics for the name and location of associated jumpers and components. Note that when a shunt is installed across a jumper pair, the chip pin is pulled to a logic-high level. If no shunt is installed across any jumper pair, the chip pin is pulled low.
  1. Configure jumpers for a quick functionality check of the EV kit (Table 1).

    Table 1. Jumper Settings for a Quick Functionality Check
    Part Pin Name Jumper Jumper Function Jumper Setting for Quick Check
    MAX9218,
    MAX9248,
    MAX9250
    R/F JP1 Selects rising- or falling-edge output strobe Low (falling edge)
    RNG1 JP4 Selects PLL operating range High-frequency range (refer to the data sheet)
    RNG0 JP7 Selects PLL operating range High-frequency range
    Active-low PWRDWN JP11 Selects chip power-up or power-down High (power-up)
    OUTEN (MAX9218/MAX9250), SS (MAX9248) JP12 Selects output enable or output disable High (output enabled for MAX9218/MAX9250), 4% spread-spectrum mode (MAX9248)
    MAX9217, MAX9247 (none) JP13 Buses logic high (DVCC) for hardwired inputs DVCC
    MOD1 (MAX9217), PRE (MAX9247) JP15 Selects output-modulation level Low (modulation off), preemphasis is disabled for MAX9247
    MOD0 (MAX9217), I.C. (MAX9247) JP16 Selects output-modulation level Low (modulation off), internally connected pin for MAX9247
    Active-low PWRDWN JP18 pin 15 to pin 16 Selects chip power-up or power-down High (power-up)
    RNG0 JP22 Selects PLL operating range High-frequency range (refer to the data sheet)
    RNG1 JP23 Selects PLL operating range High-frequency range

  2. Connect power supplies to the EV kit (Table 2).



    Table 2. Power-Supply Connections for a Quick Functionality Check
    Part Pin Name EV Board Connection Voltage
    MAX9217,
    MAX9247
    VCCIN IVCC +3.3V
    VCCPLL PVCC +3.3V
    VCCLVDS LVCC +3.3V
    VCC DVCC +3.3V
    (none) VNEG Ground
    PLL GND, LVDS GND, GND GND Ground
    MAX9218,
    MAX9248,
    MAX9250
    VCCPLL PVCC +3.3V
    VCCLVDS LVCC +3.3V
    VCC DVCC +3.3V
    VCCO OVCC +3.3V
    (none) VTEST Open
    PLL GND, LVDS GND, VCCOGND, GND GND Ground

  3. Connect all clock and control signals (Table 3).

    Table 3. Clock and Control Signals for Quick Functionality Check
    Chip Chip Pin Name EV Board Connection Signal
    MAX9217,
    MAX9247
    PCLK_IN J18 PCLK (SMA connector) 32MHz
    DE_IN JP18 Pin 13 1MHz
    RGB_IN and CNTL_IN JP18, JP19, JP20, JP21 Open
    MAX9218,
    MAX9248,
    MAX9250
    REFCLK J8 REF (SMA connector) 32MHz

  4. Once Steps 1–3 have been completed, the following signals can be observed at the outputs of the MAX9218/MAX9248/MAX9250 deserializers (Table 4).

    Table 4. MAX9218/MAX9248/MAX9250 Output States for a Quick Functionality Check
    Pin Name EV Board Connection Signal
    RGB_OUT,
    CNTL_OUT
    JP3 and JP9 Low
    Active-low LOCK JP9 Pin 23 Low
    PCLK_OUT JP9 Pin 25 32MHz
    DE_OUT JP9 Pin 21 1MHz

  5. The MAX9217/MAX9247 RGB_IN and CNTL_IN inputs have internal pull-down resistors. When an input is left open, the serializer automatically reads a logic low. Connect some inputs to 3.3V at the JP11, JP12, JP13, and JP14 headers. This can be done by setting JP13 to the DVCC position and using shunts between opposite pins of these 2 x 10 headers. The corresponding outputs on the MAX9218/MAX9248/MAX9250 deserializer should then change to a high level. For example, if RGB_IN0 (JP14 pin 1) is connected to 3.3V, then RGB_OUT0 (JP7 pin 27) should go high.
  6. Use an oscilloscope to view the serial signal by connecting a differential FET probe across the LVDS signal lines at the MAX9217/MAX9247 serializer outputs (JP17/JP18) or the MAX9218/MAX9248/MAX9250 deserializer inputs (JP4/JP6).

Notes

  1. RNG0 and RNG1 have internal pull-down resistors on the MAX9217/MAX9247 and MAX9218/MAX9248/MAX9250. To activate a logic low, these pins can be left floating.
  2. DE_IN must be switching for the MAX9217/MAX9218 chipset to work. Typically the Data Enable pin (ENAB) from a graphics controller is connected to DE_IN on the MAX9217/MAX9247 and is recovered from DE_OUT on the MAX9218/MAX9248/MAX9250. DE_IN must transition at least once every 4,194,304 cycles of PCLK_IN.
  3. The clock inputs have pads for 50Ω termination resistors to ground. The EV kit is shipped without these resistors—they are not installed. Clean transitions are especially important on the PCLK, DE_IN, and REF inputs. Install 50Ω input-termination resistors if needed to reduce reflections. Use 1% or better tolerance resistors for close matching of the inputs.
  4. Series-coupling capacitors (C28/C29 on the Rx side and C55/C58 on the Tx side) are not required for link operation. For direct-coupled operation, short the series capacitor pads with a zero ohm resistor. EV kits are shipped with 0.1µF series capacitors installed.
  5. For termination of the LVDS signal, use either the 100Ω differential (R3) termination or a 100Ω thevenin-equivalent network (R1/R2/R5/R4). Do not use both at the same time. Installing both terminations will generate large reflections (see Figure 3).
  6. Resistors R20-R46 shown on the MAX9217 schematic are only for the internal IC characterization and are not populated on the EV kit.
  7. Capacitors C1-C15 and C27-C41 shown on the MAX9218 are only for the internal IC characterization and are not populated on the EV kit. Similarly, resistors R1-R3, R6-R7, R10 and R11 are not populated on the EV kit.
Figure 3. LVDS termination options. Use only one of the above termination options; installing both terminations will generate large reflections.
Figure 3. LVDS termination options. Use only one of the above termination options; installing both terminations will generate large reflections.

Table 5. Color and Control Bit Assignments
(The following table shows the recommended video signal assignments for the parallel interfaces of the MAX9217/MAX9247 serializers and the MAX9218/MAX9248/MAX9250 deserializers. R0, G0, and B0 are the LSB.)
Graphics
Controller
Output
MAX9217 Input MAX9218 Output LCD Input
R0 RGB_IN0 RGB_OUT0 R0
R1 RGB_IN1 RGB_OUT1 R1
R2 RGB_IN2 RGB_OUT2 R2
R3 RGB_IN3 RGB_OUT3 R3
R4 RGB_IN4 RGB_OUT4 R4
R5 RGB_IN5 RGB_OUT5 R5
G0 RGB_IN6 RGB_OUT6 G0
G1 RGB_IN7 RGB_OUT7 G1
G2 RGB_IN8 RGB_OUT8 G2
G3 RGB_IN9 RGB_OUT9 G3
G4 RGB_IN10 RGB_OUT10 G4
G5 RGB_IN11 RGB_OUT11 G5
B0 RGB_IN12 RGB_OUT12 B0
B1 RGB_IN13 RGB_OUT13 B1
B2 RGB_IN14 RGB_OUT14 B2
B3 RGB_IN15 RGB_OUT15 B3
B4 RGB_IN16 RGB_OUT16 B4
B5 RGB_IN17 RGB_OUT17 B5
HSYNC CNTL_IN0 CNTL_OUT0 HSYNC
VSYNC CNTL_IN1 CNTL_OUT1 VSYNC
Not assigned CNTL_IN2 CNTL_OUT2 Not assigned
Not assigned CNTL_IN3 CNTL_OUT3 Not assigned
Not assigned CNTL_IN4 CNTL_OUT4 Not assigned
Not assigned CNTL_IN5 CNTL_OUT5 Not assigned
Not assigned CNTL_IN6 CNTL_OUT6 Not assigned
Not assigned CNTL_IN7 CNTL_OUT7 Not assigned
Not assigned CNTL_IN8 CNTL_OUT8 Not assigned
Display Enable DE_IN DE_OUT Display Enable



Agilent is a registered trademark and registered service mark of Agilent Technologies, Inc.



Related Parts
MAX9217 27-Bit, 3MHz-to-35MHz DC-Balanced LVDS Serializer Samples  
MAX9218 27-Bit, 7MHz-to-35MHz DC-Balanced LVDS Deserializer Samples  
MAX9247 27-Bit, 2.5MHz-to-42MHz DC-Balanced LVDS Serializer Samples  
MAX9248 27-Bit, 5MHz to 42MHz DC-Balanced LVDS Deserializers Samples  
MAX9250 27-Bit, 5MHz to 42MHz DC-Balanced LVDS Deserializers Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (72kB)  

© Jun 29, 2007, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 4020: Jun 29, 2007
APPLICATION NOTE 4020, AN4020, AN 4020, APP4020, Appnote4020, Appnote 4020