APPLICATION NOTE 3815

Radiated Power and Field Strength from UHF ISM Transmitters


Abstract: Short-range radios that operate at the Industrial, Scientific, and Medical (ISM) frequencies from 260MHz to 470MHz are widely used for remote keyless entry (RKE), home security, and remote control. A critical performance measurement for the radio transmitter is the power that it radiates from the antenna. This power must be high enough to make the link between the transmitter and receiver reliable, yet it must not be so high that it exceeds the radiation limits established in Part 15.231 of the FCC Regulations. This application note discusses the relationship between FCC field-strength requirements in the 260MHz to 470MHz frequency range and the radiated power and typical quantities measured on a test receiver. Tables will illustrate the values that a designer can expect to obtain in field tests.

Introduction

Very often the antennas in the transmitters for applications in the 260MHz to 470MHz Industrial, Scientific, and Medical (ISM) frequency band are so small that they radiate only a small fraction of the power available from the transmitter's power amplifier. This makes measuring the radiated power a very important task. This measurement is complicated because the radiation limits in Part 15.231 of the FCC Regulations are expressed as field strength (volts/meter) at a distance of 3 meters from the transmitter. In addition, the receive antenna, its placement, and the units used on the measuring receiver all affect the measurement of radiated power.

This application note will explain both the relationship between radiated power to field strength and the units used in the measurement receiver. Tables will illustrate the relationship between FCC field-strength requirements in the 260MHz to 470MHz frequency range and the radiated power. The typical quantities measured on a test receiver will be shown. By understanding this relationship and knowing some conversion factors, the user can determine whether measurements made at a test receiver indicate that the transmitter is close to its radiated power goal.

The Relationship Between Field Strength and Radiated Power

Power transmitted from an antenna spreads out in a sphere. If the antenna is directional, the variation of its power with direction is given by its gain, G(Θ, Φ). At any point on the surface of a sphere with radius, R, the power density (PD) in watts/square meter is given by Equation 1.

Equation 1

This expression is simply the power radiated by the transmitter, divided by the surface area of a sphere with radius, R. The gain symbol, GT, has no angular variation. This is because most of the antennas used in the 260MHz to 470MHz ISM frequency band are very small compared to the operating wavelength and, therefore, have patterns that do not vary sharply with direction. The gain is often quite small because the antennas are very inefficient radiators. For this reason, PT and GT are kept together and taken to mean the Effective Isotropic Radiated Power (EIRP) of the transmitter and antenna combination. Consequently, EIRP is the power that would be radiated from an ideal omnidirectional, i.e., isotropic, antenna.

The power density at a distance, R, from the transmitter can also be expressed as the square of the field strength, E, of the radiated signal at R, divided by the impedance of free space, designated in Equation 2 as η0. The value of η0 is 120πΩ, or about 377Ω.

Equation 2

Combining these two equations results in a simple conversion of the EIRP, which is PTGT to field strength, E, in volts/meter.

Equation 3

Alternately, Equation 3 can be rearranged to express EIRP in terms of the field strength.

Equation 4

At the 3-meter distance of the FCC requirements, the relationship is even simpler.

Equation 5

As an example, the FCC limit on average field strength at 315MHz is about 6mV/meter. Using Equation 5, the limit on average radiated power is 10.8µW, or -19.7dBm.

The conversion from field strength to EIRP is further complicated because some documents express field strength in a logarithmic, or dB, format. In the example above, the field strength of 6mV/meter could also be expressed as 15.6dBmV/meter or 75.6dBµV/meter.

Finally, the FCC radiation limits change with frequency over the 260MHz to 470MHz band. This change means that, at every frequency, one needs to calculate the field strength per the FCC requirement formula, then convert from one measurement unit to the other. In Part 15.231 the FCC sets the field-strength limit at 3750µV/meter at 260MHz, and allows a linear increase to 12500µV/meter at 470MHz.

Table 1 combines Equation 1 through Equation 5 with the FCC formula for average field-strength limits. The data in Table 1 thus provide a quick conversion at 5MHz frequency intervals for the multiple ways of characterizing the radiation strength. The gain of the transmitting antenna is assumed to be 0dB.

Table 1. EIRP vs. FCC Part 15.231 Average Field-Strength Limits
Frequency MHz Field Strength µV/meter Field Strength dBµV/meter EIRP mW EIRP dBm
260 3750 71.5 0.004 -23.7
265 3958 72.0 0.005 -23.3
270 4167 72.4 0.005 -22.8
275 4375 72.8 0.006 -22.4
280 4583 73.2 0.006 -22.0
285 4792 73.6 0.007 -21.6
290 5000 74.0 0.007 -21.1
295 5208 74.3 0.008 -20.9
300 5417 74.7 0.009 -20.6
305 5625 75.0 0.009 -20.2
310 5833 75.3 0.010 -19.9
315 6042 75.6 0.011 -19.6
320 6250 75.9 0.012 -19.3
325 6458 76.2 0.013 -19.0
330 6667 76.5 0.013 -18.8
335 6875 76.7 0.014 -18.5
340 7083 77.0 0.015 -18.2
345 7292 77.3 0.016 -18.0
350 7500 77.5 0.017 -17.7
355 7708 77.7 0.018 -17.5
360 7917 78.0 0.019 -17.3
365 8125 78.2 0.020 -17.0
370 8333 78.4 0.021 -16.8
375 8542 78.6 0.022 -16.6
380 8750 78.8 0.023 -16.4
385 8958 79.0 0.024 -16.2
390 9167 79.2 0.025 -16.0
395 9375 79.4 0.026 -15.8
400 9583 79.6 0.028 -15.6
405 9792 79.8 0.029 -15.4
410 10000 80.0 0.030 -15.2
415 10208 80.2 0.031 -15.0
420 10417 80.4 0.033 -14.9
425 10625 80.5 0.034 -14.7
430 10833 80.7 0.035 -14.5
435 11042 80.9 0.037 -14.4
440 11250 81.0 0.038 -14.2
445 11458 81.2 0.039 -14.0
450 11667 81.3 0.041 -13.9
455 11875 81.5 0.042 -13.7
460 12083 81.6 0.044 -13.6
465 12292 81.8 0.045 -13.4
470 12500 81.9 0.047 -13.3

The Relationship Between Measured Receiver Power and Radiated Power

If one restricts the units of measurement to received power and radiated power, then the relationship between received to transmitted power is well known. It is the basis for space-loss calculations in communication systems.

Starting with the power density at a distance, R (Equation 1), the power received by an antenna at this distance is simply the power density multiplied by the effective area of the receive antenna. The effective area of an antenna is defined by Equation 6.

Equation 6

The quantity, λ, is the wavelength of the transmission. Multiplying the density in Equation 1 by the effective area of the receive antenna leads to the familiar free-space-loss equation.

Equation 7

Equation 7 says that if the receive antenna gain is near unity (which is the case for a small antenna like a quarter-wave stub), the power loss at 3 meters for a transmission at about 300MHz (corresponding to a 1-meter wavelength) is approximately (1/12π)², or 31.5dB for a receiving antenna with unity gain. Although this value will probably vary from 25dB to 35dB, depending on the gain of the receiving antenna, this is a good first check of the transmitter, antennas, and test setup. If, for example, one expects an RKE transmitter circuit board to radiate -20dBm of power, then one should see somewhat less than -50dBm of power on a spectrum analyzer connected to a receive antenna with approximately unity gain, placed 3 meters away.

The Relationship Between Measured Receiver Voltage and Radiated Power

In many measurements intended to demonstrate compliance with FCC regulations, the receiver measures the RF voltage at the measurement antenna rather than the power. This happens because the FCC wants field-strength measurements, not EIRP. Because the units of field strength are volts/meter (or mV/meter or µV/meter), converting a voltage measurement to volts/meter through a calibration constant is intuitively easier.

Receive antennas manufactured primarily for measuring electromagnetic compliance have a calibration constant in units of 1/(meters). (We will discuss the meaning and derivation of this calibration constant below.) It is, thus, important that we show how the voltage measurement relates to the EIRP. When the receiver picks up the power from the antenna, the power becomes a voltage across a load resistor, Z0, which is usually 50Ω. Relating the receive voltage to the receive power by Equation 8,

Equation 8

and substituting this into Equation 7, yields an expression (Equation 9) for the received voltage in terms of the EIRP.

Equation 9

The Relationship Between Measured Receiver Voltage and Field Strength

Relating the received power, and ultimately the received voltage, to field strength can be done by using the approach shown in Equations 6 and 7. The power density is multiplied by the effective area of the receive antenna. The only difference in Equation 10 is that the power density is now expressed in terms of the field strength, E, as in Equation 2.

Equation 10

Remembering that PR is related to the received voltage by Equation 8 leads to Equation 11, which links VR to E.

Equation 11

Taking the square root of both sides shows that the received voltage is just a coefficient times the field strength. Given that most receivers have Z0 = 50Ω and that η0 = 120πΩ, the equation reduces to the simple result in Equation 12.

Equation 12

The coefficient linking the field strength, E, to the receive voltage, VR, is usually given as the ratio of E to VR. This is because VR is the measured quantity and E is the quantity that is compared to the FCC requirements. Manufacturers of antennas used for field-strength measurements list this coefficient, called the Antenna Factor (AF), in their data sheets as a function of frequency.

In terms of the variables in Equation 12, the antenna factor is given below.

Equation 13

The units in Equation 13 are either in (meters)-1 or in a dB ratio given by 20 log10 [volts/meter)/volts]. The antenna gain is expressed in terms of the power gain, so a 6dB antenna gain is a factor of 4, and a 10dB antenna gain is a factor of 10, etc. If the wavelength is 1 meter (300MHz frequency) and the antenna gain is 6dB, then the AF in Equation 13 is 4.87 (meters)-1, which would be 13.6dB (meters)-1.

One of the most commonly used receiving antennas for field-strength measurements is a Log-Periodic Antenna (LPA) with a gain that is independent of frequency over its intended measurement range. This means that its AF increases linearly with frequency. A typical LPA, the TDK RF Solutions Model PLP-3003, has an AF of 14.2dB at 300MHz, or 5.1 meters-1. Its AF vs. frequency is shown in Figure 1. Following Equation 13, the gain of this antenna is 5.6dB at 300MHz.

Figure 1. Antenna Factor (AF) vs. frequency of a typical measurement antenna.
Figure 1. Antenna Factor (AF) vs. frequency of a typical measurement antenna.

If we apply the information from Equation 13 and Figure 1 to the FCC average field-strength limit of 5417µV/meter at 300MHz, we would expect to see 1056µV measured at a 50Ω input receiver. Expressing this in dB, the 74.7dBµV/m field strength in the FCC limits would appear as 60.5dBµV in the receiver, which corresponds to -46.5dBm of power across a 50Ω load. This result is consistent with the earlier power-loss estimate. (See above where we determine that a -20dBm EIRP signal at the source would be received at about -50dBm in a receiver.)

Voltage and Power at the Measurement Receiver

Table 2 shows the voltage that would be measured with an antenna and a 50Ω receiver in compliance with the FCC field-strength limits. The AF used in Table 2 comes from the specifications for the Log Periodic antenna in Figure 1. Table 3 shows the power that would be measured with the same equipment. Table 3 uses the effective radiated power from a transmitter and antenna that corresponds to the field-strength limits, then applies the space loss and receive antenna gain to determine the power across a 50Ω load. The results in both tables are mutually consistent. Consequently, these tables give designers and users of short-range UHF transmitters a set of reference numbers to help determine whether they are meeting the FCC requirements and are radiating the needed power.

Practical Measurement Considerations

The tables in this application note give approximate values for measured power and voltage as a function of specifications such as field strength and EIRP. These values will vary when different measurement antennas are used. There are also several correction factors that one needs to make in the course of a measurement. Cable losses and mismatch losses must be taken into account, and they are frequency dependent. The measurement environment, especially the reflection from the ground or floor, can make a significant difference (as much as 6dB) in the measured receiver voltage. The ground reflection needs to be calibrated by using another reference antenna, usually a dipole. The polarization of the radiating antenna needs to matched as best as possible with the polarization of the measurement antenna. The directional pattern of the radiating device needs to be considered, even if the radiating antenna is electrically small (under 1/6 of a wavelength), because the package, test mount, and coaxial cable ground shields can introduce directional variation.

The field-strength numbers in these tables refer to the limits on the average power permitted by the FCC. Radiating a peak power level up to 20dB more than the average power limits is permitted, provided that the duration of the transmissions and the duty cycle obey some restrictions. Consequently, one needs to consider power levels that are significantly higher than those found in these tables. Because the measured values follow the field-strength limits dB for dB, adjusting the expected measurement level to ensure proper device function is not difficult. If, for instance, a product has a duty-cycle profile that permits a peak field strength at 315MHz that is 10dB higher than the FCC average field strength, then the peak field strength can now be 19.1µV/meter, or 85.6dBµV/meter. A glance at Table 2 and Table 3 indicates that the expected measured voltage and power should be in the 71dBµV and -36dBm range.

Once all these effects are measured and accommodated, then one can use the tables presented here to determine whether the transmitter is performing as designed.

Table 2. Measured Receiver Voltage as a Function of FCC Field-Strength Limits
Frequency MHz Field Strength µV/meter Field Strength dBµV/meter Meas. Antenna Gain Meas. Antenna Gain, dB Meas. Antenna Factor,
1/meter
Meas. Antenna Factor, dB(1/m) Meas. Recv. Voltage, µV Meas. Recv. Voltage, dBµV
260 3750 71.5 3.6 5.6 4.4 13.0 844 58.5
265 3958 72.0 3.6 5.6 4.5 13.1 874 58.8
270 4167 72.4 3.6 5.6 4.6 13.3 903 59.1
275 4375 72.8 3.6 5.6 4.7 13.4 931 59.4
280 4583 73.2 3.6 5.6 4.8 13.6 958 59.6
285 4792 73.6 3.6 5.6 4.9 13.8 984 5939
290 5000 74.0 3.6 5.6 5.0 13.9 1009 60.1
295 5208 74.3 3.6 5.6 5.0 14.1 1033 60.3
300 5417 74.7 3.6 5.6 5.1 14.2 1056 60.5
305 5625 75.0 3.6 5.6 5.2 14.3 1079 60.7
310 5833 75.3 3.6 5.6 5.3 14.5 1101 60.8
315 6042 75.6 3.6 5.6 5.4 14.6 1122 61.0
320 6250 75.9 3.6 5.6 5.5 14.8 1143 61.2
325 6458 76.2 3.6 5.6 5.6 14.9 1163 61.3
330 6667 76.5 3.6 5.6 5.6 15.0 1182 61.5
335 6875 7637 3.6 5.6 5.7 15.2 1201 61.6
340 7083 77.0 3.6 5.6 5.8 15.3 1219 61.7
345 7292 77.3 3.6 5.6 5.9 15.4 1236 61.8
350 7500 77.5 3.6 5.6 6.0 15.5 1254 62.0
355 7708 77.7 3.6 5.6 6.1 15.7 1270 62.1
360 7917 78.0 3.6 5.6 6.2 15.8 1286 62.2
365 8125 78.2 3.6 5.6 6.2 15.9 1302 62.3
370 8333 78.4 3.6 5.6 6.3 16.0 1318 62.4
375 8542 78.6 3.6 5.6 6.4 16.1 1333 62.5
380 8750 78.8 3.6 5.6 6.5 16.3 1347 62.6
385 8958 79.0 3.6 5.6 6.6 16.4 1361 62.7
390 9167 79.2 3.6 5.6 6.7 16.5 1378 62.8
395 9375 79.4 3.6 5.6 6.8 16.6 1388 62.9
400 9583 79.6 3.6 5.6 6.8 16.7 1402 62.9
405 9792 79.8 3.6 5.6 6.9 16.8 1414 63.0
410 10000 80.0 3.6 5.6 7.0 16.9 1427 63.1
415 10208 80.2 3.6 5.6 7.1 17.0 1439 63.2
420 10417 80.4 3.6 5.6 7.2 17.1 1451 63.2
425 10625 80.5 3.6 5.6 7.3 17.2 1463 63.3
430 10833 80.7 3.6 5.6 7.4 17.3 1474 63.4
435 11042 80.9 3.6 5.6 7.4 17.4 1485 63.4
440 11250 81.0 3.6 5.6 7.5 17.5 1496 63.5
445 11458 81.2 3.6 5.6 7.6 17.6 1506 63.6
450 11667 81.3 3.6 5.6 7.7 17.7 1517 63.6
455 11875 81.5 3.6 5.6 7.8 17.8 1527 63.7
460 12083 81.6 3.6 5.6 7.9 17.9 1537 63.7
465 12292 81.8 3.6 5.6 7.9 18.0 1546 63.8
470 12500 81.9 3.6 5.6 8.0 18.1 1556 63.8

Table 3. Measured Receiver Power as a Function of EIRP
Frequency MHz Field Strength
µV/meter
EIRP mW EIRP dBm Meas. Antenna Gain Meas. Antenna Gain, dB Meas. Recv. Power, µW Meas. Recv. Power, dBm
260 3750 0.004 -23.7 3.6 5.6 0.014 -48.5
265 3958 0.005 -23.3 3.6 5.6 0.015 -48.2
270 4167 0.005 -22.8 3.6 5.6 0.016 -47.9
275 4375 0.006 -22.4 3.6 5.6 0.017 -47.6
280 4583 0.006 -22.0 3.6 5.6 0.018 -47.4
285 4792 0.007 -21.6 3.6 5.6 0.019 -47.1
290 5000 0.007 -21.2 3.6 5.6 0.020 -46.9
295 5208 0.008 -20.9 3.6 5.6 0.021 -46.7
300 5417 0.009 -20.6 3.6 5.6 0.022 -46.5
305 5625 0.009 -20.2 3.6 5.6 0.023 -46.3
310 5833 0.010 -19.9 3.6 5.6 0.025 -46.2
315 6042 0.011 -19.6 3.6 5.6 0.025 -46.0
320 6250 0.012 -19.3 3.6 5.6 0.026 -45.8
325 6458 0.013 -19.0 3.6 5.6 0.027 -45.7
330 6667 0.013 -18.8 3.6 5.6 0.028 -45.5
335 6875 0.014 -18.5 3.6 5.6 0.029 -45.4
340 7083 0.015 -18.2 3.6 5.6 0.030 -45.3
345 7292 0.016 -18.0 3.6 5.6 0.031 -45.1
350 7500 0.017 -17.7 3.6 5.6 0.031 -45.0
355 7708 0.018 -17.5 3.6 5.6 0.032 -44.9
360 7917 0.019 -17.3 3.6 5.6 0.033 -44.8
365 8125 0.020 -17.0 3.6 5.6 0.034 -44.7
370 8333 0.021 -16.8 3.6 5.6 0.035 -44.6
375 8542 0.022 -16.6 3.6 5.6 0.035 -44.5
380 8750 0.023 -16.4 3.6 5.6 0.036 -44.4
385 8958 0.024 -16.2 3.6 5.6 0.037 -44.3
390 9167 0.025 -16.0 3.6 5.6 0.038 -44.2
395 9375 0.026 -15.8 3.6 5.6 0.039 -44.1
400 9583 0.028 -15.6 3.6 5.6 0.039 -44.1
405 9792 0.029 -15.4 3.6 5.6 0.040 -44.0
410 10000 0.030 -15.2 3.6 5.6 0.041 -43.9
415 10208 0.031 -15.0 3.6 5.6 0.041 -43.8
420 10417 0.033 -14.9 3.6 5.6 0.042 -43.8
425 10625 0.034 -14.7 3.6 5.6 0.043 -43.7
430 10833 0.035 -14.5 3.6 5.6 0.043 -43.6
435 11042 0.037 -14.4 3.6 5.6 0.044 -43.6
440 11250 0.038 -14.2 3.6 5.6 0.045 -43.5
445 11458 0.039 -14.0 3.6 5.6 0.045 -43.4
450 11667 0.041 -13.9 3.6 5.6 0.046 -43.4
455 11875 0.042 -13.7 3.6 5.6 0.047 -43.3
460 12083 0.044 -13.6 3.6 5.6 0.047 -43.3
465 12292 0.045 -13.4 3.6 5.6 0.048 -43.2
470 12500 0.047 -13.3 3.6 5.6 0.048 -43.2

The article was published in the November 2006 issue of High Frequency Magazine.

Related Parts
MAX1472 300MHz-to-450MHz Low-Power, Crystal-Based ASK Transmitter Samples  
MAX1479 300MHz to 450MHz Low-Power, Crystal-Based +10dBm ASK/FSK Transmitter Samples  
MAX7030 Low-Cost, 315MHz and 433.92MHz ASK Transceiver with Fractional-N PLL Samples  
MAX7031 Low-Cost, 308MHz, 315MHz, and 433.92MHz FSK Transceiver with Fractional-N PLL  
MAX7032 Low-Cost, Crystal-Based, Programmable, ASK/FSK Transceiver with Fractional-N PLL Samples  
MAX7044 300MHz to 450MHz High-Efficiency, Crystal-Based +13dBm ASK Transmitter Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (188.9kB)  

© Mar 01, 2007, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 3815: Mar 01, 2007
APPLICATION NOTE 3815, AN3815, AN 3815, APP3815, Appnote3815, Appnote 3815