APPLICATION NOTE 3755

High-Power White-LED Driver Operates on 1 or 2 Alkaline Cells


Abstract: A white-LED driver based on a DC-DC step-up converter operates on one or two alkaline cells, and starts with voltages as low as 0.8V.

Replacing incandescent bulbs with high-power white LEDs yields higher reliability and greater luminous efficiency. A direct connection between the LED and battery, however, is not ideal. Compared with the alkaline batteries used in most portable applications, a power source for white LEDs should act more like a current source and offer higher operating voltages. It should also regulate the LED light output to be reasonably independent of the state of the batteries.

This single-IC driver for white LEDs delivers up to 1A from one or two alkaline cells (Figure 1). A controller for inductive step-up converters, the IC includes the necessary power switches. Starting with input voltages as low as 1V, it maintains good efficiency while regulating the LED current. It can operate from 0.8V to 3V while delivering 0.5A, and from 1.5V to 3V while delivering 1A. The circuit also operates well with sources of considerable internal resistance, like batteries at their end of life.

Figure 1. This white-LED driver operates on one or two alkaline cells, with voltages starting as low as 0.8V.
Figure 1. This white-LED driver operates on one or two alkaline cells, with voltages starting as low as 0.8V.

The driver's internal gain block lets you implement a current-regulation loop with few external components: just a current-sense resistor, and an extra resistor to load the internal transconductance amplifier. A 5.1V Zener diode protects the circuitry by setting a voltage-regulation loop and by limiting output voltage when the output circuit opens.

Figure 2 shows the output-current regulation over the operating-voltage range at 0.5A (lower trace) and 1A (upper trace). Figure 3 shows the corresponding efficiencies. Adding the potentiometer circuit shown allows efficient dimming of the light output. Control inputs ONA and ONB can be set for turning the LED on and off with a toggle switch or a momentary-contact pushbutton switch. Figure 1 connects the IC permanently ON. For other ON/OFF configurations, please consult the MAX1763 data sheet.

Figure 2. Output-current regulation vs. operating voltage for the circuit in Figure 1: 1A (top), and 0.5A (bottom).
Figure 2. Output-current regulation vs. operating voltage for the circuit in Figure 1: 1A (top), and 0.5A (bottom).

Figure 3. Operating efficiency at 1A (top) and 0.5A (bottom) for the circuit in Figure 1.
Figure 3. Operating efficiency at 1A (top) and 0.5A (bottom) for the circuit in Figure 1.

A similar article appeared in the September 19, 2005 Planet Analog Supplement of EE Times.

Related Parts
MAX1763 1.5A, Low-Noise, 1MHz, Step-Up DC-DC Converter Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (44kB)  

© Mar 23, 2006, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 3755: Mar 23, 2006
APPLICATION NOTE 3755, AN3755, AN 3755, APP3755, Appnote3755, Appnote 3755