APPLICATION NOTE 3379

Built-In Features Eliminate the Need for External Relays when Using the Maxim Driver-Comparator-Load (DCL) and Parametric Measurement Unit (PMU) Chip Sets


Abstract: The following application note describes the features of Maxim's new PMU and DCL products and utilizes their characteristics for specific PMU output current requirements of less than 2mA or for output current requirements of 2mA to 50mA.

Introduction

In traditional automated semiconductor testing, the DCL and the PMU are alternately connected to the Device Under Test (DUT), using "select relays."

This application note describes the unique built-in features of the Maxim DCLs (MAX9961/62, MAX9967/68) and the PMUs (MAX9949/50, MAX9951/52) that allow the user to eliminate the cost and board space associated with mechanical relays. A secondary benefit is the ability to enhance the conventional current drive capability of low current PMU's by taking advantage of the driver component of the DCL.

Device Description

The MAX9961/62/67/68 are dual, low-power, high-speed pin electronics DCL ICs for Automated Test Equipment (ATE). Each channel includes a 500Mbps Driver, a Window Comparator, Dynamic Clamps, and an Active Load (MAX9961/62 = 2mA max, MAX9967/68 = 35mA max).

The MAX9949/50 are dual PMUs intended for ATE and other instrumentation. The small size, wide force and measurement range and high accuracy make the MAX9949-50 ideal for testers that require a PMU per pin or per site. The MAX9949/50 have a built in external buffer drive feature that can be used to expand the voltage and current range of the PMU depending on the user's application.

Application Example

The built in Force / Sense and low leakage features of the MAX9961/62/67/68 and the external buffer support of the MAX9949/50 allow them to work together to eliminate the need for external select relays.

Circuit Description

PMU Application Requiring Iout < 2mA
In this mode, the PMU is set to force and measure using its internal range select switch. The Driver is placed in the low leak mode and the PMU connection to the DUT is made through the Force pin of the DCL. (Figure 1)

Figure 1.
Figure 1.

PMU Application Requiring 2mA < Iout < 50mA
In this mode the PMU is set to force and measure using its external range select feature. The Driver reference input is connected to the Rcom output of the PMU. The PMU's current sense amp measures the voltage across the DCL Force / Sense pins. This voltage represents the DUT current across the 45 ohm driver output resistance. (Figure 2)

Figure 2.
Figure 2.

Conclusions

Maxim's DCLs and PMUs plus an analog switch eliminate the need for mechanical relays that add cost and take board space. Using a DCL increases the current drive capability when lower current PMUs are used in a design.



Related Parts
MAX9949 Dual Per-Pin Parametric Measurement Units  
MAX9950 Dual Per-Pin Parametric Measurement Units  
MAX9961 Dual, Low-Power, 500Mbps ATE Drivers/Comparators with 2mA Load  
MAX9962 Dual, Low-Power, 500Mbps ATE Drivers/Comparators with 2mA Load  
MAX9967 Dual, Low-Power, 500Mbps ATE Driver/Comparator with 35mA Load  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (45kB)  

© Dec 10, 2004, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 3379: Dec 10, 2004
APPLICATION NOTE 3379, AN3379, AN 3379, APP3379, Appnote3379, Appnote 3379