NEWS RELEASE
Increase the Runtime of Space-Constrained Wearable and IoT Applications with Industry’s Smallest Solar Harvesting Solution by Maxim Integrated
MAX20361 reduces solution size by at least 50 percent while also improving harvest efficiency
San Jose, CA and Las Vegas, NV—Jan. 11, 2021—Designers of space-constrained designs can now significantly increase runtime with the MAX20361 single-/multi-cell solar harvester with maximum power point tracking (MPPT) from Maxim Integrated Products, Inc. (NASDAQ: MXIM). The industry’s smallest solar harvesting solution is ideal for space-constrained applications such as wearables and emerging internet of things (IoT) applications.
Designers are often challenged with the tradeoff between small size and long runtime for wearable and IoT applications. By enabling solar charging in these highly space-constrained products, the MAX20361 can extend the runtime of those devices by providing a supplemental power source. This solar harvester reduces solution size by at least half compared to the closest competitor. In addition, the MAX20361 increases harvested energy with up to 5 percent better boost efficiency than the closest competitor, coupled with an adaptive MPPT approach which can improve the overall system level efficiency even further.
Key Advantages
- Smallest Size: Industry’s smallest solar harvesting solution due to reduced component size and smaller, fewer external components; at least 50 percent smaller solution size compared to the closest competitor
- Higher Efficiency: Increased boost efficiency maximizes harvested energy with up to 5 percent better boost efficiency than the closest competitor; additional harvesting gains can be achieved through adaptive MPPT features coupled with the unique integrated harvesting gauge for real-time indications of efficiency to optimize performance
Commentary
- “This device offers exciting possibilities for a new supplemental power source to continually charge the battery of a device,” said Frank Dowling, director of the Industrial and Healthcare Business Unit at Maxim Integrated. “For example, if you can harvest just 30mW of solar power per day on a 300mAHr battery system which typically runs for three weeks, you can as a result extend that runtime by over 50 percent.”
- “Innovation continues to drive adoption of consumer wearables with global revenue estimated to grow at a compound annual growth rate (CAGR) of 15 percent in the next four years,” said James Hayward, principal analyst at IDTechEx Research. “For device manufacturers, longer battery life and smaller form factor remain key product features toward market differentiation and user satisfaction.”
Availability and Pricing
- The MAX20361 is available at Maxim Integrated’s website for $2.64 (1000-up, FOB USA); also available from authorized distributors
- The MAX20361EVKIT# evaluation kit is available for $57
About Maxim Integrated
Maxim Integrated, an engineer’s engineering company, exists to solve the designer’s toughest problems in order to empower design innovation. Our broad portfolio of high-performance semiconductors, combined with world-class tools and support, delivers essential analog solutions including efficient power, precision measurement, reliable connectivity and robust protection along with intelligent processing. Designers in application areas such as automotive, communications, consumer, data center, healthcare, industrial and IoT trust Maxim to help them quickly develop smaller, smarter and more secure designs. Learn more ›