NEWS RELEASE

Micro PLC Platform Puts the Power of Industry 4.0 in the Palm of Your Hand

Maxim Integrated's Micro PLC platform provides a 10x smaller form factor, > 50% power savings, and 70x faster data processing.

San Jose, CA—September 30, 2014—Using the Micro PLC platform from Maxim Integrated Products, Inc. (NASDAQ: MXIM), designers now have the tools to implement Industry 4.0 with less power, parts, and total costs. The platform consists of five reference designs which can operate as stand-alone subsystems and be configured and tested with a laptop's USB port.

A programmable logic controller (PLC) is the core building block that controls and coordinates sensors and machinery moving throughout a factory. Each year, $800 Billion is spent on factory maintenance and lost productivity. To reduce these expenses, the global Industry 4.0 movement is working to make manufacturing smarter and more efficient. Through "smart integration" (integration aligned with solving industry-wide issues) and proprietary process technology, Maxim's Micro PLC platform delivers a 10x reduction in form factor, provides > 50% power savings, and processes digital I/O outputs up to 70x faster than ever before. The platform will immediately reduce industry maintenance costs and increase uptime.

Supporting the Industry 4.0 distributed model, Maxim has developed multiple products that are interoperable with the Micro PLC platform:

  • MAX11270: a 24-bit, 10mW, delta-sigma ADC with integrated PGA offers the highest signal-to-noise (SNR) and lowest power in its class
  • MAX17515: a 5A, 2.4V to 5.5V input, complete switch-mode power supply with built-in inductor that reduces energy loss and heat with 92% efficiency
  • MAX17552: a 4V to 60V, 100mA, ultra-small, synchronous step-down DC-DC converter, compliant to IEC61131-2 PLC standard, that reduces heat dissipation and enables up to 50% cooler operation

Key Advantages

  • Faster throughput: up to 70x faster digital I/O provides increased production throughput
  • Power efficiency: > 50% power savings, allowing fan-less operations and higher density of I/Os
  • Compact size: 10x reduction in form factor brings the full capability of a modular PLC closer to the factory floor
  • High integration: reduces component count, improves reliability, and provides diagnostics to help keep a line up and running 24/7/365

Commentary

  • "The Micro PLC platform is the result of smart integration. We used our system knowledge and analog process integration capabilities to move customers into Industry 4.0," said Jeff DeAngelis, Executive Director of Business Management at Maxim Integrated. "Now our customers can build smaller, faster, and more efficient industrial controllers that bring the vision of Industry 4.0 into the palm of their hands."
  • "It is the right time to move towards Industry 4.0," said Susie Inouye, Research Director at Databeans. "Maxim is responding to the growing importance of this trend by improving system efficiency, throughput and reliability."

Pricing

  • The MAXREFDES61# 4-channel analog input board is $39 each. The schematics, layout files, and firmware are free and available for immediate use.
  • For information on other reference designs, visit Maxim's Reference Design Center.

At electronica 2014, the Micro PLC platform will showcase Maxim's quad analog input subsystem (MAXREFDES61#), as well as the company's digital input module, digital output module, and IO-Link® master modules.

electronica 2014

Visit Maxim at electronica 2014 in Munich, Germany from November 11-14. Maxim will be located in hall A4, stand 266. For more information, please visit www.electronica.de.

About Maxim Integrated

Maxim is the leader in analog integration. From mobile to industrial solutions, we're making analog smaller, smarter, and more energy efficient. Learn more at www.maximintegrated.com.

Follow Maxim Integrated on Twitter, Facebook, Google+, and LinkedIn.

Micro PLC platform provides a smaller footprint, increased power savings and faster data processing.
Download: RGB  |  CMYK

Related Resources
MAX11270
MAX11270 24-Bit, 10mW, 130dB SNR, 64ksps Delta-Sigma ADC with Integrated PGA
MAX17515
MAX17515 5A, 2.4V to 5.5V Input, High-Efficiency Power Module
MAX17552
MAX17552 60V, 100mA, Ultra-Small, High-Efficiency, Synchronous Step-Down DC-DC Converter with 22μA No-Load Supply Current

News Contact
Ferda Millan
408-601-5429
Ferda.Millan@maximintegrated.com