electronica 2018
At electronica 2018, we’re showcasing how imagination becomes creation. Discover revolutionary ways to satisfy shifting market demand and improve lives with our smaller, more powerful, more reliable, and more intelligent solutions. Learn about our adaptive manufacturing and industrial IoT solutions and our low-power, miniaturized healthcare innovations.
We’ll also be presenting our ASIL solutions that are driving the future of the automotive industry, as well as introducing our newest high-performance building blocks that empower your relentless approach to evolving products. Through demos and discussion, you’ll experience how Maxim Integrated can help you fully realize your innovations.
Smaller, Smarter, and More Powerful ICs—It’s All at electronica 2018
electronica 2018
11/13/2018 - 11/16/2018Munich, Germany
Hall C4, Stand 440

Industry 4.0: Manufacturing Convergence
Industrial convergence requires smarter systems. Explore the latest in adaptive manufacturing and industrial IoT (IIoT) solutions. Be inspired to improve their productivity using information that leads to integration, automation, and faster time to market. By delivering “intelligence at the edge,” we partner with you to evolve Industry 4.0—and beyond.
See our most inspired IIoT solution to date—the new Go-IO reference design. It packs 20 configurable IOs in a space one-third the size of a credit card and unleashes the full power of the IIoT, enabling productivity-enhancing self-diagnostic capabilities in automated factory subsystems. It meets the increasingly stringent size and power requirements of PLCs, providing a 10x smaller solution with 50% less power consumption compared to its industry-leading predecessor, the Pocket IO.
During electronica 2018, come by to see these product demonstrations—and get a closer look at how our innovations are changing the manufacturing industry:
- Integrated soccer ball factory demonstrating Industry 4.0 principles
- Digital IO
- IO-Link
- Robust communications
- Digital isolation
- Isolated power and protection
- Thermal demonstration of synchronous 60V DC-DC converters
- uSLIC™ power modules
Blogs
| Back to Top |
Wearable Healthcare: Wellness Reimagined
Wearable healthcare is transforming, again. More than something fun to wear, new monitoring devices are enabling healthcare professionals to use them as virtual care devices enabling more real-time exchange of accurate health data, assessment of chronic conditions, and evaluation of overall well-being.
For the first time, designers can achieve continuous monitoring of ECG, heart rate, and temperature in highly accurate, wearable solutions using Health Sensor Platform 2.0 (HSP 2.0). Unlike other wearables, the data measurements collected by the HSP 2.0 can be owned by the wearer, alleviating data privacy concerns and allowing users to conduct their own data analysis. And the fully working hardware and firmware with companion watch casing cuts design and validation time by up to six months.
Become familiar with our ever-evolving Health Sensor Platform that delivers flexibility and speed in the creation of unique and highly accurate wellness applications.
During electronica 2018, we will be sharing the following product demonstrations to give you a closer look at how our innovations are changing the healthcare industry:
- Interactive motion-sensory experience with personalized wearable healthcare
- In-ear heart-rate monitor
- Health Sensor Platform 2.0
- ECG monitor and health band
- Power management IC for wearables
- Vital sign monitoring with blood pressure
Blogs
| Back to Top |
Automotive: Driving Redefined
Cameras, sensors, microprocessors, and other components for advanced driver assistance systems (ADAS) are becoming more prevalent, making the ability to manage power even more critical. Add to this, the need to ensure that safety functions consistently operate properly.
Our automotive-qualified voltage regulators, power management ICs (PMICs) and power protectors address these ADAS power requirements while achieving CISPR 25 Class 5 EMI standard compliance—with high efficiency and a smaller footprint. With smaller solutions, we can enable a high level of integration and mitigate the effects of electromagnetic interference (EMI).
Experience our newest power and battery management products, high-speed signaling components, sensors, and wireless communications devices.
LED lighting designers face increasing power, thermal, and design complexities. Which is why we’re proud to introduce our newest LED matrix manager. The MAX20092 12-switch matrix manager allows designers to migrate to higher current devices while reducing solution size and improving flexibility. It offers the industry’s lowest on-resistance internal switches and reduces thermal issues, complexity, and design costs associated with LED matrix lighting applications. With the MAX20092, you can simplify LED programmability, reduce taxation on system bus lines, enable LED current of up to 1.5A, and reduce EMI and noise.
Experience our newest power and battery management products, high-speed signaling components, sensors, and wireless communications devices. During electronica 2018, see these demonstrations for a closer look at how our innovations are changing the automotive industry:
- Automotive-grade USB
- Power management for eCall applications
- Security and authentication of automotive sensors
Learn more about our power management for ADAS solutions ›
Learn more about LED lighting solutions ›
| Back to Top |
High-Performance Building Blocks: Design Revolutionized
Our high-performance analog ICs empower you to be relentless in innovation for every application. From ultra-low power consumption to extended battery life, precision signal conversion, and rugged connectivity, these latest products deliver capabilities that push the limits of technology and ease of use to help you take your products to the next level.
This year, we’ll be introducing the world to MAX41464, MAX38888 and MAX16141—innovations that demonstrate leading advances in efficiency, size, and versatility for next-generation electronic systems. The MAX41464 is a sub-1GHz frequency-shift keying (FSK) transmitter with the industry’s highest output power of +16dBm for long-range wireless sensors used in multiple applications including building automation and security systems. As part of Maxim’s Continua™ family of backup power regulators, the MAX38888 reversible buck/boost regulator delivers an industry-leading 95% peak efficiency and is setting the standard for backup power in mission-critical applications. Finally, we will be showcasing the MAX16141, a 36V ORing FET controller with voltage and current circuit breaker for monitoring over-voltage, under-voltage, over-current, reverse-current, and over-temperature conditions in automotive power applications.
During electronica 2018, we’ll showcase the following product demonstrations, giving you a closer look at how our innovations are changing design engineering:
- nanoPower watch
- Force-touch technology with MAX11261
- CAN ESD protection with MAX13054A
- Continua™ Family of backup regulators
- ISM RF transmitter-based home automation system
- Automotive mock control unit
| Back to Top |