/* Configuration Example For DS26303-120 running in E1 mode. This Example assumes E1 operation so the function call for T1/J1 configuration has been commented out. Simply comment out the E1 configuration function call and uncomment the T1 configuration function call for T1 operation. An individual function call for J1 operation is not present because it is very similar to T1 operation and could easily be implemented in that function. This file follows C style conventions. However actual code for the function calls listed below are implementation specific and need to be added: Function Calls: write(address, data), wait(milliseconds) The following comments only indicate some of the possible clock sources that can be used for either E1 or T1/J1 operation. Master clock configuration can use multiples of n = 1, 2, 4, or 8 MCLK = Can be a n x 1.544 or n x 2.048 MHz signal for E1 or T1/J1 Operation TCLK = Must be a 2.048 MHz Signal for E1 Operation TCLK = Must be a 1.544 MHz signal for T1/J1 Operation */ void initialization_main() { /* Global Initialization Begin */ /* Reset all channels to their default values */ write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank Write(0x000A, 0xFF); // SWR, Reset All Channels /* Wait 1 ms for reset to complete */ wait (1); /* The Master Clock Select Register is important for proper */ /* device operation consult the data sheet for all possible configurations. */ write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual LIU Register Bank write(0x0006, 0x00); // MC, E1 Mode Only MCLK-2.048, TECLK & CLKA Disabled // write(0x0006, 0x00); // MC, T1/J1 Mode Only MCLK-1.544, TECLK & CLKA Disabled // write(0x0006, 0x03); // MC, T1/J1 or E1 Mode MCLK-1.544, TECLK & CLKA Disabled // write(0x0006, 0x07); // MC, T1/J1 or E1 Mode MCLK-3.088, TECLK & CLKA Disabled // write(0x0006, 0x0B); // MC, T1/J1 or E1 Mode MCLK-6.176, TECLK & CLKA Disabled // write(0x0006, 0x0F); // MC, T1/J1 or E1 Mode MCLK-12.352, TECLK & CLKA Disabled // write(0x0006, 0x01); // MC, T1/J1 or E1 Mode MCLK-2.048, TECLK & CLKA Disabled // write(0x0006, 0x05); // MC, T1/J1 or E1 Mode MCLK-4.096, TECLK & CLKA Disabled // write(0x0006, 0x09); // MC, T1/J1 or E1 Mode MCLK-8.192, TECLK & CLKA Disabled // write(0x0006, 0x0D); // MC, T1/J1 or E1 Mode MCLK-16.384, TECLK & CLKA Disabled /* Wait 1 ms for clock to settle after configuration */ wait (1); /* The GC register is able to globally control the AIS During LOS, Short Circuit */ /* Protection, Line Coding, JA Depth, JA Position, and JA Enable functions */ write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x000F, 0x80); // GC, Enable RX Internal Impedance, Disable Global Controls /* Global Initialization Complete */ /* Configuration Begin */ e1_configure(); // t1_configure(); /* Configuration Complete */ } void e1_configure() { /* E1 Initilization Begin */ /* This function assumes all ports are configured identically. Otherwise, */ /* the function needs to be revised to support individual port addressing */ /* and identification. */ /* Configure analog, remote, or digital loopback as necessary */ write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x0001, 0x00); // ALBC, Disable Analog Loopback for 8 Channels // write(0x0001, 0xFF); // ALBC, Enable Analog Loopback for 8 Channels write(0x0002, 0x00); // RLBC, Disable Remote Loopback for 8 Channels // write(0x0002, 0xFF); // RLBC, Enable Remote Loopback for 8 Channels write(0x000C, 0x00); // DLBC, Disable Digital Loopback for 8 Channels // write(0x000C, 0xFF); // DLBC, Enable Digital Loopback for 8 Channels /* Configure LOS / AIS criteria in E1 mode */ write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x000D, 0x00); // LASCS, Use G.775 Criteria for 8 Channels // write(0x000D, 0xFF); // LASCS, Use ETSI 300233 Criteria for 8 Channels write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x0003, 0x00); // TAOE, Disable Transmit All Ones for 8 Channels // write(0x0003, 0xFF); // TAOE, Enable Transmit All Ones for 8 Channels write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x000E, 0x00); // ATAOS, Disable Automatic Transmit All Ones for 8 Channels // write(0x000E, 0xFF); // ATAOS, Enable Automatic Transmit All Ones for 8 Channels write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x0012, 0x00); // OEB, Disable TX Output High Impedance for 8 Channels // write(0x0012, 0xFF); // OEB, Enable TX Output High Impedance for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0003, 0x00); // RPDE, Disable Receive Power-Down for 8 Channels // write(0x0003, 0xFF); // RPDE, Enable Receive Power-Down for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0004, 0x00); // TPDE, Disable Transmit Power-Down for 8 Channels // write(0x0004, 0xFF); // TPDE, Enable Transmit Power-Down for 8 Channels /* In single rail mode (SMRS register) with HDB3/B8ZS (LCS register) enabled, */ /* the EZDE and CVDEB registers can enable the excessive zero and code */ /* violation detection output on the RNEG pin. */ write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank // write(0x0000, 0x00); // SRMS, Disable Single Rail Mode I/O for 8 Channels write(0x0000, 0xFF); // SRMS, Enable Single Rail Mode I/O for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0005, 0x00); // EZDE, Disable Excessive Zero Detect for 8 Channels // write(0x0005, 0xFF); // EZDE, Enable Excessive Zero Detect for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0006, 0x00); // CVDEB, Enable Code Violation Detect for 8 Channels // write(0x0006, 0xFF); // CVDEB, Disable Code Violation Detect for 8 Channels /* The following six functions can be controlled individually on a per channel */ /* basis or globally using the GC register. The IAISEL, ISCPD, LCS, IJAFDS, */ /* IJAPS, and IJAE are ignored when the corresponding function in the GC */ /* register is enabled. */ write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank write(0x0005, 0x00); // IAISEL, Disable Indiv AIS During LOS for 8 Channels // write(0x0005, 0xFF); // IAISEL, Enable Indiv AIS During LOS for 8 Channels write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank write(0x0004, 0x00); // ISCPD, Enable Indiv Short Protection for 8 Channels // write(0x0004, 0xFF); // ISCPD, Disable Indiv Short Protection for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0001, 0x00); // LCS, Enable B8ZS/HDB3 Operation for 8 Channels // write(0x0001, 0xFF); // LCS, Enable AMI Operation for 8 Channels write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank // write(0x0002, 0x00); // IJAFDS, Indiv JA 32 Bit Depth for 8 Channels write(0x0002, 0xFF); // IJAFDS, Indiv JA 128 Bit Depth for 8 Channels write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank // write(0x0001, 0x00); // IJAPS, Indiv JA Transmit Path for 8 Channels write(0x0001, 0xFF); // IJAPS, Indiv JA Receive Path for 8 Channels write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank // write(0x0000, 0x00); // IJAE, Disable Indiv Jitter Attenuator for 8 Channels write(0x0000, 0xFF); // IJAE, Enable Indiv Jitter Attenuator for 8 Channels /* Configure all channels for a E1 pulse template output. This example uses */ /* the DS26303-120 device so, TS.TIMPRM = 0 for 120 ohm line impedances. If */ /* the device were a DS26303-75, TS.TIMPRM = 1 for 120 ohm line impedances. */ write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank Write(0x0010, 0x00) // TST, Select Channel 1 for Template Configuration Write(0x0011, 0x00) // TS, E1 Mode 120 ohm G.703 TX/RX Impedance Match Write(0x0010, 0x01) // TST, Select Channel 2 for Template Configuration Write(0x0011, 0x00) // TS, E1 Mode 120 ohm G.703 TX/RX Impedance Match Write(0x0010, 0x02) // TST, Select Channel 3 for Template Configuration Write(0x0011, 0x00) // TS, E1 Mode 120 ohm G.703 TX/RX Impedance Match Write(0x0010, 0x03) // TST, Select Channel 4 for Template Configuration Write(0x0011, 0x00) // TS, E1 Mode 120 ohm G.703 TX/RX Impedance Match Write(0x0010, 0x04) // TST, Select Channel 5 for Template Configuration Write(0x0011, 0x00) // TS, E1 Mode 120 ohm G.703 TX/RX Impedance Match Write(0x0010, 0x05) // TST, Select Channel 6 for Template Configuration Write(0x0011, 0x00) // TS, E1 Mode 120 ohm G.703 TX/RX Impedance Match Write(0x0010, 0x06) // TST, Select Channel 7 for Template Configuration Write(0x0011, 0x00) // TS, E1 Mode 120 ohm G.703 TX/RX Impedance Match Write(0x0010, 0x07) // TST, Select Channel 8 for Template Configuration Write(0x0011, 0x00) // TS, E1 Mode 120 ohm G.703 TX/RX Impedance Match } void t1_configure() { /* T1 Initilization Begin */ /* This function assumes all ports are configured identically. Otherwise, */ /* the function needs to be revised to support individual port addressing */ /* and identification. */ /* Configure analog, remote, or digital loopback as necessary */ write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x0001, 0x00); // ALBC, Disable Analog Loopback for 8 Channels // write(0x0001, 0xFF); // ALBC, Enable Analog Loopback for 8 Channels write(0x0002, 0x00); // RLBC, Disable Remote Loopback for 8 Channels // write(0x0002, 0xFF); // RLBC, Enable Remote Loopback for 8 Channels write(0x000C, 0x00); // DLBC, Disable Digital Loopback for 8 Channels // write(0x000C, 0xFF); // DLBC, Enable Digital Loopback for 8 Channels write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x0003, 0x00); // TAOE, Disable Transmit All Ones for 8 Channels // write(0x0003, 0xFF); // TAOE, Enable Transmit All Ones for 8 Channels write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x000E, 0x00); // ATAOS, Disable Automatic Transmit All Ones for 8 Channels // write(0x000E, 0xFF); // ATAOS, Enable Automatic Transmit All Ones for 8 Channels write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank write(0x0012, 0x00); // OEB, Disable TX Output High Impedance for 8 Channels // write(0x0012, 0xFF); // OEB, Enable TX Output High Impedance for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0003, 0x00); // RPDE, Disable Receive Power-Down for 8 Channels // write(0x0003, 0xFF); // RPDE, Enable Receive Power-Down for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0004, 0x00); // TPDE, Disable Transmit Power-Down for 8 Channels // write(0x0004, 0xFF); // TPDE, Enable Transmit Power-Down for 8 Channels /* In single rail mode (SMRS register) with HDB3/B8ZS (LCS register) enabled, */ /* the EZDE and CVDEB registers can enable the excessive zero and code */ /* violation detection output on the RNEG pin. */ write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank // write(0x0000, 0x00); // SRMS, Disable Single Rail Mode I/O for 8 Channels write(0x0000, 0xFF); // SRMS, Enable Single Rail Mode I/O for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0005, 0x00); // EZDE, Disable Excessive Zero Detect for 8 Channels // write(0x0005, 0xFF); // EZDE, Enable Excessive Zero Detect for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0006, 0x00); // CVDEB, Enable Code Violation Detect for 8 Channels // write(0x0006, 0xFF); // CVDEB, Disable Code Violation Detect for 8 Channels /* The following six functions can be controlled individually on a per channel */ /* basis or globally using the GC register. The IAISEL, ISCPD, LCS, IJAFDS, */ /* IJAPS, and IJAE are ignored when the corresponding function in the GC */ /* register is enabled. */ write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank write(0x0005, 0x00); // IAISEL, Disable Indiv AIS During LOS for 8 Channels // write(0x0005, 0xFF); // IAISEL, Enable Indiv AIS During LOS for 8 Channels write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank write(0x0004, 0x00); // ISCPD, Enable Indiv Short Protection for 8 Channels // write(0x0004, 0xFF); // ISCPD, Disable Indiv Short Protection for 8 Channels write(0x001F, 0xAA); // ADDP, Set Address Pointer to Secondary Register Bank write(0x0001, 0x00); // LCS, Enable B8ZS/HDB3 Operation for 8 Channels // write(0x0001, 0xFF); // LCS, Enable AMI Operation for 8 Channels write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank // write(0x0002, 0x00); // IJAFDS, Indiv JA 32 Bit Depth for 8 Channels write(0x0002, 0xFF); // IJAFDS, Indiv JA 128 Bit Depth for 8 Channels write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank // write(0x0001, 0x00); // IJAPS, Indiv JA Transmit Path for 8 Channels write(0x0001, 0xFF); // IJAPS, Indiv JA Receive Path for 8 Channels write(0x001F, 0x01); // ADDP, Set Address Pointer to Individual Register Bank // write(0x0000, 0x00); // IJAE, Disable Indiv Jitter Attenuator for 8 Channels write(0x0000, 0xFF); // IJAE, Enable Indiv Jitter Attenuator for 8 Channels /* Configure all channels for a T1 pulse template output */ write(0x001F, 0x00); // ADDP, Set Address Pointer to Primary Register Bank Write(0x0010, 0x00) // TST, Select Channel 1 for Template Configuration Write(0x0011, 0x07) // TS, T1 Mode 100 ohm 533-655 ft. TX/RX Impedance Match Write(0x0010, 0x01) // TST, Select Channel 2 for Template Configuration Write(0x0011, 0x07) // TS, T1 Mode 100 ohm 533-655 ft. TX/RX Impedance Match Write(0x0010, 0x02) // TST, Select Channel 3 for Template Configuration Write(0x0011, 0x07) // TS, T1 Mode 100 ohm 533-655 ft. TX/RX Impedance Match Write(0x0010, 0x03) // TST, Select Channel 4 for Template Configuration Write(0x0011, 0x07) // TS, T1 Mode 100 ohm 533-655 ft. TX/RX Impedance Match Write(0x0010, 0x04) // TST, Select Channel 5 for Template Configuration Write(0x0011, 0x07) // TS, T1 Mode 100 ohm 533-655 ft. TX/RX Impedance Match Write(0x0010, 0x05) // TST, Select Channel 6 for Template Configuration Write(0x0011, 0x07) // TS, T1 Mode 100 ohm 533-655 ft. TX/RX Impedance Match Write(0x0010, 0x06) // TST, Select Channel 7 for Template Configuration Write(0x0011, 0x07) // TS, T1 Mode 100 ohm 533-655 ft. TX/RX Impedance Match Write(0x0010, 0x07) // TST, Select Channel 8 for Template Configuration Write(0x0011, 0x07) // TS, T1 Mode 100 ohm 533-655 ft. TX/RX Impedance Match }