---------------------------------------------------------------------------------- -- -- BSDL file for design DS26522 -- -- File Name : DS26522_D2_SCT_BSDL.TXT -- -- Created by Synopsys Version 2000.11 (Nov 27, 2000) -- Modified by Maxim Integrated Products (T. Zagumny) -- -- Company : Maxim Integrated Products -- Documentation : DS26521 datasheet -- BSDL Revision : 1.1 -- Date : 4/2/2009 Thursday April 2, 2009 -- -- Device : DS26522 RevA -- Package : 144-pin CSBGA -- -- IMPORTANT NOTICE -- Maxim Integrated Products customers are advised to obtain the latest version -- of device specifications before relying on any published information contained -- herein. Maxim Integrated Products assumes no responsibility or liability -- arising out of the application of any information described herein. -- -- IMPORTANT NOTICE ABOUT THE REVISION -- -- Maxim Integrated Products customers are advised to check the revision of the -- device they will be using. All the codes for the device revisions are -- herein this BSDL file. -- -- The characters "/", "(", ")" and "*" have been removed from signal names for -- compatibility with BSDL file format. -- -- -------------------------------------------------------------------------------- entity DS26522_D2 is -- This section identifies the default device package selected. generic (PHYSICAL_Pin_MAP: string:= "CSBGA_144"); -- This section declares all the ports in the design. port ( A0 : in bit; A1 : in bit; A12 : in bit; A2 : in bit; A3 : in bit; A4 : in bit; A5 : in bit; A6 : in bit; A7 : in bit; A8 : in bit; BTS : in bit; CSB2_B : in bit; JTCLK : in bit; JTDI2 : in bit; JTMS : in bit; JTRST : in bit; MCLK : in bit; RDB_DSB : in bit; RESET_B : in bit; RSYSCLK2 : in bit; SPI_SEL : in bit; TCLK2 : in bit; TSER2 : in bit; TSYSCLK2 : in bit; TXEN2_B : in bit; WRB_RWB : in bit; D0 : inout bit; D1 : inout bit; D2 : inout bit; D3 : inout bit; D4 : inout bit; D5 : inout bit; D6 : inout bit; D7 : inout bit; RCHBLK_CLK2 : inout bit; RCLK2 : inout bit; REFCLKIO2 : inout bit; RM_RFSYNC2 : inout bit; RSIG2 : inout bit; RSYNC2 : inout bit; TCHBLK_CLK2 : inout bit; TSIG2 : inout bit; TSSYNCIO2 : inout bit; TSYNC2 : inout bit; AL_RSIGF_FLOS2 : out bit; BPCLK2 : out bit; INT_B : out bit; JTDO2 : out bit; RLF_LTC2 : out bit; RSER2 : out bit; RRING2 : linkage bit_vector (0 to 1); RTIP2 : linkage bit_vector (0 to 1); TRING2 : linkage bit_vector (0 to 1); TTIP2 : linkage bit_vector (0 to 1); VDD2 : linkage bit_vector (1 to 4); VDD2C : linkage bit; VDD2R : linkage bit_vector (1 to 5); VDD2T : linkage bit_vector (1 to 2); VSS2 : linkage bit_vector (1 to 8); VSS2C : linkage bit_vector (1 to 2); VSS2R : linkage bit_vector (1 to 5); VSS2T : linkage bit_vector (1 to 2) ); use STD_1149_1_1994.all; attribute COMPONENT_CONFORMANCE of DS26522_D2: entity is "STD_1149_1_1993"; attribute Pin_MAP of DS26522_D2: entity is PHYSICAL_Pin_MAP; -- This section specifies the pin map for each port. This information -- is extracted from the port-to-pin map file that was read in using -- the "read_pin_map" command. constant CSBGA_144: Pin_MAP_STRinG := "A0 : J2," & "A1 : J1," & "A12 : E1," & "A2 : H2," & "A3 : H1," & "A4 : G2," & "A5 : G1," & "A6 : F2," & "A7 : F1," & "A8 : E2," & "BTS : E5," & "CSB2_B : M4," & "JTCLK : M6," & "JTDI2 : L7," & "JTMS : M5," & "JTRST : L6," & "MCLK : M9," & "RDB_DSB : H3," & "RESET_B : K3," & "RSYSCLK2 : J11," & "SPI_SEL : D7," & "TCLK2 : G11," & "TSER2 : E12," & "TSYSCLK2 : H11," & "TXEN2_B : E7," & "WRB_RWB : J3," & "D0 : M3," & "D1 : L3," & "D2 : M2," & "D3 : M1," & "D4 : L2," & "D5 : L1," & "D6 : K2," & "D7 : K1," & "RCHBLK_CLK2 : M11," & "RCLK2 : L9," & "REFCLKIO2 : L10," & "RM_RFSYNC2 : L12," & "RSIG2 : L11," & "RSYNC2 : K12," & "TCHBLK_CLK2 : G12," & "TSIG2 : E11," & "TSSYNCIO2 : F12," & "TSYNC2 : F11," & "AL_RSIGF_FLOS2 : J12," & "BPCLK2 : M10," & "INT_B : K4," & "JTDO2 : M8," & "RLF_LTC2 : M12," & "RSER2 : H12," & "RRING2 : (A8, B8)," & "RTIP2 : (A9, B9)," & "TRING2 : (A11, B11)," & "TTIP2 : (A12, B12)," & "VDD2 : (J9, J10, H10, G10)," & "VDD2C : K9," & "VDD2R : (C8, C9, C10, D11, D12)," & "VDD2T : (C11, C12)," & "VSS2 : (D8, E8, E9, E10, F9, F10, G9, H9)," & "VSS2C : (K10, K11)," & "VSS2R : (A7, B7, C7, D9, D10)," & "VSS2T : (A10, B10)"; -- This section specifies the TAP ports. -- For the TAP TCK port, the parameters in the brackets are: -- First Field : Maximum TCK frequency. -- Second Field: Allowable states TCK may be stopped in. attribute TAP_SCAN_CLOCK of JTCLK: signal is (10.0e6, BOTH); attribute TAP_SCAN_in of JTDI2: signal is true; attribute TAP_SCAN_MODE of JTMS : signal is true; attribute TAP_SCAN_OUT of JTDO2: signal is true; attribute TAP_SCAN_RESET of JTRST: signal is true; -- Specifies the number of bits in the instruction register. attribute inSTRUCTION_LENGTH of DS26522_D2: entity is 3; -- Specifies the boundary-scan instructions implemented in the -- design and their opcodes. attribute inSTRUCTION_OPCODE of DS26522_D2: entity is "BYPASS (111)," & "EXTEST (000)," & "SAMPLE (010)," & "CLAMP (011)," & "USER1 (100)," & "USER2 (101)," & "USER3 (110)," & "IDCODE (001)"; -- Specifies the bit pattern that is loaded into the instruction -- register when the TAP controller passes through the Capture-IR -- state. The standard mandates that the two LSBs must be "01". -- The remaining bits are design specific. attribute inSTRUCTION_CAPTURE of DS26522_D2: entity is "001"; -- Specifies the bit pattern that is loaded into the DEVICE_ID -- register during the IDCODE instruction when the TAP controller -- passes through the Capture-DR state. attribute IDCODE_REGISTER of DS26522_D2: entity is "0000" & -- 4-bit version number "0000000010001000" & -- 16-bit part number "00010100001" & -- 11-bit identity of the manufacturer "1"; -- Required by IEEE Std 1149.1 -- This section specifies the test data register placed between TDI -- and TDO for each implemented instruction. attribute REGISTER_ACCESS of DS26522_D2: entity is "BYPASS (BYPASS, CLAMP, USER1, USER2, USER3)," & "BOUNDARY (EXTEST, SAMPLE)," & "DEVICE_ID (IDCODE)"; -- Specifies the length of the boundary scan register. attribute BOUNDARY_LENGTH of DS26522_D2: entity is 86; -- The following list specifies the characteristics of each cell -- in the boundary scan register from TDI to TDO. -- The following is a description of the label fields: -- num : Is the cell number. -- cell : Is the cell type as defined by the standard. -- port : Is the design port name. Control cells do not -- have a port name. -- function: Is the function of the cell as defined by the -- standard. Is one of input, output2, output3, -- bidir, control or controlr. -- safe : Specifies the value that the BSR cell should be -- loaded with for safe operation when the software -- might otherwise choose a random value. -- ccell : The control cell number. Specifies the control -- cell that drives the output enable for this port. -- disval : Specifies the value that is loaded into the -- control cell to disable the output enable for -- the corresponding port. -- rslt : Resulting state. Shows the state of the driver -- when it is disabled. attribute BOUNDARY_REGISTER of DS26522_D2: entity is -- -- num cell port function safe [ccell disval rslt] -- "85 (BC_4, SPI_SEL, observe_only, X), " & "84 (BC_4, BTS, observe_only, X), " & "83 (BC_4, TXEN2_B, observe_only, X), " & "82 (BC_4, A12, observe_only, X), " & "81 (BC_4, A8, observe_only, X), " & "80 (BC_4, A7, observe_only, X), " & "79 (BC_4, A6, observe_only, X), " & "78 (BC_4, A5, observe_only, X), " & "77 (BC_4, A4, observe_only, X), " & "76 (BC_4, A3, observe_only, X), " & "75 (BC_4, A2, observe_only, X), " & "74 (BC_4, A1, observe_only, X), " & "73 (BC_4, A0, observe_only, X), " & "72 (BC_4, D7, observe_only, X), " & "71 (BC_2, D7, output3, X, 70, 1, Z), " & "70 (BC_2, *, controlr, 1), " & "69 (BC_4, D6, observe_only, X), " & "68 (BC_2, D6, output3, X, 67, 1, Z), " & "67 (BC_2, *, controlr, 1), " & "66 (BC_4, D5, observe_only, X), " & "65 (BC_2, D5, output3, X, 64, 1, Z), " & "64 (BC_2, *, controlr, 1), " & "63 (BC_4, D4, observe_only, X), " & "62 (BC_2, D4, output3, X, 61, 1, Z), " & "61 (BC_2, *, controlr, 1), " & "60 (BC_4, D3, observe_only, X), " & "59 (BC_2, D3, output3, X, 58, 1, Z), " & "58 (BC_2, *, controlr, 1), " & "57 (BC_4, D2, observe_only, X), " & "56 (BC_2, D2, output3, X, 55, 1, Z), " & "55 (BC_2, *, controlr, 1), " & "54 (BC_4, D1, observe_only, X), " & "53 (BC_2, D1, output3, X, 52, 1, Z), " & "52 (BC_2, *, controlr, 1), " & "51 (BC_4, D0, observe_only, X), " & "50 (BC_2, D0, output3, X, 49, 1, Z), " & "49 (BC_2, *, controlr, 1), " & "48 (BC_4, CSB2_B, observe_only, X), " & "47 (BC_4, RDB_DSB, observe_only, X), " & "46 (BC_4, WRB_RWB, observe_only, X), " & "45 (BC_2, INT_B, output3, X, 44, 1, PULL1)," & "44 (BC_2, *, controlr, 1), " & "43 (BC_4, RESET_B, observe_only, X), " & "42 (BC_4, MCLK, observe_only, X), " & "41 (BC_4, REFCLKIO2, observe_only, X), " & "40 (BC_2, REFCLKIO2, output3, X, 39, 1, Z), " & "39 (BC_2, *, controlr, 1), " & "38 (BC_2, BPCLK2, output3, X, 37, 1, Z), " & "37 (BC_2, *, controlr, 1), " & "36 (BC_4, RCHBLK_CLK2, observe_only, X), " & "35 (BC_2, RCHBLK_CLK2, output3, X, 34, 1, Z), " & "34 (BC_2, *, controlr, 1), " & "33 (BC_2, RLF_LTC2, output3, X, 32, 1, Z), " & "32 (BC_2, *, controlr, 1), " & "31 (BC_2, AL_RSIGF_FLOS2, output3, X, 30, 1, Z), " & "30 (BC_2, *, controlr, 1), " & "29 (BC_4, RSIG2, observe_only, X), " & "28 (BC_2, RSIG2, output3, X, 27, 1, Z), " & "27 (BC_2, *, controlr, 1), " & "26 (BC_4, RM_RFSYNC2, observe_only, X), " & "25 (BC_2, RM_RFSYNC2, output3, X, 24, 1, Z), " & "24 (BC_2, *, controlr, 1), " & "23 (BC_4, RSYNC2, observe_only, X), " & "22 (BC_2, RSYNC2, output3, X, 21, 1, Z), " & "21 (BC_2, *, controlr, 1), " & "20 (BC_4, RSYSCLK2, observe_only, X), " & "19 (BC_4, RCLK2, observe_only, X), " & "18 (BC_2, RCLK2, output3, X, 17, 1, Z), " & "17 (BC_2, *, controlr, 1), " & "16 (BC_2, RSER2, output3, X, 15, 1, Z), " & "15 (BC_2, *, controlr, 1), " & "14 (BC_4, TCHBLK_CLK2, observe_only, X), " & "13 (BC_2, TCHBLK_CLK2, output3, X, 12, 1, Z), " & "12 (BC_2, *, controlr, 1), " & "11 (BC_4, TSIG2, observe_only, X), " & "10 (BC_2, TSIG2, output3, X, 9, 1, Z), " & "9 (BC_2, *, controlr, 1), " & "8 (BC_4, TSSYNCIO2, observe_only, X), " & "7 (BC_2, TSSYNCIO2, output3, X, 6, 1, Z), " & "6 (BC_2, *, controlr, 1), " & "5 (BC_4, TSYNC2, observe_only, X), " & "4 (BC_2, TSYNC2, output3, X, 3, 1, Z), " & "3 (BC_2, *, controlr, 1), " & "2 (BC_4, TSYSCLK2, observe_only, X), " & "1 (BC_4, TCLK2, observe_only, X), " & "0 (BC_4, TSER2, observe_only, X) "; end DS26522_D2;