-------------------------------------------------------------------------------- -- -- File Name : DS26503_BSDL.TXT -- Created by : Dallas Semiconductor -- Documentation : DS26503 data sheets -- -- BSDL Revision : 1.1 -- -- Date created : 07/18/2004 -- Date modified : 08/22/2005 -- -- Device : DS26503 -- Package : 64-pin LQFP -- -- IMPORTANT NOTICE -- Dallas Semiconductor customers are advised to obtain the latest version of -- device specifications before relying on any published information contained -- herein. Dallas Semiconductor assumes no responsibility or liability arising -- out of the application of any information described herein. -- -- IMPORTANT NOTICE ABOUT THE REVISION -- -- Dallas Semiconductor customers are advised to check the revision of the -- device they will be using. All the codes for the device revisions are -- herein this BSDL file. -- -- The characters "/", "(", ")" and "*" have been removed from signal names for -- compatibility with BSDL file format. -- ---------------------------------------------------------------------------------- entity DS26503_top is -- This section identifies the default device package selected. generic (PHYSICAL_PIN_MAP: string:= "LQFP_64"); -- This section declares all the ports in the design. port ( TTIP :linkage bit; TRING :linkage bit; AD7 :inout bit; AD6 :inout bit; AD5 :inout bit; AD4 :inout bit; AD3 :inout bit; AD2 :inout bit; AD1 :inout bit; AD0 :inout bit; TSYNC :inout bit; TSER :in bit; TCSS1 :in bit; TCLK :in bit; TCLKO :out bit; TPOSO :out bit; TNEGO :out bit; CS :in bit; RDDS :in bit; WRRW :in bit; RTIP :linkage bit; RRING :linkage bit; RAIS :out bit; RCLK :out bit; RSYNC :out bit; RSER :out bit; RLOF :out bit; RLOS :out bit; OUT400 :out bit; PLL_CLK :out bit; TMODE1 :in bit; TMODE2 :in bit; THZE :in bit; INT :inout bit; TSTRST :in bit; BIS0 :in bit; BIS1 :in bit; BTS :in bit; MCLK :in bit; JTRST :in bit; JTCLK :in bit; JTDI :in bit; JTDO :out bit; JTMS :in bit; ALE_A7 :in bit; A6 :in bit; A5 :in bit; A4 :in bit; A3 :in bit; A2 :in bit; A1 :in bit; A0 :in bit; TVDD :linkage bit; TVSS :linkage bit; DVDD :linkage bit_vector(1 to 3); DVSS :linkage bit_vector(1 to 3); RVDD :linkage bit; RVSS :linkage bit_vector(1 to 3) ); use STD_1149_1_1994.all; attribute COMPONENT_CONFORMANCE of DS26503_top: entity is "STD_1149_1_1993"; attribute PIN_MAP of DS26503_top: entity is PHYSICAL_PIN_MAP; -- This section specifies the pin map for each port. This information -- is extracted from the port-to-pin map file that was read in using -- the "read_pin_map" command. constant LQFP_64: PIN_MAP_STRING := "TTIP :51 ,"& "TRING :54 ,"& "AD7 :6 ,"& "AD6 :5 ,"& "AD5 :4 ,"& "AD4 :3 ,"& "AD3 :2 ,"& "AD2 :1 ,"& "AD1 :64 ,"& "AD0 :63 ,"& "TSYNC :23 ,"& "TSER :21 ,"& "TCSS1 :31 ,"& "TCLK :17 ,"& "TCLKO :18 ,"& "TNEGO :19 ,"& "TPOSO :20 ,"& "CS :60 ,"& "RDDS :61 ,"& "WRRW :62 ,"& "RTIP :41 ,"& "RRING :42 ,"& "RAIS :29 ,"& "RCLK :25 ,"& "RSYNC :26 ,"& "RSER :28 ,"& "RLOF :30 ,"& "RLOS :32 ,"& "OUT400 :27 ,"& "PLL_CLK:47 ,"& "TMODE1 :49 ,"& "TMODE2 :48 ,"& "THZE :50 ,"& "INT :46 ,"& "TSTRST :39 ,"& "BIS0 :57 ,"& "BIS1 :59 ,"& "BTS :55 ,"& "MCLK :44 ,"& "JTRST :35 ,"& "JTCLK :34 ,"& "JTDI :36 ,"& "JTDO :37 ,"& "JTMS :33 ,"& "ALE_A7 :16 ,"& "A6 :15 ,"& "A5 :14 ,"& "A4 :13 ,"& "A3 :12 ,"& "A2 :11 ,"& "A1 :10 ,"& "A0 :9 ,"& "TVDD :53 ,"& "TVSS :52 ,"& "DVDD :(58,7, 24) ,"& "DVSS :(56,8, 22) ,"& "RVDD :38 ,"& "RVSS :(40, 43, 45)"; -- This section specifies the TAP ports. -- For the TAP TCK port, the parameters in the brackets are: -- First Field : Maximum TCK frequency. -- Second Field: Allowable states TCK may be stopped in. attribute TAP_SCAN_CLOCK of JTCLK : signal is (10.0e6, BOTH); attribute TAP_SCAN_IN of JTDI : signal is true; attribute TAP_SCAN_MODE of JTMS : signal is true; attribute TAP_SCAN_OUT of JTDO : signal is true; attribute TAP_SCAN_RESET of JTRST : signal is true; -- Specifies the number of bits in the instruction register. attribute INSTRUCTION_LENGTH of DS26503_top: entity is 3; -- Specifies the boundary-scan instructions implemented in the -- design and their opcodes. attribute INSTRUCTION_OPCODE of DS26503_top: entity is "BYPASS (111)," & "EXTEST (000)," & "SAMPLE (010)," & "CLAMP (011)," & "HIGHZ (100)," & "IDCODE (001)"; -- Specifies the bit pattern that is loaded into the instruction -- register when the TAP controller passes through the Capture-IR -- state. The standard mandates that the two LSBs must be "01". -- The remaining bits are design specific. attribute INSTRUCTION_CAPTURE of DS26503_top: entity is "001"; -- Specifies the bit pattern that is loaded into the DEVICE_ID -- register during the IDCODE instruction when the TAP controller -- passes through the Capture-DR state. -- 00035143 (HEX) attribute IDCODE_REGISTER of DS26503_top: entity is "XXXX" & -- 4-bit version number for A1 [31-28] "0000000000110110" & -- 16-bit part number [27-12] "00010100001" & -- 11-bit identity of the manufacturer [11- 1] "1"; -- Required by IEEE Std 1149.1 [0] -- This section specifies the test data register placed between TDI -- and TDO for each implemented instruction. -- attribute REGISTER_ACCESS of DS26503_top: entity is "BYPASS (BYPASS, CLAMP, HIGHZ)," & "BOUNDARY (EXTEST, SAMPLE)," & "DEVICE_ID (IDCODE)"; -- Specifies the length of the boundary scan register. attribute BOUNDARY_LENGTH of DS26503_top: entity is 46; attribute BOUNDARY_REGISTER of DS26503_top: entity is -- -- num cell port function safe [ccell disval rslt] -- " 0 (BC_7, AD1 , bidir, 0, 1, 0, Z) ,"& " 1 (BC_2, * , control, 0) ,"& " 2 (BC_7, AD0 , bidir, 0, 3, 0, Z) ,"& " 3 (BC_2, * , control, 0) ,"& " 4 (BC_1, WRRW , input, X) ,"& " 5 (BC_1, RDDS , input, X) ,"& " 6 (BC_1, CS , input, X) ,"& " 7 (BC_1, BIS1 , input, X) ,"& " 8 (BC_1, BIS0 , input, X) ,"& " 9 (BC_1, BTS , input, X) ,"& " 10 (BC_1, THZE , input, X) ,"& " 11 (BC_1, TMODE1 , input, X) ,"& " 12 (BC_1, TMODE2 , input, X) ,"& " 13 (BC_1, PLL_CLK , output2, X) ,"& " 14 (BC_7, INT , bidir, 0, 15, 0, Z) ,"& " 15 (BC_2, * , control, 0) ,"& " 16 (BC_1, TSTRST , input, X) ,"& " 17 (BC_1, RLOS , output2, X) ,"& " 18 (BC_1, TCSS1 , input, X) ,"& " 19 (BC_1, RLOF , output2, X) ,"& " 20 (BC_1, RAIS , output2, X) ,"& " 21 (BC_1, RSER , output2, X) ,"& " 22 (BC_1, OUT400 , output2, X) ,"& " 23 (BC_1, RSYNC , output2, X) ,"& " 24 (BC_1, RCLK , output2, X) ,"& " 25 (BC_7, TSYNC , bidir, 0, 26, 0, Z) ,"& " 26 (BC_2, * , control, 0) ,"& " 27 (BC_1, TSER , input, X) ,"& " 28 (BC_1, TPOSO , output2, X) ,"& " 29 (BC_1, TNEGO , output2, X) ,"& " 30 (BC_1, TCLKO , output2, X) ,"& " 31 (BC_1, TCLK , input, X) ,"& " 32 (BC_1, ALE_A7 , input, X) ,"& " 33 (BC_1, A6 , input, X) ,"& " 34 (BC_1, A5 , input, X) ,"& " 35 (BC_1, A4 , input, X) ,"& " 36 (BC_1, A3 , input, X) ,"& " 37 (BC_1, A2 , input, X) ,"& " 38 (BC_1, A1 , input, X) ,"& " 39 (BC_1, A0 , input, X) ,"& " 40 (BC_7, AD7 , bidir, 0, 1 , 0, Z) ,"& " 41 (BC_7, AD6 , bidir, 0, 1 , 0, Z) ,"& " 42 (BC_7, AD5 , bidir, 0, 1 , 0, Z) ,"& " 43 (BC_7, AD4 , bidir, 0, 1 , 0, Z) ,"& " 44 (BC_7, AD3 , bidir, 0, 1 , 0, Z) ,"& " 45 (BC_7, AD2 , bidir, 0, 1 , 0, Z) "; end DS26503_top;