MAX-ECG-MONITOR

可穿戴ECG和心脏监测仪评估和开发平台


点击查看特定型号的库存状况。

说明

MAX-ECG-MONITOR评估和开发平台具有MAX30003临床级AFE,分析数据和准确跟踪心脏信号(ECG和心率),以及用户状态信号,例如温度和运动,为临床和健身应用提供非常宝贵的洞察力。利用嵌入式算法快速开发基于ECG的应用,或者利用其收集原始数据,从而开发自己的定制健康传感器算法。作为Movesense生态系统的一部分,MAX-ECG-MONITOR运行开放式应用程序编程接口(API),用于为各种基于ECG的用例开发独特的设备内app,显示休息或高运动活动期间的心率信号。

MAX-ECG-MONITOR与Android® OS设备配合,显示各个传感器的实时测量数据;平台也捕获来自于健康传感器信号的原始数据并进行储存,从而允许完全访问定制开发用例的结果和汇总。

MAX-ECG-MONITOR配有带固件的ECG/心率监测仪参考设计模块、胸带,以及适用于健身应用的干电极和适用于临床应用的湿电极。平台包括关于下载Android应用的说明。

下载应用 ›

MAX-ECG-MONITOR MAX-ECG-MONITOR 放大+

关键特性

  • 临床级ECG和心率测量及分析,基于MAX30003超低功耗Power ECG AFE,带有HR检测算法
  • 开放API,支持为基于ECG的用例开发独特的设备应用
  • 附加板载传感器,包括加速度计、陀螺仪和磁力计

应用

  • 运动强度检测
  • 内置健身和健康监测的服装
  • 健身监测胸带
  • 医用心率信号贴片

技术资料

设计指南 6778 How To Measure Biopotential ECG Using a Chest Strap Tutorial
用户指南 6732 Maxim ECG Monitor User's Guide

质量和环境数据

申请可靠性报告: MAX-ECG-MONITOR 
无铅封装的锡(Sn)晶须报告

其它资源

Software

Download the application ›

Quick Start Guide for the MAX-ECG-MONITOR

What You Need

  • MAX-ECG-MONITOR
  • Chest strap or adhesive electrodes (both provided)
  • Android® device (e.g., phone, tablet, etc.) with Bluetooth connection for data logging

Power On/Off
The MAX-ECG-MONITOR turns on automatically when it detects a heartbeat through the electrodes. A red LED flashes on the top of the monitor to indicate that it is on.

The monitor automatically powers off when no heartbeat is detected across the electrodes (for example, when the device is not worn).

Wearing the ECG Monitor

  1. Snap the monitor into the chest strap connector.
  2. Moisten the strap electrode areas with water or electrode gel.
  3. Adjust the strap length to fit tightly but comfortably around your chest below the chest muscles with the Maxim logo facing out.
  4. Ensure the moist electrode areas are firmly pressed against your skin
  5. For applications where more secured mounting is desired, use the adhesive electrodes (red) instead of the chest strap. NOTE: Detach the monitor and rinse the chest strap under running water after every use. Dry the strap and electrodes. Sweat and moisture left on the electrodes can keep the device on unnecessarily and reduce battery life.

NOTE: The adhesive electrodes are for single-time use and may be left on the skin up to a few days. More supplies can be ordered from www.maximintegrated.com.

Movesense® Showcase App
The ECG monitor can be paired with an Android-based device, such as phone or tablet, for viewing and logging data through the Movesense Showcase app for Android.

Installing the App

  1. Save the provided .apk-file to a location that you can access by phone (for example, to the phone's storage if you have a file browser or to Dropbox®).
  2. Open the file, which prompts you to install the Movesense Showcase app. The main screen of the app is shown below.

    Movesense Showcase main screen. Figure 1. Movesense Showcase main screen.

Connecting to an ECG Monitor

  1. To connect the MoveSense app to an ECG monitor, press the Movesense icon in the app—devices available for Bluetooth® connection are then displayed (see figure below).

    ECG monitors available for connection. Figure 2. ECG monitors available for connection.

  2. Click on the appropriate monitor to connect. The connection can take 10 seconds to 30 seconds to establish.

Using the App

Sensor Measurements
After a successful connection, a list appears to show all the measurement applications that are available.

  1. Scroll down the screen to reveal a complete list (see figures below, result split in two images).

    List of sensors. List of sensors.
    Figure 3. List of sensors.

  2. Select the desired measurement application.

    For example, click on the ECG item to bring up the ECG measurement screen (see figure below).

    Inactive ECG measurement application. Figure 4. Inactive ECG measurement application.

  3. Activate the measurement application by sliding the Subscribe button to the right.

    In this example, the button becomes blue and the ECG chart is displayed at the bottom of the screen (see figure below). Data is logged into a file called *_EcgActivityGraphView.csv in the local MoveSense folder.

    Activated ECG measurement application. Figure 5. Activated ECG measurement application.

Other measurements include heart rate, temperature, and motion sensing. Refer to the "Maxim ECG Monitor User's Guide" for a complete description of each available measurement.

Battery
The monitor uses a 3V lithium cell battery (CR 2025). Refer to the user's manual for instructions to replace the battery.

Got a Wearable Health Design Idea? Here’s How to Make It Accurate

Summertime Fun Outside the Classroom


型号   生产流程   工艺   样本量   不合格   FIT @ 25°C   FIT @ 55°C  

备注: 通过技术手段对故障率进行汇总,并映射到相关的材料部件号。 故障率与被测件的数量密切相关。

质量管理体系 >
环境管理体系 >

 
Status:
Package:
Temperature:

相关资料


MAXM86161
单电源、集成光模块,用于HR和SpO2测量

  • 完备的单通道、光学数据采集系统
  • 内置算法进一步增强抑制快速环境瞬态
  • 结构针对反射心率和SpO2监测进行了优化

MAX30208
±0.1°C精度、I2C接口数字温度传感器

  • 高准确度、高精度
  • 低功耗
  • 小尺寸