电子工程术语和定义,以字母H打头

0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ
H 亨:电感单位。
H-Bridge 一种类似于字母“H”的电路形式。其中负载水平连接在两对交叉线路之间。常用于直流电机驱动系统,利用位于“H”桥的“垂直”分支上的开关控制电流方向,从而改变电机转子的方向。
Half-Duplex 电路能够进行双向数据传输,但不是同时进行。
Half-Flash 一种ADC结构,它先用一组比较器量化产生高数字位,再用数/模转换器(DAC)从输入减去该电压,然后再将余下的输入进行量化,获得低数字位。另请参考应用笔记748:ADC中的ABC
Half-Wave Rectifier

A half-wave rectifier converts an AC signal to DC by passing either the negative or positive half-cycle of the waveform and blocking the other. Half-wave rectifiers can be easily constructed using only one diode, but are less efficient than full-wave rectifiers.

Since diodes only carry current in one direction, they can serve as a simple half-wave rectifier. Only passing half of an AC current causes irregularities, so a capacitor is usually used to smooth out the rectified signal before it can be usable.

Half-wave rectifier circuit with capacitor filter and a single diode.

Half-wave rectifier circuit with capacitor filter and a single diode.

Half-wave and full-wave rectifiers

Alternating current (AC) periodically changes direction, and a rectifier converts this signal to a direct current (DC), which only flows in one direction. A half-wave rectifier does this by removing half of the signal. A full-wave rectifier converts the full input waveform to one of constant polarity by reversing the direction of current flow in one half-cycle. One example configuration for full-wave rectification is the full bridge rectifier, which uses four diodes to create a pulsating DC output.

Half-wave and full-wave rectifier waveforms

A half-wave rectifier creates a purely positive signal by blocking the negative half-cycle, while a full-wave rectifier does this by changing the direction of the negative half-cycle.

What is the efficiency of a half-wave rectifier?

Since only half of the input waveform is passed, the efficiency of a half-wave rectifier is lower than that of a full-wave rectifier. The maximum efficiency of a half-wave rectifier is about 40.5%, and the maximum efficiency of a full-wave rectifier is twice that.

Handover 在无线蜂窝网络中将正在进行的呼叫切换到不同信道或单元,亦称为“越区切换”。
Harmonic Distortion 指在器件输入信号中并不存在,但出现在器件输出的频率成份。削波是产生谐波的常见原因,另外,非线性失真也会产生谐波。
HART 高速可寻址远程传感器(HART)通信协议通常用于数字信号传输,数字信号叠加在4-20mA电流环的模拟信号上。

HART协议采用频移键控(FSK)技术,数字“0”调制为2200Hz正弦信号,数字“1”调制为1200Hz正弦信号,波特率为1200bps。这两个频率信号可以很容易地叠加到模拟电流环的信号(频率范围通常在DC至10Hz)上,两者不会相互影响。HART协议的特点在于通过同一线路同时传输模拟和数字信号。

HAST 强加速应力测试;强加速蒸发及温度。
HB LED 高亮度LED是新一代LED照明方案,为各种应用提供足够的照明亮度,例如:如汽车内部/外部、显示器、室内与建筑物照明、任务操作与普通照明、投影仪显示器、背光显示和信号灯等。

请参考:高亮度LED (HB LED)驱动方案
HBT 异质结双极晶体管。
HD 谐波失真。
HD2 请参考:二次谐波失真
HDLC 高级数据链路控制:一种用于点到点及多点通信的ITU-TSS链路层协议。
HDLC Controller 请参考:HDLC
HDSL 高速率数字用户链路:一种早期的DSL技术,电话公司仍使用它以1.5Mbps配置T1线路,需要两对双绞线。
HDTV 高清晰度电视:用于传输电视信号的全数字系统,分辨率远远高于传统的模拟标准(PAL、NTSC及SECAM)。高清晰度电视机可显示多种分辨率(与普通电视机的36万像素相比,其分辨率高达两百万像素)。HDTV还具有改善色编码以及无损耗重现数字技术等优势。
Heat Sink 为发热电子部件提供热传导的机械装置,用于器件散热。大多数散热器为铝制品,利用片状结构增大表面积,提高热量向周围环境散发的能力。
Heating-Ventilation-Air Conditioning 请参考:HVAC
heatsink 请参考:散热
HEMT 高电子迁移率晶体管。
Hertz 请参考:Hz
HF 高频。
HGLL 高增益、低线性。
Hi-Z 高阻表示没有任何驱动的输出信号状态,该信号处于开路状态,由此,其它输出引脚(例如,总线上的其它器件)可以驱动该信号,或者可以由无源器件(通常为上拉电阻)确定信号电平。
High Bit-Rate Digital Subscriber Line 请参考:HDSL
high impedance 请参考:高阻
High-Brightness LED 请参考:HB LED
High-Definition Television 请参考:HDTV
High-Side 通常指连接于电源与负载之间的元件。高边电流检测系统通过测量电源和负载之间电阻两端的压降检测电流。
High-Speed Downlink Packet Access 请参考:HSDPA
High-Speed Packet Access 请参考:HSPA
High-Speed Serial Interface 请参考:HSSI
High-Speed Uplink Packet Access 请参考:HSUPA
High-Z 请参考:高阻
Home RF 家用射频的商标名称,利用天线、发射机传送无线信号,提供家庭联网技术。
Home-Rf 请参考:Home RF
HomePlug HomePlug (PowerLine)是一种通过电力线传输数据的工业标准,可传输音频、视频及控制信号等。HomePlug是家庭插电联盟(HomePlug Powerline Alliance)的商标,电力线是这一通信方式中的常见术语。

请参考:电力线产品网页

PLC是电力线通信的首字母缩写。
HomeRF 请参考:Home RF
hot carrier diode 请参考:肖特基二极管
Hot-Swap 一种电源线控制器,它允许在系统带电时插拔或更换电路板或其它器件。热插拔器件一般能够在出现过压、欠压或浪涌电流时为系统提供保护,防止故障、误操作及硬件损坏。
HotSwap 请参考:热插拔
HP-IB 请参考:GPIB
HR 高可靠性。
HSDPA 高速下行分组接入(HSDPA)是HSPA针对无线和蜂窝手机或数据卡应用的3G无线接口标准,用于提高当前UMTS标准的数据速率、改善通信业务量。
HSPA 高速分组接入(HSPA)汇集了无线和蜂窝手机或数据卡应用的无线接口标准,用于提高当前UMTS标准的数据速率、改善通信业务量。
HSSI 高速串行接口:一种数据速率为2Mbps至52Mbps的短距离通信标准。
HSUPA 高速上行分组接入(HSUPA)是HSPA针对无线和蜂窝手机或数据卡应用的3G无线接口标准,用于提高当前UMTS标准的数据速率、改善通信业务量。
HTML 超文本链接标识语言:用于创建网页的编程语言。
HTS 高温半导体。
HTTP 超文本传送/传输协议。
Human Body Model 一种ESD测试方法,其中ESD发生器由一个100pF电容及一个1.5kΩ的串联电阻组成。

参考下列应用笔记,这些应用笔记讨论了ESD的产生和对电子系统的危害,以及人体模型、机械模型的测试,IEC兼容性、设计方案等内容。

HVAC 加热、通风及空气调节:工业术语,在建筑物内负责加热、通风和空气调节的系统或设备,HVAC系统的目标是达到舒适(温度和湿度)、高空气质量的环境,并节省能源。

Hz 赫兹:频率单位,表示每秒周期数或cps。