电子工程术语和定义,以字母C打头

0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ
C 1. 电容、电容器。

2. 库仑。

3. 视频信号的颜色分量(另请参考“Y/C”定义)。

C/N 载波噪声比。
C13 connector 请参考:IEC
C14 connector 请参考:IEC
CA 共阳极。
Cable 请参考:CATV
Cable Television 请参考:CATV
Cable TV 请参考:CATV
CAD 计算机辅助设计。
CAN 控制器局域网。CAN协议是由ISO 11898定义的国际标准。
capacitance 请参考:电容
Capacitance

What is Capacitance?

Capacitance is the amount of charge that can be stored at a given voltage by an electrical component called a capacitor. The unit of capacitance is the Farad (F) and a 1F capacitor charged to 1V will hold one Coulomb of charge. A capacitor is a passive electronic component that consists of two conductive plates separated by an insulating material called a dielectric. A voltage applied to the plates creates an electric field across the dielectric, which causes the plates to accumulate a charge. The charge remains after the voltage source is removed, allowing energy to be stored until the capacitor is discharged (allowing the stored energy to perform work).

What are the factors that affect capacitance?

The size of the conductive plates and the permittivity of the insulating dielectric material determine capacitance.

What is the effect of capacitance?

The larger the capacitance of a capacitor, the longer it takes to charge and discharge. This means it takes more time for voltage to build up (charge) or fall (discharge). This makes capacitance useful for filtering out small voltage variations that last only a short length of time, i.e., high-frequency transients.

What is parasitic capacitance and why is it important in electronic circuits?

Unintended (parasitic) capacitance exists between any two conducting materials – the closer their proximity and size, the greater the value. This must be factored into the design of a circuit as it can affect the speed at which it operates. For example, a large transistor may allow faster switching, but its larger size means a larger parasitic capacitance exists between its terminals and this may slow the speed of the circuit driving it.

How is capacitance measured?

Capacitance is measured using a capacitance meter. A 1F capacitor would be quite big – the size of a small bottle. For this reason, capacitance values used in electronic circuits are in the microfarad to nanofarad range.

Learn more: How to build a DC-DC Power Supply - Tutorial

Capacitive Crosstalk 信号从一条传输线/引线通过电容耦合至相邻传输线/引线的现象。
Capacitive Voltage Regulator 请参考:电荷泵
capacitor 请参考:Capacitance
Capacitor 电容是一种无源电子元件,由两个电极及其间的介电材料构成。在电极上施加电压会在电介质两侧产生电场,导致电极累计电荷。移除电源后,电场和电荷在放电之前保持不变,存储电能。

电容(或C,单位为法拉),表示给定电压下存储电荷的数量(一法拉电容充电至一伏特电压时将保存一库仑电荷)。

Capacitor Charge Pumps 请参考:电荷泵
CardBus PC卡的32位版标准(以前称为PCMCIA)。
Carrier-free 请参考:UWB
CAS 列地址选通:通知DRAM接受选定地址为列地址的信号,与RAS及行地址配合可选择DRAM的某一位。
CAT 3 请参考:CAT3
cat 5 请参考:CAT5
CAT3 3类:表示以太网电缆,符合EIA/TIA-568的第三类标准,允许高达10Mbps的数据传输速率。
CAT5 5类:表示以太网电缆,符合EIA/TIA-568的第五类标准,允许高达100Mbps的数据传输速率。
Category 3 请参考:CAT3
Category 5 请参考:CAT5
CATV 最初称为“共用天线电视”,现在指任何一种通过电缆分配的有线电视系统。
CBR 固定比特率。
CC/CV Charger 恒定电流/恒定电压电池充电器。
CCCv 恒流/恒压。
CCD 电荷耦合器件:数码相机使用的两种主要图像传感器的一种。拍摄照片时,CCD被通过相机镜头的光线感光。数千甚至数百万个微小像素通过CCD将光信号转换成电子。先测量每个像素的累积电荷,然后再将其转换为数字量,最后一步在CCD以外的模数转换器(ADC)中完成。
CCFL 冷阴极荧光灯:常用作LCD显示器的背光。
CCFLs 请参考:CCFL
CCFT 冷阴极荧光管:常用作LCD显示器的背光。
CCK 补码键控。
CCM 连续传导模式,交叉连接模块。
CDC 时钟分配电路。
CDD 时钟分配器件或时钟分配驱动器。
CDF-AEC-Q100 请参考:AEC-Q100
CDIP 请参考:DIP
CDMA 码分多址:一种采用扩频技术的蜂窝电话体制。与GSM或其他采用TDMA的系统不同,CDMA并不为每个用户都分配一个指定频率,每一信道都能使用整个可用频谱。每路语音信号采用伪随机序列编码。
CDR 时钟/数据恢复。
CE Control 芯片使能控制。
CE Gating 请参考:芯片使能选通
Cell-Site 请参考:BTS
centimeter 请参考:cm
centimetre 请参考:cm
CH 切比雪夫(滤波器)。
Ch. to Ch. Skew (Ps Max) 信道至信道偏移。同一信号在不同信道的相位差(延时/偏移)。以ps (最大值)为单位进行测量。
Channel Associated Signaling 随路信令(CAS):一些包括“信令”功能伴随数据的通信协议。随路信令协议的每个数据信道有一种信令方式(与之相对的是专用信令信道)。

亦称为强取比特信令。
Chans. 信道。
Charge Coupled Device 请参考:CCD
Charge Injection 与模拟开关相关的参数。随着模拟开关的打开或关断,少量电荷可从数字控制线上通过电容耦合至模拟信号通路。
Charge Pump 一种用电容储能并将能量传送到输出的电源,可以提升或降低电源电压。电荷在调节器和开关电路的控制下从一个电容转移到另一个电容。

Maxim提供稳压型或非稳压型两种电荷泵,以及内置电荷泵的IC,用于提升内部电压。

请参考应用笔记2031:DC-DC Converter Tutorial及应用笔记660:"Regulator topologies for battery-powered systems"。
Charge Termination Method 电池充电器用来确定终止充电的方法。
CHATEAU 信道化T1、E1及通用HDLC控制器。
Chip 1. 集成电路:包含了众多晶体管和其它元件,并且相互连接在单片半导体材料上的半导体器件。

2. 码:用于直序扩频系统。
Chip-Enable Gating 一种微处理器监控功能,可防止在电源低于规定电压时错误地写入数据。当主电源电压低于最小安全工作门限时,该电路从主微处理器或微控制器断开芯片使能信号通道。
Chipping Rate 请参考:Mcps
chroma 请参考:彩色副载波
Chrominance 复合视频信号的彩色分量,与亮度分量组合后构成完整的图像信号。
CID 连续相同数字。
CIM 电缆完整性监视器。
Circuit Board 请参考:印制电路板
Circuit Simulator

Circuit Simulator

A circuit simulator is a piece of software that emulates the behavior of a real hardware circuit before it is built. The circuit simulator can be used to verify that a hardware design is behaving correctly and producing the desired output signal for a specified set of inputs. The reliability of the tool depends on the creation of accurate mathematical models that describe the behavior of the circuit components in multiple variable scenarios including component tolerances, temperature and supply voltage.

What Design Tools Does Maxim Have?

Our portfolio of design tools provides you with the assistance you need to simplify and shorten your design process. These design tools help in multiple tasks, from IC selection to circuit design, analysis, and validation to BOM delivery and PCB layout. These include advanced system and sub-system level integrated circuit design tools such as the EE-Sim® design and simulation environment and the OASIS offline simulator.

What Can These Circuit Simulation Tools Do?

These tools include a portfolio of power devices available to design and simulate. You can quickly recalculate compensation after component changes, set component derating values, and perform efficiency calculations. They provide the flexibility to simulate user defined line transients as well as AC and steady-state conditions for user defined line and load settings. Other useful features include the ability to compare two designs, create custom user plots and reports, while schematics, plots and bill-of-materials can be exported in multiple file formats. Additional resources can be found in the form of product selectors, online calculators, SPICE models, IBIS models and CAD files.

Learn MoreDesign Tools

CISC 复杂指令集计算机(CISC):计算机硬件设计用于支持复杂指令,与RISC (精简指令集计算机)架构相反。
Class 请参考:放大器类
Class A A类放大器是最简单的放大器类型,对于任何输出波形,其输出级的晶体管始终处于导通状态(不会完全关断)。这类放大器具有极佳的线性特性,但效率很低。
Class AB AB类放大器结合了A类放大器和B类放大器结构,其效率高于A类放大器,失真低于B类放大器。

通过对电路中的两个晶体管进行偏置,使信号接近零(B类放大器引入非线性的工作点)时两个晶体管导通;大信号时,晶体管转换到B类工作方式。

由此可见,小信号时两个晶体管均保持有效工作,类似于A类放大器;大信号时,相应于波形的每半周,只有一个晶体管保持有效状态,类似于B类放大器。

Class B B类放大器的输出级晶体管只在信号波形的半个周期(180度)导通,为了对整个信号进行放大使用了两个晶体管,一个用于正输出信号,另一个用于负输出信号。

B类放大器的效率远远高于A类放大器,但由于两个晶体管从通到断过程中存在交越点,失真较大。

Class C C类放大器采用开关放大器架构,其晶体管的导通时间低于周期的一半(180度以下) -- 通常还会更低。例如:晶体管可能只在信号发生偏移的开始10%导通,只输出一个脉冲信号。

由于晶体管在绝大多数时间处于关断状态,打开时处于完全导通状态,因此,C类放大器的效率非常高。同时也会产生很大的失真,常见于RF电路,这类应用中利用谐振电路恢复原始信号以减小失真。C类放大器还可用于对失真度要求不高的低保真系统,例如警笛的扬声器驱动器。

Class D D类放大器的输出为开关波形,开关频率远远高于需要恢复的音频信号的最高频率。经过低通滤波后,输出波形的平均值与实际的音频信号保持一致。

由于工作时输出级晶体管处于完全导通或完全关断状态,不会进入晶体管的线性工作区(这是导致其它类型放大器低效的原因),D类放大器具有极高效率(高达90%,甚至更高)。现代D类放大器可以达到与AB类放大器同等级别的保真度。

Class G G类放大器与AB类放大器相同,但它采用了两路或更多的供电电源。工作在小信号电平时,放大器采用较低的电源电压供电。随着信号电平的提升,放大器自动切换到适当的电源电压。

由于只在必要时采用高压供电,而AB类放大器则始终采用高压供电,G类放大器的效率高于AB类放大器。

Class H H类放大器对放大器输出级电路的电源电压进行调整,使其不会高于所要支持的信号摆幅。这有助于降低与该电源相连的输出电路的功耗,使放大器在任何输出功率下工作在AB类放大器的最高效率。

H类放大器的设计比其它放大器复杂,需要额外的控制电路来预测、控制电源电压。

click 请参考:喀嗒声
Click-and-Pop “喀哒”声与“劈啪”声是指音频设备在以下情况下时,耳机和/或扬声器产生的令人反感的瞬间信号,这些信号处于音频波段:
  • 上电(接通电源)
  • 掉电(断开电源)
  • 退出关断状态(事先已接通电源)
  • 强制关断(未断开电源)
Click/Pop Reduction 一种在上电、关机、连接等过程中抑制“喀哒”声和“劈啪”声 ― 不希望出现的瞬态噪声的功能。
Clock and Data Recovery 从单线/通道、串行数据流中提取并重建时钟与数据信息的过程。
Clock Distribution Device 请参考:CDD
Clock Distribution Driver 请参考:CDD
Clock Jitter 通常希望一个周期性波形(特别是时钟)跨过特定门限的时间非常精确,与该理想值的偏差称为抖动。

更多信息和详细说明,请参考:

Clock Recovery 请参考:时钟及数据恢复
Clock Recovery Data 请参考:时钟及数据恢复
Clock Reduction 请参考:时钟降频
Clock Throttling 一种通常为减少器件发热而降低IC时钟频率或占空比的方法。
Clock Timing

Electronic devices perform tasks in response to the periodic oscillation of an electrically varying digital voltage that acts as a clock timing signal. On the other hand, human time (also known as “real” time) is measured in seconds, minutes, hours, days, months, and years as dictated by the rotational cycles of the earth. For electronic devices, such as a smart watch, to perform their tasks when required by a user, they must store a digital representation of real time, which is then kept in sync by the digital clock timing signal. In an electronic device, clock timing information is maintained by its Real Time Clock (RTC) circuitry. This will usually be located within the device microcontroller or may be a separate IC on the system board

 real time clock timing

Figure 1 Clock timing can be provided by a discrete RTC IC on a system board

Why Use an RTC?

If the main power source for an electronic device fails, then real-time clock timing information will be lost and will need to be reset once power has been restored. While many portable IoT devices have the functionality to reset the time using a wireless connection to a remote master, 2 this type of communication places an extra power drain on the battery (and obviously can only occur if a wireless signal is available). In the absence of a wireless signal, the only (and clearly less desirable) alternative is for the user to manually reset the time, which may not be always straightforward or even possible. An RTC circuit allows a system to keep track of real time long after a main power failure.

Where Are RTCs Used?

Clock timing is important in many different applications, such as industrial (utility meters, point-of-sale equipment, fire alarms, gaming machines, video security), consumer (digital cameras, portable GPS devices, mobile game devices, satellite receivers, TVs) as well as in portable and home medical equipment.

How Does an RTC Keep Time?

A 32.768kHz quartz tuning-fork crystal oscillator is the standard clock timing reference for most electronic applications. The real-time clock maintains timing and date information by counting seconds, which requires a 1Hz clock signal derived from the 32.768kHz crystal oscillator. The time and date information are stored in a set of registers, which is accessed through a communication interface, such as I2C. The crystal may be external to the RTC or integrated within the same package. For applications requiring higher accuracy, an integrated MEMS (microelectromechanical system) resonator is used as the clock timing reference.

Related Pages:

cm 厘米:1/100米,0.39英寸。
CMF 电流模式反馈。
CMI 插入矩阵编码。
CML 电流模逻辑。
CMOS 互补型金属氧化物半导体技术,采用p沟道和n沟道MOS晶体管对儿实现。
CMR 请参考:CMRR
CMRR 共模抑制比:差分放大器抑制同相和反相输入端共模信号的能力。

请参考设计讲座:Understanding Common-Mode Signals
CMVR 请参考:输入CMVR (V)
CNC 计算机数字控制。
CO 粗调。
Code Division Multiple Access 请参考:CDMA
CODEC 压缩/解压缩编解码的缩写,代表任何一种数据压缩或解压缩技术。codec可以用软件、硬件或两者组合实现。
COG 玻璃衬底芯片。
Coherent Sampling 即周期信号取样,其中信号周期的整数倍与预先确定的取样窗口相匹配。
COLC 校准环路电容。
Cold Cathode Fluorescent Lighting 请参考:CCFL
Cold Cathode Fluorescent Tube 请参考:CCFT
color signal 请参考:彩色信号
Color Subcarrier 一种调制载波,添加到电视信号内,用于承载彩色成份。

例如:在NTSC电视中,3.579545MHz彩色副载波通过两个彩色差分信号正交调制,并加入亮度信号。PAL电视标准采用4.43362MHz的副载波频率。

请参考: Video Basics

Column-Address-Strobe 请参考:CAS
Common Mode Rejection Ratio 请参考:CMRR
Common-Mode 请参考:共模信号
Common-Mode Signals 共模信号是作用在差分放大器或仪表放大器同相、反相输入端的相同信号。例如,平衡线对中引入到两个平衡端的噪声电压。另外一个例子是加在平衡线上的直流电压(例如:由于信号源与接收器之间的地电位差而产生的直流电平)。

对于理想的差分放大器,可以完全消除共模信号输出,这是由于差分输入(同相和反相)抵消掉了相同的输入成分。衡量这一特性的参数称为共模抑制比或CMRR。

请参考设计讲座:Understanding Common-Mode Signals
comp 请参考:比较器
Comp. Prop. Delay 比较器传输延时,是输入超过比较器阀值与输出状态改变之间的延时。
compander 信号处理技术通过数据压缩和扩展改善动态范围和信噪比。

信号在传输前需要进行非线性变换,在接收端进行逆变换。放大小信号、衰减大信号。由于小信号被放大,与传输通道相比降低了噪声。

用于数字、PCM、数据传输以及模拟系统。Dolby是常见的基于压缩扩展的降噪系统。
companding 请参考:压缩扩展器
Comparator 比较器的功能是接受两路模拟信号输入、通过比较输入产生一路二进制输出信号, 表示哪一路输入电压较高。如果同相端(+)输入高于反相端(-)输入,输出为高电平;如果反相端(-)输入高于同相端(+)输入,输出为低电平。

从一定意义上讲,比较器类似于一个1位ADC。

没有负反馈环路的运算放大器既是一个简单的比较器。较高的电压增益能够使其分辨出极小的输入电压之差。但是,运算放大器的这种应用速率很低,而且缺少一些特殊功能,例如:滞回、内部基准等。

应用笔记886: 比较器的合理选择详细介绍了比较器的工作原理、性能指标、共同特性, 以及如何为您的设计选择最合适的比较器。
complementary 请参考:推挽
Complete Central Office Line Interface 中心局线:电话线。
Complex instruction set computer 请参考:CISC
CompoNet CompoNet是4线制工业总线,采用主从架构。用于较低等级的网络,例如传感器和激励的通信,发送数据位或字信息。总线可支持最多256个从机,数据速率为93.75kbps至4Mbps,网络传输线长度可达1500米,可能需要使用中继器。底层协议采用CIP。
Constant Current Constant Voltage 请参考:CC/CV充电器
Contact Bounce 当机械开关或继电器闭合时,开关单元通常会发生反弹,当然,这个动作只出现在开关最终接通之前的瞬间。如果后续电路对开关的瞬态动作比较敏感的话,则需考虑解决这一问题。利用开关去抖电路可以消除瞬态影响。
Contact Discharge 一种ESD (静电放电)测试方法,其中ESD发生器与被测器件(DUT)直接连接。
Controller 请参考:DC-DC控制器
Controller Area Network 请参考:CAN
Coplanar Line 表示一些位于同一平面上的线,其中任何两条相交线均处于同一平面 — 即共面。
Coulomb 库仑(简称C)是电荷的标准计量单位。

以查利·奥古斯丁·库仑的名字而命名,表示一法拉电容充电至一伏特时所累计的电荷数;或者一安培电流在一秒钟内传输的电荷数。

Coulomb Counter 请参考:电池电量计
Coulomb Counting 请参考:电池电量计
CP 可比较部分。
CPGA 陶瓷引脚栅格阵列,一种IC封装技术。
cps 请参考:Hz
CPU Throttling 请参考:时钟降频
CR 请参考:锂电池
CRC 循环冗余码校验:一种经过数据计算、用来捕捉传输误码的校验值。译码器计算接收数据的CRC并将其与编码器计算的CRC (附于数据之后)进行比较,如果二者不匹配则表明数据在传输时被破坏。根据算法及CRC码的比特数,可得出包含足够的用来校准数据的冗余信息。
CRIL 命令寄存器与接口逻辑。
Cross Talk 请参考:电容性串扰
Crossover 在输出级(或类似的放大级,用一个器件上拉信号、另一个器件下拉信号),高边器件打开、低边器件关闭(反之亦然)的区域。
Crosstalk 请参考:电容性串扰
Crowbar Circuit 撬棍电路是一种电源保护电路,当电压/电流超出限定范围时能够快速切断(“撬棍”)电源。实际应用中,短路将导致保险丝断开或触发其它保护,关闭电源。

可通过SCR、硅器件或其它机械短路装置实现。

该名称可能源于在大电流应用中用一段金属丝产生机械短路,或者是撬棍电路的I-V曲线。

请参考:保护与隔离产品
CRT 阴极射线管(CRT)显示设备利用电子束对磷光涂层的击打成像。电子束由真空玻璃管的一端发出,在静电场和/或电磁场的控制下,击打另一端的涂层使其发光(电子对磷光物质的击打),从而可以显示图像。
Cryptanalysis 一种破解密码的技术或学科。
CS 片选。
CSA 请参考:电流检测放大器
CSP 晶片级封装:一种用焊球取代引脚,使封装尺寸最小的IC封装技术。加热时焊球融化并与电路板上的焊盘焊接在一起。
CTIM 重试超时电容。
CTON 启动定时器电容。
current 请参考:安培
current controlled voltage source 请参考:互阻放大器
Current Mode Feedback 一种用于高速放大器的运放替代拓扑。对反馈阻抗敏感且不能用作积分器。
Current Mode PWM 请参考:电流模式控制器
Current Sensing 请参考:电流检测放大器
Current Sensor 请参考:电流检测放大器
Current-Mode Controller 一种在负载电流和输入电压变化下,能够通过逐周期地改变峰值电感电流调节其输出电压,最终得到稳定输出的直流-直流开关调节器。
Current-Sense Amplifier 通过测量电流通道上电阻的压降检测电流的放大器,电流检测放大器输出与被测电流成正比的电压或电流。
cycles 请参考:Hz
Cyclic Redundancy Check 请参考:CRC