关键词: energy measurement, power distribution units, PDUs 関連製品
用户指南 5473
78M6618 PDU1 Firmware Quick Start Guide
摘要 :The 78M6618 PDU1 Firmware is a turnkey energy measurement solution optimized for use in single-phase AC power distribution Units (PDUs). At the sensor interface, the 78M6618 with PDU1 Firmware provides eight sense inputs for current and two sense inputs for voltage (single-phase). At the host interface, either a UART or SPI interface can be used to issue configure the device and access the measurement data.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content,
contact us.