用户指南 5297

78M6613 Evaluation Board User Manual


摘要 : The Teridian™ 78M6613 Evaluation Board is an electrical measurement unit for performing measurements of up to two single-phase AC loads. It incorporates the 78M6613 power- and energy-measurement IC and connects to a PC through a USB cable such as the one provided in the demo kit. The Evaluation Board demonstrates the capability of the 78M6613 energy-meter controller chip for measurement accuracy and overall system use.

The board is preprogrammed with Firmware Demo Code (file name 6613_OMU_S2+2_URT_V1_1x.hex) in the flash memory of the 78M6613 IC that allows evaluation of the IC’s capabilities.