应用笔记 5507

Understanding the DS1WM Synthesizable 1-Wire Bus Master


摘要 :

Communication with 1-Wire® slave devices requires a 1-Wire master. There are numerous ways to build a 1-Wire master (see reference design 4206, "Choosing the Right 1-Wire Master for Embedded Applications"). This document describes the DS1WM, a synthesizable 1-Wire master that can be implemented in an application-specific integrated circuit (ASIC) or field-programmable gate array (FPGA). The free DS1WM IP is available by request at https://support.maximintegrated.com/1-Wire.


Introduction

With the growing popularity and diversity of 1-Wire devices, more engineers are facing the task of how to integrate a 1-Wire master into their systems. Reference design 4206, "Choosing the Right 1-Wire Master for Embedded Applications," describes various options. This document focuses on the DS1WM synthesizable 1-Wire bus master that can be implemented as a function block of an application-specific integrated circuit (ASIC) or field-programmable gate array (FPGA). The DS1WM core uses little chip area (~3470 gates plus two bond pads). It also generates the entire 1-Wire timing by hardware, reducing the initial software development time and cost. Thus the entire application software can be written in high-level language. Besides the 1-Wire communication signal DQ, the DS1WM also provides a control signal STPZ, which assists in meeting the power requirements of certain 1-Wire slaves and allows for large networks with many slaves or extensive cabling. Figure 1 shows the typical DS1WM application circuit. The DS1WM is available for free in both Verilog and VHDL formats.

Figure 1. The DS1WM typical application circuit.
Figure 1. The DS1WM typical application circuit.

Description

Similar to a memory device, the DS1WM connects to the user's system through an 8-bit data bus, using 3 address lines and the usual control signals (Figure 2). An internal divider chain converts any suitable system clock to a 1MHz signal, which in turn controls the 1-Wire timing. The DS1WM supports standard and overdrive 1-Wire communication in single-bit or byte mode, as well as modified timing for long line applications. The host interface and 1-Wire port signals are described in Table 1. Figures 3 to 5 and Table 2 specify the host interface waveforms and timing.

Figure 2. The DS1WM block diagram.
Figure 2. The DS1WM block diagram.

Table 1. Signal Descriptions

Name Type Function
MR I Master reset. Causes the DS1WM to perform an internal reset with the same result as a power-on reset. MR is not gated by %-overbar_pre%EN%-overbar_post%. The signal is recognized as active by any rising edge on the pin (no minimum duration requirement).
CLK I System clock signal. The clock-divider block converts this signal into a ~1.0MHz clock, which in turn controls the 1-Wire timing. The duty cycle should be approximately 50%. See the Clock Divisor Register description for the logically permissible CLK frequencies. The physically permissible upper limit depends on the characteristics of the ASIC/FPGA chosen for implementation.
A[2:0] I Address lines of the host interface to access the various memory-mapped device registers. See the Memory Map for register addresses.
%-overbar_pre_title%ADS%-overbar_post% I Active-low address strobe of the host interface. The state of the address lines A[2:0] is copied to an internal latch on the rising edge of the address strobe. See the Host Interface Timing diagrams (Figures 3, 4, and 5) for details.
%-overbar_pre_title%EN%-overbar_post% I Active-low general enable signal of the host interface. See the Host Interface Timing diagrams (Figures 3, 4, and 5) for details.
D[7:0] I/O Bidirectional data bus of the host interface, three-stated. The DS1WM drives these signals during the host read cycle (Figure 3). At all other times, these signals are in a high impedance state, allowing the host to communicate with other devices on the data bus.
%-overbar_pre_title%WR%-overbar_post% I Active-low write enable signal of the host interface. The state of the data bus D[7:0] is copied to the addressed register on the rising edge of the %-overbar_pre%WR%-overbar_post% signal. %-overbar_pre%WR%-overbar_post% should be inactive (high) unless the host wants to write to the DS1WM. See the Host Interface Timing diagrams (Figures 3 and 5) for details. If both %-overbar_pre%RD%-overbar_post% and %-overbar_pre%WR%-overbar_post% are active at the same time, %-overbar_pre%WR%-overbar_post% dominates.
%-overbar_pre_title%RD%-overbar_post% I Active-low read enable signal of the host interface. When active, the DS1WM puts the contents of the selected register on the data bus for the host to read. %-overbar_pre_sentence%RD%-overbar_post% should be inactive (high) unless the host wants to read from the DS1WM. See the Host Interface Timing diagram (Figure 4) for details. If both %-overbar_pre%RD%-overbar_post% and %-overbar_pre%WR%-overbar_post% are active at the same time, %-overbar_pre%WR%-overbar_post% dominates.
DQ I/O IO driver for the 1-Wire bus. This is an open-drain bidirectional port, which requires a pullup resistor to VCC. For the permissible pullup resistor range, refer to the data sheet of the 1-Wire slaves in the application. The minimum value also depends on the drive characteristics and logic thresholds of the ASIC/FPGA chosen for implementation.
STPZ O Active-low control signal for an external P-channel transistor to bypass the pullup resistor at certain times. See the Control Register description, bits STPEN and STP_SPLY, and the STPZ timing diagrams (Figures 10 to 13) for details.
INTR O Interrupt signal of the host interface. The power-on default polarity is active low, but can be changed to active high through the IAS bit in the Interrupt Enable Register. The INTR signal is inactive unless interrupts are enabled through the Interrupt Enable Register and a qualifying interrupt condition exists. For details see the Interrupt Register description. Reading the Interrupt Register changes the INTR signal to its inactive state.

Figure 3. Host interface write cycle.
Figure 3. Host interface write cycle.

Figure 4. Host interface read cycle.
Figure 4. Host interface read cycle.

Figure 5. Host interface timing, issuing a 1-Wire Reset.
Figure 5. Host interface timing, issuing a 1-Wire Reset.

Table 2. Host Interface Timing Specifications

Symbol Parameter Conditions Min Max Units
tADS Address strobe width Notes 1, 2 60   ns
tAH Address hold time Notes 1, 2 0   ns
tAR Address latch to read Notes 1, 2 60   ns
tAS Address setup time Notes 1, 2 60   ns
tAW Address latch to write Notes 1, 2 60   ns
tDH Data hold time Note 1 30   ns
tDS Data setup time Note 1 30   ns
tES Enable setup time Note 1 60   ns
tHZ RD to floating data delay Note 1 0 100 ns
tPDI Presence detect to INTR Note 1 0 100 ns
tRD RD strobe width Note 1 125   ns
tREN Enable hold time from RD Note 1 20   ns
tRVD Delay from RD to data Note 1   60 ns
tWEN Enable hold time from WR Note 1 20   ns
tWR WR strobe width Note 1 100   ns
tWRST WR high to reset Note 1 0 100 ns

Note 1: These values depend on the process used to realize the DS1WM. Values shown are for example purposes only.
Note 2: If %-overbar_pre%ADS%-overbar_post% is tied low, tAR and tAW are measured from tES. In this case, the falling edge of %-overbar_pre%RD%-overbar_post% or %-overbar_pre%WR%-overbar_post% must occur at least tES + tAR or tES + tAW after the falling edge of %-overbar_pre%EN%-overbar_post%.

The host processor communicates with the DS1WM through 6 registers, which are accessed through 3 address lines A[2:0]. Table 3 shows the memory map.

Table 3. Memory Map

Address A2 A1 A0 Access Description
00h 0 0 0 Write/read Command Register
01h 0 0 1 Write/read Transmit/Receive Buffer
02h 0 1 0 Read Interrupt Register
03h 0 1 1 Write/read Interrupt Enable Register
04h 1 0 0 Write/read Clock Divisor Register
05h 1 0 1 Write/read Control Register

Register Descriptions

Command Register
This register is accessed to generate a 1-Wire reset/presence-detect cycle and to activate or deactivate the Search ROM accelerator. In addition to these two functions, the Command Register contains 2 bits to control the DQ pin directly.

Command Register Bitmap

ADDR b7 b6 b5 b4 b3 b2 b1 b0
00h X X X X OW_IN FOW SRA 1WR
This register is read/write. The power-on default is 08h (OW_IN = 1). Bits 4 to 7 have no function; they always read 0 and cannot be set to 1.

Bit Description Definition
OW_IN: DQ Input (Read only)
Purpose: Reading the logic state of the DQ pin. Sampling takes place on every falling edge of the CLK signal.
Code: 1: The voltage at DQ is above VIHMIN (default).
0: The voltage at DQ is below VILMAX.
Conditions: This function is always enabled. OW_IN changes to 1 upon power-on reset or a master reset (MR pin).
Usage: In conjunction with FOW to perform 1-Wire communication beyond the 1-Wire Reset and 1-Wire Read/Write functions.
FOW: Force 1-Wire
Purpose: Directly driving the DQ pin under host timing control.
Code: 1: Activates DQ pulldown
0: Ends DQ pulldown (default)
Conditions: This function must be enabled by first writing the EN_FOW bit in the Control Register (address 05h) to 1. Otherwise, FOW has no effect. If both EN_FOW and FOW are 1, the 1-Wire Reset and the 1-Wire Transmit/Receive function (address 01h) have no effect. FOW returns to 0 upon power-on reset or master reset (MR pin). Changing EN_FLOW to 0 has the same effect as writing FOW to 0.
Usage: Generating DQ signaling beyond the 1-Wire Reset and 1-Wire Read/Write functions. To read from the 1-Wire bus, change FOW to 0, then wait as needed and read the OW_IN bit. As a safety precaution, if FOW is written to 1 while the STPZ signal is active (low), the STPZ signal immediately changes to inactive (high).
SRA: Search ROM Accelerator
Purpose: Activating the search ROM accelerator.
Code: 1: The search ROM accelerator is activated.
0: The search ROM accelerator is not activated (default).
Conditions: This function is always enabled. SRA returns to 0 upon a power-on reset, a master reset (MR pin), or when written to 0.
Usage: The search ROM accelerator saves time when executing the 1-Wire Search algorithm. See the Search Accelerator Operation section for more information.
1WR: 1-Wire Reset
Purpose: Generating a reset/presence detect sequence on the 1-Wire bus.
Code: 1: A reset/presence detect cycle is in progress.
0: The reset/presence detect cycle is completed (default).
Conditions: This function is always enabled. 1WR returns to 0 upon a power-on reset, a master reset (MR pin) or the completion of the 1-Wire reset/presence detect cycle. A 1-Wire reset/presence-detect cycle can be aborted by writing this bit to 0.
Usage: Writing this bit to 1 starts a 1-Wire reset/presence detect cycle and affects the PD and PDR bits in the Interrupt Register (address 02h).

Transmit/Receive Buffer

This is the location to which the host processor writes a data byte to be transmitted on the 1-Wire bus. If the 1-Wire slave is in a state to respond with data, the host writes a byte FFh to this register and then, after the byte is transmitted, reads this register again to retrieve that data sent by the 1-Wire slave.

ADDR b7 b6 b5 b4 b3 b2 b1 b0
01h Data7 Data6 Data5 Data4 Data3 Data2 Data1 Data0
This register is read/write. The power-on default is 00h.

Bit Description Definition
Data[7:0]: Transmit/Receive Data
Purpose: Providing data for transmission on the 1-Wire bus; accessing data received from 1-Wire bus.
Code: N/A
Conditions: 1-Wire communication can be performed in bit mode or in byte mode (default). In bit mode, only Data0 is relevant. Bit mode is selected by writing the BIT_CTL bit in the Control Register (address 05h) to 1. Data[7:0] returns to 00h upon a power-on reset or a master reset (MR pin).
Usage: General 1-Wire communication except for 1-Wire reset. The 1-Wire speed is selected by the OD bit in the Control Register (address 05h).

Interrupt Register

This register provides access to flags from current status, transmit, receive, and 1-Wire reset operations. All of these flags can generate an interrupt on the INTR pin if the corresponding enable bit is set in the Interrupt Enable Register. To clear the INTR signal, the Interrupt Register must be read. Reading the Interrupt Register always sets the INTR pin inactive even if not all flags are cleared.

Interrupt Register Bitmap

ADDR b7 b6 b5 b4 b3 b2 b1 b0
02h OW_LOW OW_SHORT RSRF RBF TEMT TBE PDR PD
This register is read only. The power-on default is 0Eh (TEMT, TBE, PDR = 1, PD = 0).

Bit Description Definition
OW_LOW: 1-Wire Event
Purpose: Signaling the arrival of a slave on the 1-Wire bus.
Code: 1: A slave has arrived.
0: No slave arrival since the last reading of the Interrupt Register (default).
Conditions: This function is always enabled. OW_LOW returns to 0 upon reading the Interrupt Register, a power-on reset or a master reset (MR pin).
Usage: A slave arriving on the idle bus (= no communication) generates a spontaneous presence pulse, which sets this bit. A short circuit on the idle bus also sets this bit.
OW_SHORT: 1-Wire Shorted
Purpose: Signaling a short circuit on the 1-Wire bus.
Code: 1: The 1-Wire bus is shorted.
0: The 1-Wire bus is in normal operating conditions (default).
Conditions: This function is always enabled. OW_SHORT returns to 0 upon reading the Interrupt Register, a power-on reset or a master reset (MR pin).
Usage: Prior to generating a 1-Wire reset or time slot, the DS1WM checks whether the 1-Wire bus is idle high. If the bus is low at that time, no communication can take place. This situation is signaled as a short circuit.
RSRF: Receive Shift Register Full
Purpose: Signaling the status of the Receive Shift Register.
Code: 1: The Receive Shift Register is full.
0: The Receive Shift Register is empty or receiving data (default).
Conditions: This function is always enabled. RSRF returns to 0 when the Receive Shift Register content is transferred to the Receive Buffer (address 01h) for the host to read, upon power-on reset, or a master reset (MR pin).
Usage: When the RSRF gets set and the RBF is not set (i.e., meaning the Receive Shift Register is full and the Receive Buffer flag is clear), the transfer takes place on the rising edge of the internal 1MHz clock.
RBF: Receive Buffer Full
Purpose: Signaling the status of the Receive Buffer.
Code: 1: There is new data in the Receive Buffer.
0: There is no new data in the Receive Buffer (default).
Conditions: This function is always enabled. RBF returns to 0 upon reading the Receive Buffer (address 01h), a power-on reset, or a master reset (MR pin). Reading the Interrupt Register without first having read the Receive Buffer triggers another interrupt if ERBF = 1 & RBF = 1.
Usage: Normal communication with 1-Wire slaves. If not using interrupts, poll the Interrupt Register to detect events. If using the RBF interrupt (ERBF = 1), read the Receive Buffer prior to reading the Interrupt Register.
The process to use the RBF flag looks like this:
  1. Write FF to the TX buffer and enable the TBE flag.
  2. Wait for the interrupt pin to trigger.
  3. When the interrupt occurs, read the interrupt register and confirm TBE set.
  4. Clear ETBE bit and now set the ETMT bit.
  5. Wait for the interrupt pin to trigger.
  6. When the interrupt occurs, read the interrupt register and confirm ETMT set.
  7. Clear the ETMT bit and now set the ERBF bit.
  8. Wait for the interrupt pin to trigger.
  9. When the interrupt occurs, read the interrupt register and confirm RBF set.
  10. Read the RX Buffer.
  11. Clear the ERBF after reading the RX Buffer.
TEMT: Transmit Shift Register Empty
Purpose: Signaling the status of the Transmit Shift Register.
Code: 1: The Transmit Shift Register is empty, ready for new data (default).
0: The Transmit Shift Register is busy sending data.
Conditions: This function is always enabled. TEMT returns to 0 when the Transmit Buffer content (address 01h) is transferred to the Transmit Shift Register. TEMT changes to 1 upon power-on reset or a master reset (MR pin).
Usage: The transfer takes place on the internal 1MHz clock as soon as the TBE is set.
TBE: Transmit Buffer Empty
Purpose: Signaling the status of the Transmit Buffer.
Code: 1: The Transmit Buffer is empty, ready for new data (default).
0: The Transmit Buffer is waiting for the Transmit Shift Register to finish sending data.
Conditions: This function is always enabled. TBE returns to 0 upon writing to Transmit Buffer (address 01h). TBE changes to 1 upon power-on reset or a master reset (MR pin).
Usage: Normal communication with 1-Wire slaves.
PDR: Presence Detect Result
Purpose: Signaling the result of the presence detect cycle.
Code: 1: No presence pulse was detected (default).
0: A presence pulse was detected.
Conditions: This function is always enabled. PDR changes to 1 upon power-on reset or a master reset (MR pin) or if no presence is detected.
Usage: Normal communication with 1-Wire slaves.
PD: Presence Detect
Purpose: Signaling the completion of a 1-Wire reset/presence detect cycle.
Code: 1: The most recent reset/presence detect is completed.
0: There was no reset/presence detect cycle since last reading the Interrupt Register (default).
Conditions: This function is always enabled. PD returns to 0 upon reading the Interrupt Register, a power-on reset or a master reset (MR pin).
Usage: Normal communication with 1-Wire slaves.

Interrupt Enable Register
The Interrupt Enable Register allows the system programmer to specify the source of interrupts which will cause the INTR pin to be active, and to define the active state for the INTR pin. When a Master Reset is received all bits in this register are cleared to 0 disabling all interrupt sources and setting the active state of the INTR pin to LOW. The INTR pin is reset to an inactive state by reading the Interrupt Register.

Interrupt Enable Register Bitmap

ADDR b7 b6 b5 b4 b3 b2 b1 b0
03h EOWL EOWSH ERSF ERBF ETMT ETBE IAS EPD
This register is read/write only. The power-on default is 00h.

Bit Description Definition
EOWL: Enable 1-Wire Low Interrupt
Purpose: Enabling the interrupt upon arrival of a slave on the 1-Wire bus.
Code: 1: The OW_LOW interrupt is enabled.
0: The OW_LOW interrupt is disabled (default).
Conditions: None. EOWL returns to 0 upon power-on reset or a master reset (MR pin).
Usage: This interrupt is useful in applications where 1-Wire slaves come and go, e. g., access control using iButton® devices as keys.
EOWSH: Enable 1-Wire Short Interrupt
Purpose: Enabling the interrupt upon a short circuit of the 1-Wire bus.
Code: 1: The OW_SHORT interrupt is enabled.
0: The OW_SHORT interrupt is disabled (default).
Conditions: None. EOWSH returns to 0 upon power-on reset or a master reset (MR pin).
Usage: This interrupt is useful in access control applications, alarming the host processor of potential tampering or sabotage.
ERSF: Enable Receive Shift Register Full Interrupt
Purpose: Enabling the interrupt upon the Receive Shift Register Full condition.
Code: 1: The RSRF interrupt is enabled.
0: The RSRF interrupt is disabled (default).
Conditions: None. ERSF returns to 0 upon power-on reset or a master reset (MR pin).
Usage: This interrupt can be used to ensure that you don't have data in both the RX Buffer and the RX Shift Register. If both do have data you need to read twice to clear out the buffer.
ERBF: Enable Receive Buffer Full Interrupt
Purpose: Enabling the interrupt upon the Receive Buffer Full condition.
Code: 1: The RBF interrupt is enabled.
0: The RBF interrupt is disabled (default).
Conditions: None. ERBF returns to 0 upon power-on reset or a master reset (MR pin).
Usage: This interrupt is useful during 1-Wire communication, informing the host processor that the receive buffer has data ready for reading.
ETMT: Enable Transmit Shift Register Empty Interrupt
Purpose: Enabling the interrupt upon the Transmit Shift Register Empty condition.
Code: 1: The TEMT interrupt is enabled.
0: The TEMT interrupt is disabled (default).
Conditions: None. ETMT returns to 0 upon power-on reset or a master reset (MR pin).
Usage: This interrupt is useful to know when the 1-Wire wire bits are all transmitted.
ETBE: Enable Transmit Buffer Empty Interrupt
Purpose: Enabling the interrupt upon the Transmit Buffer Empty condition.
Code: 1: The TBE interrupt is enabled.
0: The TBE interrupt is disabled (default).
Conditions: None. ETBE returns to 0 upon power-on reset or a master reset (MR pin).
Usage: This interrupt is useful during 1-Wire communication, informing the host processor that the transmit buffer is empty, ready for new data.
IAS: INTR Active State
Purpose: Setting the active state polarity of the INTR signal
Code: 1: The INTR polarity is active high.
0: The INTR polarity is active low (default).
Conditions: None. IAS returns to 0 upon power-on reset or a master reset (MR pin).
Usage: If the INTR signal is used, this bit matches the signal polarity to the host processor's needs.
EPD: Enable Presence Detect Interrupt
Purpose: Enabling the interrupt upon the completion of a 1-Wire reset/presence detect cycle.
Code: 1: The PD interrupt is enabled.
0: The PD interrupt is disabled (default).
Conditions: None. EPD returns to 0 upon power-on reset or a master reset (MR pin).
Usage: This interrupt is useful during 1-Wire communication, informing the host processor that the 1-Wire reset/presence detect (PD) cycle is completed and that the result is found in the PDR bit of the Interrupt Register (address 02h). EPD is to be enabled it before the 1-Wire reset/PD cycle. Then you wait for the interrupt and when the interrupt occurs you read to confirm PD was the cause.

Clock Divisor Register
The 1-Wire timing requires a 1MHz internal clock. The DS1WM generates this clock frequency from an external reference on the CLK pin. The external clock should have a 50% duty cycle is preferred. The Clock Divisor Register lets the host processor control a clock divider and prescaler to get from the external CLK signal as close as possible to the 1MHz needed for 1-Wire timing. The clock divisor must be configured before communication on the 1-Wire bus can take place. If using an FPGA, it is recommended to replace the clock-divider block with FPGA clock resources to generate the 1MHz internal clock. This avoids gated clocks in the FPGA.

Clock Divisor Register Bitmap

ADDR b7 b6 b5 b4 b3 b2 b1 b0
04h CLK_EN X X DIV2 DIV1 DIV0 PRE1 PRE0
This register is read/write. The power-on default is 00h. Bits 5 and 6 have no function; they always read 0 and cannot be set to 1.

Bit Description Definition
CLK_EN: Enable 1-Wire Timing System
Purpose: Enabling the circuit that controls the 1-Wire timing.
Code: 1: The 1-Wire timing system is enabled.
0: The 1-Wire timing system is disabled (default).
Conditions: CLK_EN returns to 0 upon power-on reset or a master reset (MR pin).
Usage: As a precondition for 1-Wire communication, this bit must be written to 1. To save power at times without 1-Wire communication, this bit can be changed to 0.
DIV[2:0]: Binary Divider Ratio
Purpose: Configuring the binary divider to generate, together with the prescaler, a 1µs clock that governs the entire 1-Wire timing.
Code: 000b: Divide by 1 (pass through, default)
001b: Divide by 2
010b: Divide by 4
011b: Divide by 8
100b: Divide by 16
101b: Divide by 32
110b: Divide by 64
111b: Divide by 128
Conditions: DIV[2:0] returns to 000b upon power-on reset or a master reset (MR pin).
Usage: As a precondition for 1-Wire communication, these bits must be written to the appropriate value, which depends on the available master clock frequency. See Table 4 for guidance.
PRE[1:0]: Prescaler Ratio
Purpose: Configuring the prescaler to generate, together with the binary divider, a 1µs clock that governs the entire 1-Wire timing.
Code: 00b: Divide by 1 (pass through, default)
01b: Divide by 3
10b: Divide by 5
11b: Divide by 7
Conditions: PRE[1:0] returns to 00b upon power-on reset or a master reset (MR pin).
Usage: As a precondition for 1-Wire communication, these bits must be written to the appropriate value, which depends on the available master clock frequency. See Table 4 for guidance.

Table 4. Clock Divisor Register Settings

Min CLK Frequency (MHz) Max CLK Frequency (MHz) Max CLK Error (%) Overall Divider Ratio DIV2 DIV1 DIV0 PRE1 PRE0
1 1.25 25 1 0 0 0 0 0
2 2.5 25 2 0 0 1 0 0
3 3.75 25 3 0 0 0 0 1
4 < 5 25 4 0 1 0 0 0
5 < 6 20 5 0 0 0 1 0
6 < 7 17 6 0 0 1 0 1
7 < 8 14 7 0 0 0 1 1
8 < 10 25 8 0 1 1 0 0
10 < 12 20 10 0 0 1 1 0
12 < 14 17 12 0 1 0 0 1
14 < 16 14 14 0 0 1 1 1
16 < 20 25 16 1 0 0 0 0
20 < 24 20 20 0 1 0 1 0
24 < 28 17 24 0 1 1 0 1
28 < 32 14 28 0 1 0 1 1
32 < 40 25 32 1 0 1 0 0
40 < 48 20 40 0 1 1 1 0
48 < 56 17 48 1 0 0 0 1
56 < 64 14 56 0 1 1 1 1
64 < 80 25 64 1 1 0 0 0
80 < 96 20 80 1 0 0 1 0
96 < 112 17 96 1 0 1 0 1
112 < 128 14 112 1 0 0 1 1
128 < 160 25 128 1 1 1 0 0
160 < 192 20 160 1 0 1 1 0
192 < 224 17 192 1 1 0 0 1
224 280 25 224 1 0 1 1 1
320 < 384 20 320 1 1 0 1 0
384 < 448 17 384 1 1 1 0 1
448 560 25 448 1 1 0 1 1
640 800 25 640 1 1 1 1 0
896 1120 25 896 1 1 1 1 1

Example: If the system clock frequency is 15MHz, the closest overall divider ratio to reach 1MHz is 14. This corresponds to a value of 87h to be written to the Clock Divisor Register. The clock error in this case is (15/14) -1, or 7%.

Control Register
The host processor accesses this register to select the desired operating mode of the DS1WM. These modes include 1-Wire power delivery, recharge accelerator, single bit mode vs. byte mode, long line mode, and presence pulse masking. Correct use of these functions increases the data integrity on the 1-Wire bus.

Control Register Bitmap

ADDR b7 b6 b5 b4 b3 b2 b1 b0
05h X OD BIT_CTL STP_SPLY STPEN EN_FOW PPM LLM
This register is read/write. The power-on default is 00h. Bit 7 has no function; it always reads 0 and cannot be set to 1.

Bit Description Definition
OD: 1-Wire Speed
Purpose: Selecting the speed to be used for 1-Wire communication.
Code: 1: Overdrive speed is selected.
0: Standard speed is selected (default).
Conditions: None. OD returns to 0 upon power-on reset or a master reset (MR pin).
Usage: With most 1-Wire slaves, the power-on default is standard speed. With those parts, the speed change to overdrive requires that the 1-Wire slaves first receive the appropriate switching command at standard speed. After that, the OD bit of the DS1WM must be changed to 1. To switch back to standard speed, change the OD bit to 0 and issue a 1-Wire reset (see Command Register, address 00h).
BIT_CTL: Bit Control
Purpose: Selecting bit mode or byte mode for 1-Wire communication.
Code: 1: The DS1WM operates in bit mode.
0: The DS1WM operates in byte mode (default).
Conditions: None. BIT_CTL returns to 0 upon power-on reset or a master reset (MR pin).
Usage: Most 1-Wire communication occurs in byte mode (power-on default). If bit mode is selected, only the least significant bit in the Transmit/Receive buffer is used/valid. Consequently, the corresponding full/empty bits in the Interrupt Register (address 02h) are set after 1 time slot rather than 8 time slots in byte mode.
STP_SPLY: Strong Pullup Power Delivery
Purpose: Activating the strong pullup power delivery function. This function uses the STPZ pin to control a p-channel transistor to bypass the 1-wire pullup resistor.
Code: 1: The strong pullup power delivery is activated.
0: The strong pullup power delivery is not activated (default).
Conditions: This function must be enabled by first writing the STPEN bit in the Control Register to 1. STP_SPLY returns to 0 upon power-on reset or a master reset (MR pin).
Usage: Some 1-Wire slaves need extra power, e.g., to program EEPROM, measure temperature or perform numeric calculations. Depending on the operating environment, the 1-Wire pullup resistor must be bypassed to maintain the minimum voltage required by the slave to function properly. The host processor must set STP_SPLY to 1 before the slave's high current demand begins and should write STP_SPLY to 0 after the high current phase has ended.
STPEN: Active Pullup Enable
Purpose: Enabling active pullup to minimize the rise time on a heavily loaded 1-Wire bus. This function uses the STPZ pin to control a p-channel transistor to temporarily bypass the 1-wire pullup resistor.
Code: 1: The active pullup is enabled.
0: The active pullup is disabled (default).
Conditions: None. STPEN returns to 0 upon power-on reset or a master reset (MR pin).
Usage: Since it improves the power supply situation of parasitically powered 1-Wire slaves, active pullup should always be enabled. Active pullup must be enabled when operating the 1-Wire bus near the minimum permissible pullup voltage, or with a long bus cable or with multiple slave devices. After a power-on reset, the active pullup is disabled. See Table 6, STPZ Timing Specification, for details.
EN_FOW: Enable Force 1-Wire
Purpose: Enabling the Force 1-Wire command.
Code: 1: The Force 1-Wire command is enabled.
0: The Force 1-Wire command is disabled (default).
Conditions: None. EN_FOW returns to 0 upon power-on reset or a master reset (MR pin).
Usage: Generating DQ signals beyond 1-Wire Reset and 1-Wire read/write functions. For more details, see the FOW bit description of the Command Register (address 00h).
PPM: Presence Pulse Masking
Purpose: Pre-empting the presence pulse generated by 1-Wire slaves.
Code: 1: Presence pulse masking is enabled.
0: Presence pulse masking is disabled (default).
Conditions: None. PPM returns to 0 upon power-on reset or a master reset (MR pin).
Usage: In a long-line environment, presence pulses generated by 1-Wire slaves can cause ringing on the bus. Presence pulse masking can prevent adverse effects caused by the presence pulse. If PPM is 1, the presence detect result (PDR bit of the Interrupt Register, address 02h) is always 0, even if the is no 1-Wire slave on the bus. See Table 5, DQ Signal Timing Specification, for details.
LLM: Long Line Mode
Purpose: Modifying the standard speed timing to be more adequate for a long line application environment.
Code: 1: Long line mode is enabled.
0: Long line mode is disabled (default).
Conditions: None. LLM returns to 0 upon power-on reset or a master reset (MR pin).
Usage: Long line mode changes the Write 1 low time, data sampling time, and recovery time. See Table 5, DQ Signal Timing Specification, for details.

1-Wire Port Description

The 1-Wire port uses the signals DQ and STPZ. The 1-Wire communication takes place on DQ. The DS1WM supports the following 1-Wire communication waveforms: reset/presence-detect cycle, write-zero time slot, write-one time slot, and read-data time slot.

Reset/Presence-Detect Cycle
This signal (Figure 6) consists of two elements: the DS1WM pulldown during the reset-low time tRSTL, and the tRSTH window during which, after a delay of tPDH, a 1-Wire slave pulls the line low for tPDL to signal its presence. To test for a presence pulse, the DS1WM first waits for tPDW and then during tPDSW samples the voltage on DQ. Note that the DS1WM does not control the duration of tPDH and tPDL.

The DS1WM can be configured to mask the presence generated by slaves (see Control Register, bit PPM). If the PPM bit is 1, the DS1WM generates a presence pulse (dotted line) that begins as tPPMS and lasts until tPPME.

Figure 6. Reset/presence detect cycle.
Figure 6. Reset/presence detect cycle.

Write-Zero Time Slot
This time slot (Figure 7) consists of two elements: the DS1WM pulldown as specified by tW0L and the recovery time tREC0. The sum of tW0L and tREC0 is identical to tSLOT.

Figure 7. Write-zero time slot.
Figure 7. Write-zero time slot.

Write-One Time Slot
This time slot (Figure 8) consists of two elements: the DS1WM pulldown as specified by tW1L and the remainder of the time slot.

Figure 8. Write-one time slot.
Figure 8. Write-one time slot.

Read-Data Time Slot
This time slot (Figure 9) consists of three elements: the DS1WM pulldown as specified by tW1L; the slave pulldown time; and the remainder of the time slot. At tMSR, the DS1WM samples the voltage on DQ. Note that a 1-Wire slave, when responding with a zero, starts pulling the DQ line low before tW1L is expired.

Figure 9. Read-data time slot.
Figure 9. Read-data time slot.

Table 5. DQ Signal Timing Specifications (Note 1)

Symbol Parameter Conditions Min Max Units
τ Time base period (Note 2) 0.8 1 µs
tSLOT Time-slot duration Standard speed, LLM = 0 56 70 µs
Standard speed, LLM = 1 64 80
Overdrive speed 8 10
tW0L Write-zero low time Standard speed 48 60 µs
Overdrive speed 6.4 8
tW1L Write-one/read low time Standard speed, LLM = 0 4.8 6 µs
Standard speed, LLM = 1 6.4 8
Overdrive speed 0.8 1
tMSR Read sample time Standard speed, LLM = 0 12 15 µs
Standard speed, LLM = 1 19.2 24
Overdrive speed 1.6 2
tREC0 Write-zero recovery time Standard speed, LLM = 0 8 10 µs
Standard speed, LLM = 1 16 20
Overdrive speed 1.6 2
tRSTL Reset low time Standard speed 480 600 µs
Overdrive speed 56 70
tRSTH Reset high time Standard speed 384 480 µs
Overdrive speed 46.4 58
tPDW Presence-detect wait time Standard speed, LLM = 0 8 10 µs
Standard speed, LLM = 1 8 10
Overdrive speed 1.6 2
tPDSW Presence-detect sample window Standard speed, LLM = 0 48.8 61 µs
Standard speed, LLM = 1 60.8 76
Overdrive speed 6.4 8
tPPMS Presence-pulse mask START Standard speed only 16 20 µs
tPPME Presence-pulse mask end Standard speed only 72 90 µs

Note 1: The timing values depend on the internal logic. If the I/O drivers are slow, these times will change accordingly.
Note 2: System Clock CLK input frequency and Clock Divisor Settings according to Table 4.

STPZ Timing

If enabled (see Control Register, STPEN bit), the STPZ signal activates an external p-channel transistor at certain times to speed up the recharge of the 1-Wire bus. This function is generally needed at overdrive speed and with larger networks at standard speed. Figures 10 and 11 show the STPZ signal for the reset/presence-detect cycle and communication waveforms.

Figure 10. STPZ timing during the reset/presence detect cycle.
Figure 10. STPZ timing during the reset/presence detect cycle.

Figure 11. STPZ timing during read/write time slots.
Figure 11. STPZ timing during read/write time slots.

Several 1-Wire slaves need extra power at certain times during the communication protocol. The extra power-supply delivery function is enabled through the STP_SPLY bit in the Control Register. If both STPEN and STP_SPLY are enabled, the STPZ signal remains active (low) whenever possible (see Figures 12 and 13).

Figure 12. STPZ timing with power delivery during the reset/presence detect cycle.
Figure 12. STPZ timing with power delivery during the reset/presence detect cycle.

Figure 13. STPZ timing with power delivery during read/write time slots.
Figure 13. STPZ timing with power delivery during read/write time slots.

Table 6. STPZ Timing Specifications (Note 1)

Symbol Parameter Conditions Min Max Units
tON1 Active time for presence detect Standard speed 6.4 8 µs
Overdrive speed 0.8 1
tON2 Active time for presence detect recovery   8 10 µs
tON3 Active time for write-one recovery (Notes 2, 3) Standard speed 51.2 64 µs
Overdrive speed 7.2 9
tON4 Active time for write-zero recovery (Notes 2, 3) Standard speed 6.4 8 µs
Overdrive speed 0.8 1
tDLY1 Delay time for presence detect   0.8 1 µs
tDLY2 Delay time for presence detect recovery (Note 4) Standard speed 399.2 499 µs
Overdrive speed 31.2 39
tDLY3 Delay time for write-one and write-zero recovery   0.8 1 µs
tOFF1 Turn-off time for 1-Wire Reset   1.6 2 µs
tOFF2 Turn-off time for write-one and write-zero (Note 5) 0.8 1 µs

Note 1: The timing values depend on the internal logic. If the I/O drivers are slow, these times will change accordingly.
Note 2: There is no timing difference for sending out and receiving bits within a byte. The difference comes when the last bit of the byte is finished being sent out. At this point, the signal is either enabled continuously until the next reset or time slot begins, or enabled only for tON3 or tON4.
Note 3: When performing a read versus a write time slot, the master provides the same active time for write-one and write-zero. However, the input from the DQ line is sensed every 1µs for a high value. If DQ is high, the STPZ signal is enabled. If the DQ line is low, the STPZ signal remains disabled until the high is sensed. In all write time slots, a high is sensed immediately.
Note 4: This parameter is the time delay until the master begins to monitor the DQ input level. If the line is already high, then STPZ will be enabled. If not, it will wait to enable STPZ until the next state machine clock after the DQ line has recovered.
Note 5: The very first bit in a byte transmission has an extended tOFF2 of 4µs due to the order of states the master's state machine runs through.

Device Operation

After power-on, the host first accesses the Clock Divisor Register to write the appropriate values for the prescaler and divider and to enable the 1-Wire timing system. If the application uses the STPZ output, the STPEN bit in the Control Register must be set. If the application uses the INTR signal, the host writes to the Interrupt Enable Register to define the INTR active state polarity and to select the conditions under which the INTR signal is to be activated. This concludes the setup phase. Now the DS1WM is ready to operate at standard speed and in byte mode.

Generating a 1-Wire Reset/Presence-Detect Cycle
The host writes the code 01h to the Command Register. If the Presence Detect Interrupt is enabled (EPD bit), the host could perform other tasks while the DS1WM is busy with the reset/presence-detect cycle. After the cycle is completed, the host reads the Interrupt Register (PDR bit) to see whether a presence pulse was detected.

Writing a Byte to the 1-Wire Line
To send a byte on the 1-Wire bus, the user writes the desired data to the Transmit Buffer. The data is then moved to the Transmit Shift Register where it is shifted serially onto the bus LSB first. A new byte of data can then be written to the Transmit Buffer. As soon as the Transmit Shift Register is empty, the data will be transferred from the Transmit Buffer and the process repeats. Each of these registers has a flag that may be used as an interrupt source. The Transmit Buffer Empty (TBE) flag is set when the Transmit Buffer is empty and ready to accept a new byte. As soon as a byte is written into the Transmit Buffer, TBE is cleared. The Transmit Shift Register Empty (TEMT) flag is set when the Shift Register has no data in it and is ready to accept a new byte. As soon as a byte of data is transferred from the Transmit Buffer, TEMT is cleared and TBE is set.

Reading a Byte from the 1-Wire Line
To read data from the 1-Wire bus, a slave device must first be ready to transmit depending on commands already received from the DS1WM. Reading from the 1-Wire line is similar to writing. The host initiates a read by writing an FFh byte to the Transmit Buffer. The wired-AND of the written data and the data from the slave device is then shifted into the Receive Shift Register. When the Receive Shift Register is full, the data is transferred to the Receive Buffer, where it can be accessed by the host. If the slave device is not ready to transmit, the data received is identical to that transmitted. The Receive Buffer Register can also generate interrupts. The Receive Buffer flag (RBF) is set when data is transferred from the Receive Shift Register and cleared when the host reads the register. If RBF is set, no further transmissions should be made on the 1-Wire bus or else data may be lost, as the byte in the Receive Buffer will be overwritten by the next received byte.

1-Wire Communication in Bit Mode
To activate the bit mode, the host writes the BIT_CTL bit in the Control Register to 1. Subsequent communication between host and DS1WM is the same as in byte mode. However, only the least significant bit in the transmit/receive buffer is relevant.

Changing Between Standard and Overdrive Speed
To switch between 1-Wire speeds, the host writes the OD bit in the Control Register to 1 (overdrive) or to 0 (standard). Any 1-Wire communication after updating the OD bit takes place at the new speed. Long line mode (LLM bit) is a variant of standard speed.

Meeting Slave Extra Power Requirements
The 1-Wire slave data sheets specify when, during a function command, extra power is required. To accommodate such a slave, the host operates the DS1WM using reset, byte, or bit functions to get the slave close to the state where the extra power is needed. Then the host sets both the STPEN and the STP_SPLY bits in the Control Register. Next the host performs the byte or bit read/write operation, after which the slave needs extra power. Then the host waits until the high-power phase is over and accesses the Control Register again to write the STP_SPLY bit to 0. The STPEN bit can remain set. The power delivery function works only if the STPZ pin is connected to a transistor, as shown in Figure 1.

Search Accelerator Operation

Application note 187, "1-Wire Search Algorithm," explains how the Search ROM function works. The search accelerator is a feature that minimizes the communication between host and DS1WM when performing a 1-Wire search. The search accelerator of the DS1WM is identical to the accelerator in the DS2480B. Therefore, the search fundamentals of application note 192, "Using the DS2480B Serial 1-Wire Line Driver" ("OWSearch" section), are also valid for the DS1WM. Of course, the DS2480B-specific command and echo bytes do not apply here.

Before the search accelerator can be used, a 1-Wire reset/presence-detect cycle must have been performed and the Search ROM command (F0h) must have been sent out in byte mode. Now the search accelerator is activated by writing the SRA bit in the Command Register to 1.

After the search accelerator is activated, the host must send 16 bytes to complete a single Search ROM pass on the 1-Wire bus. These bytes are constructed as follows:

First Byte

7 6 5 4 3 2 1 0
r3 x3 r2 x2 r1 x1 r0 x0
Etc.

16th Byte

7 6 5 4 3 2 1 0
r63 x63 r62 x62 r61 x61 r60 x60

In this scheme, the index (values from 0 to 63, "n") designates the position of the bit in the ROM ID of a 1-Wire device. The character "x" marks bits that act as a filler and do not require a specific value (don't care bits). The character "r" specifies the selected bit value to write at that particular bit in case of a conflict during the execution of the ROM search.

For each bit position n (values from 0 to 63) the DS1WM generates three time slots on the 1-Wire bus. These are referenced as:

b0 for the first time slot (read data)
b1 for the second time slot (read data)
b2 for the third time slot (write data)

The DS1WM determines the type of time slot b2 (write-one or write-zero) as follows:

b2 = rn if conflict (as chosen by the host)
= b0 if no conflict (there is no alternative)
= 1 if error (there is no response)

The 16 response bytes that the host reads from the Receive Buffer during a complete pass through a Search ROM function using the search accelerator are constructed as follows:

First Byte

7 6 5 4 3 2 1 0
r'3 d3 r'2 d2 r'1 d1 r'0 d0
Etc.

16th Byte

7 6 5 4 3 2 1 0
r'63 d63 r'62 d62 r'61 d61 r'60 d60

As before, the index (values from 0 to 63, "n") designates the position of the bit in the ROM ID of a 1-Wire device. The character "d" marks the discrepancy flag in that particular bit position. The discrepancy flag is 1 if there is a conflict or no response in that particular bit position, and 0 otherwise. The character " r' " marks the actually chosen path at that particular bit position. The chosen path is identical to b2 for the particular bit position of the ROM ID.

To perform a Search ROM sequence, one starts with all bits rn being 0s. In case of a bus error, all subsequent response bits r'n are 1's until the Search Accelerator is deactivated by writing the SRA bit in the Command Register to 0. Thus, if r'63 and d63 are both 1, an error has occurred during the search procedure and the last sequence must be repeated. Otherwise r'n (n = 0...63) is the ROM ID of the device that has been found and addressed. If the host wishes to execute a memory function with this slave, first the search accelerator needs to be deactivated.

If the host wants to continue with the ROM search to identify the remaining 1-Wire slaves, it first must instruct the DS1WM to turn off the search accelerator, perform a 1-Wire reset/presence-detect cycle, and transmit the Search ROM command. Then the search accelerator must be activated again.

For the next Search ROM sequence, reuse the previous set rn (n = 0…63) but set rm to 1, with "m" being the index number of the highest discrepancy flag that is 1, and set all ri to 0 with i > m.

All parts are found if the highest discrepancy occurs in the same bit position for two consecutive passes.

Application Information

FPGAs or ASICs integrate the designed DS1WM. In Figure 14, the design module with a microprocessor can offload the 1-Wire communication to the DS1WM.

Figure 14. Typical FPGA or ASIC application.
Figure 14. Typical FPGA or ASIC application.

Verification

The industry typically denotes the level of verification of an IP block with the following conventions:

  • Gold IP has been to target silicon.
  • Silver IP has been to target silicon in FPGA.
  • Bronze IP has been verified in silicon models with logical timing closure.
  • In-development IP has not yet been verified.

Note: The DS1WM has achieved silver status.

Deliverables

The DS1WM package comes complete with:

  • Verilog HDL
  • VHDL
  • Verilog test bench
  • Readme information on setup and scripts

The free DS1WM IP is available by request at https://support.maximintegrated.com/1-Wire.

Summary

The DS1WM synthesizable 1-Wire bus master is an alternative to performing 1-Wire communication through "bit-banging." It can be embedded in an FPGA or ASIC, where it appears as a memory-mapped device. The DS1WM supports the communication- and power-delivery requirements of all 1-Wire slave devices.