应用笔记 4921

Temperature Compensation using Bias and Modulation Current with PHY1078


摘要 : This application note discusses the temperature-sensing function of the Phyworks PHY1078, a burst-mode laser driver and limiting amplifier for use within fiber optic modules for FTTx applications. The document also shows the relationship between bias and modulation-DAC values and the actual currents that are measured at the BIAS and LASER outputs. With this article, the user will be able to determine the correct look-up table (LUT) values for both bias and modulation current over temperature, based on known laser characteristics.


This document is written for a highly specific application and contains information about proprietary technology, and is only available to customers whose requirements closely match the application. To request the full document, please complete the form below.

Please enter information in English only.


应用笔记 4921,AN4921, AN 4921, APP4921, Appnote4921, Appnote 4921