应用笔记 4792

利用USB至JTAG接口板编程MAX1441

By: Youssof Fathi

摘要 : MAX1441信号调理集成电路(IC)用于支持电容式接近检测传感器设计,适用于汽车无源遥控门禁(PKE)及其它系统。接口板作为生产测试系统的一部分,用于编程、测试包括MAX1441在内的终端产品。为此,Maxim开发了MAXQUSBJTAG-KIT USB至JTAG接口板,本文介绍该接口板与MAX1441应用电路的连接。

引言

MAX1441为信号调理集成电路(IC),支持电容式接近检测传感器设计,适用于汽车无源遥控门禁(PKE)及其它系统。MAX1441具有两个独立的接触/接近检测通道,支持该IC的完备套件包括:
  1. 集成开发环境MAX-IDE,提供汇编、编译、用户界面和闪存编程器功能。
  2. 例程代码和典型应用固件。
  3. 经过完全测试的评估(EV)系统MAX1441EVSYS,包括接口硬件、应用电路和带两个触摸盘的触摸板。

用于生产测试系统的JTAG接口

生产测试系统需要利用接口板编程、测试包括MAX1441在内的终端产品,有三种方式可供选择:
  1. 开发一个定制接口板或从第三方购买JTAG接口板,确认能够配合MAX1441使用。
  2. 在MAX1441EVKIT控制电路的基础上修改跳线设置,然后从评估板取出MAX1441,请参考MAX1441EVKIT数据资料配置MAX1441EVKIT电路板。
  3. 采用Maxim提供的USB至JTAG接口板MAXQUSBJTAG-KIT
只要电路正常工作,以上三种方式都切实可行。第一种方式,定制接口板或从第三方购买接口板需要用户参与大量工作、花费大量时间,用户需要验证接口板是否与MAX1441兼容并确保可靠通信;第二种方式比较成熟,因为Maxim每块评估板都在出厂之前经过工厂验证,对MAX1441的工作和接口功能进行了严格测试。但是,这种方法需要改变评估板的设置,每个测试系统都需要一个专用的评估板;第三种方法采用MAXQUSBJTAG-KIT接口板,这种方式非常简单,容易操作,因为该接口板已经过验证,确保与MAX1441可靠通信。

本文详细介绍了MAXQUSBJTAG-KIT接口板与MAX1441典型应用电路的连接,这里给出的相关信息适用于任何符合JTAG通信协议的电路板和器件,包括微处理器。

接口连接

图1所示为MAX1441与MAXQUSBJTAG-KIT板的JTAG接口相连接的应用电路。注意:电路图中,JTAG线需要上拉电阻,是该应用电路的一部分。通常,上拉电阻是测试系统的一部分,不必在应用电路板上重复安装上拉电阻。

图1. 连接MAX1441应用电路与MAXQUSBJTAG-KIT板的JTAG接口
图1. 连接MAX1441应用电路与MAXQUSBJTAG-KIT板的JTAG接口

图2显示了相关配置:带测试插座的应用电路板;连接到MAX1441第二通道输入的触摸板;以及连接到计算机(图中未显示)的MAXQUSBJTAG-KIT板。注意,应用电路板带有一个测试插座,用于工程设计,实际应用电路中不需要安装。

图2. MAX1441应用电路板和MAXQUSBJTAG-KIT连接配置
图2. MAX1441应用电路板和MAXQUSBJTAG-KIT连接配置

按照图2搭建设置,运行整个系统。首先,参考MAX1441EVSYS数据资料安装相关软件;然后利用MAX1441EVSYS软件包中的MAX-IDE应用程序作为用户界面,编程MAX1441;最后,参考MAX1441的数据资料及其它支持文档,包括:MAXQ®系列用户指南或针对MAXQ微控制器的用户指南,对器件进行操作、定义寄存器。
下一步
EE-Mail 订阅EE-Mail,接收关于您感兴趣的新文档的自动通知。
© , Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.
APP 4792:
应用笔记 4792,AN4792, AN 4792, APP4792, Appnote4792, Appnote 4792