应用笔记 4080
DS2703的通信流程图
摘要 : DS2703 SHA-1电池包认证IC提供可靠的加密方案,确保各种便携式应用中锂离子电池包的合法性。DS2703可接受11种功能命令,且每个命令均具有特定时序,要正确的执行命令必须遵循该时序。本应用笔记提供了完整的传输时序以及DS2703所有可能的通信时序流程图。
绪论
DS2703 SHA-1电池包认证IC提供可靠的加密方案,确保各种便携式应用中锂离子(Li+、Li-ion)电池包的合法性。该器件采用安全散列算法(SHA-1)来认证主机系统(如,手机、PDA或其它便携式计算设备)中电池包的合法性。将DS2703集成到电池包中,可确保主机鉴别出未授权的电池包,从而避免这种电池包影响系统性能或伤害用户。DS2703可接受11种功能命令,且每个命令均具有特定时序,要正确的执行命令必须遵循该时序。本应用笔记提供了完整的传输时序说明以及DS2703所有可能的通信时序流程图。
传输时序
通过1-Wire®端口访问DS2703的协议如下:- 初始化
- 网络地址命令
- 功能命令
- 数据传输(并不是所有命令都带有数据传输)
网络寻址命令
一旦检测到总线上有一个或多个从机设备,主机可以发出下列网络寻址命令中的一个:Read、Match、Search或Skip命令。图1给出了各网络寻址命令的传输流程图。
图1. DS2703的网络寻址命令流程图
功能命令
初始化和网络寻址命令结束后,DS2703准备接收总线主机发出的功能命令。表1包含了DS2703可接受的11种功能命令,以及这些命令的简单说明。图2所示为DS2703正确执行各命令所需的流程图。需要主机发出相同时序的功能命令在流程图中用单个支路表示。表1. 所有的功能命令
COMMAND | HEX | FUNCTION |
Write Challenge | 0C | Writes 64-bit challenge for SHA-1 processing; required prior to all Compute MAC and Compute Next Secret commands |
Compute MAC Without ROM_ID and Return MAC | 36 | Computes hash of W0–W15 with logical 1's in place of the ROM_ID |
Compute MAC With ROM_ID and Return MAC | 35 | Computes hash of W0–W15 with the ROM_ID |
Load Secret | 5A | Writes the 64-bit secret to supplied data; requires programming voltage on DQ |
Compute Next Secret Without ROM ID | 30 | Generates new global secret; requires programming pulse |
Compute Next Secret With ROM ID | 33 | Generates new unique secret; requires programming pulse |
Lock Secret | 6A | Sets lock bit to prevent changes to the secret; requires programming pulse |
Set Overdrive | 8B | Sets 1-Wire interface timings to OVERDRIVE; requires programming pulse |
Clear Overdrive | 8D | Sets 1-Wire interface timings to STANDARD; requires programming pulse |
Activate Thermistor | A9 | Activates the THM output for thermistor measurement; activation occurs within 50µs of command completion and continues until the VB capacitor is discharged |
Reset | BB | Resets the DS2703 (software POR) |

图2. DS2703的功能命令流程图