应用笔记 2046

Using the DS2751 Battery Fuel Gauge in Multiple-Cell Battery Pack Applications


摘要 : The DS2751 Li+/NiMH battery Fuel Gauge IC is designed to monitor single-cell Lithium-ion (Li-ion) or 3-cell NiMH battery packs. However, with the appropriate circuit modifications, the DS2751 fuel gauge can also be used to monitor a 2-cell Li-ion battery pack. This application note presents a reference circuit that can be used to implement the use of the DS2751 battery fuel gauge to measure the remaining capacity of a 2-cell Li-ion battery pack. Detailed descriptions of the key components of the circuit are discussed, including configuration issues for the DS2751 itself.

Introduction

The DS2751 multichemistry battery fuel gauge has an operating range such that it can be used in singlecell Lithium Ion/Polymer packs or 3-cell Nickel packs. However, many applications necessitate more cells in a series stack. The DS2751 can still be used as a fuel gauging IC in those applications by dividing the multiple cell voltage down to an acceptable level. This method allows the use of all the features of the DS2751 including integrated 25mΩ sense resistor, temperature/voltage/current measurement, current accumulation (coulomb counting), 32-bytes of EEPROM, and a single wire communication interface.

Overview

The schematic in Figure 1 illustrates a possible solution for using the DS2751 in a two cell application. Although not required for basic fuel gauging as described in AN131, this circuit presents a method to measure the dual cell voltage. In this application, PIO is used to switch the comparator output to drive one of its supply rails across the resistor dividing network. With PIO low, the voltage at VIN is half of the dual cell voltage, and with PIO high, VIN is 0V. To provide constant power to the DS2751, a low dropout voltage regulator (LDO) is required to step down the dual cell voltage to an acceptable level. A dual cell protector is also necessary to protect the cells from fault conditions. As shown in the schematic, all components for this circuit must reside on the contact side (as opposed to the cell side) of the protector.

Figure 1. DS2751 in a 2-cell Li+/Polymer battery pack.
Figure 1. DS2751 in a 2-cell Li+/Polymer battery pack.

Detailed Description

The recommended supply voltage for the DS2751 ranges from 2.5V to 5.5V, so the LDO output voltage must be chosen accordingly. The LDO must also have a low quiescent current and be able to handle the input voltage presented by a multiple cell stack. The MAX1726 with a 5V output satisfies all criteria. It supports a 12V maximum input voltage and draws 2µA of supply current. The 5V output is used because the LDO efficiency decreases as the input voltage increases above the output voltage. With a nominal input voltage of 7.6V, this is the optimum output voltage. The 5V output also ensures that the VDD voltage remains above the VIN voltage for all conditions. To prevent data loss in the DS2751, the SHDN pin of the MAX1726 should be connected to the input voltage as shown in Figure 1. This will ensure the MAX1726 does not enter shutdown mode, which would remove power from the DS2751. The 1µF input and output capacitors are data sheet recommended. Please refer to the MAX1726 data sheet for application specific capacitor selection.

The maximum reportable voltage from the DS2751 voltage register (addresses 0Ch and 0Dh) is 4.99V. A dividing scheme is thus necessary to drop the cell stack voltage to a measurable level. For this purpose, two precision 100kΩ resistors are used to divide the stack voltage in half. The constant DC current drain from the resistors would be prohibitive for battery-powered applications, so a comparator is used to switch the current on and off. The TLV3701 nanopower comparator is used for switching because it can withstand supply voltages up to 16V, and lists a 560nA typical supply current. The DS2751 open-drain PIO pin is used as the control pin for the comparator switch. The PIO pin automatically changes to a high-impedance state if the DQ line is low for more than 2 seconds, or if the DS2751 enters sleep mode. A 100kΩ pullup resistor to the LDO output ensures that PIO will be a logic high in this state. The other comparator input is connected to the positive terminal of the bottom cell in the stack. This configuration produces a differential voltage at the comparator inputs for both PIO logic levels. The 47pF capacitor from PIO to ground helps to stop negative undershoot when PIO is driven low.

With the comparator output low, the voltage at VIN is 0V. Because of this, the undervoltage sleep enable (UVEN) function must be disabled, or the DS2751 will never transition to active mode. To disable UVEN, a value of 0 is written to bit 3 of address 31h. When a voltage measurement is needed, the PIO bit in the special feature register (bit 6, address 08h) is set to 0 followed by a delay of at least 6.8ms. This delay is necessary for the DS2751 to update the voltage register with the new voltage at the VIN pin. After reading the voltage register, the PIO bit is set back to 1. The total cell stack voltage is calculated by multiplying the voltage register value by 2. Experimental results showed that adding an additional 0.1V to the doubled voltage register value produced a cell stack voltage accurate to 99%. The additional 0.1V is needed to account for the voltage drop from the comparator positive rail to the comparator output.

For protection of the cell stack, any multiple-cell standalone protector supporting NMOS or PMOS FETs can be used. The standalone protector is placed on the cell side of the DS2751, as illustrated in Figure 1. With this configuration, power to all external components will be disconnected via the protection FETs if a fault condition occurs. When the fault condition is corrected, the discharge FET will again be turned on, and all components will be powered up. As long as the UVEN function is disabled, the DS2751 can go to sleep in only one condition: If the PMOD bit is set to 1 (recommended), and DQ is a logic low for > 2s (pack disconnect). This causes the DS2751 to revert to a low power sleep mode and cease temperature, voltage, current, and accumulated current measurements. Reconnecting the pack and pulling DQ high causes the DS2751 to return to active mode.

The configuration shown in Figure 1 assumes an internal 25mΩ sense resistor. Please refer to the DS2751 data sheet for help choosing an appropriate external sense resistor for your application. All other passive components shown in Figure 1 are included for filtering and ESD protection as shown in the DS2751 data sheet.

Summary

Although the DS2751 is specifically designed for single-cell Lithium Ion/Polymer packs or 3-cell Nickel packs, it can be used as a monitoring and fuel-gauging device in applications that require more cells in the series stack. A comparator and LDO must be added to the complete solution, but the proposed components only add 2.6µA of supply current. With the UVEN function disabled, the numerous benefits of the DS2751 can be utilized in multiple cell applications. The benefits include high-precision coulomb counting with an integrated current sense resistor, 32 bytes of lockable user EEPROM, temperature, voltage and current measurements, a unique 64-bit ROM address, and a single wire serial communication interface.


相关型号
DS2751 免费样品
下一步
EE-Mail 订阅EE-Mail,接收关于您感兴趣的新文档的自动通知。
Download 下载,PDF格式
© , Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.
APP 2046:
应用笔记 2046,AN2046, AN 2046, APP2046, Appnote2046, Appnote 2046