系统板 6134

MAXREFDES43#:I2C SHA-256安全认证设计



MAXREFDES43#为基于I2C的安全认证参考设计,用于外设与Xilinx FPGA之间的安全认证。利用提供的示例代码,FPGA与DS28C22执行质询-响应序列,以确保模块、外设或子系统的真实性。DS28C22通过I2C总线通信,提供标准通信接口。MAXREFDES43#配备有Pmod™连接器,以便利用Avnet ZedBoard™立即进行测试。设计的简单性确保快速适应要求安全性的任何外设。

更多信息请参考详细资料标签页。包括原理图、PCB文件及物料单(BOM)在内的设计文件可从设计资源标签页下载。根据申请,在签署保密协议之后可提供固件。

特性

  • SHA-256安全认证
  • I2C接口
  • 源代码示例
  • Pmod兼容规格

竞争优势

  • 强加密安全认证
  • 带硬件加速,实现快速性能

应用

  • 强加密安全认证
  • 带硬件加速,实现快速性能
MAXREFDES43#系统板 MAXREFDES43#系统板 放大+


MAXREFDES43#参考设计框图 MAXREFDES43#参考设计框图 放大+

Introduction

The proliferation of Internet-connected or Internet of Things (IoT) devices manifests itself in multiple applications including industrial, medical, and energy solutions. This increased connectedness requires enhanced security to protect IP, enable system features using software, and prevent counterfeiting. The MAXREFDES43# subsystem reference design uses the DS28C22 to immediately implement SHA-256 authentication on Xilinx FPGAs over an I2C serial bus. The MAXREFDES43# differs from the MAXREFDES34#, which uses the DS28E15 to communicate over the single-contact 1-Wire® bus. The reference code defines a SHA-256 processor on the host FPGA.


MAXREFDES43# System Board 放大+

Figure 1. The MAXREFDES43# subsystem design block diagram with development platform.

Detailed Description of Hardware

The MAXREFDES43# interfaces with FPGA development boards using a 6-pin Pmod connector as illustrated. The MAXREFDES43# is configured with jumpers, J3 and J4, to allow for configuration with the ZedBoard and with alternate configurations. Both configurations are shown below. To interface with the ZedBoard, place jumpers between pins 2 and 3 of both J3 and J4. When plugging the MAXREFDES43# into a host board, make sure to correctly align the pins with the host Pmod connector, as shown in Figure 2 and Figure 3.

Pmod connector.Figure 2. Pmod connector.

Figure 3. The MAXREFDES43# subsystem design correctly inserted into the ZedBoard development platform. Note that the MAXREFDES43# board is plugged into the top row of the Pmod connector on the ZedBoard.

Table 1 shows the supported platforms and ports.

Table 1. Supported Platforms and Ports

Supported Platforms Ports
ZedBoard platform (Zynq®-7020) JA1

For symmetric authentication schemes like SHA-256, protection of both the secure authenticator secret key, along with the FPGA secret key, are important. Symmetric authentication implementations with poor FPGA secret key security can be risky. To this end, the DS28C22 uses DeepCover® techniques to protect against invasive and noninvasive attacks on its secret key; the reference design spells out various techniques to protect the FPGA secret key.

Additional detail on secret key protection techniques may be found in application note 5803, "Safeguard Your FPGA System with a Secure Authenticator."

Detailed Description of Firmware for ZedBoard Platform

The MAXREFDES43# firmware design supports the ZedBoard kit and targets an ARM® Cortex®-A9 processor placed inside a Xilinx Zynq system-on-chip (SoC).

The firmware allows for immediate interfacing to the hardware. The firmware is written in C, developed using the Xilinx SDK tool, based on the Eclipse open source standard.

The firmware program sequence is used to compute and lock the secret (CLS), write page data to the DS28C22, and authenticate the DS28C22. The complete source code speeds customer development. Code documentation resides in the corresponding firmware platform files.

Quick Start

Required equipment:

  • Windows® PC with two USB ports
  • MAXREFDES43# board
  • MAXREFDES43# supported platform (i.e., the ZedBoard kit)

Download, read, and carefully follow each step in the appropriate MAXREFDES43# Quick Start Guide.


ARM is a registered trademark and registered service mark of ARM Limited.
Cortex is a registered trademark of ARM Limited.
DeepCover is a registered trademark of Maxim Integrated Products, Inc.
Eclipse is a trademark of Eclipse Foundation, Inc.
HyperTerminal is a registered trademark of Hilgraeve, Incorporated.
ISE is a registered trademark of Xilinx, Inc.
Pmod is a trademark of Digilent Inc.
Windows is a registered trademark and registered service mark of Microsoft Corporation.
Windows XP is a registered trademark and registered service mark of Microsoft Corporation.
Xilinx is a registered trademark and registered service mark of Xilinx, Inc.
Zedboard is a trademark of ZedBoard.org.
Zynq is a registered trademark of Xilinx, Inc.

Quick Start

Required equipment:

  • Windows® PC with two USB ports
  • MAXREFDES43# board
  • MAXREFDES43# supported platform (i.e., the ZedBoard kit)

Download, read, and carefully follow each step in the appropriate MAXREFDES43# Quick Start Guide.

Firmware Files
The associated firmware files for the ZedBoard Platform (Zynq-7020) are available upon request. Please contact the .


 
Status:
Package:
Temperature:

DS28C22
DeepCover安全存储器,带有I2C SHA-256和3Kb用户EEPROM

  • 基于SHA-256的对称加密、双向安全认证模型
  • 专用硬件加速SHA引擎,产生SHA-256 MAC
  • 对256位、用户可编程密钥以及输入质询进行有效的安全认证