回到顶部

MAXREFDES70#:高精度、长电池生命热量/流量计

MAXREFDES70

参考设计免责声明 参照  重要声明和免责声明  涵盖参考设计和其他Maxim资源

描述

精度、性价比,超声流量计为液体和气体流量测量带来一个关键性的变化。流量计对于收费、漏泄检测以及关键自然资源的保护至关重要,是公用事业及水、气、热等工业配送系统的核心设备。当前使用最广的机械式流量计利用运动部件测量管道中液体的速度。这些运动部件容易随时间推移发生磨损、精度降低,往往要求在10年之内进行更换。Maxim Integrated的MAXREFDES70#超声传播时间流量计在管道的上行和下行两个方向的压电传感器之间发送和接收信号。通过测量上行和下行超声波传输的TOF差,利用成熟的数字信号处理技术,即可计算得到精度非常高的流量值。

MAX35101是热量/流量计系统的核心。MAX35101集成了自动TOF测量所需的全部功能,包括超声脉冲发射和检测、TOF计算、温度测量和实时时钟(RTC)。MAX35101能够工作在可配置的自动事件定时模式,要求的主机微控制器介入非常少,从而降低系统的总功耗。

MAXREFDES70#参考设计(图1)演示MAX35101 TOF转换器的典型应用。请注意,流量计未经校准,仅仅作为开发定制热量/流量计的高性能平台。关于校准的详细信息,请联系制造商。 

系统框图


图1. MAXREFDES70#参考设计方框图。

特征

  • 高精度
  • 大量程
  • 超低功耗(电池生命达20年)
  • 结构紧凑、成本低

  • maxrefdes70fig00

    maxrefdes70fig00

  • MAXREFDES70

    This flow meter reference design sends and receives ultrasound waves between piezoelectric transducers, and uses the time of flight difference to calculate a very accurate flow rate. MAXREFDES70

Icon

设计, 制作, 测试

图中的电路板已经完成封装和测试。

 

细节部分

细节部分

Detailed System Description

Flow Measurement
The MAXREFDES70# heat/flow meter is based upon the time-of-flight or transit-time measurement principle as shown in Figure 2. The system utilizes two piezoelectric transducers, which function as both ultrasound wave transmitters and receivers.


Figure 2. MAXREFDES70# reference design flow velocity calculation.

The heat/flow meter alternatively transmits and receives ultrasound waves between the two transducers. The ultrasound pulses are first transmitted in the direction of the fluid flow (downstream) and then against the fluid flow (upstream).

The ultrasound pulses move faster downstream than upstream, the TOF difference between the downstream and upstream is proportional to the flow velocity. The larger the TOF difference, the faster the fluid flows. When the fluid stops flowing, the TOF difference is 0, ideally. The MAX35101’s sophisticated digital processing circuits, precise analog front-end circuits, and automatic calculation algorithms make the ultrasonic TOF measurement highly accurate and reliable. Refer to the MAX35101 IC datasheet for details.

The MAXREFDES70# reference design uses a DN20 spool body from Audiowell Electronics Co., Ltd. The spool body dimensions are shown in Figure 2. Other types of spool bodies work for different flow velocity and volumetric flow rate requirements.

The basics of flow rate calculation work as follows. Assume the speed of a sound wave in the fluid at a specific temperature is C0, the downstream TOF TA > B is given by:

where D is the diameter of the spool body pipe, L is the length from reflection mirror A to reflection mirror B, v is the flow velocity.

The upstream TOF TB > A is given by:

Take the TOF difference of the upstream and downstream:

Thus yielding:

ΔT × (C0² - v²) = 2 × L × v

Because the flow velocity is orders of magnitude slower than the sound speed in liquids, we can ignore the v² item in the above equation. The flow velocity v is then given by:

v = (ΔT × C0²)/(2 × L)

The simple volumetric flow rate is given by:

q = v × A

where A is the crosssection area of the spool body pipe.

Because the flow rate and the temperature of the fluid continuously change, the heat/flow meter calculates the flow velocity and volumetric flow rate piecewise. The total volumetric flow is the integration of the piecewise volume:

where t is the time elapsed after the start of metering, which is denoted as time zero.

Attention must be paid to the real world volumetric flow rate calculation. The above volumetric flow rate q is the theoretical calculation. Because of the blocking effect of the two ultrasound signal reflection mirrors in the pipe, flow differences at the pipe’s surface, effects of laminar and turbulent flow, and the manufacturing discrepancies of each spool body, the calculated volumetric flow rate must be calibrated against an accurate reference flow rate to get the real-world flow rate. This is done by taking data points for multiple flow rates, and storing the gain factors for each calculated flow rate in a lookup table. After each piecewise flow rate is calculated, in the lookup table, use the interpolation method to find the corresponding gain factor and adjust the calculated flow rate to get the real world flow rate. The MAXREFDES70# firmware implements this gain factor correction as an example.

Energy Measurement

After a gain factor-corrected piecewise volumetric flow rate is available, the water mass flow rate at a specific temperature is given by:

m = q × ρ

where ρ is the water density at a specific temperature.

Known inlet (hot) and outlet (cold) temperatures, the energy flow rate is given by:

e = m × (Hhot - Hcold)

where Hhot, Hcold are the enthalpies of water at the pipe inlet and outlet temperatures. Usually, Hhot - Hcold is denoted as ΔH.

Same as the volumetric flow, the heat/flow meter calculates the energy flow (either heating or cooling) rate piecewise. The total energy flow is the integration of the piecewise energy:

Hardware Description

The MAXREFDES70# reference design system block diagram is shown in Figure 1.

The meter needs to be activated before use. First, press and release the button on the meter cover (SW2 button) to turn on the LCD display. Then, press and hold the button for more than 10s to activate the meter. This operation is required only one time.

MAX35101 Time-to-Digital Converter with Analog Front-End
The MAX35101 lies at the center of the system, a time-to-digital converter with built-in amplifier and comparator, is built as a complete analog front-end solution for the ultrasonic heat meter and flow meter markets.

With automatic differential TOF measurement, this device simplifies computation of liquid flow. Early edge detection ensures measurements are made with consistent wave patterns to greatly improve accuracy and eliminate erroneous measurements. The built-in arithmetic logic unit provides TOF difference measurements. A programmable receiver hit accumulator can be utilized to minimize the host microprocessor access.

For temperature measurement, the MAX35101 supports up to four 2-wire PT1000/500 platinum resistive temperature detectors (RTD).

The MAX35101 offers an event timing mode that is configurable and runs cyclic algorithms to minimize microprocessor interactivity and increase battery life.

The real-time clock provides time-of-day monitoring and one programmable alarm and watchdog functionality.

A simple op-code based on a 4-wire SPI interface allows any microcontroller to effectively configure the device for its intended measurement.

On-board user flash allows the MAX35101 to be nonvolatile configurable and provides nonvolatile energy use data to be logged.

Microcontroller
The heat/flow meter is controlled by the EFM32ZG110 energy-friendly, ARM Cortex-M0+ CPU, 32-bit microcontroller. The microcontroller runs at 14MHz internal clock and has 32KB internal flash.

The microcontroller communicates with the MAX35101 and the LCD module through the SPI interface and several GPIO pins. The MAX35101 is set to work in event timing mode, requiring very minimal interaction from the microcontroller, thus conserving battery life. The MAX35101 wakes up the microcontroller periodically with an interrupt request. The microcontroller does a very short data processing and usage logging step and then enters/re-enters into deep sleep mode.

User Interface: Control Button and Liquid Crystal Display (LCD)
Press and release the SW2 button to turn on the 3x16-character LCD. After the LCD is on, press and release the SW2 button to recursively display the following information menus:

  • Maxim Integrated company banner
  • Real-time clock
  • Hot and cold PT1000 sensor temperatures
  • TOF difference
  • Flow rate
  • Total volumetric flow
  • Total energy used

Press and release the SW2 button to also access the following configuration menus:

  • TOF Difference Measurement Frequency (TDF) register
  • TOF Difference Measurements (TDM) register
  • Temperature Measurement Frequency (TMF) register
  • Temperature Measurements (TMM) register

When the information menus are displayed, press the button for more than 2s to turn off the LCD. If there is no operation on the button, the LCD stays on for 2 hours and then turns off.

When the configuration menus are displayed, press and release the SW2 button to change the register values. A long press (more than 2s) and release of the SW2 button sends the value to the MAX35101 register.

Because the LCD module draws very little power (normally less than 1mA) in display mode, the LCD module is powered directly by the microcontroller GPIO pins.

MAX4721 Analog Switch
The MAX4721 low-voltage, low-on-resistance (RON), dual single-pole/single-throw (SPST) analog switch is used to isolate the LCD module SPI interface when the LCD is powered off. The switch reduces the current leakage to the LCD module down to 5nA, thus conserving battery life.

Factory Real-Time Clock Setting
The MAXREFDES70# heat/flow meter firmware implements the MAX35101 RTC factory setting by using the SW2, SW3, and SW4 buttons. During factory production process, press SW2 and then press SW3. This will bring up the RTC clock setting menu and follow the menu instructions to set the RTC clock. Refer to the firmware for details.

Tamper Detection Operation
The MAX35101 provides a single-pin input that can be connected to a device case switch and used for tamper detection. Upon detection of a case switch event, the CSWA in the Control register and the CSWI bit in the Interrupt Status register are set and the INT device pin is asserted (if enabled). The SW1 tactile button on the circuit board is a normally closed tactile switch. A meter manufacturer can configure the SW1 switch to open position during production, e.g., pressing the SW1 switch using the meter case top cover. The firmware then monitors the CSW pin state for tamper detection.

Firmware Description

The heat/flow meter firmware is based on an interrupt driven design model. After power-up, the microcontroller configures the GPIO pins, system clocks, LCD module, and sets the MAX35101 to a preconfigured event timing mode. Most of the time, the microcontroller is in the power-saving sleep mode, woken up only by the interrupt requests from the MAX35101 to do very quick data processing and usage logging.

The flowcharts of the two major firmware modules are shown in Figure 3 and Figure 4, respectively. These include the main function and interrupt service routine (ISR) modules.


Figure 3. MAXREFDES70# firmware main function flowchart.


Figure 4. MAXREFDES70# firmware interrupt service routine flowchart.

Quick Start

Follow the ensuing procedure to set up the MAXREFDES70# in a real metering environment.

Procedure

  1. Stop the water flow by shutting down the inlet valve.
  2. Place the MAXREFDES70# heat/flow meter in the inlet section of the water pipe, use the included copper joints, if necessary. Seal the junctions, if needed. Place the meter in a position that avoids generating air bubbles.
  3. Insert the hot RTD sensor in the temperature sensor tube of the spool body. Fasten the RTD sensor, making sure there is no water leakage.
  4. Insert the cold RTD sensor in the temperature sensor tube of the outlet pipe. Fasten the RTD sensor, making sure there is no water leakage.
  5. Open the outlet and the inlet valves.
  6. If the meter is not activated, first, press and release the button on the meter cover (SW2 button) to turn on the LCD display. Then, press and hold the button for more than 10s to activate the meter. This operation is required only one time.
  7. Press and release the button to recursively read the real-time clock, hot and cold PT1000 sensor temperatures, TOF difference, flow rate, total volumetric flow, and total energy used. In the configuration menus, a user can change the:
    • TOF Difference Measurement Frequency (TDF) register
    • TOF Difference Measurements (TDM) register
    • Temperature Measurement Frequency (TMF) register
    • Temperature Measurements (TMM) register
  8. Refer to the MAX35101 datasheet for register details.

Lab Measurements

The MAXREFDES70# design was verified and tested under typical application cases. Basically speaking, the MAX35101 is capable of measuring any water flow rates with the proper spool body dimensions and water pipe structure. The current spool body has a diameter of 20mm, a reflection mirror distance of 71.7mm. Based on the expected volumetric flow rates, other spool body sizes can be easily used and tested against good references.

Figure 5 shows the accuracy that can be achieved by the MAXREFDES70#. This accuracy plot was obtained by using a popular electromagnetic reference water meter to calibrate the MAXREFDES70#. The meter was set in the following condition for TOF measurement: TDF = 0.5s, TDM = 5 measurements. At very low flow rate, the electromagnetic water meter has a relative large error itself.


Figure 5. MAXREFDES70# flow rate comparison.

Figure 6 shows one typical RTD sensor test results. The MAXREFDES70# firmware uses the standard RTD1000 resistances as lookup table to calculate the RTD sensor temperature. The meter was set in the following condition for temperature measurement: TMF = 1s, TMM = 5 measurements. For more accurate temperature measurement, each RTD sensor must be calibrated against the standard RTD1000 resistances.


Figure 6. MAXREFDES70# temperature test.

The temperature difference between the hot RTD sensor and the cold RTD sensor is used to calculate the energy consumption. It is important to use matched RTD pairs for one meter. The accuacy of the temperature difference is captured by putting the two sensors in the same temperature environment, and reading the temperature difference of the two RTDs. Figure 7 shows typical meter temperature diference test results.


Figure 7. MAXREFDES70# temperature difference test.

References

  1. F.J. Arregui, C.V. Palau, L. Gascón and O. Peris, “Evaluating domestic water meter accuracy. A case study,” in Pumps, Electromechanical Devices and Systems Applied to Urban Water Management, edited by Enrique Cabrera and Enrique Cabrera Jr., 343–352 (Swets & Zeitlinger Publishers, 2003).

Maxim设备 (2)

器件号 名称 产品线 购买 设计套件和评估模块
MAX35101 集成模拟前端的时间数字转换器 表计与电能测量 立即购买 Design Kits
MAX4721 4.5Ω、双路SPST模拟开关,UCSP封装 模拟开关和多路复用器 立即购买 Design Kits

Maxim设备 (2)

器件号 产品线
表计与电能测量
集成模拟前端的时间数字转换器
模拟开关和多路复用器
4.5Ω、双路SPST模拟开关,UCSP封装

设计资料 (9)

标题 类型 尺寸 日期
No Title PDF 75KB 2019-07-09
rd70_efm32_v02_00 ZIP 1MB 2019-07-09
No Title PDF 1012KB 2019-07-09
Microsoft Word - MAXREFDES70_BOM_RB.docx PDF 22KB 2019-07-09
maxrefdes70_cad_ra ZIP 133KB 2019-07-09
rd70_v02_00 ZIP 2MB 2019-07-09
rd70_efm32_v01_00 ZIP 1MB 2019-07-09
maxrefdes70_bom_ra PDF 94KB 2019-07-09
rd70_v01_00 ZIP 2MB 2019-07-09
日期 类型
2019-07-09

No Title

(PDF, 75KB)

2019-07-09

rd70_efm32_v02_00

(ZIP, 1MB)

2019-07-09

No Title

(PDF, 1012KB)

2019-07-09

Microsoft Word - MAXREFDES70_BOM_RB.docx

(PDF, 22KB)

2019-07-09

maxrefdes70_cad_ra

(ZIP, 133KB)

2019-07-09

rd70_v02_00

(ZIP, 2MB)

2019-07-09

rd70_efm32_v01_00

(ZIP, 1MB)

2019-07-09

maxrefdes70_bom_ra

(PDF, 94KB)

2019-07-09

rd70_v01_00

(ZIP, 2MB)

MAXREFDES70 相关视频

查看所有视频