参考电路 4163

电信热插拔参考设计有效解决输入瞬间过压及掉电问题



概述

典型的电信系统必须能够满负荷工作在-36V至-72V两个电压源,另外还必须提供雷电感应、高压脉冲以及输入电压在几毫秒内跌落到0V情况下的保护措施。可插拔线卡通常包含一个从高压到低压的DC-DC转换器,该转换器带有热插拔保护电路。当线卡带电插入一个背板时,该电路可以限制浪涌电流,使其略高于满负荷电流。板上滤波电容充满电后,热插拔电路还必须提供一个电源就绪信号(/PGOOD),以开启后续的DC-DC转换器。本文详细介绍了对热插拔电路的要求。大部分要求与AdvancedTCA® (ATCA®)一级热插拔电路相同。

典型电信系统要求

  1. 输入电压范围:-43V至-72V
  2. 输入采用双二极管“或”逻辑
  3. -32V至-36V关闭(二极管之前的电源)
  4. 80W (最大)输入功率,CLOAD = 680µF
  5. 耐压-150V,1ms过压脉冲¹
  6. 掉电支持,0V,从-43V输入电压开始16ms的瞬时掉电;在此期间/PGOOD必须保持低电平
  7. 43V启动时,浪涌电流 ≤ 1.5倍满负荷电流

参考设计特性和考虑

  1. 欠压闭锁(UVLO)上升门限可以设置到~43V,过压闭锁(OVLO)上升门限可以设置到 ≥ 72V。
  2. 安装在输入端的两个100V肖特基二极管实现两个独立电源的“或”逻辑。
  3. UVLO下降门限可以设置到~32V,必须满足电信系统规范第6项,电压降低UVLO下降门限时,/PGOOD保持有效,系统保持正常工作。
  4. VIN = 43V时PIN = 80W,输入电流为1.86A。
  5. 对于U1、C3、C4和Q2,70V TVS二极管能够将输入电压钳位在一个安全电平。这个二极管可以直接跨接在输入端,或MAX5921热插拔控制器的VDD–VEE引脚,并且串联一个5Ω电阻与VIN隔离。
  6. 从43V到32V跌落的16ms时间内,储能电容(C3)存储足够的能量支持80W负载的供电。该电容通过一个电阻充电,以限制充电电流,使其保持在电信系统规范第7项中规定的输入浪涌电流的一小部分。放电期间,肖特基二极管旁路这个充电限流电阻。
  7. 断路器最低触发门限可选,容许在43V时设置为2.8A,150%启动浪涌电流,电压低至32V时,保持2.5A满负荷工作。

概述

典型的电信系统必须能够满负荷工作在-36V至-72V两个电压源,另外还必须提供雷电感应、高压脉冲以及输入电压在几毫秒内跌落到0V情况下的保护措施。可插拔线卡通常包含一个从高压到低压的DC-DC转换器,该转换器带有热插拔保护电路。当线卡带电插入一个背板时,该电路可以限制浪涌电流,使其略高于满负荷电流。板上滤波电容充满电后,热插拔电路还必须提供一个电源就绪信号(/PGOOD),以开启后续的DC-DC转换器。本文详细介绍了对热插拔电路的要求。大部分要求与AdvancedTCA® (ATCA®)一级热插拔电路相同。

典型电信系统要求

  1. 输入电压范围:-43V至-72V
  2. 输入采用双二极管“或”逻辑
  3. -32V至-36V关闭(二极管之前的电源)
  4. 80W (最大)输入功率,CLOAD = 680µF
  5. 耐压-150V,1ms过压脉冲¹
  6. 掉电支持,0V,从-43V输入电压开始16ms的瞬时掉电;在此期间/PGOOD必须保持低电平
  7. 43V启动时,浪涌电流 ≤ 1.5倍满负荷电流

参考设计特性和考虑

  1. 欠压闭锁(UVLO)上升门限可以设置到~43V,过压闭锁(OVLO)上升门限可以设置到 ≥ 72V。
  2. 安装在输入端的两个100V肖特基二极管实现两个独立电源的“或”逻辑。
  3. UVLO下降门限可以设置到~32V,必须满足电信系统规范第6项,电压降低UVLO下降门限时,/PGOOD保持有效,系统保持正常工作。
  4. VIN = 43V时PIN = 80W,输入电流为1.86A。
  5. 对于U1、C3、C4和Q2,70V TVS二极管能够将输入电压钳位在一个安全电平。这个二极管可以直接跨接在输入端,或MAX5921热插拔控制器的VDD–VEE引脚,并且串联一个5Ω电阻与VIN隔离。
  6. 从43V到32V跌落的16ms时间内,储能电容(C3)存储足够的能量支持80W负载的供电。该电容通过一个电阻充电,以限制充电电流,使其保持在电信系统规范第7项中规定的输入浪涌电流的一小部分。放电期间,肖特基二极管旁路这个充电限流电阻。
  7. 断路器最低触发门限可选,容许在43V时设置为2.8A,150%启动浪涌电流,电压低至32V时,保持2.5A满负荷工作。

电信热插拔参考设计

电信热插拔参考设计采用MAX5921热插拔控制器,如图1所示。
Figure 1. MAX5921 telecom reference design schematic.
图1. MAX5921电信参考设计原理图

启动特性

ULVO上升电压门限由分压电阻² (R1+R2):R3设置为:

Equatioin 1

虽然输入UVLO上升开启门限由分压比(R1+R2):R3设定,输入UVLO下降关闭门限由分压比R2:R3设定。因为启动期间,一旦产生输出电压,Q2会短接至R1。

输入电压缓慢上升到UVLO升压门限时,会产生图2所示波形。这种情况发生在:

VIN - VS1 = VIN - VEE + VF(D1) ≈ 42.4V

栅极电压升至中间值,控制输出电压的摆率为2.2V/ms,以此限制输出电容(C4)的充电电流。输入电流(IC4 + IC3)峰值为1.75A。当VOUT达到它的最终值,输入电流降至充电电流(IC3)。

图2. VIN上升时的导通特性
通过选择C2可以控制启动时的输入浪涌电流。

Equation 2

由此,浪涌电流限制在 ≤ 1.5倍的启动电流(43V输入时,1.86A)。较小的C2会增大浪涌电流。

比如,如果C2 = 12nF,IINRUSH = 2.55A,接近所要求的2.8A。

图2所示为输入浪涌电流。

图3与图2类似,只是图中/PGOOD在VGATE达到最终值7ms后、VOUT达到其最终值15ms后输出低电平。
Figure 3. Turn-on characteristics with active-low PGOOD.
图3. /PGOOD的开启特性

热插拔过程将要结束时,Q2短接至R1、UVLO下降门限被设定在大约32V,满足电信系统规范的第3、第6项要求。

Equation 3

图4所示为启动时C3的充电过程,因为C3的初始充电电流在VIN = 50V时只有~100mA峰值,所以充电时间与输出负载无关,充电时间大约为10s。在启动10s后或出现一次欠压后,才能提供电压跌落支持。
Figure 4. C3 storage capacitor charge at turn-on.
图4. 导通时C3储能电容充电

掉电保护

电压跌落期间的保持时间按照以下步骤计算:

P = 80W and C3 = 5400µF

掉电可能发生在最差工作条件下: VIN = 43V, 此时:

VOUT = VIN - VF(D1) = 43V - 0.55V = 42.45V

一旦输入电压开始下降,VOUT将下降一个D4二极管的压降,或额外的0.6V,下降至41.85V。

下降期间,由C3提供负载供电,并且/PGOOD在达到以下条件之前保持有效:

UVLOMAX = 33.6V = [VCAP - VF(D4) + VF(Q1)] or VCAP = 34.8V

Equation 4

因此,电容可以有10%的误差,计算所得的保持时间为16.4ms。
输入电压下降时,如果D1或D2没有导通,C3通过体二极管Q1为MAX5921的输入供电。因此,在欠压期间,MAX5921正常工作并提供有效的/PGOOD。

在长达16ms的输入电压跌落期间(从VIN = 43V跌落到VOUT = 32V),通过C3可以维持输出功率为80W。上电时,C3通过电阻R11充电。C4在启动时充电,为了防止C3充电电流超过输入浪涌电流,选择C3 x R11的时间常数为4860ms。因此,在上电10s后才能提供掉电保护支持。

图5所示为掉电保护波形图,图中初始功率约为
4.185A × 41.85V ≈ 175W (注意:一旦断开输入电源,输出电压将由于D4的正向导通而下降)。
Figure 5. Waveforms at dropout.
图5. 电压跌落时的波形
从43V开始下降,16ms后输出电压下降至31.5V,功率约为3.15A × 3.15V ≈ 99W。由此可以看出:C3存储能量足以支持掉电保护的需求。

过压锁定

OVLO上升电压门限由分压比R4:R5设定:

Equation 5
 

断路器触发门限
 

选择适当的断路器触发门限以保证在VIN达到指定的最小值以前或初始上电时不会触发断路。因此,断路触发门限需要根据较大的80W/32V = 2.5A或(1.5 × 80W)/43V = 2.8A进行计算。由于在16ms瞬时掉电期间由C3为负载供电,在此期间没有电流通过检流电阻。电阻R7按照下式设置触发门限:

Equation 6

脉冲过压保护
 

MAX5921需要提供100V以上的输入瞬变保护,可以参考以下两个电路:

  1. 一个电路中,在+VIN和MAX5921的VDD引脚之间串联了一个5.6Ω电阻(R8),VDD和VEE引脚之间连接了一个TVS二极管(D3)。这种情况下,只有MAX5921得到保护,C3、C4和Q2的额定值应该> 150V瞬变。
  2. 另一个电路中,在逻辑“或”二极管后面直接将TVS二极管连接VIN各端,为整个电路提供,选用SMBT70A (D3)限制瞬态脉冲,使其 ≤ 100V,并在75V时可以通过 < 1mA的电流。电路由D3提供输入电压保护,在0.2焦耳电容放电产生的脉冲(见注释1)冲击下提供有效保护。
仅保护MAX5921

图6图7中,D3提供器件的输入瞬态保护。安装R8,只有MAX5921受保护,出现0.2焦耳的输入脉冲(见注释1)。

图6. 脉冲过压保护特性,仅保护MAX5921,最初的9µs.

图7. 脉冲过压保护特性,仅保护MAX5921,最初的9ms

VDD - VSS限定在84.4V,输入电流出现一个宽度为4µs、峰值为46A的三角尖峰。

VIN上升3ms,峰值达到165V或比最初的50V高出115V。VOUT - VEE也随着VIN上升至高于0V初始值的115V。MAX5921的输入瞬变和OVLO电路保护机制引起短暂的栅极关闭,输入脉冲在输出端被抑制。栅极关闭期间,C3为输出供电。

整个电路的保护

图8图9所示波形是短接R8时的测试结果,能够为MAX5921、Q1以及Q1的后续电路提供保护。

图8. 脉冲过压保护特性;完整的电路保护;最初的10ms

图9. 脉冲过压保护特性;完整的电路保护;最初的10s

VIN需要大约6µs的时间从初值上升至98V或50V,并且在30µs内下降到~65V,然后经过6ms下降到初始值。输入电压峰值伴随一个峰值为66A、宽度为6µs的三角形电流尖峰。这个电流完全流过D3。

栅极电压在500ns内下降至接近0V,在~12ms内恢复至正常值。关闭Q1抑制输入瞬变。

VOUT - VEE会在最初的100ns内上升至~60V,然后会快速下降到一个较宽的50V脉冲,持续6µs,然后在6ms内返回到正常电平。除了栅极关闭的最初400ns,输入脉冲在输出端被完全抑制掉。在VGATE返回到其正常值,瞬变恢复之前,由C3为负载供电。

总结

本文提供的电信热插拔参考设计能够满足典型电信系统的规范要求,支持 ≥ 16ms的有效保持时间。过压脉冲保护可以仅提供给MAX5921或也可以为整个电路提供过压脉冲保护。如果用户只要求用D3保护MAX5921,可以切断R8的短路线。切断R8两端的短路线后,C3和C4的额定值为160V。Diodes公司的TVS二极管SMBT70A是瞬态过压保护的关键—其它TVS二极管不能胜任本设计的要求。

材料清单

Qty. Designator Component Manufacturer and Part Number
1 C1 4.7nF ±10%, 50V ceramic capacitor (0805) Vishay VJ0805Y472KXACW1BC
1 C2 15nF ±10%, 50V ceramic capacitor (0805) Vishay VJ0805Y153KXACW1BC
2 C3a, C3b 2700µF ±10%, 100V electrolytic capacitors Panasonic ECD-S2AP272CA
1 C4 680µF ±10%, 100V electrolytic capacitor Panasonic ECD-S2AP681BA
3 D1, D2, D4 10A or 16A, 100V Schottky diodes (D2PAK) Vishay MBRB10H100CT-E3/45,
ST Microelectronics STPS16H100CG,
or Vishay 16CTQ100SPBF
1 D3 70V TVS diode (SMB) Diodes Inc. SMBT70A
1 Q1 150V, 16mΩ n-channel MOSFET (D2PAK) Fairchild FDB2532 or
Vishay SUM85N15-19-T1-E3
1 Q2 100V, bipolar PNP transistor (SOT23) Fairchild BSS63
1 R1 68.1kΩ ±1% thick-film resistor (0603) Vishay CRCW0603154KFKEA
1 R2 255kΩ ±1% thick-film resistor (0603) Vishay CRCW0603255KFKEA
2 R3, R5 10.0kΩ ±1% thick-film resistors (0603) Vishay CRCW060310K0FKEA
1 R4 576kΩ ±1% thick-film resistor (0603) Vishay CRCW0603576KFKEA
1 R6 91kΩ ±5% thick-film resistor (0805) Vishay CRCW080591K0JNEA
1 R7 12mΩ thick-film resistor (2512) Vishay WSL2512R0120FEA
1 R8 5Ω ±1% thick-film resistor (2512) Vishay CRCW25125R00FKEG
1 R9 680Ω ±1% thick-film resistor (0603) Vishay CRCW0603680RFKEA
1 R10 21.3kΩ ±1% thick-film resistor (1210) Vishay CRCW121021K3FKEA
1 R11 510Ω ±1% thick-film resistor (2512) Vishay CRCW2512510RFKEG
1 R12 1kΩ ±1% thick-film resistor (0603) Vishay CRCW06031K00FKEA
1 R13 10Ω ±1% thick-film resistor (0603) Vishay CRCW060310R0FKEA
1 U1 Hot-swap controller IC, -100V Maxim MAX5921AESA

测试PCB

Figure 10. Component layout.
图10. 器件布局
Figure 11. Top layer.
图11. 顶层
Figure 12. Bottom layer.
图12. 底层

参考文献

  1. 0.2焦耳的测试脉冲通过一个18µF电容(充电至150V)对电路输入端放电产生,电路电源通过10mH电感隔离。本测试方法参照Telstra公司CAN 051 775 55中传输设备的电源和接地规范1555。
  2. 在UVLO和OVLO计算中没有考虑电阻公差。VUVH、VUVL和VOVH取自MAX5921数据资料。

 
Status:
Package:
Temperature: