-
- Can a Supercapacitor Replace Your Battery for Backup Power
- What Can You Create with Frequency Synthesizers?
- How Fast and Safe Will 5G Wireless Networks Be
- These Industrial Communications ICs are Oldies but Goodies for Good Reason
- DIY Engineering Projects for Your Valentine
- Why Embedded Systems Designers Should Care About OpenSSL
- Balancing Power Demands of High-Voltage Automotive Power Applications
- PUF Technology Protects Against Invasive Attacks
- 快速、高精度电池管理系统助力更安全的电动汽车
- MAXIM远程调谐器方案帮助简化车载音响系统设计
- Moving Toward Value-Based Healthcare Using Wearables and Patient-Generated Data
- A Smarter Way to Design Touchscreens
- Want to Avoid Counterfeiting?
- Ultra-Small Wearable Healthcare Design Platform
- 打开口袋,释放工业4.0的洪荒之力
- Solving EMI Challenges in LED Headlamps
- embedded world 2017
- 工程设计是为傻瓜准备的(我就是活生生的例子)
- See & Hear Maxim Technologies at Mobile World Congress
- Keeping Cars Safe and Reliable Via ISO 26262 Certification
- Fast (But Not Too Fast) Op Amps for Reliable Very Low-Power Systems
- Shade-Proof Your Solar with Maxim Solar Cell Optimizers
- How Machine Learning Can Speed Up Your Design Cycle
- MakeWithMaxim Design Contest
- IO-Link —“智造”无限可能!
- How 3D Printers Help You Evaluate ICs
- Optical Networking Technologies OFC 2017
- How You Can Help Bring 20.8 Billion Connected Things Into the World
- 参考设计不仅仅是IC,而是完备的系统
- 工业4.0来势汹涌,“模拟整合”是主要受益者之一
- Putting the power of Industry 4.0 in your Pocket
- Battery fuel gauge ICs do more
- Reference Designs: Game Changers for Complex Projects
- 为什么黑客急不可耐地想进入您的汽车
- 您的家居可能越来越智能——但防止黑客的安全性又如何呢?
- What’s Your Favorite IoT Platform? Vote Today!
- 实现智能电网故障的快速、高精度检测
- Template
- 隔离电源参考设计
- 多通道、通用模拟输入 参考设计
- Fitness/Wellness Wearables Reference Design Saves Development Time and Effort
- Simplifying Design of Pulse Rate/Blood-Oxygen Wearables
- Don’t Design the Next Useless IoT Gadget
- Exactly What the Doctor Ordered: Cars that Monitor Their Own Health and Yours
- Reducing Component Count in Factory Automation Applications
- Maxim Highlights Auto, Wearable Healthcare Tech at CES
- Cut 6 Months Off Health Application Design Cycle
- Future Engineers Make with Maxim at Yale’s YHack Hackathon
- Interesting Inventions Inspire Ingenuity
- Ants Have Their Own Smart Cities—Why Can’t We?
- Proximity Sensing Made Easier
- Get Longer Battery Life By Lowering Quiescent Current
- Eat Pie and Win a Dev Board
- Why System Monitoring ICs Are Good Analog Insurance
- Who is nanoMan?
- Why Now Is the Time to Consider Wired Interface Solutions
- Get to Market Quickly with Your Secure Wearable Health Designs
- Why Powerline Communications is Great for Noisy Industrial Environments
- How Factory Automation Can Support Reshoring
- Don’t Become the Next Hacking Headline
- One Smart Design: Low IQ Boost Converter
- A Look at the Future of Wearable Healthcare Design
- 为什么摄像头接口对ADAS系统设计至关重要
- Reduce Calibration Costs for Industrial Process Control
- Making Smart Energy Even Smarter Via nanoPower Technology
- We Love Startups! Let Us Help You Prototype Quickly
- Safeguard IoT Designs with Holistic Approach to Security
- Surprising Facts About the Cost to Operate Your Electric Car
- 让黑客远离您的POS终端
- 高级汽车照明——重新定义更高性能与安全性
- Applying Peak Current Mode Control for High Performance in Switching Regulators
- iButton背后的故事
- Meeting Big Demands for Power in Small Devices
- The Jedi Master – Cyber-Physical Systems and Industrial Convergence
- 快速了解如何利用NFC保护您的系统
- Test Engineer Celebrates 25 Years at Maxim
- 支持虚拟医疗的三种创新技术
- nanoMan:使用这款电源设计仿真工具
- Designing Accurate, Wearable Optical Heart Rate Monitors
- Maxim Interns Showcase Summer Projects
- Protect Your Medical Device Endpoints with Secure Authenticators
- Are Your Power Supplies Doing the Job?
- 特斯拉的Model 3改用PMAC同步驱动电机
- Learn 3 Key Ways to Lock In Security for Your IoT Design
- Recloser Controllers Maintain Smart Grid Uptime
- Operate Your Design from a Single Battery, with the Right Converter
- Show Your Engineering Ingenuity in Summer of Love Contest
- SDR Baseband Processing—Flexibly and Cost-Effectively
- Embedded Security ICs Safeguard PCs and Payments
- Want Your Oven to Play Your Favorite U2 Song?
- Choosing the Right Power Management ICs for Automotive Designs
- 设计耳戴式设备?微型PMIC可有效提升电池寿命
- Webinar: Learn Why It’s Smart to Have a Low IQ
- Why Sensors Are the Next Big Thing
- Building a Self-Balancing Robot with Feature-Rich Featherboard
- Helping You Create Rugged, Long-Lasting Mil/Aero Designs
- Why You Can’t Afford to Overlook Design Security
- Why Iso-Buck Converters Are Better than Flyback Converters
- Learn Ways to Improve Power Efficiency—Free Seminar
- Are Machines Taking Over?
- Are You Doing Enough to Build Trust in Our Connected World?
- Aggies Invent: 48 Hours from Idea to Prototype
- IoT World: From IoT Patterns to Blockchain Security
- Building the Self-Aware Digital Factory
- Flexound Systems Brings Immersive Dimension to Music
- Better Battery Runtimes Without Characterization
- Driving Greater Performance and Safety from Advanced Automotive Lighting
- 安全IC如何保护IoT设备中的数据传输
- How Fast Can You Solve This Crossword Puzzle?
- Why Not Design a Smaller PLC?
- 5 Blog Posts You Don’t Want to Miss
- Q&A: Maxim's Randall Wollschlager on Designing the Future Car
- Simplify Power Circuit Design with Simulation
- How Medical Wearables Enhance Quality of Life
- IO-Link Handbook Presents Primer on Designing Sensors and Masters
- ELIV 2017: Learn Ways to Design Safer, Smarter Cars
- Infomart Creates Tiny Power-over-Ethernet Devices
- Advancing Safety and Infotainment for Cars of Today and the Future
- How PA Linearization Solves Key Challenge for Remote PHY Fiber Nodes
- 更安全、更智能汽车的必经之路
- Many Technologies Are Vying for Your IoT Wide Area Network Design
- Are Your IoT Devices Immune to Cyberattacks?
- Machine Learning Club Drives Data Science Demand
- Designing Tiny, Connected Products? Don’t Miss this Webinar
- How Factory Automation Can Support Reshoring
- How Can We Create One Trillion Connected Devices?
- Modular System Speeds Up IoT Design Cycle
- Keep Designs Cool with a Tiny, Low-Power Temperature Sensor
- Circuit Protection You Might Not Have Thought About
- 你无法盗取一个并不存在的密钥
- See Demos of Turnkey Security ICs at TRUSTECH
- Synchronous Switching Regulators: Talk Time or Standby Time?
- 5 Ways Solar Power Usage Will Change By 2037
- What Kind of World Will One Trillion Connected Devices Produce?
- Can We Fix the Cybersecurity Mess?
- Three Great Personal Gadgets for Engineers
- Secure TLS in Connected Devices with a Companion Security IC
- Are There One Trillion Things to Connect?
- Maxim to Demo High-Speed SerDes Links and More at CES 2018
- Achieve Precision Control of Vibration for Wearables
- Secure Microcontrollers Safe from Spectre and Meltdown Flaws
- How to Stop an Invasive Attack on Your Design
- Smaller, Lower Power 4-20mA Sensor Transmitters for Industrial Equipment
- 利用安全电量计防止假冒电池
- Get Technical Tips from Maxim in the Lab Videos
- 如何通过电池电量计建立客户信任
- Sustaining the IoT—What Will This Take?
- With Reference Designs, No Need to Reinvent the Wheel
- How a Software Isolation Solution Protects IoT Devices
- AM Radio in Your Electric Vehicle? Not Always
- Get Technical Tips from Maxim Unfiltered Videos
- Wirelessly Charge Your Next Design
- 数字健康技术如何改善预防性保健护理
- A Look at the Latest Battery Technology from Tesla
- #MakewithMaxim Inspires Engineering Inventiveness
- Extend Vehicle Driving Range with Accurate Battery Management System
- 需要更紧凑封装的即插即用电源?您找对地方了
- Powering Motor Encoders and Resolvers
- Kids Invent Their Future at Upcoming Invention Convention
- Catch this Webinar If You're Designing Hearables and Wearables
- Flow Battery Technologies for Utility-Scale Systems
- High-Speed Serial Links for ADAS and Infotainment
- Got an IoT Design Idea? Enter Our Contest
- 谁是WiFi设备的背后英雄
- 遇见“达尔文”,为IoT而生的全新微控制器“物种”
- Which Type of Analog Hero Are You?
- How Security ICs Address New Medical Device Regulations
- Deminar: 3 Ways that Analog ICs Can Strengthen Your Design
- On-Demand Webinar: Hardware Security with PUF Technology
- The Beauty of Precision Op Amps
- Kid Inventors Showcase STEM Skills at California Invention Convention
- How iButton Can Enhance Food Quality
- Why Your Audio DAC or Digital Amp Should Spec Dynamic Range Instead of SNR
- Increase Motion Control System Accuracy with Higher Performance RS-485 Transceivers
- Designing Secure, Scalable Contactless Payment Systems
- High-Bandwidth Serial Links for Safer Cars
- Keeping an Eye on Battery SOC in Wearables and Hearables
- Get High-Speed USB Port Protection for Industrial Voltages
- Don’t Worry – Isolate All Those Digital Signals
- Keep Tabs on Essential Electronic Loads with Supervisory ICs
- Optical Sensing Opens New Opportunities in Healthcare
- LED Bulb Inspires Creation of Maintenance-Free Cybernetic House
- A Better Listening Experience Starts with the Right Stereo Audio Codec
- Quieting the Noise: Meeting EMI Standards in Power Supply Designs
- Making Sweet Music with Raspberry Pi
- Putting Intelligence in the IoT
- Got a Wearable Health Design Idea? Here’s How to Make It Accurate
- What Will You Create with Optical Biosensors?
- How Can We Power Our Invisible Intelligence?
- What Can GPS Do for Your Design?
- Keeping the IoT Safe from Hackers
- Idea to IoT Product in Just Days? Talk to zGlue
- Regulate Car Battery Voltages for ADAS Applications
- Open-Source Framework Detects Memory Corruptions in Embedded Software
- Stop Straining Your Portables—Refine Your Power Strategies
- Choosing the Best Type of Temperature Sensor
- How to Stop Physical Tampering of Mobile POS Systems
- Summertime Fun Outside the Classroom
- Do You Trust Your Smart Medical Device?
- 支持常电工作电子设备的高性能PMIC
- nanoMan Meets DARWIN—and Powerful Things Happen
- Consider Your WLAN Power-Supply Temperature and PCB Size Carefully
- Why on Earth Don’t You Include a Clock in Your Design?
- Reinforced Digital Isolator Ensures Safety in Industrial Environments
- CAN Bus Continues Its Grand Popularity – in Automotive, IoT, and Automation
- Who Had the Winning Project in Our MAX32620FTHR Design Contest?
- Reaching for the Golden Ring: 4 Key Elements for Industrial Convergence
- 4 Ways to Extend Runtime of Small, Battery-Powered Electronics
- How Are You Managing Thermal Requirements of Shrinking Industrial Sensors?
- Accurate, Wrist-Based Heart-Rate Monitoring—Six Months Faster
- Getting a Finger on the Pulse of Well-Being
- LED Controllers Make Headlight System Design a Snap
- Smaller, Smarter, and More Powerful ICs—It’s All at electronica 2018
- Managing Low and High LED Currents for Matrix and Pixel Lighting
- An Ideal Diode Can Be an Engineer’s Best Friend
- 新PLC开发平台支持产业融合
- 7 Key Steps to Empowering Innovation
- Empowering Secure PIN-on-Glass Payments at TRUSTECH 2018
- Engineering Intern Creates Heat-Sensing Robot with LoRa Technology
- So Many Smart Devices, So Many Security Vulnerabilities
- Why Embedded Systems Designers Should Care About OpenSSL
- CES 2019 Preview
- Secure Authenticators Protect Artificial Pancreas
- A Simple Way to Increase Factory Uptime
- Simpler, More Efficient Secure Companion ICs for the IoT
- Secure Provisioning Platform Makes It Easier to Protect IoT Designs
- University Students Gain Industry 4.0 Experience with Smart Factory Demo
- Want Traffic Updates from Your Toilet?
- 如何延长电池供电设备的运行时间呢?方法如下
- Why Embedded Systems Designers Should Care About OpenSSL
- 5 Cool Gadgets that Engineers Might Want to Unwrap
- An Insider's View of Analog Artistry at electronica 2018
- One Way to Replace Power Rail Clusters in Small Electronic Devices
- Engineers Had Better Be Careful with Algorithms and AI
- Makers Make the Most of Analog ICs
- Get Inspired to Think Big and Design Small
- How LED Backlight Drivers Enable Bigger, Higher Resolution Automotive Displays
- How IoT Sensors Help Ensure Freshness and Quality of Perishables
- Fish Tanks Don’t Need Security—Unless They’re Part of the IoT
- How Manufacturing Systems Can Evolve to Enable the Industrial IoT
- 致力于打造更智能、更可持续的未来
- Squeeze More Out of Your Portable Electronics
- Cook Up Something Yummy for Pi Day
- Happy Birthday, James Kirk
- Using Optical Sensors to Detect Particles
- You Be the Judge of Creative Student Inventors
- Maxim Is Going to the Dogs in 2020
- 轻松实现您的USB-C设计
- 适用于IIOT设计的微型、高能效IO-LINK收发器
- How Ceramic Voltage References Enhance Long-Term Drift Performance
- What’s Needed to Implement Today’s Industrial IoT Architecture
- How Security Supervisors Safeguard IoT Devices
- On-Demand Webinar: Your FPGA Design Starts with the Right Power Supply
- Tips for Choosing Precise, Power-Efficient GNSS Receivers for Location-Based Applications
- Digital Instrument Clusters: Why Functional Safety is Important
- Channel Your Engineering Ingenuity for Star Wars Day
- How Will the Industrial IoT Architecture Evolve
- New Power Management Design Guides for Smart Buildings and Smart Factories
- Get Better Performance from Your ADAS Camera Systems
- How to Save Time and Space with Power Supply Designs
- Reference Designs: Designed, Built, and Tested—So You Won’t Have To
- Understand How Physically Unclonable Function Technology Can Benefit Your Design
- Meet Vehicle Emissions Standards with Supervisory and Watchdog-Timer ICs
- How to Derive More System Efficiency from Battery-Powered Designs
- 更高吞吐率、更低成本的半导体测试方案
- Want to Protect Your USB Port Without Slowing It Down?
- Sensors Expo: See Wearable Healthcare Technologies in Action
- 4 Reasons to Register for a Free Design Startup Pack
- How to Efficiently Power Tiny Industrial Sensors
- Don’t Go Breaking Your Heart to Add ECG to Your Wearable
- What You Need to Know About Battery Management Challenges
- System Loads Are No Match for This Current-Sense Amplifier
- Power Conversion Efficiency for Portable Designs
- Why Authenticators SHOULD be THE Key to Your Smart Lock
- Can Wearables Get People Off the Couch
- How Dynamic Voltage Scaling Saves Power in Wearables
- Can Wearables Reduce Healthcare Costs?
- How to Get Louder, Richer Sound from Micro Speakers
- When Is a Digital Output Not Just a Digital Output? When It’s Also a Digital Input!
- 3 Reasons to Use a Discrete Real-Time Clock in Your Wearable Design
- How Secure Authenticators Prevent Counterfeiting of Medical Disposables
- How to Minimize Power in Clocking Applications
- Are Sensor Clones Stealing Away Your Customers?
- Maxim Summer Interns Showcase Their Technical Talents
- What’s Driving Industry 4.0?
- Breakout Boards Give You a Head Start on Your Design
- RS-485 Just Got a Major Stamina Boost!
- Why Shrinking Sizes of RTCs Is Good News for Your Portable Designs
- The Ins and Outs of Voltage Supervisor ICs
- See If You Can Steal These Keys
- How Power Management ICs Support Smart Buildings
- How Analog ICs Fuel Wireless IoT Sensors
- Drive HB LEDs to Brighter Heights for Automotive Applications and More
- nanoPower Technology Translates into Happy Users
- Smartphone for Seniors Gets Smarter with Health Monitoring
- 为无线Android耳机提供高精度电池SoC数据
- Are Your Car Battery Packs in Danger of Failing?
- How an Old Digital Dog Can Learn New Analog Tricks
- CCCamp Badge is More than an Entry Ticket – It’s a Sensor-Rich Reference Design
- 5 Ways a MyMaximAir Guitar Gets Real with These Electronic Instruments Account Enhances Productivity
- Stress Your Power Supply, Not Yourself
- How to Drive Micro Speakers to Their Maximum Power Rating
- How to Get Accurate In-Ear Heart-Rate and SpO2 Monitoring
- Scare Up Some Electronic Tricks and Treats This Halloween
- How Wearables Can Become a More Integral Part of Healthcare
- Why Long Battery Life is the Lifeblood of Thread IoT Sensors
- Keep Perishables Safe with Reliable Temperature Monitoring
- Ask Michael: How Do I Make My High-Current Sensor IO-Link Compatible?
- PUI Audio Delivers Clean, Clear Sound from Tiny Speakers
- How Analog ICs Support Seismic Signal Detection
- Reference Designs with ECAD Files Mean Faster Circuit Design
- How GSEE-TECH Cut 6 Months from Analog Input Module Development Cycle
- 3 Ways an Integrated Bio-algorithm Sensor Hub Simplifies Wearable Designs
- Intelligent Buildings Get Smarter and Smarter
- Why New ICs Are Needed to Bring Intelligence to the Edge
- Learn How You Can Design a Power Supply in 5 Minutes
- Ask Michael: Swipe Right for the Isolated Gate Driver That’s a Perfect Match for GaN/SiC Switches
- Experience Wireless Battery Management at CES 2020
- Can Wearables Help Prevent the Silent Killer?
- Holiday Gift-Giving Guide: 5 Hot Tech Gadgets for Engineers
- Simplify System Power Design for Your Automotive Displays
- Add Diode ORing Without Losing Efficiency
- Function-Rich Diving Computer Fueled by Analog and Power Management ICs
- Getting to Reliable Sensor Data: Interaction Between Electronics, Optics, and Mechanical Design
- Calterah Semiconductor Delivers High-Performance, Power-Efficient mmWave Radar Tech
- Your Guide to the Advantages of Pack-Side Fuel Gauging
- How to Extend the Life of Your Smart Factory’s Wireless Beacons
- Power Up Internal Circuits While Simplifying Diagnostics for Signal Monitoring Applications
- Digital Input Design
- 抢占电动滑板车、电动自行车及其他位置跟踪IoT的电源设计挑战先机
- Future of Industrial Automation Demos at Embedded World
- How to Create Accurate Performance-Tracking Sports Wearables
- Quickly Simulate DC-DC Converters with SIMPLIS-Based Tool
- Guide to LiDAR Sensors for Self-Driving Cars
- Analog PAM4 Chipset in Hyperscale Data Centers
- Are Biometric Sensors the Key to Healthier Horses…and Humans?
- Is Pulse Transit Time Needed for Accurate Blood-Pressure Monitoring from Wearables?
- Need to Design Small, Reliable Earbuds in a Hurry? Sometimes It Pays to Play It Cool…
- MediaTek Taps Into GMSL SerDes Technology for Automotive Infotainment Solution
- How Analog Devices Are Enhancing LUXROBO’s IoT and Robotics Development Platform
- Say “No More” to Tedious Calculations for E Series Values
- How Secure Authentication Protects Your Automotive Designs from Counterfeiting
- How NCATEST Raised Performance and Lowered Power of Its Automated Test Equipment
- Ensuring Employee Safety During an Unprecedented Time
- How LiDAR Delivers Critical Distance-Sensing for Self-Driving Cars
- Why Does It Take a Pandemic to Realize the Value of Remote Patient Monitoring?
- What’s in Photoplethysmography Data? A Look at the Interaction Between Sensor Performance and Algorithms
- Charging Your Car’s Battery – in 1898
- Prioritizing Customer Focus to Save Lives
- How Capacitors Provide a Window into the Real Value of a Battery
- What’s All the Fuss About Cryptography?
为什么摄像头接口对ADAS系统设计至关重要
2017年5月18日
![]() |
作者: Jim Harrison 特邀博主,林肯科技通讯业务部 |
汽车正在快速演化成一台安全联网的自动驾驶机器人,能够感测环境、进行思考并采取自主措施。变化更快的也许是小型自动驾驶公共车辆——出租车、拼车或公交车,能够将我们从公共交通站、市中心或办公区域带到想去的地方(最后一公里)。
其中一个例子是2015年10月推出的NAVYA ARMA自动驾驶电动巴士。这台小型巴士能够安全搭载15名乘客,时速高达28英里,目前正在欧洲和美国的许多社区进行测试或运营,并于CES 2017期间亮相拉斯维加斯街头。
观察周围环境
无论是小型汽车还是公共巴士,自动驾驶车辆都需要摄像头、雷达或激光雷达来感测周围的环境。利用这些传感器组合,汽车的高级驾驶辅助系统(ADAS)就能够检测车辆四周的环境。配备多个视频摄像头(至少5个,但通常多达8个)是系统的关键。车辆前方以及后置的摄像头需要高灵敏度和快速响应,以帮助监测交叉路口和碰撞,并正在迅速普及成为许多小汽车和SUV的标准配置。所有全景摄像头的组合为紧急制动辅助系统、自适应巡航控制、盲点检测、倒车盲点警示系统、车道偏离警告/自动车道保持提供可靠的信息,以及不久之后,您的爱车将支持交通标识识别系统,所以您将永远不会超过限速。
至关重要的摄像系统
举个例子,特斯拉(Tesla)汽车上的最新硬件套件采用了NVIDIA Drive PX 2处理平台,分别从8个摄像头、超声传感器组合和1个雷达系统获取数据。该平台可从支持自动巡航(AutoCruise)的高能效掌上模块扩展成为支持全自动驾驶、功能强大的AI超级计算机。系统能够实时了解车辆周围的情况,在高清晰度地图上精准的定位自己,并规划安全的前进路径。系统结合深度学习、传感器融合和全景视觉来改变驾驶体验。
摄像系统的性能对于安全辅助或自动驾驶车辆至关重要。当然,摄像头分布在车辆周围,往往与CPU相距甚远。其性能决定了ADAS能够看到多远的物体、能够检测到多小的物体,以及信息的传输速度——取决于分辨率、动态范围和帧速率。鉴于这些设备提供的信息的关键性,高误码率是不能容忍度的,因为其数据速率也是非常高的。在全景视图系统中,每个摄像头的视频流通常为1280 × 800像素分辨率,帧刷新率为30 f/s。
汽车中使用了大量的总线或网络,包括CAN、LIN、FlexRay、MOST、LVDS及以太网。但视频链路要求的数据速率排除了LVDS和以太网之外的所有总线类型。
更好的解决方案
一种更好的方案是吉比特多媒体串行链路(GMSL),它是以太网的无压缩替代方案。因此,与以太网相比,GMSL的数据速率快10倍,电缆成本降低50%,且EMC性能更好。Maxim提供MAX96707和MAX96708 GMSL串行器/解串器芯片,采用电流型逻辑(CML),具有极高的抗噪性,能够通过50 Ω低成本同轴电缆或100 Ω双绞线电缆传输数据,距离长达15m。器件能够与串行码率高达1.74Gbps的兆像素摄像头配合工作。摄像头数据时钟为12.5MHz至87MHz × 12位 + H/V数据,或36.66MHz至116MHz × 12位 + H/V数据(使用内部编码)。IC之间以及与外部源之间共用一个9.6kbps至1Mbps 的I2C控制通道,用于更新和设置。值得一提的是,器件能够在检测到误码时自动重发控制数据。控制通道被多路复用到串行链路,无论是否有视频通道。
MAX96707串行器IC具有可编程预加重/预减重,以驱动较长的电缆。器件能够对视频和控制数据进行检错,具有交叉点开关,用于双摄像头选择。串行输出提供可编程扩频。芯片采用小尺寸、24引脚、4 x 4mm TQFN封装,使用1.7至1.9V电源。最大电源电流为88mA。
图1. MAX96707功能框图
MAX96708解串器可跟踪扩频串行输入的数据,芯片的自适应均衡极大地降低了误码率。输出交叉点开关提高了灵活性。IC的核心电源范围为1.7至1.9V,I/O电源为1.7至3.6V。器件采用32引脚5 x 5mm TQFN封装。
图2. MAX96708COAXEVKIT#开发套件
两款芯片工作在-40º至115ºC温度范围,拥有±8kV接触放电保护和±15kV气隙静电放电保护,符合IEC 61000-4-2和ISO 10605标准。两款器件均满足汽车标准AEC-Q100。经销商提供评估套件(图2)。
毫无疑问,如果我正在设计一套自动驾驶系统,一个关键的问题就是与摄像头进行可靠的通信。我会在实际车辆配置和最差噪声条件下仔细检查所有摄像头连接的误码率,因此GMSL技术很可能为这一关键领域提供最佳的成功机会,在满足行业标准的同时提供高可靠性。