-
- Can a Supercapacitor Replace Your Battery for Backup Power
- What Can You Create with Frequency Synthesizers?
- How Fast and Safe Will 5G Wireless Networks Be
- These Industrial Communications ICs are Oldies but Goodies for Good Reason
- DIY Engineering Projects for Your Valentine
- Why Embedded Systems Designers Should Care About OpenSSL
- Balancing Power Demands of High-Voltage Automotive Power Applications
- PUF Technology Protects Against Invasive Attacks
- 快速、高精度电池管理系统助力更安全的电动汽车
- MAXIM远程调谐器方案帮助简化车载音响系统设计
- Moving Toward Value-Based Healthcare Using Wearables and Patient-Generated Data
- A Smarter Way to Design Touchscreens
- Want to Avoid Counterfeiting?
- Ultra-Small Wearable Healthcare Design Platform
- 打开口袋,释放工业4.0的洪荒之力
- Solving EMI Challenges in LED Headlamps
- embedded world 2017
- 工程设计是为傻瓜准备的(我就是活生生的例子)
- See & Hear Maxim Technologies at Mobile World Congress
- Keeping Cars Safe and Reliable Via ISO 26262 Certification
- Fast (But Not Too Fast) Op Amps for Reliable Very Low-Power Systems
- Shade-Proof Your Solar with Maxim Solar Cell Optimizers
- How Machine Learning Can Speed Up Your Design Cycle
- MakeWithMaxim Design Contest
- IO-Link —“智造”无限可能!
- How 3D Printers Help You Evaluate ICs
- Optical Networking Technologies OFC 2017
- How You Can Help Bring 20.8 Billion Connected Things Into the World
- 参考设计不仅仅是IC,而是完备的系统
- 工业4.0来势汹涌,“模拟整合”是主要受益者之一
- Putting the power of Industry 4.0 in your Pocket
- Battery fuel gauge ICs do more
- Reference Designs: Game Changers for Complex Projects
- 为什么黑客急不可耐地想进入您的汽车
- 您的家居可能越来越智能——但防止黑客的安全性又如何呢?
- What’s Your Favorite IoT Platform? Vote Today!
- 实现智能电网故障的快速、高精度检测
- Template
- 隔离电源参考设计
- 多通道、通用模拟输入 参考设计
- Fitness/Wellness Wearables Reference Design Saves Development Time and Effort
- Simplifying Design of Pulse Rate/Blood-Oxygen Wearables
- Don’t Design the Next Useless IoT Gadget
- Exactly What the Doctor Ordered: Cars that Monitor Their Own Health and Yours
- Reducing Component Count in Factory Automation Applications
- Maxim Highlights Auto, Wearable Healthcare Tech at CES
- Cut 6 Months Off Health Application Design Cycle
- Future Engineers Make with Maxim at Yale’s YHack Hackathon
- Interesting Inventions Inspire Ingenuity
- Ants Have Their Own Smart Cities—Why Can’t We?
- Proximity Sensing Made Easier
- Get Longer Battery Life By Lowering Quiescent Current
- Eat Pie and Win a Dev Board
- Why System Monitoring ICs Are Good Analog Insurance
- Who is nanoMan?
- Why Now Is the Time to Consider Wired Interface Solutions
- Get to Market Quickly with Your Secure Wearable Health Designs
- Why Powerline Communications is Great for Noisy Industrial Environments
- How Factory Automation Can Support Reshoring
- Don’t Become the Next Hacking Headline
- One Smart Design: Low IQ Boost Converter
- A Look at the Future of Wearable Healthcare Design
- 为什么摄像头接口对ADAS系统设计至关重要
- Reduce Calibration Costs for Industrial Process Control
- Making Smart Energy Even Smarter Via nanoPower Technology
- We Love Startups! Let Us Help You Prototype Quickly
- Safeguard IoT Designs with Holistic Approach to Security
- Surprising Facts About the Cost to Operate Your Electric Car
- 让黑客远离您的POS终端
- 高级汽车照明——重新定义更高性能与安全性
- Applying Peak Current Mode Control for High Performance in Switching Regulators
- iButton背后的故事
- Meeting Big Demands for Power in Small Devices
- The Jedi Master – Cyber-Physical Systems and Industrial Convergence
- 快速了解如何利用NFC保护您的系统
- Test Engineer Celebrates 25 Years at Maxim
- 支持虚拟医疗的三种创新技术
- nanoMan:使用这款电源设计仿真工具
- Designing Accurate, Wearable Optical Heart Rate Monitors
- Maxim Interns Showcase Summer Projects
- Protect Your Medical Device Endpoints with Secure Authenticators
- Are Your Power Supplies Doing the Job?
- 特斯拉的Model 3改用PMAC同步驱动电机
- Learn 3 Key Ways to Lock In Security for Your IoT Design
- Recloser Controllers Maintain Smart Grid Uptime
- Operate Your Design from a Single Battery, with the Right Converter
- Show Your Engineering Ingenuity in Summer of Love Contest
- SDR Baseband Processing—Flexibly and Cost-Effectively
- Embedded Security ICs Safeguard PCs and Payments
- Want Your Oven to Play Your Favorite U2 Song?
- Choosing the Right Power Management ICs for Automotive Designs
- 设计耳戴式设备?微型PMIC可有效提升电池寿命
- Webinar: Learn Why It’s Smart to Have a Low IQ
- Why Sensors Are the Next Big Thing
- Building a Self-Balancing Robot with Feature-Rich Featherboard
- Helping You Create Rugged, Long-Lasting Mil/Aero Designs
- Why You Can’t Afford to Overlook Design Security
- Why Iso-Buck Converters Are Better than Flyback Converters
- Learn Ways to Improve Power Efficiency—Free Seminar
- Are Machines Taking Over?
- Are You Doing Enough to Build Trust in Our Connected World?
- Aggies Invent: 48 Hours from Idea to Prototype
- IoT World: From IoT Patterns to Blockchain Security
- Building the Self-Aware Digital Factory
- Flexound Systems Brings Immersive Dimension to Music
- Better Battery Runtimes Without Characterization
- Driving Greater Performance and Safety from Advanced Automotive Lighting
- 安全IC如何保护IoT设备中的数据传输
- How Fast Can You Solve This Crossword Puzzle?
- Why Not Design a Smaller PLC?
- 5 Blog Posts You Don’t Want to Miss
- Q&A: Maxim's Randall Wollschlager on Designing the Future Car
- Simplify Power Circuit Design with Simulation
- How Medical Wearables Enhance Quality of Life
- IO-Link Handbook Presents Primer on Designing Sensors and Masters
- ELIV 2017: Learn Ways to Design Safer, Smarter Cars
- Infomart Creates Tiny Power-over-Ethernet Devices
- Advancing Safety and Infotainment for Cars of Today and the Future
- How PA Linearization Solves Key Challenge for Remote PHY Fiber Nodes
- 更安全、更智能汽车的必经之路
- Many Technologies Are Vying for Your IoT Wide Area Network Design
- Are Your IoT Devices Immune to Cyberattacks?
- Machine Learning Club Drives Data Science Demand
- Designing Tiny, Connected Products? Don’t Miss this Webinar
- How Factory Automation Can Support Reshoring
- How Can We Create One Trillion Connected Devices?
- Modular System Speeds Up IoT Design Cycle
- Keep Designs Cool with a Tiny, Low-Power Temperature Sensor
- Circuit Protection You Might Not Have Thought About
- 你无法盗取一个并不存在的密钥
- See Demos of Turnkey Security ICs at TRUSTECH
- Synchronous Switching Regulators: Talk Time or Standby Time?
- 5 Ways Solar Power Usage Will Change By 2037
- What Kind of World Will One Trillion Connected Devices Produce?
- Can We Fix the Cybersecurity Mess?
- Three Great Personal Gadgets for Engineers
- Secure TLS in Connected Devices with a Companion Security IC
- Are There One Trillion Things to Connect?
- Maxim to Demo High-Speed SerDes Links and More at CES 2018
- Achieve Precision Control of Vibration for Wearables
- Secure Microcontrollers Safe from Spectre and Meltdown Flaws
- How to Stop an Invasive Attack on Your Design
- Smaller, Lower Power 4-20mA Sensor Transmitters for Industrial Equipment
- 利用安全电量计防止假冒电池
- Get Technical Tips from Maxim in the Lab Videos
- 如何通过电池电量计建立客户信任
- Sustaining the IoT—What Will This Take?
- With Reference Designs, No Need to Reinvent the Wheel
- How a Software Isolation Solution Protects IoT Devices
- AM Radio in Your Electric Vehicle? Not Always
- Get Technical Tips from Maxim Unfiltered Videos
- Wirelessly Charge Your Next Design
- 数字健康技术如何改善预防性保健护理
- A Look at the Latest Battery Technology from Tesla
- #MakewithMaxim Inspires Engineering Inventiveness
- Extend Vehicle Driving Range with Accurate Battery Management System
- 需要更紧凑封装的即插即用电源?您找对地方了
- Powering Motor Encoders and Resolvers
- Kids Invent Their Future at Upcoming Invention Convention
- Catch this Webinar If You're Designing Hearables and Wearables
- Flow Battery Technologies for Utility-Scale Systems
- High-Speed Serial Links for ADAS and Infotainment
- Got an IoT Design Idea? Enter Our Contest
- 谁是WiFi设备的背后英雄
- 遇见“达尔文”,为IoT而生的全新微控制器“物种”
- Which Type of Analog Hero Are You?
- How Security ICs Address New Medical Device Regulations
- Deminar: 3 Ways that Analog ICs Can Strengthen Your Design
- On-Demand Webinar: Hardware Security with PUF Technology
- The Beauty of Precision Op Amps
- Kid Inventors Showcase STEM Skills at California Invention Convention
- How iButton Can Enhance Food Quality
- Why Your Audio DAC or Digital Amp Should Spec Dynamic Range Instead of SNR
- Increase Motion Control System Accuracy with Higher Performance RS-485 Transceivers
- Designing Secure, Scalable Contactless Payment Systems
- High-Bandwidth Serial Links for Safer Cars
- Keeping an Eye on Battery SOC in Wearables and Hearables
- Get High-Speed USB Port Protection for Industrial Voltages
- Don’t Worry – Isolate All Those Digital Signals
- Keep Tabs on Essential Electronic Loads with Supervisory ICs
- Optical Sensing Opens New Opportunities in Healthcare
- LED Bulb Inspires Creation of Maintenance-Free Cybernetic House
- A Better Listening Experience Starts with the Right Stereo Audio Codec
- Quieting the Noise: Meeting EMI Standards in Power Supply Designs
- Making Sweet Music with Raspberry Pi
- Putting Intelligence in the IoT
- Got a Wearable Health Design Idea? Here’s How to Make It Accurate
- What Will You Create with Optical Biosensors?
- How Can We Power Our Invisible Intelligence?
- What Can GPS Do for Your Design?
- Keeping the IoT Safe from Hackers
- Idea to IoT Product in Just Days? Talk to zGlue
- Regulate Car Battery Voltages for ADAS Applications
- Open-Source Framework Detects Memory Corruptions in Embedded Software
- Stop Straining Your Portables—Refine Your Power Strategies
- Choosing the Best Type of Temperature Sensor
- How to Stop Physical Tampering of Mobile POS Systems
- Summertime Fun Outside the Classroom
- Do You Trust Your Smart Medical Device?
- 支持常电工作电子设备的高性能PMIC
- nanoMan Meets DARWIN—and Powerful Things Happen
- Consider Your WLAN Power-Supply Temperature and PCB Size Carefully
- Why on Earth Don’t You Include a Clock in Your Design?
- Reinforced Digital Isolator Ensures Safety in Industrial Environments
- CAN Bus Continues Its Grand Popularity – in Automotive, IoT, and Automation
- Who Had the Winning Project in Our MAX32620FTHR Design Contest?
- Reaching for the Golden Ring: 4 Key Elements for Industrial Convergence
- 4 Ways to Extend Runtime of Small, Battery-Powered Electronics
- How Are You Managing Thermal Requirements of Shrinking Industrial Sensors?
- Accurate, Wrist-Based Heart-Rate Monitoring—Six Months Faster
- Getting a Finger on the Pulse of Well-Being
- LED Controllers Make Headlight System Design a Snap
- Smaller, Smarter, and More Powerful ICs—It’s All at electronica 2018
- Managing Low and High LED Currents for Matrix and Pixel Lighting
- An Ideal Diode Can Be an Engineer’s Best Friend
- 新PLC开发平台支持产业融合
- 7 Key Steps to Empowering Innovation
- Empowering Secure PIN-on-Glass Payments at TRUSTECH 2018
- Engineering Intern Creates Heat-Sensing Robot with LoRa Technology
- So Many Smart Devices, So Many Security Vulnerabilities
- Why Embedded Systems Designers Should Care About OpenSSL
- CES 2019 Preview
- Secure Authenticators Protect Artificial Pancreas
- A Simple Way to Increase Factory Uptime
- Simpler, More Efficient Secure Companion ICs for the IoT
- Secure Provisioning Platform Makes It Easier to Protect IoT Designs
- University Students Gain Industry 4.0 Experience with Smart Factory Demo
- Want Traffic Updates from Your Toilet?
- 如何延长电池供电设备的运行时间呢?方法如下
- Why Embedded Systems Designers Should Care About OpenSSL
- 5 Cool Gadgets that Engineers Might Want to Unwrap
- An Insider's View of Analog Artistry at electronica 2018
- One Way to Replace Power Rail Clusters in Small Electronic Devices
- Engineers Had Better Be Careful with Algorithms and AI
- Makers Make the Most of Analog ICs
- Get Inspired to Think Big and Design Small
- How LED Backlight Drivers Enable Bigger, Higher Resolution Automotive Displays
- How IoT Sensors Help Ensure Freshness and Quality of Perishables
- Fish Tanks Don’t Need Security—Unless They’re Part of the IoT
- How Manufacturing Systems Can Evolve to Enable the Industrial IoT
- 致力于打造更智能、更可持续的未来
- Squeeze More Out of Your Portable Electronics
- Cook Up Something Yummy for Pi Day
- Happy Birthday, James Kirk
- Using Optical Sensors to Detect Particles
- You Be the Judge of Creative Student Inventors
- Maxim Is Going to the Dogs in 2020
- 轻松实现您的USB-C设计
- 适用于IIOT设计的微型、高能效IO-LINK收发器
- How Ceramic Voltage References Enhance Long-Term Drift Performance
- What’s Needed to Implement Today’s Industrial IoT Architecture
- How Security Supervisors Safeguard IoT Devices
- On-Demand Webinar: Your FPGA Design Starts with the Right Power Supply
- Tips for Choosing Precise, Power-Efficient GNSS Receivers for Location-Based Applications
- Digital Instrument Clusters: Why Functional Safety is Important
- Channel Your Engineering Ingenuity for Star Wars Day
- How Will the Industrial IoT Architecture Evolve
- New Power Management Design Guides for Smart Buildings and Smart Factories
- Get Better Performance from Your ADAS Camera Systems
- How to Save Time and Space with Power Supply Designs
- Reference Designs: Designed, Built, and Tested—So You Won’t Have To
- Understand How Physically Unclonable Function Technology Can Benefit Your Design
- Meet Vehicle Emissions Standards with Supervisory and Watchdog-Timer ICs
- How to Derive More System Efficiency from Battery-Powered Designs
- 更高吞吐率、更低成本的半导体测试方案
- Want to Protect Your USB Port Without Slowing It Down?
- Sensors Expo: See Wearable Healthcare Technologies in Action
- 4 Reasons to Register for a Free Design Startup Pack
- How to Efficiently Power Tiny Industrial Sensors
- Don’t Go Breaking Your Heart to Add ECG to Your Wearable
- What You Need to Know About Battery Management Challenges
- System Loads Are No Match for This Current-Sense Amplifier
- Power Conversion Efficiency for Portable Designs
- Why Authenticators SHOULD be THE Key to Your Smart Lock
- Can Wearables Get People Off the Couch
- How Dynamic Voltage Scaling Saves Power in Wearables
- Can Wearables Reduce Healthcare Costs?
- How to Get Louder, Richer Sound from Micro Speakers
- When Is a Digital Output Not Just a Digital Output? When It’s Also a Digital Input!
- 3 Reasons to Use a Discrete Real-Time Clock in Your Wearable Design
- How Secure Authenticators Prevent Counterfeiting of Medical Disposables
- How to Minimize Power in Clocking Applications
- Are Sensor Clones Stealing Away Your Customers?
- Maxim Summer Interns Showcase Their Technical Talents
- What’s Driving Industry 4.0?
- Breakout Boards Give You a Head Start on Your Design
- RS-485 Just Got a Major Stamina Boost!
- Why Shrinking Sizes of RTCs Is Good News for Your Portable Designs
- The Ins and Outs of Voltage Supervisor ICs
- See If You Can Steal These Keys
- How Power Management ICs Support Smart Buildings
- How Analog ICs Fuel Wireless IoT Sensors
- Drive HB LEDs to Brighter Heights for Automotive Applications and More
- nanoPower Technology Translates into Happy Users
- Smartphone for Seniors Gets Smarter with Health Monitoring
- 为无线Android耳机提供高精度电池SoC数据
- Are Your Car Battery Packs in Danger of Failing?
- How an Old Digital Dog Can Learn New Analog Tricks
- CCCamp Badge is More than an Entry Ticket – It’s a Sensor-Rich Reference Design
- 5 Ways a MyMaximAir Guitar Gets Real with These Electronic Instruments Account Enhances Productivity
- Stress Your Power Supply, Not Yourself
- How to Drive Micro Speakers to Their Maximum Power Rating
- How to Get Accurate In-Ear Heart-Rate and SpO2 Monitoring
- Scare Up Some Electronic Tricks and Treats This Halloween
- How Wearables Can Become a More Integral Part of Healthcare
- Why Long Battery Life is the Lifeblood of Thread IoT Sensors
- Keep Perishables Safe with Reliable Temperature Monitoring
- Ask Michael: How Do I Make My High-Current Sensor IO-Link Compatible?
- PUI Audio Delivers Clean, Clear Sound from Tiny Speakers
- How Analog ICs Support Seismic Signal Detection
- Reference Designs with ECAD Files Mean Faster Circuit Design
- How GSEE-TECH Cut 6 Months from Analog Input Module Development Cycle
- 3 Ways an Integrated Bio-algorithm Sensor Hub Simplifies Wearable Designs
- Intelligent Buildings Get Smarter and Smarter
- Why New ICs Are Needed to Bring Intelligence to the Edge
- Learn How You Can Design a Power Supply in 5 Minutes
- Ask Michael: Swipe Right for the Isolated Gate Driver That’s a Perfect Match for GaN/SiC Switches
- Experience Wireless Battery Management at CES 2020
- Can Wearables Help Prevent the Silent Killer?
- Holiday Gift-Giving Guide: 5 Hot Tech Gadgets for Engineers
- Simplify System Power Design for Your Automotive Displays
- Add Diode ORing Without Losing Efficiency
- Function-Rich Diving Computer Fueled by Analog and Power Management ICs
- Getting to Reliable Sensor Data: Interaction Between Electronics, Optics, and Mechanical Design
- Calterah Semiconductor Delivers High-Performance, Power-Efficient mmWave Radar Tech
- Your Guide to the Advantages of Pack-Side Fuel Gauging
- How to Extend the Life of Your Smart Factory’s Wireless Beacons
- Power Up Internal Circuits While Simplifying Diagnostics for Signal Monitoring Applications
- Digital Input Design
- 抢占电动滑板车、电动自行车及其他位置跟踪IoT的电源设计挑战先机
- Future of Industrial Automation Demos at Embedded World
- How to Create Accurate Performance-Tracking Sports Wearables
- Quickly Simulate DC-DC Converters with SIMPLIS-Based Tool
- Guide to LiDAR Sensors for Self-Driving Cars
- Analog PAM4 Chipset in Hyperscale Data Centers
- Are Biometric Sensors the Key to Healthier Horses…and Humans?
- Is Pulse Transit Time Needed for Accurate Blood-Pressure Monitoring from Wearables?
- Need to Design Small, Reliable Earbuds in a Hurry? Sometimes It Pays to Play It Cool…
- MediaTek Taps Into GMSL SerDes Technology for Automotive Infotainment Solution
- How Analog Devices Are Enhancing LUXROBO’s IoT and Robotics Development Platform
- Say “No More” to Tedious Calculations for E Series Values
- How Secure Authentication Protects Your Automotive Designs from Counterfeiting
- How NCATEST Raised Performance and Lowered Power of Its Automated Test Equipment
- Ensuring Employee Safety During an Unprecedented Time
- How LiDAR Delivers Critical Distance-Sensing for Self-Driving Cars
- Why Does It Take a Pandemic to Realize the Value of Remote Patient Monitoring?
- What’s in Photoplethysmography Data? A Look at the Interaction Between Sensor Performance and Algorithms
- Charging Your Car’s Battery – in 1898
- Prioritizing Customer Focus to Save Lives
- How Capacitors Provide a Window into the Real Value of a Battery
- What’s All the Fuss About Cryptography?
应对电池老化,用电量计赢得客户信任
2018年3月1日
![]() |
作者: Bakul Damle Maxim Integrated电池管理业务总监 |
最近,您可能听说了这则新闻 — 智能手机制造商为了适应电池的老化而将旧型号的产品降速,以防止电池老化的手机意外关机。
虽然本意是好的,但该新闻仍然引起了客户的强烈反对,很大程度上是因为客户无法获得详细的电池信息,以及厂商没有对管理旧电池的方式做出明确的说明。这一事件也确实引发了人们的关注,且提升了向客户提供可靠电池信息的重要性。
管理老化电池并不难
目前使用的大多数移动设备采用锂离子电池,电池性能会随时间推移下降。电池容量会变小、内部阻抗变大。老化电池的负载较重时,与轻载相比,可利用的容量较小,这是因为旧电池比新电池的阻抗高。
在您的电池供电设计中集成电量计IC为管理旧电池提供了相对简单的途径。除了许多电量计提供的充电状态(SOC)数据外,Maxim ModelGauge™ m5 IC等新型电量计也提供以下数据基准点:
- 可用容量和报告容量
- 老化
- 定时器
- 剩余工作时间
- 周期
- 老化预测
- 电池电阻
您可根据客户的期望决定披露哪些信息,这有助于他们更好地管理电池供电设备,帮助建立客户对电池管理方式的信任。
以下我们较为详细地讨论一下各个参数。
可用容量和报告容量
ModelGauge m5的空电量补偿特性估算理论剩余容量(RemCapMIX,假设理想电池条件)和可用容量(RemCapAV,考虑负载、温度和老化因素)。可用容量会随负载或温度的任何变化而立刻发生变化。然而,这会造成数值的突然跳变,取决于负载或温度变化。例如,即使没有连接充电器,如果仅仅是从重载变为轻载,看到可用容量发生跳变可能会引起混淆。为缓解这一问题,可使用报告容量(RemCapREP)将剩余容量传递至用户界面。报告容量不会像可用容量那样发生突然变化。负载发生变化时,其轨迹仅仅是重新瞄准可用容量估算的相同剩余工作时间。
图1. 可用容量和报告容量为设备用户提供电池寿命指标
老化
电量计中的老化寄存器是当前满容量与原始设计容量的百分比,一般随电池使用时间的推移发生下降。
定时器
定时器允许电量计跟踪电池的老化,采用自IC首次连接到电池以来的绝对时间。部分Maxim电量计也定期将该信息备份到片上非易失存储器,作为学习功能的一部分。对于其他电量计,主机系统可定期保存该信息,并在掉电时将其恢复到IC。
剩余工作时间
在特定负载以及假设负载或功率下的剩余工作时间(TTE),是另一个非常有用的参数。启动高负载任务之前,系统可查询电量计,检查电池是否支持成功完成该任务所需的预期运行时间。该措施可用于防止高负载任务发生中断,从而防止意外崩溃,特别是电池电量较低时。系统可主动采取电源管理措施,仅允许轻载任务,或者提示消费者电池电量太低,无法支持某些高负载功能。
周期
周期寄存器保存电池经历过的充电/放电周期总次数,对部分以及完整周期进行累计,就像汽车上的里程表一样。
Cycle+老化预测
Cycle+老化预测估算消费者在电池寿命期间可利用的周期次数。Model Gauge m5算法监测电池容量随时间发生的变化,并计算电池容量下降到预设门限所需的周期次数。该预测可用于及时更换电池,或者采取其他电池管理措施,通过动态改变充电特性来延长电池寿命。
电池电阻
电阻寄存器包含计算的电池内阻平均值,是通过将开路电压与长时间内负载或充电条件下的测量电压进行比较实现的,一般随电池使用时间的推移逐渐增大。
延长运行时间、提高性能
为进一步增强用户体验,电量计IC可提供一些主动电池管理能力。例如,许多Maxim电量计包括一种名为动态电池电源的特性,允许优化CPU性能,实现更好的运行时间。这是通过将CPU降速到正好能够防止系统奔溃的水平来实现的。例如,在许多单节电池供电的应用中,系统要求至少3.3V电压才能正确工作。通过将电量计配置为动态电池电源,可将系统的负载控制或限制到电池的能力范围之内,确保不会低于最低系统电压,直到电池电量到达极低状态,此时可从容地关闭系统。所以,用户既可获得延长运行时间,又能避免电池欠压造成意外崩溃。如果没有类似动态电池电源的功能,系统制造商实际上就相当于盲目地限制系统性能,从而招致客户的反感。
部分Maxim电量计还拥有可编程、高速电流比较器,可监测和控制峰值负载,防止造成电池崩溃。这些比较器被触发时,向主机系统发送报警,后者即可采取相应的电源管理措施,降低峰值负载/尖峰。可将可编程门限设定为低于电池保护器限值,防止意外触发电池硬关断。这些比较器也可用于确保系统遵守电量计提供给主机系统的动态电源建议。
图2. 使用MAX17055电量计IC,动态电源功能估算放电期间的电源容量
总而言之,客户希望获得清晰的电池信息,以及运行时间与电池寿命相关的可能达到的性能平衡。凭借电量计IC,您能够为客户提供丰富的可靠电池信息。特别是Maxim电量计,不但提供各种能够延长运行时间的工具,而且也能够实现最高系统性能,帮助您赢得客户的信任。