应用笔记753

MAX1452 Serial Communications


Abstract: The MAX1452 utilizes asynchronous serial data communication via a single-pin interface. This application note provides a detailed description of the serial communication system used and should be read in conjunction with the MAX1452 data sheet.

This application note describes the serial communications system used in the MAX1452, and it is best read in conjunction with the MAX1452 data sheet. It expands on the serial communications information contained in the data sheet and provides communication examples.

MAX1452 Digital Mode

The MAX1452 digital input/output (DIO) provides single-pin serial communications with internal control functions and memory. All command inputs flow into a set of 16 registers, which form the interface register set (IRS). Additional levels of command processing are provided by control logic, which takes its inputs from the IRS. A bidirectional 16-bit latch buffers data to and from the 16-bit calibration registers and internal (8-bit-wide) EEPROM locations. Figure 3 shows the relationship between the various serial commands and the MAX1452's internal architecture.

Communication Protocol

The DIO serial interface is used for asynchronous serial data communications between the MAX1452 and a host calibration test system or computer. The MAX1452 automatically detects the baud rate of the host computer when the host transmits the initialization sequence. Baud rates between 4800 and 38,400 can be detected and used. The data format is always 1 start bit, 8 data bits, and 1 stop bit. The 8 data bits are transmitted LSB first, MSB last. A weak pullup can be used to maintain a logic 1 on DIO while the MAX1452 is in digital mode. This is to prevent unintended 1 to 0 transitions on this pin, which would be interpreted as a communication start bit. Communications are allowed only when the Secure-Lock™ byte is disabled (i.e., CL[7:0] = 00HEX) or UNLOCK is held high.

Initialization Sequence

The first command byte sent to the MAX1452 after power-up or following receipt of the re-initialization command is used by the MAX1452 to learn the communication baud rate. The initialization sequence is a 1-byte transmission of 81 hex, as follows:
The start bit, shown in bold above, initiates the baud-rate synchronization. The 8 data bits 81 hex (LSB first) follow this and then the stop bit, also shown in bold above. The MAX1452 uses this sequence to calculate the time interval for a 1-bit transmission as a multiple of the period of its internal oscillator. The resulting number of oscillator clock cycles is then stored internally as an 8-bit number (BITCLK). Note that the device's power supply should be stable for a minimum period of 1ms before the initialization sequence is sent. This allows time for the power-on reset function to complete and DIO to be configured by the Secure-Lock byte or UNLOCK.

Re-Initialization Sequence

The MAX1452 provides for re-establishing or relearning the baud rate. The re-initialization sequence is a 1-byte transmission of FF hex, as follows:
When a serial re-initialization sequence is received, the receive logic resets itself to its power-up state and waits for the initialization sequence. The initialization sequence must follow the re-initialization sequence to re-establish the baud rate.

Serial Interface Command Format

All communication commands into the MAX1452 follow the format of a start bit, 8 command bits (a command byte), and a stop bit. The command byte controls the contents of the interface register set and comprises a 4-bit interface register set address (IRSA) nibble and a 4-bit interface register set data (IRSD) nibble. The IRS byte command is structured as follows:

IRS[7:0] = IRSD[3:0] , IRSA[3:0]
All commands are transmitted LSB first. The first bit following the start bit is IRSA[0], and the last bit before the stop bit is IRSD[3], as follows:
Half of the register contents of the IRS are used for data hold and steering information. Data writes to two locations within the IRS cause immediate action (command execution). These locations are at addresses 9 and 15, and are the command register to internal logic and re-initialize commands, respectively. Table 9 shows a full listing of IRS address decoding.

Command sequences can be written to the MAX1452 as a continuous stream, for example, start bit, command byte, stop bit, start bit, command byte, stop bit, etc. There are no delay requirements between commands while the MAX1452 is receiving data.

Command Register to Internal Logic (CRIL)

A data write to the CRIL location (IRS address 9) causes immediate execution of the command associated with the 4-bit data nibble written. All EEPROM and calibration register Read and Write, together with EEPROM ERASE, commands are handled through the CRIL location. CRIL is also used to enable the MAX1452 analog output and to place output data (serial digital output) on DIO. Table 10 shows a full listing of CRIL commands.

Serial Digital Output

DIO is configured as a digital output by writing a Read IRS (RdIRS) command (5 hex) to the CRIL location. On receipt of this command, the MAX1452 outputs a byte of data, the contents of which are determined by the IRS pointer (IRSP[3:0]) value at location IRSA[3:0] = 8 hex. The data is output as a single byte, framed by a start bit and a stop bit. Table 12 lists the data returned for each IRSP address value.

Once the RdIRS command has been sent, all connections to DIO must be tri-stated to allow the MAX1452 to drive the DIO line. Following receipt of the RdIRS command, the MAX1452 drives DIO high after one byte time. The MAX1452 holds DIO high for a single bit time and then asserts a start bit by driving DIO low. The start bit is then followed by the data byte and a stop bit. Immediately following transmission of the stop bit, the MAX1452 will tri-state DIO, releasing the line. The MAX1452 will then be ready to receive the next command sequence one byte time after releasing DIO.

Note that there will be time intervals before and after the MAX1452 has sent the data byte when all devices on the DIO line will be tri-stated. It is recommended that a weak pullup be applied to the DIO line during these time intervals to prevent unwanted transitions. In applications where DIO and the analog output (OUT) are not connected, a pullup resistor should be connected permanently to DIO. If the MAX1452 DIO and OUT are connected, then it is important that this common line not be loaded during analog measurements. Under this circumstance, a suitable sequence of events would be as follows:

  1. Connect a pullup resistor to the DIO/OUT line (preferably using a relay).
  2. Send the RdIRS command.
  3. Tri-state the user connection (set to high impedance).
  4. Receive data from the MAX1452.
  5. Activate the user connection (pull DIO/OUT line high).
  6. Release the pullup resistor.
Figure 1 shows an example transmit/receive sequence with the RdIRS command (59 hex) being sent and the MAX1452 responding with a byte value of 10 hex.

Figure 1. DIO output data format.
Figure 1. DIO output data format.

Internal Clock Settings

Following initial power-up, or after a power reset, all of the calibration registers within the MAX1452 contain 00 hex and must be programmed. Note that, in analog mode, the internal registers are refreshed automatically from EEPROM.

When starting the MAX1452 in digital mode, special attention should be paid to the 3 CLK bits: 3MSBs of the configuration register. The frequency of the MAX1452 internal oscillator is measured during production testing, and a 3-bit adjustment (calibration) code is calculated and stored in the upper-3 bits of EEPROM location 161 hex (EEPROM upper-configuration byte). The MAX1452 internal clock controls all timing functions, including the signal-path gain, DAC functions, and communications. It is recommended that, while in digital mode, the configuration register CLK bits be assigned the values contained in EEPROM (the upper-configuration byte). The 3 CLK bits represent a two's complement number with a nominal clock adjustment of 9% per bit. Table 15 shows the codes and adjustment available.

Any change to the CLK bit values contained in the configuration register must be followed by the MAX1452 baud-rate learning sequence (the re-initialize and initialize commands). To maximize the robustness of the communication system during clock resetting, change the CLK bits by only 1LSB value at a time. The recommended setting procedure for the configuration register CLK bits is therefore as follows: Use a minimum baud rate of 9600 during the setting procedure to prevent potential overflow of the MAX1452 baud-rate counter with clock values near maximum.

The following example is based on a required CLK code of 010 binary:
Step 1. Read the CLK bits (3MSBs) from EEPROM location 161 hex CLK = 010 binary.
Step 2. Set the CLK bits in the configuration register to 001 binary.
Step 3. Send the re-initialize command, followed by the initialize (baud-rate learning) command.
Step 4. Set the CLK bits in the configuration register to 010 binary.
Step 5. Send the re-initialize command, followed by the initialize (baud-rate learning) command.
The frequency of the internal oscillator can be checked at any time by reading the value of BITCLK[7:0]. This 8-bit number represents the number of internal oscillator cycles corresponding to one cycle (one bit time) of the communications baud rate.

Erasing and Writing the EEPROM

The internal EEPROM must be erased (bytes set to FF hex) prior to programming the desired contents. The MAX1452 is supplied in a nominally erased state except for byte 161 hex and bytes 16B hex. The 3MSBs of byte 161 hex contain the internal oscillator calibration setting. Byte 16B hex is set to 00 hex to allow serial communication regardless of the status of "UNLOCK."

When erasing the EEPROM, you first save the 3MSBs of byte 161 hex. Following erasure, these 3 bits must be rewritten, together with the Secure-Lock byte value of 00 hex. Failure to do this can cause the part to stop communicating. Do not remove power from the device before rewriting these values.

The internal EEPROM can be erased entirely with the ERASE command or erased partially with the PageErase command (see Table 10, CRIL command). It is necessary to wait 6ms after issuing an ERASE or PageErase command. Any attempt to communicate with the part or to interrupt power before 6ms have elapsed can produce indeterminate states within the EEPROM.

To erase a page in EEPROM (PageErase command): First load the required page number (see Table 1) into the IRS location IEEA[3:0]. Then send a CRIL PageErase command (79 hex).

To write a byte to EEPROM: Load IRS locations IEEA[9:8], IEEA[7:4], and IEEA[3:0] with the byte address (Address[9:0]). Load IRS locations DHR[7:4] and DHR[3:0] with the 8 data bits to be written (Data[7:0]). Send the EEPROM WRITE command to CRIL (19 hex).

To read a byte from EEPROM: Load IRS locations IEEA[9:8], IEEA[7:4], and IEEA[3:0] with the byte address (Address[9:0]). Send a READ EEPROM command to the CRIL register (49 hex); this loads the required EEPROM byte into DHR[7:0]. Load IRS location IRSP[3:0] with 00 hex (return DHR[7:0]). Send the READ IRSP command to the CRIL register (59 hex).

Multiplexed Analog Output

The MAX1452 provides the facility to output analog signals while in digital mode via the read analog (RdAlg) command. One byte time after receiving the RdAlg command, the internal analog signal determined by the ALOC[3:0] register (see Table 14) is multiplexed to OUT. The signal remains connected to OUT for the duration set by the ATIM[3:0] register. The ATIM function uses the communication baud rate as a timing basis. See Table 13 for details. At the end of the period determined by ATIM[3:0], the analog signal is disconnected from the analog output and OUT resumes a tri-state condition. The MAX1452 can receive further commands on DIO 1 byte after resuming a tri-state condition on OUT. Figure 2 illustrates the timing of this scheme.

The MAX1452 DIO is tri-stated for the duration that the analog output is active. This is to allow the OUT and DIO pins to be connected in parallel. When DIO and OUT are connected in parallel, the host computer must also tri-state its communications connection to the MAX1452. This requirement will produce periods when all connections to DIO are tri-stated simultaneously, making it necessary to have a weak pullup resistor applied to DIO during these periods. See the "Serial Digital Output" section for more details.

A "continuous-output" mode is available for the analog output and is selected by setting ATIM[3:0] to F hex. This mode can be used only when DIO and OUT are separate. While in this mode and following receipt of the RdAlg command or any other command, DIO tri-states for a period of 32,769 byte times. Once this period has elapsed, DIO enters receive mode and will accept further command inputs. The analog output is always active while in continuous mode.

Note: The internal analog signals are not buffered when connected to OUT. Any loading of OUT while one of these internal signals is being measured is likely to produce measurement errors. Do not load the OUT pin when reading internal signals, such as BDR, FSOTC, etc.

Figure 2. Analog-output timing.
Figure 2. Analog-output timing.

Figure 3. Schematic of MAX1452 serial command structure and hardware.
Figure 3. Schematic of MAX1452 serial command structure and hardware.

Communication Command Examples

The following is a selection of examples of the command sequences for various functions within the MAX1452.

Example 1: Change the baud-rate setting, and check communications. Note: If communication with the MAX1452 is lost due to a system baud-rate change before sending the re-initialization command, a power reset will have to be applied in order to guarantee the initialization condition.
Command
Action
FF hex
Re-initialize part ready for baud-rate learning.
 
Change system baud rate to new value.
81 hex
Learn baud rate.
F8 hex
Load 15 (F hex) to IRSP[3:0] register.
59 hex
Read IRS.
 
Host computer must be ready to receive data on the serial line within one (baud-rate) byte time of sending the Read IRS command. The MAX1452 will return CA hex (IRSP values of 10 to 15 are configured to return CA hex for communication-checking purposes).


Example 2: Read the lookup table pointer (TEMP-INDEX).
Command
Action
78 hex
Load 7 to IRSP[3:0] register.
59 hex
Read IRS.
 
Host ready to receive data within one byte time of sending the Read IRS command. The MAX1452 will return the current TEMP-INDEX pointer value.


Example 3: Enable the BDR measurement on the OUT pin for 3.4-seconds duration with a 9600 baud rate.
Command
Action
1B hex
Load 1 (BDR measurement) to ALOC[3:0] register.
CA hex
Load 12 to the ATIM[3:0] register: (212+1) 8/9600 = 3.4secs.
69 hex
RdAlg
 
The DIO pin is tri-stated, and the OUT pin is connected internally to the BDR pin for a duration of approximately 3.4secs.


Example 4: Write 8C40 hex to the FSODAC register.
Command
Action
00 hex
Load 0 hex to the DHR[3:0] register.
41 hex
Load 4 hex to the DHR[7:4] register.
C2 hex
Load C hex to the DHR[11:8] register.
83 hex
Load 8 hex to the DHR[15:12] register.
36 hex
Load 3 (FSODAC) to the ICRA[3:0] register.
09 hex
Ld ICR
 
8C40 hex is written to the FSODAC register.


Example 5: Write 8C40 hex to the FSODAC lookup table location at TEMP-INDEX 40. This example uses the PageErase command to clear the relevant section of the EEPROM and assumes that none of the existing data in that section is required to be kept.
Command
Action
A6 hex
Load A hex (page number corresponding to EEPROM locations 280 hex and 281 hex) to the IEEA[3:0] register.
79 hex
PageErase command.
 
Wait 6ms before sending any further commands.
06 hex
Load 0 hex to the IEEA[3:0] register.
87 hex
Load 8 hex to the IEEA[7:4] register.
28 hex
Load 2 hex to the IEEA[9:8] (IRSP[3:0]) register.
00 hex
Load 0 hex to the DHR[3:0] register.
41 hex
Load 4 hex to the DHR[7:4] register.
19 hex
Write EEPROM. 40 hex is loaded to EEPROM address 280 hex, which is the low-byte location corresponding to a TEMP-INDEX pointer value of 40.
16 hex
Load 1 to the IEEA[3:0] register. IEEA[7:4] and IEEA[9:8] already contain 8 and 2, respectively.
C0 hex
Load C hex to the DHR[3:0] register.
81 hex
Load 8 hex to the DHR[7:4] register.
19 hex
Write EEPROM. 8C hex is loaded to EEPROM address 281 hex, which is the high-byte location corresponding to a TEMP-INDEX pointer value of 40.

Tables

Table 1. EEPROM Memory Address Map
Page
Low-Byte Address (Hex)
High-Byte Address (Hex)
TEMP-INDEX[7:0]
Contents
0
000
001
00
ODAC Lookup Table
03E
03F
1F
1
040
041
20
07E
07F
3F
2
080
081
40
0BE
0BF
5F
3
0C0
0C1
60
0FE
0FF
7F
4
100
101
80
13E
13F
9F
5
140
141
A0
15E
15F
AF to FF
160
161
-
Configuration
162
163
-
Reserved
164
165
-
OTCDAC
166
167
-
Reserved
168
169
-
FSOTCDAC
16A
16B
-
Control Location
16C
16D
-
52 General-Purpose User Bytes
17E
17F
-
6
180
181
-
19E
19F
-
1A0
1A1
80
FSODAC Lookup Table
1BE
1BF
8F
7
1C0
1C1
90
1FE
1FF
AF to FF
8
200
201
00
23E
23F
1F
9
240
241
20
27E
27F
3F
A
280
281
40
2BE
2BF
5F
B
2C0
2C1
60
2FE
2FF
7F


Table 2. Registers
Register
Description
CONFIG
Configuration Register
ODAC
Offset DAC Register
OTCDAC
Offset Temperature Compensation DAC
FSODAC
Full-Span Output DAC
FSOTCDAC
Full-Span Output Temperature Compensation DAC


Table 3. Configuration Register (CONFIG[15:0])
Field
Name
Description
15:13
OSC[2:0]
Oscillator frequency setting. Factory preset; do not change.
12
REXT
Logic '1' selects external RISC and RSTC.
11
CLK1M EN
Logic '1' enables CLK1M output driver.
10
PGA Sign
Logic '1' inverts INM and INP polarity.
9
IRO Sign
Logic '1' for positive input-referred offset (IRO). Logic '0' for negative input-referred offset (IRO).
8:6
IRO[2:0]
Input-referred offset (IRO) coarse offset adjustment.
5:2
PGA[3:0]
Programmable-gain amplifier gain setting.
1
ODAC Sign
Logic '1' for positive offset DAC output. Logic '0' for negative offset DAC output.
0
OTCDAC Sign
Logic '1' for positive offset TC DAC output. Logic '0' for negative offset TC DAC output.


Table 4. Input-Referred Offset (IRO[2:0])
IRO Sign, IRO[2:0]
Input-Referred Offset, Correction as % of VDD
Input-Referred Offset, Correction at VDD = 5VDC in mV
1,111
+1.25
+63
1,110
+1.08
+54
1,101
+0.90
+45
1,100
0.72
+36
1,011
0.54
+27
1,010
+0.36
+18
1,001
+0.18
+9
1,000
0
0
0,000
0
0
0,001
-0.18
-9
0,010
-0.36
-18
0,011
-0.54
-27
0,100
-0.72
-36
0,101
-0.90
-45
0,110
-1.08
-54
0,111
-1.25
-63


Table 5. PGA Gain Setting (PGA[3:0])
PGA[3:0]
PGA Gain (V/V)
0000
36
0001
48
0010
60
0011
72
0100
84
0101
96
0110
108
0111
120
1000
132
1001
144
1010
156
1011
168
1100
180
1101
192
1110
204
1111
216


Table 6. TEMP-INDEX Typical Values
Temperature
TEMP-INDEX[7:0]
(°C)
Decimal
Hexadecimal
-40
20
14
25
65
41
85
106
6A
125
134
86


Table 7. EEPROM ODAC and FSODAC Lookup-Table Memory Map
TEMP- INDEX[7:0]
EEPROM Address ODAC,
Low Byte and High Byte
EEPROM Address FSODAC,
Low Byte and High Byte
00 hex
000 hex and 001 hex
200 hex and 201 hex
to
to
to
7F hex
0FE hex and 0FF hex
2FE hex and 2FF hex
80 hex
100 hex and 101 hex
1A0 hex and 1A1 hex
to
to
to
AF hex
15E hex and 15F hex
1FE hex and 1FF hex


Table 8. Control Location (CL[15:8])
Field
Name
Description
15:8
CL[15:8]
Reserved.
7:0
CL[7:0]
Control location. Secure-Lock is activated by setting this to FF hex, disabling DIO serial communications and connecting VOUT to PGA output.


Table 9 IRSA Decoding
IRSA[3:0]
Description
0000
Write Irsd[3:0] to Dhr[3:0] (Data-Hold Register).
0001
Write Irsd[3:0] to Dhr[7:4] (Data-Hold Register).
0010
Write Irsd[3:0] to Dhr[11:8] (Data-Hold Register).
0011
Write Irsd[3:0] to Dhr[15:12] (Data-Hold Register).
0100
Reserved.
0101
Reserved.
0110
Write Irsd[3:0] to Icra[3:0] or Ieea[3:0] (Internal Calibration Register Address or Internal Eeprom Address Nibble 0).
0111
Write Irsd[3:0] to Ieea[7:4] (Internal Eeprom Address, Nibble 1).
1000
Write Irsd[3:0] to Irsp[3:0] or Ieea[9:8] (Interface Register Set Pointer Where Irsp[1:0] Is Ieea[9:8]).
1001
Write Irsd[3:0] to Cril[3:0] (Command Register to Internal Logic).
1010
Write Irsd[3:0] to Atim[3:0] (Analog Time-Out Value on Read).
1011
Write Irsd[3:0] to Aloc[3:0] (Analog Location).
1100-1110
Reserved.
1111
Write Irsd[3:0] = 1111bin to Any Irsa to Re-Initialize the Receive Serial Port.


Table 10. CRIL Command Codes
CRIL[3:0]
Name
Description
0000
LdICR
Load Internal Calibration Register at address given in ICRA with data from DHR[15:0].
0001
EEPW
EEPROM Write of 8 bits from DHR[7:0].
0010
ERASE
Erase all of EEPROM.
0011
RdICR
Read Internal Calibration Register as pointed to by ICRA and load data into DHR[15:0].
0100
RdEEP
Read Internal EEPROM location and load data into DHR[7:0].
0101
RdIRS
Read Interface Register Set Pointer IRSP[3:0].
0110
RdAlg
Output the multiplexed analog signal onto OUT the serial pin as an output. The analog location is specified in ALOC[3:0], and the duration (in byte times) that the signal is asserted onto the pin is specified in ATIM[3:0].
0111
PageErase
Page-erase the page of the EEPROM as pointed to by IEEA[9:6]. There are 64 bytes per page and thus 12 pages in the EEPROM.
1000-1111
Reserved
Reserved.


Table 11. ICRA Decode
ICRA[3:0]
Name
Description
0000
CONFIG
Configuration Register
0001
ODAC
Offset DAC Register
0010
OTCDAC
Offset Temperature Coefficient DAC Register
0011
FSODAC
Full-Scale Output DAC Register
0100
FSOTCDAC
Full-Scale Output Temperature Coefficient DAC Register
0101
-
Reserved. Do not write to this location (flash test).
0110 to 1111
-
Reserved. Do not write to this location.


Table 12. IRSP Decode
IRSP[3:0]
Returned value
0000
DHR[7:0]
0001
DHR[15:8]
0010
IEEA[3:0], ICRA[3:0] concatenated
0011
CRIL[3:0], IRSP[3:0] concatenated
0100
ALOC[3:0], ATIM[3:0] concatenated
0101
IEEA[7:0]
0110
IEED[7:0], EEPROM data byte
0111
TEMP-INDEX[7:0]
1000
BitClock[7:0]
1001
Reserved, internal flash test data
1010-1111
11001010 (CAhex)


Table 13. ATIM Definition
ATIM[3:0]
Duration of Analog Signal Specified in Byte Times (8 Bit Time)
0000
20 + 1 = 2 byte times
0001
21 + 1 = 3 byte times
0010
22 + 1 = 5 byte times
0011
23 + 1 = 9 byte times
0100
24 + 1 = 17 byte times
0101
25 + 1 = 33 byte times
0110
26 + 1 = 65 byte times
0111
27 + 1 = 129 byte times
1000
28 + 1 = 257 byte times
1001
29 + 1 = 513 byte times
1010
210 + 1 = 1025 byte times
1011
211 + 1 = 2049 byte times
1100
212 + 1 = 4097 byte times
1101
213 + 1 = 8193 byte times
1110
214 + 1 = 16,385 byte times
1111
In this mode, OUT is continuous; however, DIO will accept commands after 32,769 byte times. Do not parallel-connect DIO and OUT.


Table 14. ALOC Definition
ALOC[3:0]
Analog Signal
Description
0000
OUT
PGA Output
0001
BDR
Bridge Drive
0010
ISRC
Bridge Drive Current Setting
0011
VDD
Internal Positive Supply
0100
VSS
Internal Ground
0101
BIAS5U
Internal Test Node
0110
AGND
Internal Analog Ground (approximately half of VDD)
0111
FSODAC
Full-Scale Output DAC
1000
FSOTCDAC
Full-Scale Output TC DAC
1001
ODAC
Offset DAC
1010
OTCDAC
Offset TC DAC
1011
VREF
Bandgap Reference Voltage (nominally 1.25V)
1100
VPTATP
Internal Test Node
1101
VPTATM
Internal Test Node
1110
INP
Sensor's Positive Input
1111
INM
Sensor's Negative Input


Table 15. CLK Code (3MSBs of Configuration Register)
CLK Code
(bin)
Clock
Adjustment
011
+27%
010
+18%
001
+9%
000
0
111
-9%
110
-18%
101
-27%




相关型号
MAX1452 低成本、高精度传感器信号调理器 免费样品  
MAX1455 低成本、汽车传感器信号调理器 免费样品  


下一步
EE-Mail 订阅EE-Mail,接收关于您感兴趣的新文档的自动通知。
Download 下载,PDF格式 (187kB)  

© Jul 22, 2002, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 753: Jul 22, 2002
应用笔记753, AN753, AN 753, APP753, Appnote753, Appnote 753