应用笔记701

Using the DS32kHz with Maxim Real-Time Clocks


Abstract: This application note describes how to reduce current consumption when using the DS32kHz with Maxim real-time clocks (RTCs).

Overview

This application note is intended to answer some frequently asked questions about using the DS32kHz temperature-compensated crystal oscillator (TCXO) and Maxim real-time clocks (RTCs).

Using the DS32kHz

The DS32kHz has four pins that are required for operation: VCC, VBAT, GND, and 32kHz_OUT. The VCC, VBAT, and GND are power-supply connections and must either be connected to a positive supply or grounded. The 32kHz_OUT signal is intended to drive the X1 input of the RTC. The X2 pin of the RTC should be allowed to float when driving the X1 input with an oscillator.
The DS32kHz ICC and IBAT specifications are measured with no output load. The input characteristics of the oscillator on a RTC determine how much additional current the DS32kHz will consume. The additional current can significantly increase the size of the battery needed for operation.

Choosing an RTC

Maxim Integrated has a wide selection of RTCs from which to choose. Some of these devices were designed using a P-WELL process while the more recent devices have been designed using the first-generation N-WELL process. The second-generation N-WELL RTCs incorporate improvements that reduce the current consumption of the TCXO/RTC combination. The following data shows the current consumed by typical devices from each process. The data were taken at a battery voltage of 3.5V at +25°C.
KEY:
Ind = Individual Currents; DS32kHz with output open, RTC with crystal attached and running.
Direct = DS32kHz driving the RTC X1 input directly.
RC = DS32kHz driving the RTC with a 1MΩ resistor in series with a 100pF capacitor to the X1 input.


Table 1. N-WELL (First Generation)
Mode DS32kHz IBAT (µA) DS1306 IBAT (nA)
Ind 1.60 518
Direct 11.9 386
RC 2.14 584
Table 2. N-WELL (Second Generation)
Mode DS32kHz IBAT (µA) DS1337 ICC (nA)
Ind 1.59 612
Direct 3.73 626
RC 2.11 622
Table 3. P-WELL
Mode DS32kHz IBAT (µA) DS1202 IBAT (nA)
Ind 1.63 625
Direct 87.1 3410
RC 2.17 685
Note the RTC in each of the aforementioned tables are different RTCs. This accounts for the difference in the clock currents when comparing the tables.
If the RTC has an oscillator-enable bit, the oscillator must be enabled. If the bit is not enabled, additional current is drawn and the clock may not operate.
Table 4. RTC LIST
P-WELL Devices First Generation N-WELL Devices Second Generation N-WELL Devices
DS1202 DS12885 DS1337
DS12885 DS1302 DS1338
DS1283 DS1305/DS1306 DS1339
DS1284 DS1307 DS1672
DS1384 DS1315  
DS14285 DS1500/DS1501  
DS1384 DS1315  
  DS1602  
  DS1670/DS1673/DS1677  
  DS1685  
  DS1688/DS1689  
  DS17285/DS17485/DS17885  

Summary

When using P-WELL and first-generation N-WELL RTC devices, use an RC circuit to achieve the minimum possible timekeeping current.
The second-generation N-WELL devices use only slightly more current with an RC circuit.


相关型号
DS1284 看门狗计时器  
DS12885 实时时钟 免费样品  
DS12R885 带有恒压涓流充电器的RTC 免费样品  
DS1302 带涓流充电的时钟芯片 免费样品  
DS1305 带有闹钟的串行实时时钟 免费样品  
DS1306 带有闹钟的串行实时时钟 免费样品  
DS1307 64 x 8、串行、I²C实时时钟 免费样品  
DS1308 低功耗I²C RTC,带有56字节NV RAM 免费样品  
DS1315 隐含时钟芯片 免费样品  
DS1337 I²C串行实时时钟 免费样品  
DS1338 I²C RTC,带有56字节NV RAM 免费样品  
DS1339 I²C串行实时时钟 免费样品  
DS1340 I²C RTC,带有涓流充电器 免费样品  
DS1341 低电流I²C RTC,可配合高ESR晶体使用 免费样品  
DS1342 低电流I²C RTC,可配合高ESR晶体使用 免费样品  
DS1371 I²C、32位二进制计数器看门狗时钟 免费样品  
DS1374 I²C、32位二进制计数器看门狗RTC,带有涓流充电器和复位输入/输出 免费样品  
DS1384 看门狗实时时钟控制器  
DS1390 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS1391 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS1392 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS1393 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS14285 实时时钟,带有非易失RAM控制器  
DS1500 Y2K兼容、看门狗RTC,带有非易失控制  
DS1501 Y2K兼容、看门狗实时时钟 免费样品  
DS1558 看门狗时钟,带有NV RAM控制器 免费样品  
DS1602 历时计数器  
DS1670 便携系统控制器 免费样品  
DS1672 I²C、32位二进制计数器RTC 免费样品  
DS1673 便携系统控制器 免费样品  
DS1677 便携系统控制器 免费样品  
DS1678 实时事件记录器 免费样品  
DS1685 3V/5V实时时钟 免费样品  
DS1688 3V/5V、串行实时时钟,带有NV RAM控制器  
DS1689 3V/5V、串行实时时钟,带有非易失RAM控制器  
DS17285 3V/5V实时时钟 免费样品  
DS17485 3V/5V实时时钟 免费样品  
DS17885 3V/5V实时时钟 免费样品  
DS32KHZ 32.768kHz温补晶振 免费样品  


下一步
EE-Mail 订阅EE-Mail,接收关于您感兴趣的新文档的自动通知。
Download 下载,PDF格式 (67.1kB)  

© Feb 15, 2002, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 701: Feb 15, 2002
应用笔记701, AN701, AN 701, APP701, Appnote701, Appnote 701