应用笔记6415

How to Install the USB Driver for Evaluation Kits/Systems That Use the FTDI UART-to-USB Converter Chip (Windows Vista, Windows 7, and Windows 10 Support)


Abstract: This is a quick-start guide for EV kits and EV systems that use the FTDI FT232BL (or FT232BM) UART-to-USB converter chip (32-pin TQFP) implemented with Maxim VID = 0x0B6A PID = 0x434D for the purpose of the USB PC connection. This USB driver allows the EV kit software to support Windows Vista, Windows 7, and Windows 10.

Overview

This document provides a quick guide for EV kits and EV systems that use the FTDI FT232BL (or FT232BM) UART-to-USB converter chip (32-pin TQFP) implemented with Maxim VID = 0x0B6A PID = 0x434D for the purpose of the USB PC connection. This USB driver allows the EV kit software to support Windows Vista®, Windows® 7, and Windows 10.

Follow these steps to start evaluating the EV kit now. The MAX6581 Evaluation Kit (MAX6581EVKIT) is used in the example figures.

  1. Plug in the USB cable into a EV kit board and allow Windows to update the driver.
  2. Make sure the Device Manager displays the information under Ports and Universal Serial Bus controllers as shown in Figure 1.

    Device Manager window. Figure 1. Device Manager window.

  3. In this example, the MAX6581 Evaluation Kit software is open. Notice the status bar at the bottom displays MAX6581EVKIT not connected. This is an indication that the driver needs to be updated.

    MAX6581EVKIT is not connected. Figure 2. MAX6581EVKIT is not connected.

  4. Download the file FTDI_VID_PID_x86_x64_CDM_2.0.6.00.zip Maxim’s EV Kit Software webpage at: www.maximintegrated.com/evkitsoftware.
  5. Unzip the file FTDI_VID_PID_x86_x64_CDM_2.0.6.00.zip.
  6. Within the directory FTDI_VID_FTDI_PID_x86_x64_CDM_2.06.00\usb_driver, double-click CDM20600.exe.
  7. Click the Run button. See Figure 3 and Figure 4.

    Pop-up menu to install driver. Figure 3. Pop-up menu to install driver.

    Installing the driver. Figure 4. Installing the driver.

  8. Open the MAX6581 Evaluation Kit GUI. The board should be connected as shown in Figure 5.

    MAX6581EVKIT is connected. Figure 5. MAX6581EVKIT is connected.

If you get this far, you are ready to evaluate the part. If you continue to have problems connecting, refer to the document in the same driver directory named USB_Driver_Help_200.pdf.



Windows and Windows Vista are registered trademarks and registered service marks of Microsoft Corporation.



相关型号
MAX6581 精度为±1°C的8通道温度传感器 免费样品  
MAX6639 2通道温度监测器,提供双路、自动PWM风扇速度控制器 免费样品  
MAX7500 数字温度传感器和温度监测看门狗,带有总线闭锁保护 免费样品  
MAX9611 高边、电流检测放大器,带有12位ADC和运算放大器/比较器 免费样品  


下一步
EE-Mail 订阅EE-Mail,接收关于您感兴趣的新文档的自动通知。
Download 下载,PDF格式 (269.8kB)  

© Aug 10, 2017, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 6415: Aug 10, 2017
应用笔记6415, AN6415, AN 6415, APP6415, Appnote6415, Appnote 6415