设计指南5413

State Machine Logic in Binary-Coded Decimal (BCD)-Formatted Real-Time Clocks


Abstract: When developing code to operate a real-time clock (RTC), it is often beneficial to understand how the clock core operating logic has been defined. This tutorial discusses the counter-chain structure used in Maxim's binary-coded decimal (BCD)-formatted RTCs. It provides some insight into the expected chip behavior if improper or illegal contents are somehow installed.

A similar version of this article appears on Electronic Design, July 2012.

Introduction

When developing code to operate a real-time clock (RTC), it is often beneficial to understand how the clock core operating logic has been defined. We all have a fundamental comprehension of how a clock and calendar should operate when properly programmed, but this application note also provides some insight into the expected chip behavior if improper or illegal contents are somehow installed.
A basic real-time clock counter chain found in many of Maxim's binary-coded decimal (BCD)-formatted RTCs (such as the DS12885 and DS1302) is illustrated in Figure 1.
Figure 1. RTC counter chain structure.
Figure 1. RTC counter chain structure.
Each counter register has defined minimum and maximum values, and most are preset to their appropriate minimums on initial power application. As a natural function of timekeeping, when the Seconds count reaches the maximum value, the next increment causes a carry to the Minutes register and the Seconds rolls over to the minimum value. A Minutes rollover carries to the Hours; the Hours rollover carries to both the Date and arbitrary Day-of-Week registers; the Date rollover carries to the Month register; the Month rollover carries to the Year register; and if applicable, the Year rollover carries to the Century register. Table 1 lists the registers and associated range of legal values.
Table 1. RTC Register Range and Carry Function
Register Minimum (hex) Maximum (hex) Carry to Register
Hundredths 00 99 Seconds
Seconds 00 59 Minutes
Minutes 00 59 Hours
Hours (12-hour mode) 41 72 AM PM, PM AM + Day & Date
Hours (24-hour mode) 00 23 Day & Date
Day 01 07
Date 01 31* Month (*Month and Year dependent)
Month 01 12 Year
Year 00 99 Century (register or bit)
Century 00 99
Some variations on the counter implementation may include a 'Hundredths of a Second' register (precedes Seconds), and a Century bit to flag the Year register rollover.

Register Descriptions

For each register, the normal state machine logic is to increment the BCD count from the minimum to the defined maximum, and then roll back over to the minimum while applying the carry to the next register. For an example, the Date register BCD count sequence for a 30-day month would be 01h...09h, 10h...19h, 20h...29h, 30h, and then roll back to 01h.
Maxim does not critique the values a user might install during operation, so the ramifications of loading improper values are based upon the specific component and which register(s) was actually involved. Illogical time and date entries may result in unexpected operation.
The Hundredths of a Second register (if applicable) counts from 00h to 99h. The next increment causes the counter to roll over to 00h and the carry is applied to the Seconds register. All 8 bits in this register are read/write capable. Devices containing this register are internally clocked from the 4kHz time base (32.768kHz/8).
The Seconds register counts from 00h to 59h. The next increment causes the counter to roll over to 00h and the carry is applied to the Minutes register. Only the least significant 7 bits in this register are usually read/write capable. Most devices not containing a Hundredths of a Second register are internally clocked from the 1Hz time base.
The Minutes register also counts from 00h to 59h. The next increment causes the counter to roll over to 00h and the carry is applied to the Hours register. Only the least significant 7 bits in this register are read/write capable.
The Hours register accommodates either a 12-hour format (with an AM/PM designator) or a 24-hour clock. A control bit (usually bit6 = 12/%-overbar_pre%24%-overbar_post%) is used to identify the clock operating mode. Only the least significant 7 bits in the Hours register are read/write capable. In the 24hour Mode (bit6 = 0), the Hours register counts from 00h to 23h. The next increment causes the counter to roll-over to 00h and the carry is applied to both the Date and Day registers.
In the 12-hour mode (bit6 = 1), the Hours register count sequence, starting at "12AM", counts 52h, 41h...49h, 50h, and then 51h. The next increment causes the counter to roll over to 72h with the carry applied to the %-overbar_pre%AM%-overbar_post%/PM bit (PM = 1). The register then counts 72h, 61h...69h, 70h, 71h and the next increment causes the counter to roll over to 52h as PM is cleared, with the carry applied to both the Date and Day registers. For clarification, 12 midnight is 12:00:00 AM and 12 noon is 12:00:00 PM.
The Day (Day-of-Week) register is the most simplistic counter, with an intended content of 01h to 07h. The next increment causes the counter to roll over to 01h with no carry. Should a user accidentally deposit a 00h content into this register, there is no adverse effect upon the other timekeeping registers, but the first week of clock operation will have 8 days (0 7). The Day register only has three functioning bits, so even though it initially seems impossible for the user to load a value greater than 7, any hex value > 7 written would store the bad value logic-ORd with the three functioning bits (07h) (e.g., writing 1Fh would store a 07h, or writing F5h would store a 05h). Normal calendar convention is to define Sunday= 1, but that definition is arbitrary and fully under the user's control.
The Date register counts from 01h to the defined end of the present Month. The end of the month is dependent upon the present Month and Year content (in the case of February). Only the least-significant 6 bits in the Date register are read/write capable. Table 2 lists the three options.
Table 2. Last Date of Month
Calendar Month Numeric Month End Date
January, March, May, July, August, October, December 1, 3, 5, 7, 8, 10, 12 31
April, June, September, November 4, 6, 9, 11 30
February 2 28 (typical year), 29 (leap year)
The Month register counts from 01h to 12h. The next increment causes the counter to roll over to 01h and the carry is applied to the Year register. To address Y2K issues in the late 20th Century, a Century bit was included in the MSB of the Month register on components that did not include a full 8-bit Century register. This Century bit facilitated easy detection of the century change, as the bit changes state upon a Year register rollover from 99h to 00h. Care should be taken when loading new calendar values to avoid corrupting the Century bit logic condition. Please refer to the register map for the specific component in question; conventional register placement leaves bits 7 and 4:0 as read/write capable.
The Year register counts from 00h to 99h. The next increment causes the counter to roll over to 00h and the carry is applied to either the Century register or the Century bit, whichever is applicable to the component in question. All 8 bits in this register are read/write capable.
Leap Year compensation is based upon the era of the specific chip design, and applicability is normally annotated on the cover page of that data sheet. For most chip designs that do not include a Century register, the Leap Year compensation functions properly through 2099 and is assumed to be the result of this expression:
If MODULO (CALENDAR_YEAR/4) == 0
Due to the era of existing chip designs, many of today's RTC components containing a Century register apply the same algorithm solely upon on content of the Year register, and therefore will incorrectly designate 2100 as a leap year.
The DS1347 RTC utilizes the full Gregorian algorithm to determine Leap Year adjustments for February:
	Leap_Year = 0							; default to No
	If MODULO (CALENDAR_YEAR/4) == 0				; divisible by 4?
		If MODULO (CALENDAR_YEAR/100) == 0			; divisible by 100?
			If MODULO (CALENDAR_YEAR/400) == 0		; divisible by 400?
				Leap_Year = 1
			end			; if
		else
				Leap_Year = 1
		end				; if
	end					; if
The Century register (if applicable) counts from 00h to 99h. All 8 bits in this register are read/write capable.

Results When Illegal Data Is Written

Up to this point, we have discussed the proper counting methods used by the RTC, given the legal range of values for the register in question. Occasionally a question may arise concerning expected counter behavior when improper values were initially installed. The answer is deterministic, and only requires a copy of the component's register map to arrive at a conclusion.
To access the result of loading an improper value, perform a Logic AND of the written value with the write-enabled bits in the register in question.
If the resulting content is less than the register's maximum counter value, the register should subsequently increment from that AND-ed value. Rollover will occur when the bit states in the register eventually coincide with the expected maximum value for that counter (12h or 00010010b as shown in Example 1).
Example 1: Write 2Ah into the Month register of a DS1337 serial RTC
From the product specification, the Month register content was verified to match the register description above.
BCD Binary
2Ah 00101010 Write to Month
9Fh 10011111 Enabled bits in Month register (with Century bit)
0Ah 00001010 Resulting content of "0Ah" after writing the Month
12h 00010010 Logic match for "maximum value"
If the resulting content is greater than the register's maximum counter value, the register should subsequently increment from that AND-ed value to some unpredictable rollover condition. In this case, not only was the hour value illogical, but setting bit6 also changed the functionality of the Hours counter to 12-hour Mode. Prediction of the roll-over point is illogical and results may vary, based upon that specific chip design.
Example 2: Write FFh into the Hours register of a DS1390 low-voltage RTC
From the product specification, the Hours register content was verified to match the register description above.
BCD Binary
FFh 11111111 Write to Hours
7Fh 01111111 Enabled bits in Hours register
7Fh 01111111 Resulting content of "7Fh" when reading the Hours
Example 3: Write 38h into the Hours register of a DS1341 low-current RTC
From the product specification, the Hours register content was verified to match the register description above.
Since bit6 (12/%-overbar_pre%24%-overbar_post%) was not set, the component would be running in 24-hour mode, and 38h is obviously past the normal 24-hour mode register maximum of 23h. The resulting time error is difficult to estimate, given an unstated period of operation between when the value was corrupted and when it was detected.
BCD Binary
38h 00111000 Write to Hours
7Fh 01111111 Enabled bits in Hours register
38h 00111000 Resulting content of "38h" when reading the Hours
Example 4: Write AAh into the Seconds register of a DS1302 trickle-charge timekeeping chip
From the product specification, the Seconds register content deviates from the register description above; the inclusion of the CH bit (bit7) requires some further understanding of that bit's functionality.
Since only 7 bits are used for the Seconds value, the counter was actually written to 2Ah. "CH" stands for Clock Halt.
With CH = 1, the oscillator is stopped and the counters do not increment, so it will never increment or roll over with CH set. The resulting time loss is difficult to estimate, given an unstated period of this idle (noncounting) condition before detection/correction.
BCD Binary
AAh 10101010 Write to Seconds
FFh 11111111 Enabled bits in Seconds register
AAh 10101010 Resulting content of "AAh" when reading the Seconds
Example 5: Write 2Dh into the Date register of a DS1338 serial RTC
From the product specification, the Date register content was verified to match the register description above.
BCD Binary
2Dh 00101101 Write to Date
3Fh 00111111 Enabled bits in Hours register
2Dh 00101101 Resulting content of "2Dh" when reading the Hours

Summary

In conclusion, we have discussed the counter chain structure utilized in Maxim's BCD-formatted RTCs, the derivation of unique calendar events, and Leap Year/Century handling. Additionally, using published register information and the deterministic nature of the state machine logic, some behavioral traits resulting from errant programming can be recognized during the system debugging phase. This symptom recognition can reduce a product's time to market.


相关型号
DS1243 64k NV SRAM,带有隐含时钟 免费样品  
DS1244 256k NV SRAM,带有隐含时钟 免费样品  
DS1248 1024k NV SRAM,带有隐含时钟 免费样品  
DS1251 4096k NV SRAM,带有隐含时钟 免费样品  
DS1254 2M x 8 NV SRAM,带有隐含时钟  
DS12885 实时时钟 免费样品  
DS12887 实时时钟 免费样品  
DS12887A 实时时钟 免费样品  
DS12C887 实时时钟 免费样品  
DS12C887A 实时时钟 免费样品  
DS12R885 带有恒压涓流充电器的RTC 免费样品  
DS12R887 带有恒压涓流充电器的RTC  
DS1302 带涓流充电的时钟芯片 免费样品  
DS1305 带有闹钟的串行实时时钟 免费样品  
DS1306 带有闹钟的串行实时时钟 免费样品  
DS1307 64 x 8、串行、I²C实时时钟 免费样品  
DS1308 低功耗I²C RTC,带有56字节NV RAM 免费样品  
DS1315 隐含时钟芯片 免费样品  
DS1318 并行接口历时计数器 免费样品  
DS1337 I²C串行实时时钟 免费样品  
DS1338 I²C RTC,带有56字节NV RAM 免费样品  
DS1339 I²C串行实时时钟 免费样品  
DS1339A 低电流I²C串行实时时钟 免费样品  
DS1339B 低电流、I2C、串行实时时钟,可配合高ESR晶振工作 免费样品  
DS1340 I²C RTC,带有涓流充电器 免费样品  
DS1341 低电流I²C RTC,可配合高ESR晶体使用 免费样品  
DS1342 低电流I²C RTC,可配合高ESR晶体使用 免费样品  
DS1343 低电流SPI/3线RTC 免费样品  
DS1344 低电流SPI/3线RTC 免费样品  
DS1347 小电流、SPI兼容实时时钟 免费样品  
DS1375 I²C数字输入RTC,带有闹钟功能 免费样品  
DS1388 I²C RTC/监控电路,带有涓流充电器和512字节EEPROM 免费样品  
DS1390 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS1391 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS1392 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS1393 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS1394 低电压SPI/3线接口RTC,带有涓流充电器 免费样品  
DS1500 Y2K兼容、看门狗RTC,带有非易失控制  
DS1501 Y2K兼容、看门狗实时时钟 免费样品  
DS1511 Y2K兼容、看门狗实时时钟 免费样品  
DS1553 64kB非易失、Y2K兼容时钟RAM  
DS1554 256k非易失、Y2K兼容时钟RAM 免费样品  
DS1556 1M非易失、Y2K兼容时钟RAM 免费样品  
DS1557 4M非易失、Y2K兼容时钟RAM 免费样品  
DS1558 看门狗时钟,带有NV RAM控制器 免费样品  
DS1629 数字温度计及实时时钟/日历 免费样品  
DS1642 非易失时钟RAM  
DS1643 非易失时钟RAM  
DS1644 非易失时钟RAM  
DS1646 非易失时钟RAM  
DS1647 非易失时钟RAM  
DS1670 便携系统控制器 免费样品  
DS1673 便携系统控制器 免费样品  
DS1678 实时事件记录器 免费样品  
DS1685 3V/5V实时时钟 免费样品  
DS17285 3V/5V实时时钟 免费样品  
DS17287 3V/5V实时时钟 免费样品  
DS1742 Y2K兼容、非易失时钟RAM  
DS1743 Y2K兼容、非易失时钟RAM  
DS1744 Y2K兼容、非易失时钟RAM 免费样品  
DS1746 Y2K兼容、非易失时钟RAM 免费样品  
DS1747 Y2K兼容、非易失时钟RAM 免费样品  
DS17485 3V/5V实时时钟 免费样品  
DS17487 3V/5V实时时钟 免费样品  
DS17885 3V/5V实时时钟 免费样品  
DS17887 3V/5V实时时钟 免费样品  
DS3231 超高精度、I²C接口、集成RTC/TCXO/晶体  
DS3231M ±5ppm, I²C实时时钟 免费样品  
DS3232 超高精度、I²C RTC,集成晶体和SRAM  
DS3232M ±5ppm、内置SRAM的I²C实时时钟 免费样品  
DS3234 超高精度、SPI总线RTC,集成晶体和SRAM  


下一步
EE-Mail 订阅EE-Mail,接收关于您感兴趣的新文档的自动通知。
Download 下载,PDF格式 (82.9kB)  

© Sep 17, 2012, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 5413: Sep 17, 2012
设计指南5413, AN5413, AN 5413, APP5413, Appnote5413, Appnote 5413