应用笔记1212

Pulsed Sensor Extends Battery Life


Abstract: The following application note demonstrates a power-saving circuit that pulses a sensor for 1 second every 30 minutes. Designed to monitor levels of salt crystals in a water softener, the circuit consumes an average of 70µA.

A similar idea appeared in the January 1, 1998 issue of EDN.
Activating the sensor circuit in Figure 1 for 1 second every 30 minutes reduces the circuit's 20mA supply current to an average of 70µA. For a battery consisting of three AA cells, this pulsed operation extends the battery life to several years.
Figure 1. Powered by three AA cells, this optoelectronic sensor has a battery life of several years.
Figure 1. Powered by three AA cells, this optoelectronic sensor has a battery life of several years.
The sensor shown is an optocoupler with an infrared-emitting diode. Designed to monitor the level of salt crystals in a water softener, it relies on a reflection from the crystals to generate a "no-alarm" level of emitter current in the phototransistor (Q3). As the salt level drops past the sensor's position, this current level makes a step change downward.
When the drop across R7 equals the reference voltage in the comparator/reference device (IC2), comparator B's output goes high and releases the manual reset on the voltage monitor (IC3). After a minimum reset-delay interval of 140ms, Q4 turns on and sounds the buzzer. Comparator A monitors the battery voltage via R1 and R2; at levels above 3V, it activates the IR-emitting diode (D3) by turning on the constant-current sink consisting of Q2 and associated components. Thus, the buzzer sounds for 1 second every 30 minutes if the battery voltage is below 3V, or if the salt level is low
.
Power for the sensor is available only when Q1 turns on. Q1 is controlled by IC1—a microprocessor supervisor configured as a time-base generator. (IC1 consumes less power and has a smaller footprint than the alternative 556 timer or a 555 timer with multistage counters. It also eliminates the large capacitors otherwise required.) Connected directly across the battery, it draws 60µA at 4.5V and 40µA at 3.0V.
IC1's external connections cause its internal watch-dog timer to cycle repeatedly. With C2 = 1.5µF as shown, the internal timeout is 3.6 seconds, and connecting WDS high multiplies this value by 500, extending it to the desired 30 minutes. Each timeout produces a reset pulse that applies power to the remaining circuitry by turning on Q1 for an interval of 1 second (approximately). From the MAX6304 data sheet:
tRESET = (2.67) (C1) (in µF) = 1.25 seconds
tWATCHDOG = (2.67) (C2) (in µF) (500) = 30 minutes.


相关型号
MAX6304 +5V、低功耗、微处理器监控电路,带有可调节的复位/看门狗定时器 免费样品  
MAX811 4引脚微处理器电压监测器,带有手动复位输入 免费样品  
MAX933 超低功耗、低成本比较器、内置2%电压基准 免费样品  


下一步
EE-Mail 订阅EE-Mail,接收关于您感兴趣的新文档的自动通知。
Download 下载,PDF格式 (73.4kB)  

© Jan 01, 1998, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 1212: Jan 01, 1998
应用笔记1212, AN1212, AN 1212, APP1212, Appnote1212, Appnote 1212