应用笔记1122

Optimizing Audio Bridged Tied Load Amplifiers


Abstract: This audio bridge-tied load (BTL) amplifier application note describes a unique architecture that minimizes the differential output distortion and noise (THD+N).

Low-voltage systems driving loudspeakers often employ a bridged-amplifier configuration that effectively doubles the voltage swing at the transducer (speaker). In a typical bridge-amplifier circuit (Figure 1), an AC-coupled inverting stage with gain drives one side of the speaker. It also drives a second unity-gain inverting amplifier, which drives the other side of the speaker.

Figure 1. This conventional bridged amplifier features two amplifiers in tandem.
Figure 1. This conventional bridged amplifier features two amplifiers in tandem.

Bridged amplifiers usually incorporate a matched pair of amplifiers, but the first amplifier dominates overall performance because its output noise and distortion are replicated in the second amplifier. You can eliminate this drawback by placing the two amplifiers in a non-cascaded configuration, in which one is inverting and the other in non-inverting (Figure 2). Both amplify the same input signal, so neither one reproduces noise, distortion, or clipping introduced by the other.

Figure 2. This circuit optimizes the Figure 1 configuration by apportioning gain between the two amplifiers.
Figure 2. This circuit optimizes the Figure 1 configuration by apportioning gain between the two amplifiers.

As a key improvement in Figure 2, DC bias for the non-inverting circuit is derived from the inverting amplifier's source resistor. (Bias is required because the input is AC coupled). Using the other amplifier's source resistor as a bias source lowers the component count and eliminates signal injection into the high-impedance bias source (VCC/2, applied to the top amplifier's non-inverting input).

Another advantage in Figure 2 is the elimination of DC gain in the non-inverting amplifier. For the circuit shown, C2 sets the -3dB point at half the input cutoff frequency, and R1/C1 sets the input highpass cutoff frequency at 100Hz.

A similar version of this article appeared in the November 19, 2001 issue of Electronic Design magazine.



相关型号
MAX4167 高输出驱动、精密的低功耗、单电源、满摆幅输入/输出运算放大器,带有关断 免费样品  
MAX4168 高输出驱动、精密的低功耗、单电源、满摆幅输入/输出运算放大器,带有关断 免费样品  
MAX4337 SC70/SOT23-8封装、50mA输出电流、满摆幅输入/输出运算放大器,带有关断/静音 免费样品  
MAX4338 SC70/SOT23-8封装、50mA输出电流、满摆幅输入/输出运算放大器,带有关断/静音 免费样品  


下一步
EE-Mail 订阅EE-Mail,接收关于您感兴趣的新文档的自动通知。
Download 下载,PDF格式 (36kB)  

© Jun 24, 2002, Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.

APP 1122: Jun 24, 2002
应用笔记1122, AN1122, AN 1122, APP1122, Appnote1122, Appnote 1122