This SDK complements the
1-Wire® Drivers installation package with documentation and examples to aid 1-Wire project development under Microsoft OS platforms. The 1-Wire SDK includes 1-Wire API for .NET API examples in VB.NET and C#, along with TMEX API examples in C, C++, Pascal (Borland Delphi), and Microsoft Visual Basic. The new Compact.NET 1-Wire API has been added as well. It is aimed at Windows
® CE/Mobile platforms and was written entirely in C# for Microsoft's Compact .NET framework. All examples are provided with source. Both 32-bit and 64-bit examples are included.
The following are links to legacy 1-Wire SDKs.