Glossary Definition for femtobasestation

Glossary Term: femtobasestation 

Definition

A femto base station (also called an Access Point Base Station, femtocell, femtobasestation or femto basestation) is an in-home base station. Like a standard base station, it connects cell phone voice and data to the cell phone network, but it serves a smaller area (the home).

A femto base station benefits the service provider because it offloads cell tower traffic. Subscribers benefit from superior signal strength, due to the proximity of the unit -- especially where a cellular signal is weak or not available.

Femto base stations augment the normal network and replicates the usual telecommunications infrastructure. Connection to the cell phone network is provided by VoIP over the Internet.

More on femto base stations and information on Maxim's femto base station chipsets.

Synonyms
  • Femto Base Station
  • femtocell
  • Access Point Base Station
  • femto basestation

Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add