Glossary Definition for differential-signal

Glossary Term: differential-signal 

Definition

Most electrical signals are single-ended, comprised of a single wire and ground. Differential signals use two wires which are the inverse of each other -- when one swings positive, the other swings negative in equal magnitude. The receiving circuit looks only at the difference between the two, ignoring any common-mode voltage. This "push-pull" arrangement reduces the impact of electrical interference because external noise will affect both wires equally and the common-mode rejection will ignore the noise.

Examples: RS-422, RS-485, professional audio signal standards (especially for microphones), the signal lines employed by Ethernet, and the standard twisted-pair analog telephone (POTS) line.

Also see the tutorial, Understanding Common-Mode Signals.

Synonyms
  • Differential
  • Balanced
  • Twisted-Pair
See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add