Glossary Definition for Source

Glossary Term: Source 

Definition

1. One of the three terminals that comprise a FET. A voltage on the gate controls the current flow between the source and drain.

2. A "voltage source" or "current source" is an idealized generator of voltage or current in a circuit. These sources can be AC or DC, controlled or constant.


Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add