Glossary Definition for PWM

Glossary Term: PWM 

Definition

1. A method for using pulse width to encode or modulate a signal. The width of each pulse is a function of the amplitude of the signal.

2. A technique used to modulate the power delivered to a load.

In DC-DC switching regulators, the pulse width driving the main power switch (and hence, the duty cycle) is varied to maintain the desired output voltage. In DC motor-control applications, pulse width is used to vary motor speed.

See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add