Glossary Definition for NRZ

Glossary Term: NRZ 

Definition

Non Return to Zero: A binary encoding scheme in which ones and zeroes are represented by opposite and alternating high and low voltages, and where there is no return to a zero (reference) voltage between encoded bits. That is, the stream has only two values: low and high.
Synonyms
  • Non Return To Zero
See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add