Glossary Definition for MxTNI

Glossary Term: MxTNI 

Definition

MxTNI™ (Maxim Tiny Network Interface, formerly called TINI) is Maxim's trademark for the industry's smallest web server. The MxTNI platform consists of a microcontroller that includes the facilities necessary to connect to the Internet. The platform is a combination of broad based I/O, a full TCP/IP stack and an extensible Java runtime environment that simplifies development of network-connected equipment.
Related Parts
  • DS80C400 - Network Microcontroller
  • DS80C390 - Dual CAN High-Speed Microprocessor
  • DS80C410 - Network Microcontrollers with Ethernet and CAN
  • DS80C411 - Network Microcontrollers with Ethernet and CAN

Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add