Glossary Definition for Electromotive-Force

Glossary Term: Electromotive-Force 

Definition

Volt (or Volts): Unit of measure for electromotive force (EMF), the electrical potential between two points. An electrical potential of 1 volt will push 1 ampere of current through a 1-ohm resistive load.

Using a common plumbing analogy, voltage is similar to water pressure and current is analogous to flow (e.g. liters per minute).

In equations, the symbol E is often used (as in: E = IR). V is the symbol for the unit of measure, Volt.

Synonyms
  • voltage
  • Electromotive Force
  • V
  • EMF
  • E
See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add