Glossary Definition for EIA-485

Glossary Term: EIA-485 

Definition

RS-485 and RS-422 are serial interface standards in which data is sent in a differential pair (two wires, or twisted pair cable), which allows greater distances and higher data rates than non-differential serial schemes such as RS-232. See: Differential Signaling.

RS-485 and RS-422 can be configured for full-duplex or half-duplex bus systems.

See Selecting and Using RS-232, RS-422, and RS-485 Serial Data Standards to learn about the differences between RS-232, RS-422, and RS-485.

Synonyms
  • RS-422/RS-485
  • RS-485
  • RS-422
  • RS422
  • RS485
  • EIA-422

Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add