Glossary Definition for Daytime-Running-Lamp

Glossary Term: Daytime-Running-Lamp 

Definition

Daytime Running Lamps (DRLs) are white lights mounted on the front of an automobile. Mandated in many countries, they automatically switch on when the key is turned and are intended for daytime use, to increase the visibility of the automobile. They are typically built with LEDs.

See: High-Brightness LED Drivers

Synonyms
  • Daylight Running
  • Daytime Running Light
  • Daytime Running Lamp
Related Parts
  • MAX16805 - EEPROM-Programmable, High-Voltage, 350mA LED Drivers with LED Current Foldback
See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add